-mv option to use with the C674x

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Introduction

Page 11 of the C6747 datasheet mentions:

“The C674x CPU combines the performance of the C64x+ core with the floating-point capabilities of the C67x+ core.”

To make use of this hybrid core (C64x+ plus C67x+), you should use -mv6740 as the compiler option when building a project for C674x. The processor works with the mv64x+ option, but then you will be just using the C64x+ features, not the C67x (floating point). Similarly, the processor works with the mv67p or mv6700 options, but then you lose the C64x+ features.

C6000cores.JPG

Important Steps

C674x-mv.jpg\

Code Generation Tools support for C674x

Support for C674x core began at CGT 6.1.5, but it is recommended to use version 6.1.9 or later because some bugs (cite please) were corrected for this core.


For example, if you are using CGT 6.1.5 you will not be able to find the C674x (-mv6740) in the dropdown list. For this case, you have some solutions:

1) Update the CGT to 6.1.8/9 or later;

2) You can simply type –mv6740 in the box on the top of Compiler tab of Build Options. So just replace –mv6400+ (or whatever option is there) with –mv6740 and click OK. It is going to work even if the option is not in the dropdown list.

3) Extract the bti6000.dll file attached to the \bin directory of your 6.1.x Code Generation Tools (replacing the existing one). Usually, the default installation path for Code Generation Tools is: C:\Program Files\C6000Code Generation Tools 6.1.x

So you would replace the file in the directory: C:\Program Files\C6000Code Generation Tools 6.1.x\bin

If you have the CCS version that comes with the DSK, the path is: C:\CCStudio_v3.3\C6000\cgtools\bin

You will need to re-start CCS (Code Composer Studio) for the changes to take effect.

E2e.jpg For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article -mv option to use with the C674x here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment

Comments

Comments on -mv option to use with the C6747


Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox