IEEE 1149.7

From Texas Instruments Embedded Processors Wiki

(Redirected from 1149.7)
Jump to: navigation, search
Translate this page to   

Contents

IEEE 1149.7

IEEE 1149.7 is complementary superset of the widely adopted IEEE 1149.1 (JTAG) standard that has been in use for more than two decades. IEEE 1149.7 was ratified by the IEEE in Dec 2009. The persistent link to the specification at the IEEE is at http://ieeexplore.ieee.org/servlet/opac?punumber=5412864.

While IEEE 1149.7 adds substantial functionality to the existing standard, it is important to note that it is not a replacement for IEEE 1149.1. Backward compatibility is maintained so that any board or system that integrates chips that support either standard is amenable to test or debug procedures.

Benefits

The new standard offers embedded designers several benefits, including:

Relationship to Other Standards

Status

Presentations

Press


Leave a Comment

Comments

Comments on IEEE 1149.7


Db said ...

It's evidently been ratified as of December 2009, and will be published in February 2010 ...

can we get updates about what the actual standard covers? Example, does it still use ZBS?

--db 12:39, 14 February 2010 (CST)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox