AM18x + WL1271

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

General Platform Description

The development platform is primarily based on the AM1808 kit by Mistral. An extension card provided by Mistral serves as a wireless connectivity add-on.

Key Properties

                                              Lsr.png                                                  Mistral-smaller-logo.png




AM1808.jpg

General HW Description and Block Diagram

The WL1271 connectivity solution is available in the form of a daughter board.This board connects to the AM1808 board. This board will be interfaced to the EVM through the Expansion connectors J29 and J30. Generally the daughter board is plugged to the connector J29 of the AM1808 EVM and the BT signals are connected using the FRC cable. The daughter board uses 5V power available on the EVM to generate the required VBAT (3.6V) and VIO (1.8V) for the WL1271 module. 

Block diagram.jpg 

Figure: Block diagram showing the interconnection between WLAN connectivity board and the AM1808 EVM board.

 


 

Connectivity Expansion Card Description

This daughter board contains an LSR module which is based on a WL1271 Wireless LAN and a Bluetooth combo chip.

The wireless LAN and Bluetooth  share one antenna which is mounted directly on the connectivity board.



1271 Connectivity Expansion Card Pin Assignment

The following table shows the pin assignment from the connectivity expansion card to the Main EVM:


WL1271 Signal Connection to AM1808 EVM
Signal type Signal Name on the WL1271 module Connection to AM1808 EVM Board Mistral AM1808 Connection
Bluetooth - Host I/F    BT_FUNCT5

Optional signal.

No Connect
Bluetooth - Host I/F BT_EN GPIO on AM1808. ACLKR / GP0[15]
Bluetooth - Host I/F; HCI_TX UART lines on the AM1808. UART1_RXD
Bluetooth - Host I/F HCI_RX UART lines on the AM1808 UART1_TXD
Bluetooth - Host I/F HCI_CTS UART lines on the AM1808 UART1_RTS
Bluetooth - Host I/F HCI_RTS UART lines on the AM1808 UART1_CTS
Bluetooth - Host I/F BT_FUNCT2 Optional signal that can be connected to an AM1808 GPIO AXR8 /CLKS1 /ECAP1_APWM1 /GP0[0]
Bluetooth - Host I/F AUD_IN McBSP on the AM1808 DX1
Bluetooth - Host I/F AUD_OUT McBSP on the AM1808 DR1
Bluetooth - Host I/F AUD_CLK McBSP on the AM1808 CLKR1
Bluetooth - Host I/F AUD_FSYNC McBSP on the AM1808 FSR1
Bluetooth - Host I/F BT_FUNCT4 Optional signal No Connect
WLAN Host I/F WL_EN AM1808 GPIO UHPI_HHWIL /UPP_CH1_ENABLE /GP6[9]
WLAN Host I/F SDIO_CMD AM1808 MMC/SDIO_CMD MMCSD1_CMD
WLAN Host I/F SDIO_D0 AM1808 MMC/SDIO_D0 MMCSD1_DAT[0]
WLAN Host I/F SDIO_CLK AM1808MMC/SDIO_CLK MMCSD1_CLK
WLAN Host I/F SDIO_D3 AM1808 MMC/SDIO_D3 MMCSD1_DAT[3]
WLAN Host I/F SDIO_D1 AM1808 MMC/SDIO_D1 MMCSD1_DAT[1]
WLAN Host I/F SDIO_D2 AM1808 MMC/SDIO_D2 MMCSD1_D[2]
WLAN Host I/F WLAN_IRQ AM1808 GPIO UHPI_HCNTL1 /UPP_CH1_START /GP6[10]
WLAN Host I/F WL_UART_DBG Optional signal No Connect
WLAN Host I/F WL_RS232_RX Optional signal No Connect
WLAN Host I/F WL_RS232_TX Optional signal No Connect

Getting Started Guide

Follow this link to access the Getting Started Guide that describes the HW setting, WLAN and BT driver installation and basic connection to the WLAN AP:
Getting Started Guide

See Also



Links

Follow this link for the LSR Module Product web page LSR Module product page
Follow this link for the WL1271 module datasheet
Follow this link for the Mistral WL271 daughtercard web page Mistral WL271 daughtercard product page



HomepageIcon.jpgHOME

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox