Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

AM335x-PSP 04.06.00.08 Release Notes

From Texas Instruments Wiki
Jump to: navigation, search

Content is no longer maintained and is being kept for reference only!

TIBanner.png
AM335x-PSP 04.06.00.08 Release Notes
Linux PSP

AM335x PSP 04.06.00.08

Content is no longer maintained and is being kept for reference only!

Release Notes

Release Date:  August 1, 2012

Introduction

This is Release 04.06.00.08 of AM335x Linux PSP. This release supports:

The Linux PSP serves to provide a fundamental software platform for development, deployment and execution of Linux based applications on Texas Instruments silicon.

The Linux kernel and U-Boot software in this release are based on the following open source repositories:


Component Version Base Repository Base Tag (or commit id)
Linux Kernel v3.2 http://arago-project.org/git/projects/?p=linux-am33x.git;a=summary d3f8f7cc6d6ee6f50d3cfee335ad0994ad910d1c
U-Boot 2011.09 http://git.denx.de/?p=u-boot.git;a=summary v2011.09


The code base for Linux kernel, U-Boot and power management firmware included in this release is hosted at the following repositories:

Component Repository & Branch Release Tag
Linux Kernel http://arago-project.org/git/projects/?p=linux-am33x.git;a=shortlog;h=refs/heads/AM335XPSP_04.06.00.08
(The kernel obtained directly from the above repository needs PM firmware to build when building using default configuration. Link to PM firmware repository containing the firmware binary is available below in this table. Copy the firmware binary .bin file into the firmware/ folder of the kernel sources)
v3.2_AM335xPSP_04.06.00.08
U-Boot http://arago-project.org/git/projects/?p=u-boot-am33x.git;a=shortlog;h=refs/heads/AM335XPSP_04.06.00.08 v2011.09_AM335xPSP_04.06.00.08
Power Management Firmware http://arago-project.org/git/projects/?p=am33x-cm3.git;a=shortlog;h=refs/heads/AM335XPSP_04.06.00.08 AM335xPSP_04.06.00.08


Obtaining the Release Package

The PSP release package can be obtained from TI's Technology and Software Publicly Available (TSPA) download site.


Dependencies

Tool/Component Description Release Version Required for
Code Composer Studio (CCS) IDE and ARM compiler 5.1.0.09000 Building CCS based flash writers
Arago Toolchain GCC ARM cross compiler 2011.09 (GCC 4.5.3) Building Linux kernel, U-Boot, Linux examples
Filesystem Target filesystem NA Linux boot


Documentation

The User's Guide provides instructions on how to use the PSP Release package.

The AM335x-PSP 04.06.00.08 Features and Performance Guide provides information on various device driver features and provides performance numbers.


What's Supported

The Linux PSP package supports the following components:

  • SPL and U-Boot v2011.09 supporting SPI, NAND, MMC/SD and Ethernet boot modes
  • Linux Kernel v3.2 and device drivers
  • CCS based NAND flash writers.
  • Linux examples.


Linux feature support on EVM (Rev 1.1A and above)
Peripheral Instance Support Status
UART UART0 Supported.
UART1 Supported in SDK using Bluetooth module
UART2 Supported
UART3 Planned
UART4 Planned
UART5 Planned
Ethernet Switch CPSW0 Supported. IEEE1588 support planned.
SPI SPI0 Supported
SPI1 Not available in EVM
I2C I2C0 Supported
I2C1 Supported
McASP McASP0 Not available in EVM
McASP1 Supported
DCAN DCAN0 Not available in EVM
DCAN1 Supported
EDMA EDMA0 Supported
Timer Timer0 Not Tested (Not used in Linux)
Timer1 Supported (Schedule Tick)
Timer2 Supported (Clocksource)
Timer3 Not Tested (Not used in Linux)
Timer4 Not Tested (Not used in Linux)
Timer5 Supported (CPSW Interrupt pacing)
Timer6 Supported (CPSW Interrupt pacing)
Timer7 Not Tested (Not used in Linux)
Watchdog timer Supported
RTC RTC0 Supported
ePWM eHRPWM0 Not available in EVM
eHRPWM1 Not available in EVM
eHRPWM2 Supported (used by Haptics module on EVM)
eQEP0 Not available in EVM
eQEP1 Not available in EVM
eQEP2 Not available in EVM
eCAP0 Supported in PWM mode (APWM), used as LCD backlight control. Capture mode not supported.
eCAP1 Not available in EVM
eCAP2 Not available in EVM
Touchscreen/ADC TSCADC0 Touchscreen supported, Raw ADC not supported.
MMC/SD MMC/SD0 Supported
MMC/SD1 Supported (Profile 2)
MMC/SD2 Not available in EVM
GPIO GPIO0 Supported
GPIO1 Supported
GPIO2 Supported
GPIO3 Tested using WLAN/Bluetooth in SDK
USB USB0 Supported
USB1 Supported
GPMC GPMC0 NAND is Supported, NOR is planned.
LCD Controller LCDC0 GLCD is supported, Character LCD is not supported in EVM
Power Management CPU Idling Planned (only ARM WFI supported currently)
Dynamic Voltage and Frequency Scaling (DVFS) Supported
DeepSleep0 Supported (Suspend-to-RAM)
On-board components Accelerometer Supported
Ambient Light Sensor Supported
Temperature Sensor Supported
Haptics Supported
GPIO keypad Supported


Linux support feature support on BeagleBone (Rev A3 and above)
Peripheral Support Status
UART0 Supported.
Ethernet Switch Supported.
MMC/SD0 Supported.
USB0 Supported.
USB1 Supported.
Power Management Supported as in EVM


Linux support feature support on EVM-SK (Rev 1.2B and above)
Peripheral Support Status
UART0 Supported.
LCD Supported.
Touchscreen Supported.
McASP (audio) Supported.
Ethernet Switch (both ports) Supported
MMC/SD0 Supported.
USB0 Supported.
USB1 Supported.
Power Management Supported as in EVM
Accelerometer Supported.
GPIO-keypad Supported.
GPIO-LED Supported.


The PSP package also includes:

  • Pre-built binaries for U-Boot, Linux kernel, flash writers and examples
  • Relevant Documents


New in this Release

  • Support for EVM-SK (Rev 1.2B and later)
  • Ethernet Switch
    • Support for two external ports as independent network interfaces
    • Support for VLAN and ALE entry configuration interface
  • Suspend-to-RAM (DeepSleep0) with DDR3 support
  • DDR3 support in U-Boot
  • Support for SPI and Ethernet boot modes in U-Boot


Fixed in this Release

This section lists issues fixed in this release:

ALSA

Issue Identifier
Issue Headline
SDOCM00089719 ALSA: loopback fails when driver is built as module


Base Port

Issue Identifier
Issue Headline
SDOCM00091114 BasePort: Pin Mux: debugfs shows wrong values
SDOCM00091865 BasePort: Interrupts in bank 4 are not handled


Ethernet

Issue Identifier
Issue Headline
SDOCM00086213 Ethernet: "#ethtool eth0" is not showing complete information of Ethernet device
SDOCM00091636 Ethernet: CPSW: must turn off the AM335x internal delay feature on transmit clock


MMC/SD

Issue Identifier
Issue Headline
SDOCM00085920 MMC/SD: Beaglebone: multiple times of insert and remove mmc modules with R/W operation causes dut to hang
SDOCM00092044 MMC/SD: HSPE bit needs to be set when MMC/SD clock is above 25MHz


Power Management

Issue Identifier
Issue Headline
SDOCM00091540 Power Management: BeagleBone: cpufreq should not set frequencies greater than 500MHz when device is powered using USB
SDOCM00090692 Power Management: I/O error observed when copy files from one USB drive to another USB driver along with suspend resume operation.
SDOCM00090696 Power Management: “LCDC sync lost” and “Kernel core reported suspend failure” messages appear when MMC/SD to MMC/SD file copy along with suspend resume operation
SDOCM00090962 Power Management: Resume operation fails on some beaglebone boards (~1/3 of boards tested)
SDOCM00091029 Power Management: USB: Resume operation take 90 seconds if connected USB device is removed during suspend operation
SDOCM00091208 Power Management: shut down TSC/ADC during suspend if TSC wake is not required
SDOCM00092110 Power Management: 'pll_lock' macro does not correctly wait for PLL lock to happen
SDOCM00093513 Power Management: Fix erratum 1.0.15: OPP50 on MPU domain is not supported


U-Boot

Issue Identifier
Issue Headline
SDOCM00089686 U-Boot: EVM: fails when profile 2 is selected to boot using mmc1
SDOCM00092035 U-Boot: boot fails on using uEnv.txt for setting environment variables


USB

Issue Identifier
Issue Headline
SDOCM00088841 USB: Video capture : USB video capture is not working for 640x480 resolution and exit with the message "select timeout"
SDOCM00089422 USB: Wifi driver can not be initialized on AM335x EVM (works on BBB)
SDOCM00090435 USB: using USB2Ethernet interface leads to kernel oops
SDOCM00090439 USB: while transfer big file from EVM to laptop through Atheros wifi dongle a kernel oops occurs
SDOCM00090690 USB: audio: Corrupted audio heard after pause
SDOCM00091275 USB: audio: kernel crashes when attempting to remove mass storage gadget
SDOCM00093764 USB: kernel panic when proc_read() is done after removing g_ether module


Known Issues

This section lists known issues in this release.

Audio

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00086121 ALSA: Audio loopback prints error messages The warnings are harmless and can be ignored.
SDOCM00089663 SD card removal results in noise during ALSA playback/loopback None
SDOCM00088830 ALSA: arecord: Unable to capture audio at exact 24KHz sample rate None


Base Port

This section notes issues with U-Boot and basic kernel board support.

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00085443 WDT1 timeout inaccurate. None
SDOCM00086716 HWMOD warnings upon doing WDT file operations The warning is harmless and can be ignored.
SDOCM00085737 After soft reboot, dhcp or tftp sometimes timeout in U-Boot. Power cycle the board (hard reboot).


Ethernet

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00086066 Ethernet: MAC address configuration is not supported in kernel None
SDOCM00086717 EVM: NFS: arecord takes longer than expected time to record file to NFS filesystem None
SDOCM00085982 Beaglebone: UDP client performance at 100Mbps and the throughput is less than 1 Mbps UDP performance drops suddenly after 95Mbps. UDP rate needs to be throttled to 95Mbps for better performance.
SDOCM00091328 Ethernet: Performance drops to half with file storage IO in progress None
SDOCM00090654 Ethernet: kernel crashes if removing ethernet module without bringing down network interface Bring down the network interface before removing ethernet module


I2C

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00087207 I2C controller timeout for some slave devices connected on i2c1 at 400KHz Operating at 100Khz does not cause these timeouts.


MMC/SD

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00085738 mmcsd write performance is very low when card is mounted as sync. It is highly recommended to use async mode for good MMC/SD performance
SDOCM00085770 MMC 8bit is not supported. None
SDOCM00087204 EVM: write protection for mmc1 in daughter board doesn't work None
SDOCM00089663 SD card removal results in noise during ALSA playback/loopback None
SDOCM00090498 MMC: hsmmc driver doesnt support 1.8v MMC cards None
SDOCM00090756 MMC1: One SD card could not be used as rootfs when in slot1; The same card works in slot0 This issue happens with one card at the moment and needs further debug.
SDOCM00090970 MMC1 in profile 2: some SD or MMC cards cause DUT to hang None


NAND

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00086033 Nand mtdtest oob test and subpage test fail. None
SDOCM00090530 Nand performance in this release is lower than the previous (04.06.00.06) release. None


On-board Components

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00091115 AM335X: HAPTICS doesn't work on all board revisions update CPLD to version 1.0E or later.


Power Management

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00087097 cpu_idle reports wrong power consumption numbers for WFI and DDR SR states None
SDOCM00089584 cpufreq: Unable to change OPP in AM335x evm This issue is because of misbehavior of I2C client contained inside the CPLD on the EVM. BeagleBone can be used to test CPUFreq on AM335x. BeagleBone does not have a CPLD and does not suffer from the same limitation as the EVM.
SDOCM00090470 Suspend/Resume during MMC/SD write using dd with large block size write causes the file write to not complete Please use "sync" command before suspending to avoid losing data. Also, please use small block size (eg 512/1024 bytes) for transfer if there is chance of system going to suspend while transfer is going on.
SDOCM00090946, SDOCM00094203 Suspend: Sometimes (~25 times out of 1000), DUT might abort the suspend process and come back safely to prompt When this happens, user space can and should retry the suspend operation.
SDOCM00090689 AM335x: USB: aplay/arecord exit with error if system is suspended while playback/recording is ongoing This issue is because of limitation of USB audio stack in Linux and can be observed on a PC too. Please wait for USB audio to finish before suspending or alternately, retry the audio operation after resume completes.
SDOCM00091071 AM335x: Suspend-to-RAM does not reduce core voltage None.
SDOCM00091498 AM335x: cpuidle C2 state is not entered None. This is a known issue. See note in user's guide.
SDOCM00091330 AM335x: i2cdetect throw timeout errors and after that dut hangs after soft reboot On the EVMs where this issues comes up, i2c usage in suspend-resume via cpufreq should be avoided by disabling cpufreq in the kernel.
SDOCM00094261 AM335x [USB] System does not wake up on inserting USB devices in Suspend state. None. Using other wakeup modes is recommended.


SPI

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00094016 SPI: SPI_IOC_MESSAGE or read hangs when data read byte is above 158 and bits per words is 16. For any SPI transfer > 160 bytes, select 8 bits-per-word mode.


UART

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00085586 UART: hardware flow control is not working This is an issue because of mis-configuration of CPLD present on EVM. The UART driver is expected to work correctly with flow-control. Bluetooth module on EVM used UART flow control successfully.


USB

Issue Identifier
Issue Headline
Known Workaround(s)
SDOCM00085670 USB: NFS stops working when CDC/RNDIS gadget module is inserted with Arago FS None. This is being tracked as a filesystem issue. http://arago-project.org/cgi-bin/bugzilla3/show_bug.cgi?id=11
SDOCM00085673 USB File storage gadget: instability when pendrive connected to host port exposed as storage media from gadget port to PC None
SDOCM00087173 USB: MassStorageGadget: Issues when MMC card is used as storage media or gadget port None
SDOCM00087229 USB: PIO mode read performance numbers are almost 50% less as compared to that of DMA mode read performance Use DMA mode of operation if performance is critical. There are some outstanding issues with DMA mode, please go through the rest of this table for information regarding them.
SDOCM00089374 USB: High cpu loading with CDC gadget when connected to another EVM or local loopback None
SDOCM00089782 USB command verifier (CV) test fails None
SDOCM00091464 USB: UVC: The UVC camera does not capture the frames after several times of camera turned off and on None
SDOCM00087342, , SDOCM00089599 USB: CPPI4.1 DMA locks up when CPU mode transfer is done in parallel to DMA transfer. Sometimes USB resets are seen. Use PIO mode when there is possibility of control transfer in parallel to DMA transfers. Such as when using WiFi and mass storage together or when connecting and disconnecting devices connected to a hub port when DMA transfers are active on another port. Please refer to USB User's Guide for detail on how to enable PIO mode.


Installation and Usage

Please look for detailed installation and usage instructions in the AM335x PSP User's Guide

Upgrade and Compatibility Information

There are no known incompatibilities from previous release.

Technical Support and Product Updates

For further information or to report any problems, contact http://community.ti.com or http://support.ti.com.

OMAP Linux Mailing List: http://vger.kernel.org/vger-lists.html#linux-omap