Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

AM335x-PSP 04.06.00.09-rc2 Release Notes

From Texas Instruments Wiki
Jump to: navigation, search

Content is no longer maintained and is being kept for reference only!

TIBanner.png
AM335x-PSP 04.06.00.09 Release Notes
Linux PSP

AM335x PSP 04.06.00.09

Content is no longer maintained and is being kept for reference only!

Release Notes

Release Date:  December 21, 2012

Introduction

This is release 04.06.00.09 of the AM335x Linux PSP. The PSP is part of the Sitara SDK. This PSP release supports:

The Linux PSP serves to provide a fundamental software platform for development, deployment and execution of Linux based applications on Texas Instruments silicon.

The code base for Linux kernel, U-Boot and power management firmware included in this release is hosted at the following repositories:

Component Repository & Branch Release Tag
Linux Kernel http://arago-project.org/git/projects/?p=linux-am33x.git;a=shortlog;h=refs/heads/v3.2-staging
(The kernel obtained directly from the above repository needs PM firmware to build when building using default configuration. Link to PM firmware repository containing the firmware binary is available below in this table. Copy the firmware binary .bin file into the firmware/ folder of the kernel sources)
v3.2_AM335xPSP_04.06.00.09-rc2
U-Boot http://arago-project.org/git/projects/?p=u-boot-am33x.git;a=shortlog;h=refs/heads/amsdk-05.06.00.00 v2011.09_AM335xPSP_04.06.00.08
Power Management Firmware http://arago-project.org/git/projects/?p=am33x-cm3.git;a=shortlog;h=refs/heads/master AM335xPSP_04.06.00.09-rc2


Dependencies

Tool/Component Description Release Version Required for
Code Composer Studio (CCS) IDE and ARM compiler 5.1.0.09000 Building CCS based flash writers
Arago Toolchain GCC ARM cross compiler 2011.09 (GCC 4.5.3) Building Linux kernel, U-Boot, Linux examples
Filesystem Target filesystem NA Linux boot



Feature Addition:

  • RTC Runtime PM Support
  • TSC/ADC: IIO and MFD framework migration
  • ADC driver support
  • tps65217: Set PMIC to shutdown using RTC module
  • USB PHY Wakeup support

    Note: Since in DS0 usb wakeup can not be supported on current silicon, by default USB wakeup is kept disabled.

  • CPSW: Promiscuous mode support
  • CPSW: Support the HWTSTAMP ioctl and the CPTS


Bug Fixes and Cleanup:

  • PWM: ecap: Resets the PWM output to low on stop
  • net: ethernet: fix kernel OOPS when remove davinci_mdio module
  • SDOCM00094923: NFS mount fails with "DHCP/BOOTP: ignoring delayed packet" messages
  • mtd: nand: omap: fix race condition in omap_wait()
  • mtd: nand: omap2: Fix for uncorrectable error
  • mtd: nand: omap2: Fix bit flip in data area due to bit flip in OOB
  • mtd: nand: omap2: Fix ECC read for 16-bit NAND part
  • ARM: OMAP2+: am335x: Fix xbar channel implementation for odd channels
  • SDOCM00085443 - ARM: OMAP2+: am335x: Change the wdt1 func clk src to per_32k clk
  • SDOCM00086716 - Fix omap_hwmod wdt2: _wait_target_disable failed error message
  • ARM: OMAP: AM33XX: PM: Fix potential deadlock in resume process due to MPU leaving GPIO0 enabled
  • USB:
  • Build warning fixes
  • usb: musb: Fixes for invalid parameter passed for dev_dbg()
  • SDOCM00097396 - Babble workaround fix
  • SDOCM00097395 - Rx race condition
  • SDOCM00091956 - The debugfs support for usb testmode
  • SDOCM00091464 - The UVC camera doesn't capture frames after several times of off and on
  • SDOCM00095817 - AM335x: CPPI DMA RX does not handle the dummy byte in ZLP

 

Documentation

The User's Guide provides instructions on how to use the PSP Release package.

The AM335x-PSP 04.06.00.08 Features and Performance Guide provides information on various device driver features and provides performance numbers.

Installation and Usage

Please look for detailed installation and usage instructions in the AM335x PSP User's Guide

Upgrade and Compatibility Information

There are no known incompatibilities from previous release.

Technical Support and Product Updates

For further information or to report any problems, contact http://community.ti.com or http://support.ti.com.

OMAP Linux Mailing List: http://vger.kernel.org/vger-lists.html#linux-omap