AM335x General Purpose EVM HW User Guide

From Texas Instruments Wiki
Jump to: navigation, search
AM335x General Purpose Evaluation Module (TMDXEVM3358) Hardware User Guide


Introduction

This document describes the hardware architecture of the AM335x Evaluation Module (EVM) (Part # TMDXEVM3358) which is based on the Texas Instruments AM335x processor. This EVM is also commonly known as the AM335x General Purpose (GP) EVM.


Description

The AM335x General Purpose EVM is a standalone test, development, and evaluation module system that enables developers to write software and develop hardware around an AM335x processor subsystem. The main elements of the AM335x subsystem are already available on the base board of the EVM which gives developers the basic resources needed for most general purpose type projects that encompass the AM335x as the main processor. Furthermore, additional, "typical" type peripherals are built into the EVM such as memory, sensors, LCD, Ethernet PHY, etc. so that prospective systems can be modeled quickly without significant additional hardware resources.

The following sections give more details regarding the EVM.


EVM System View

The System View of the AM335x General Purpose EVM consists the baseboard, daughterboard, and LCD display board stacked together and connected through standard throughhole connectors. See the pictures below of the EVM.

Gpevm7.JPG Gpevm bottom.JPG
Figure 1: AM335x General Purpose EVM Figure 2: AM335x Baseboard Bottom View



Schematics/Design/Errata Files

Be sure to view the Errata document for important notes

System Description

System Board Diagram

The complete AM335x General Purpose EVM is partitioned across three different boards for modularity. The GP EVM consists of the baseboard (processor and main power supply), daughterboard (external peripherals), and the LCD display board (LCD and touchscreen).

am335x_evm_system_boardview_diagram.jpg


Figure 3: AM335x EVM System Board Diagram


The functional block diagram of the AM335x 15x15 baseboards is as given below: The functional block diagram of the AM335x General Purpose Daughterboard is as given below: The block diagram of the AM335x LCD A Board is as given below:
Base 15 15 block.JPG Gp block.JPG Lcd block.JPG
Figure 4: AM335x 15x15 Baseboard Block Diagram Figure 5: AM335x General Purpose Daughterboard Block Diagram Figure 6: AM335x LCD A Block Diagram


Processor

The AM3358ZCZ processor is the central processor to this EVM. All the resources on the board surround the AM3358 processor to provide development capabilities for hardware and software. See the AM3358 datasheet and TRM for the details about the processor.

There are system configuration signals, SYSBOOT, that can be set on the EVM to define some startup parameters on the AM335x processor. See the Configuration/Setup section later for more details.

Clocks

The EVM has several clocks to support the AM3358 processor. The main clock for the processor is derived from a 24MHz crystal. An on-board oscillator in the AM3358 generates the base clock and subsequent module clocks as needed within the AM3358 processor. A 32kHz clock for the RTC on the AM3358 is derived from a 32kHz crystal on the board.

Reset Signals

SYS_RESETn is a signal running to several peripherals and AM335x which performs a reset on those peripherals. SYS_WARMRESETn is accerted by the pushbutton and is used to force a reset of the AM335x. AM335x can also pulldown on the RESET_INOUTn signal to cause the SYS_RESETn line to go active.

Power System

This section describes how the power supply will be implemented.


Power Source

AM335x Baseboard uses an external AC to +5VDC (rated 2.5A min) power adapter. The switch near to the power cable is used for power ON/OFF. The main power is off when the power switch is in the position away from the power supply jack. The main power is on when the power switch is in the position closest to the power supply jack.


Power adapter.JPG


Figure 7: AM335x Power Adapter



Note: When powering this EVM, always use the recommended power supply (CUI/V-Infinity Part Number EMSA050300-P6P-SZ, Model 3A-182WP05) or equivalent model having output voltage of +5VDC, output current max 3.0 Amp, and Efficiency Level V as well as the applicable regional product regulatory/safety certification requirements such as (by example) UL, CSA, VDE, CCC, PSE, etc. Examples of equivalent models include SMI18-5-V-P6 or SWI18-5-N-P6. A power supply is no longer included in the kit.

Note: Mounted to this EVM is a UL-recognized component, RoHS-compliant Lithium rechargeable battery (Seiko MS920SE: Nominal voltage 3V, Nominal capacity 11.0 mAh, UL File No. MH15628)

  • This battery should only be replaced by a trained technician.
  • This battery is intended for use at ordinary temperatures where the EVM is not operated above a high temperature of 60°C or below a low temperature of -20°C.


batterycaution1.jpg

Power Nets

The power nets used in the AM335x Baseboard schematics are listed in the below tables.

Net Description
V1_8DDR Power supply for DDR2 SDRAM
GND_OSC0 isolated ground for OSC0 main clock source
GND_OSCRTC isolated ground for RTC oscillator
DGND main ground reference net
V3_3D digital 3.3V power
V5_0D digital 5.0V power
GNDUSB0 local ground for USB0 connector shield
GNDUSB1 local ground for USB1 connector shield
V1_8D digital 1.8V power
VSDMMC0 digital SDMMC0 power supply (1.8V or 3.3V)
VBAT main unregulated power supply (may be tied to 5V)

(needs to be 3.7 to 5.5V)

VCOM_BAT COM connector VBAT supply (must be 3.6V)
VEXPD Unregulated power supply for expansion board
GND_ADC Local ground for the ADC
VADC Power supply for the ADC
GND_ETH Ethernet Gb/s isolated ground
V1_2D Power supply 1.2V
VHDMI_IO Power supply for HDMI transceiver I/O
V5_0USB 5.0V power supply for the VBUS on USB
V1_1D Power supply for AM335x core
GNDA_TSC Local analog ground for touch screen
VDDH_PHY Ethernet VDDH_REG power supply
VETH_AVDD_3_3 Ethernet 3.3V analog power supply
VETH_VDDIO Ethernet I/O power supply
VDDL_PHY Ethernet main digital supply
VADDL_PHY Ethernet analog supply
VETH_LX Ethernet LX power supply

Table 1: AM335x Baseboard Power Nets


Net Description
DGND main ground reference net
V3_3D digital 3.3V power
V5_0D digital 5.0V power
V1_8D digital 1.8V power
VSDMMC1 digital SDMMC1 power supply (1.8V or 3.3V)
VBAT main unregulated power supply (may be tied to 5V)

(needs to be 3.7 to 5.5V)

VEXPD Variable power supply for expansion board
GND_ADC Local ground for the ADC
VADC Power supply for the ADC
V1_0PHY Ethernet Gb/s 1.0 PHY supply
V1_0APHY Ethernet Gb/s 1.0V analog PHY supply
V2_5PHY Ethernet Gb/s 2.5V PHY supply
GND_ETH Ethernet Gb/s isolated ground
VLCD_VCC 3.3V power supply for LCD
VLCD_AVDD Analog power supply for LCD 10V
VLCD_VGH LCD VGH TFT supply 15V
VLCD_VGL LCD VGL TFT supply -7V

Table 2: AM335x General Purpose Daughterboard Power Nets

The power sequencing requirements of the AM335X processor (see the AM335x datasheet) are handled automatically by the TPS65910 PMIC.


Power Management IC Power Supplies

The AM335x Baseboard uses the TPS65910 power management IC.

The I2C0 on AM335x is used to control the Smart Reflex port and control port on the TPS65910.

For AM335x, the following power supplies from the TPS65910A are used.


TPS65910 Power Supply AM335x Power Rail Voltage
VAUX2 (300mA) VDDSHV1, 3, 5,6 (500mA) 3.3V (rails that are 3.3V)
VDIG1 (300mA) VDDSHV1, 3, 5, 6 (500mA) 1.8V (rails that are 1.8V)
VMMC (300mA) VDDSHV4 (60mA) & VDDSHV2 1.8V/3.3V
VDD2 SMPS (1500mA) VDD_CORE (1000mA) 1.1V
VDD1 SMPS (1500mA) VDD_MPU (1500mA) 1.2V
No supply needed VDD_RTC 1.1V
VRTC VDDS_RTC (10mA) 1.8V
VIO_SMPS (1000mA) VDDS_DDR (200mA) 1.8V (or 1.5V for DDR3)
VIO_SMPS (1000mA) VREFSSTL (10mA) 0.9V or 0.75V
VDAC (150mA) VDDS (100mA) 1.8V
VDIG2 (300mA) VDDS_SRAM_CORE_BG

(40mA)||1.8V

VDIG2 (300mA) VDDS_SRAM_MPU_BB (40mA) 1.8V
VDIG2 (300mA) VDDS_PLL_DDR (25mA) 1.8V
VDIG2 (300mA) VDDS_PLL_CORE_LCD (25mA) 1.8V
VDIG2 (300mA) VDDS_PLL_MPU (25mA) 1.8V
VDIG2 (300mA) VDDS_OSC (10mA) 1.8V
VAUX1 (300mA) VDDA1P8V_USB0/1 (50mA) 1.8V
VAUX33 (150mA) VDDA3P3V_USB0/1 (10mA) 3.3V
VAUX33 (150mA) USB_VBUS0/1 3.3V
VPLL (50mA) VDDA_ADC 1.8V
VDD3 SMPS (100mA) Not Used -
VIO_SMPS (1000mA) DDR2 SDRAM (320mA) 1.8V

Table 3: AM335x Power supplies from TPS65910A



APM Sense Resistors

The AM335x Baseboard has the following subsystems with current sense resistors. These resistors allow the power to be measured on each power rail to check AM335x power requirements during real time software execution. The value of the resistors is selected to provide the best dynamic range when using a TI INA226 converter. In fact an INA226 converter is installed on the base board for both the VDD_CORE and VDD_MPU power supply rails of the AM335x. The other power rails have sense resistors but have their measurement connections attached to 2pin standard headers so that they can be read easily by a multimeter or connected to an INA226 converter EVM.

Note the value of the sense resistors for the VDD_CORE and VDD_MPU were selected to give better dynamic range for active power modes rather than sleep/low power modes. If power is to be measured for VDD_CORE or VDD_MPU for sleep/low power modes then this sense resistor value should be changed to give better shunt voltage values.


Voltage Net Sense Resistor Value
VDD_CORE 0.05ohm
VDD_MPU 0.05ohm
VDDSPLLMPU 2ohm
VDDS_SRAMMPU_BB 2ohm
VDDS_SRAM_CORE_BG 2ohm
VDDA1P8V_USB0 1ohm
VDDA3P3V_USB0 2ohm
VDDS_PLL_DDR 2ohm
VDDS_DDR 0.24ohm
SA_VDDSHV1 0.24ohm
SA_VDDSHV2 0.24ohm
SA_VDDSHV3 0.24ohm
SA_VDDSHV4 0.24ohm
SA_VDDSHV5 0.24ohm
SA_VDDSHV6 0.24ohm
SA_VDDS 0.24ohm
SA_VDDA_ADC 1ohm
VDDS_PLL_CORE_LCD 2ohm
VDDS_RTC 2ohm
VDDS_OSC 2ohm

Table 4: AM335x Baseboard APM Sense Resistors

Configuration/Setup

The GP EVM has many different subsystems to allow development around the AM335x's capabilities. Most of these subsystems are fixed with regard to address locations and pin assignments. However, there are some functions that can be changed by configuring the EVM with switches. For the GP EVM, some of the AM335x pins are connected to different subsystems based on the CPLD profile number that is active. (The CPLD profile number is selected by a 4bit DIP switch on the GP daughterboard.) The CPLD is thus used primarily as a pin mux switch.

Additionally, the AM335x has SYSBOOT pins that can be configured a certain way using two 8bit DIP switches on the base board. These SYSBOOT switches will configure the AM335x to different settings. For instance, the boot method of the processor can be setup by setting certain of these DIP switches to particular settings. SW3 DIP switch has the switches that set the SYSBOOT[0..7] and SW4 DIP switch has the switches that set the SYSBOOT[8..15]. See the AM335x TRM and datasheet for the actual definitions of each of the SYSBOOT signals. The SW3 DIP switch 1 corresponds to SYSBOOT(0), SW3 DIP2 = SYSBOOT(1), etc. The SW4 DIP switch 1 corresponds to SYSBOOT(8), SW4 DIP2 = SYSBOOT(9), etc. When the DIP switch is off, then the corresponding SYSBOOT signal is pulled high. When the DIP switch is on, then the corresponding SYSBOOT signal is pulled low. Also, see the GP EVM base board schematic for more details.

CPLD

The general purpose daughterboard has a CPLD on it with connections to the major AM335x signals. The Altera EPM2210 is used to do active muxing of non-critical signals. It is also available for test logic that may be used for extra-EVM tests. AM335x can communicate and read the configuration of the muxes inside the CPLD by using the I2C bus. I2C0 of the AM335x is connected to the CPLD and an I2C slave is implemented within the CPLD. The I2C address is 0x35.

To control the configuration of the muxes inside the CPLD, user can select the required profiles by using three switches as shown in the below figure. Switches 1 to 3 control the profile that the CPLD, and thus the EVM, operates in. Switch 1 of the DIP switch is the lsb in the profile number and Switch 3 of the DIP switch is the msb of the profile number so possible profiles numbers are 0 to 7. See the pin mux section later in this document for a description of the AM335x pin definitions for each of the 8 profiles. The fourth DIP switch is reserved and should always be off.


Cpld profile sw1.JPG


Figure 8: AM335x CPLD Profile Switch



I2C Address Assignments

In the AM335x GP EVM boards, each separate board has an I2C ID memory that contains the details of the identity of that board such as it's configuration, etc. (see sections below for more details on the memories' contents). All the ID memories use I2C0 from AM335x (as does the Smart Reflex to the PMIC) so that software can always check I2C0 at the defined I2C addresses for the presence of a board and its contents. Therefore, the baseboard is the only board that has the ID memory set to 0x50, the daughterboard's addresses are all 0x51 (only one daughterboard is ever connected at a time), and the LCD (display board) is at 0x52.

AM335x Baseboard Function AM335x I2C Port Address
Baseboard ID memory I2C0 0x50
AM335x PMIC Smart Reflex I2C0 0x12
AM355x PMIC Control I2C0 0x2D

Table 5: AM335x Baseboard I2C Bus Addresses

AM335x GP Daughterboard Function AM335x I2C Port Address
AIC3106 Audio codec I2C1/I2C2 0x1B
General Purpose Daughterboard ID memory I2C0 0x51
Accelerometer I2C1/I2C2 0x18
Ambient Light Sensor I2C1/I2C2 0x39
Temperature Sensor I2C1/I2C2 0x48
CPLD Control I2C0 0x35
I/O Expander 0 I2C1/I2C2 0x20
I/O Expander 1 I2C1/I2C2 0x21

Table 6: AM335x GP Daughterboard I2C Bus Addresses

AM335x LCD A Board Function AM335x I2C Port Address
LCD A Board ID memory I2C0 0x52
Touch Screen Controller I2C0 0x4A
TLC59108 I2C0 0x40

Table 7: AM335x LCD A Board I2C Bus Addresses


I2C ID Memory

Each of the three boards in the EVM have a dedicated I2C EEPROM which contains specific identity/configuration information for that board. In addition, there is available space in each memory for user specific configuration information.

The part number of the memory device is pn#CAT24C256WI-GT3.

Name Size (bytes) Contents
Header 4 MSB 0xEE3355AA LSB
Board Name 8 Name for board in ASCII "A33515BB" = AM335x 15x15 Base Board
Version 4 Hardware version code for board in ASCII "1.0A" = rev. 01.0A
Serial Number 12 Serial number of the board. This is a 12 character string which is:

WWYY4P16nnnn where: WW = 2 digit week of the year of production YY = 2 digit year of production nnnn = incrementing board number

Configuration 32 Codes to show the configuration setup on this board. For the available EVM's supported, the following codes are used: ASCII "SKU#01" = base board for gen purpose evm ASCII "SKU#02" = base board for industrial motor control evm Remaining 26 bytes are reserved
Ethernet MAC Address #0 6 MAC Address for AM335x Ethernet MAC #1
Ethernet MAC Address #1 6 MAC Address for AM335x Ethernet MAC #2 or PRU #0
Ethernet MAC Address #2 6 MAC Address for AM335x PRU #1 (if used)
Available 32702 Available space for other non-volatile codes/data

Table 8: AM335x 15x15 Baseboard EEPROM Data


Name Size (bytes) Contents
Header 4 MSB 0xEE3355AA LSB
Board Name 8 Name for board in ASCII "A335GPBD" = AM335x General Purpose Daughterboard
Version 4 Hardware version code for board in ASCII "1.0A" = rev. 01.0A
Serial Number 12 Serial number of the board. This is a 12 character string which is:

WWYY4P13nnnn where: WW = 2 digit week of the year of production YY = 2 digit year of production nnnn = incrementing board number

Configuration 32 Codes to show the configuration setup on this board. For the available EVM's supported, the following codes are used: ASCII "SKU#00" = standard gp daughterboard configuration Remaining 26 bytes are reserved
CPLD Version 8 CPLD code version for board in ASCII "CPLD1.0A" = rev. 01.0A of the CPLD
Available 32700 Available space for other non-volatile codes/data

Table 9: AM335x General Purpose Daughterboard EEPROM Data


Name Size (bytes) Contents
Header 4 MSB 0xEE3355AA LSB
Board Name 8 Name for board in ASCII "A335LCDA" = AM335x LCD A Board
Version 4 Hardware version code for board in ASCII "1.0A" = rev. 01.0A
Serial Number 12 Serial number of the board. This is a 12 character string which is:

WWYY4P15nnnn where: WW = 2 digit week of the year of production YY = 2 digit year of production nnnn = incrementing board number

Configuration 32 Codes to show the configuration setup on this board (codes to be assigned TBD)
Available 32708 Available space for other non-volatile codes/data

Table 10: AM335x LCD A Board EEPROM Data



AM335x EVM Functional Block Descriptions

This section describes major functional blocks of the AM335x EVM System.


Board Identity Memory

Each of the boards contains a serial EEPROM that contains board specific data that allows the processor to automatically detect which board is connected and the version of that board. Other hardware specific data can be stored on this memory device as well. The part number of the memory device is pn#CAT24C256WI-GT3. See the Configuration/Setup section for details on the data in this memory.


SDMMC0 Connector

The SDMMC0 connector on the Base Board is a Morethanall card socket #MHC-W21-601. This is a standard SD/MMC Card type of connector. It is connected to the MMC0 port of the AM335x processor. Check the AM335x data sheet and TRM for supported card types/densities.

The Pin assignment is as given below.


Pin No Memory Card PIN No.
MMC plus & MMC mobile & MMC & RS-MMC & SD#1 RSV/DAT3
MMC plus & MMC mobile & MMC & RS-MMC & SD#2 CMD
MMC plus & MMC mobile & MMC & RS-MMC & SD#3 GND
MMC plus & MMC mobile & MMC & RS-MMC & SD#4 VCC
MMC plus & MMC mobile & MMC & RS-MMC & SD#5 CLK
MMC plus & MMC mobile & MMC & RS-MMC & SD#6 GND
MMC plus & MMC mobile & MMC & RS-MMC & SD#7 DAT0
MMC plus & MMC mobile & SD#8 DAT1
MMC plus & MMC mobile & SD#9 DAT2
MMC plus & MMC mobile#10 DAT4
MMC plus & MMC mobile#11 DAT5
MMC plus & MMC mobile#12 DAT6
MMC plus & MMC mobile#13 DAT7
miniSD#1 CD/DAT3
miniSD#2 CMD
miniSD#3 GND
miniSD#4 VCC
miniSD#5 CLK
miniSD#6 GND
miniSD#7 DAT0
miniSD#8 DAT1
miniSD#9 DAT2
miniSD#10 NC
miniSD#11 NC

Table 11: AM335x SDMMC0 Connector Pin Details



Gbit Ethernet

The AM335x baseboard has a Gbit Ethernet transceiver Atheros AR8031_AL1A that is connected to J15.

The reset on the transceiver is driven by the board system reset SYS_RESETn and the individual reset ETHER_RESETn signal that is controlled by GIO SA_GMII1_COL. A 25MHz crystal drives the clock signal for the AR8031. The Ethernet INT pin is sent to the AM335x SA_GMII1_CRS pin for interrupt.

Note: The GP EVM PCB does not support external delay for the clock signals on the RGMII interface. The AR8031A PHY can be setup to use internal clock delay mode once booting is complete. Therefore there may be problems in function/performance when booting in Gb mode or when running Gb Ethernet Mode before the AR8031A PHY is configured properly. See the EVM Errata.

The PHYAD pins are left unconnected for setting the PHY's address so it is by default 0x01.


Pin No Signal Name Description
1 DGND Ground
2 V3_3D Power 3.3V supply
3 ETHER_D3P Ethernet Data 3 POSITIVE
4 ETHER_D3N Ethernet Data 3 NEGATIVE
5 ETHER_D2P Ethernet Data 2 POSITIVE
6 ETHER_D2N Ethernet Data 2 NEGATIVE
7 ETHER_D1P Ethernet Data 1 POSITIVE
8 ETHER_D1N Ethernet Data 1 NEGATIVE
9 ETHER_D0P Ethernet Data 0 POSITIVE
10 ETHER_D0N Ethernet Data 0 NEGATIVE
D1 PHY_LED_ACTn
D2 DGND Ground
D3 DGND Ground
D4 PHY_LED_1000n
M1 NC
M2 NC
SHLD1 DGND Ground
SHLD2 DGND Ground

Table 12: AM335x Gbit Ethernet Pin Details

The baseboard has one Gb/s Ethernet PHY and RJ-45 connector for the MII1 port. The RJ-45 connector used to communicate with external Ethernet and for testing with external loopback cable.


Base ethernet1.JPG


Figure 9: AM335x Baseboard Ethernet




USB

The AM335x ZCZ package supports 2 USB ports. The USB ports are on the base board and connected to a microUSB AB connector and a standard A connector. The ESD device TPD4012 and common choke filter ACM2012 (TDK) are used on the USB signals before they are connected to the AM335x pins. The microAB connector has its ID pin tied to ground through a 120K resistor by default so that the port looks like a B device.


Pin No Signal Name Description
1 VUSB_VBUS0 USB0 BUS VOLTAGE
2 USB0_CONN_DM USB0 DATA MINUS
3 USB0_CONN_DP USB0 DATA PLUS
4 USB0_ID USB0 IDENTIFICATION
5 DGND Ground

Table 13: AM335x USB Port0


Pin No Signal Name Description
1 VUSB_VBUS1 USB1 BUS VOLTAGE
2 USB1_CONN_DM USB1 DATA MINUS
3 USB1_CONN_DP USB1 DATA PLUS
4 DGND Ground


Table 14: AM335x USB Port1


COM – Mobile Connectivity Expansion Connector

The AM335x baseboard supports TI MCS COM6/7 form factor wireless boards through the J11 COM connector which is a Samtec card edge type connector pn# MEC. This connector thus supports COM6/7 types of boards, and more details about this connector can be found in the MCS COM6/7 board documents.

The COM connector requires 3.6V 442mA on the power supply. Thus a TPS79501 LDO regulator is used to provide this voltage supply from the base 5.0V supply.

The signals on the COM board are all 1.8V voltage level. Thus voltage translators are placed to convert to/from 3.3V of the AM335x rail for a particular signal which is running at 3.3V.



NOR Flash Memory

The GP daughterboard has flash memory which is a NOR type of flash so that the AM335x's access to/from NOR flash function can be tested. The part number of the memory used is Numonyx pn#M29W128GL which is a 16MB (x16 width) flash memory. The GPMC signals are used to communicate with this memory. The GPMC signals are muxed with other signals in AM335x. Also, several other devices connect to the GPMC signals on the baseboard and the daughterboard. boot from NoR is currently not supported on EVM.

Ambient Light Sensor

The ambient light sensor on the GP daughterboard detects and reports the intensity of light luminescence in the human visual spectrum. The part number of the light sensor used is TAOS pn#TSL2550. The AM335x interfaces to the light sensor through I2C.

I2C1 is used and it is muxed in a TXS0102 using mux signal MUXCTRL_I2C1 which comes from the CPLD (based on the selected profile number).



RS-232 Connectors

The baseboard has one RS-232 connector (DB9 male) for one of the UART's. The general purpose daughterboard has 3 more DB9 RS-232 connectors (male). The muxes on this daughterboard (implemented in the CPLD) allow the UART's on the AM335x processor to be connected to these 3 connectors. UART0 is always connected to the DB9 connector on the base board. See the pin use document later in this user guide for the profiles which support connection of the UART's 1 through 5 to these connectors on the daughterboard. When a profile is selected that enables a UART for use, the UART's are assigned to the DB9 connectors from UART1 to UART5 starting at J10, then to J12, to J14, and then back around to J10. Therefore, when enabled by the profile selection:

AM335x UART1 => J10

AM335x UART2 => J12

AM335x UART3 => J14

AM335x UART4 => J10

AM335x UART5 => J12

Furthermore, these connectors can be connected together (through cable) to provide loopback testing. The MAX3232E is used for the RS-232 level translation.


SDMMC1 Connector

The baseboard has one SDMMC connector for the SDMMC0 port. This general purpose daughterboard has 1 more SDMMC connector for the MMC1 interface.


Base sd mmc.JPG


Figure 10: AM335x Baseboard SDMMC Connector



The Pin assignment of the GP daughterboard SDMMC1 connector is the same as the base board SDMMC0 connector. Refer to that signal table for signal assignments


CAN

The general purpose daughterboard has 1 CAN transceiver and connector for the CAN0 interface. The CAN transceiver that is used is the TI ISO1050 and the connector is a DB9 male connector.



Pin No Signal Name Description
1 Reserved Upgrade Path
2 CAN_L Dominant Low
3 CAN_GND Ground
4 Reserved Upgrade Path
5 CAN_SHLD Shield, Optional
6 GND Ground, Optional
7 CAN_H Dominant High
8 Reserved Upgrade Path
9 CAN_V+ Power, Optional

Table 15: AM335x General Purpose Daughterboard CAN Connector Pin Details


A PSM712 transient voltage suppressor and RSZ-3.305HP isolated voltage regulator are connected to the ISO1050 for full industrial connection. The AM335x side line filters are calculated for a max CAN transmission speed of 10MHz.


I2C Expander

This general purpose daughterboard has two I2C I/O expanders. The I/O expander that is used is the TI TCA6408A. The I2C addresses of the expander chip are set to 0x20 and 0x21. Each I/O expander has 4 inputs and 4 outputs.

The use for each of these inputs and outputs:

I/O No. In/Out Description
0 In Expansion Header
1 In Expansion Header
2 In Expansion Header
3 In Expansion Header
4 Out LED
5 Out LED
6 Out LED
7 Out LED

Table 16: AM335x General Purpose Daughterboard I2C Expander 0


I/O No. In/Out Description
0 In Expansion Header
1 In Expansion Header
2 In Expansion Header
3 In Expansion Header
4 Out LED
5 Out LED
6 Out LED
7 Out LED

Table 17: AM335x General Purpose Daughterboard I2C Expander 1


ADC Inputs

The general purpose LCD A board has a resistive touchscreen on the LCD (see the LCD/touchscreen section for more details.) The touchscreen uses 4 of the 8 ADC input channels. The remaining 4 channels are connected to isolated connectors so that a signal can be input into them for testing. J8 connector on the GP daughterboard is used to get the analog data from the touch screen and also for manual testing,


Audio Volume Controls

In some of the profiles, audio is enabled. Switches for audio volume control are enabled in these profiles to aid in developing audio applications. These switches are connected to the eOEP. These switches are pushbutton switches to allow realistic actuation of the volume controls.


Accelerometer

An accelerometer is included on the GP daughterboard to allow motion data to be captured/used by the software. The accelerometer is mounted as close to the center of the board as possible to allow the most useful/dynamic data. The ST Micro model LIS331DLH accelerometer is used and is connected via I2C to the AM335x. The I2C address is 0x18. I2C1 is used and it is muxed in a TXS0102.

Keypad

Pushbutton switches (6) are attached to GIO's via a scanning method to allow a keypad to be used. These switches are powered and scanned to see if a switch is pressed (high) or if the switch is not pressed (low on scan line). The hardware debounce capacitors are not installed by default so software must handle the noise associated with the mechanical bouncing of the switches.


Signal Port No Pin No Event
See pin use document 1 25 Keypad SCN 0
See pin use document 1 26 Keypad SCN 1
See pin use document 1 27 Keypad SCN 2
See pin use document 1 21 Keypad POWER A
See pin use document 1 22 Keypad POWER B

Table 18: AM335x GP Daughter Board GPIO keypad signals


Gp keypads.JPG



Figure 11: AM335x GP Keypad


Haptics Mechanical Vibrator

A Micro Precision pico haptics motor on the GP Daughterboard is used to signal events via mechanical vibration. This is a 304-100 PicoHaptic device which is triggered by a CPLD signal through a FET switch. Thus the profile mode defines which AM335x GIO will turn on this haptics vibrator.


Audio Buzzer

The PUI Audio AI-1027-TWT on the GP Daughterboard is used as an audio buzzer. This is a 2700Hz continuous buzzer that is triggered via a signal from the CPLD through a FET switch. Thus the profile mode defines which AM335x GIO will turn on this audio buzzer.


Temperature Sensor

A TI TMP275 temperature sensor on the GP Daughterboard is used to report ambient temperature. It is controlled by I2C and the I2C address is 0x48.

I2C1 is used and it is muxed in a TXS0102.


NAND Flash Memory

The general purpose daughterboard has a Micron NAND Flash Memory. This is a MT29F2G08ABAEAWP 2Gb 8bit wide flash memory. The footprint is set to allow the 16bit version to be placed instead although there is no plan for this. This memory was placed on the daughterboard to allow active muxing of its signals and allow NOR/MMC1 connection.

Pin No Signal Description
1 NC
2 NC
3 NC
4 NC
5 NC
6 NC
7 NAND_WAIT NAND wait
8 NAND_OEn NAND output enable
9 NAND_CSn NAND chip select
10 NC
11 NC
12 VDDSHV1 Power supply
13 DGND Ground
14 NC
15 NC
16 NAND_BE0n_CLE NAND Byte Enable 0 / Command Latch Enable
17 NAND_ADVN_ALE NAND Address Valid / Address Latch Enable
18 NAND_WEn NAND Write Enable
19 NAND_WPn NAND Write Protect
20 NC
21 NC
22 NC
23 NC
24 NC
25 DGND Ground
26 NAND_D8 NAND Data
27 NAND_D9 NAND Data
28 NAND_D10 NAND Data
29 NAND_D0 NAND Data
30 NAND_D1 NAND Data
31 NAND_D2 NAND Data
32 NAND_D3 NAND Data
33 NAND_D11 NAND Data
34 VDDSHV1 Power supply
35 NC
36 DGND Ground
37 VDDSHV1 Power supply
38 NC
39 VDDSHV1 Power supply
40 NAND_D12 NAND Data
41 NAND_D4 NAND Data
42 NAND_D5 NAND Data
43 NAND_D6 NAND Data
44 NAND_D7 NAND Data
45 NAND_D13 NAND Data
46 NAND_D14 NAND Data
47 NAND_D15 NAND Data
48 DGND Ground

Table 19: AM335x NAND Pin Details


Audio

The TLV320AIC3106 audio codec is used on the general purpose daughterboard. This codec is controlled from AM335x by I2C which is at address 0x1B.


LCD Screen

The LCD is a Three Five 7in WVGA (800x480) RGB LCD panel part number #TFC-S9700RTWV43TR- 01B. It is a 24bit RGB TFT LCD with 27 white LED's for backlight (controlled by one power regulator). The connector is FPC 60pin pn #FH28- 60S-0.5SH(05).

The LED backlight on the LCD is controlled by a TPS61081 PWM controlled LED driver.


Resistive Touch Screen

Pin Name Direction Description
AN0 / XPUL In Analog input 1
AN1 / XNUR In Analog input 2
AN 2/ YPLL In Analog input 3
AN 3/ YNLR In Analog input 4
AN 4 / Wiper In Analog input 5

Table 20: LCD A Resistive Touch Screen Pin Details


SPI Flash Memory

There is a SPI based Flash Memory on the daughterboard of the EVM. This is a 64Mb memory Winbond W25Q64CV. See the pin use description for the profile that supports connection to the SPI memory. Due to connection requirements for other devices that share the same pins as the SPI memory, the GP EVM is not designed to operate at the max SPI clock rate as shown in the AM335x datasheet.


WLAN/BT Module

There is a Wireless LAN and Bluetooth card connector on the GP EVM. This connector contains a card with a WL1271 WLAN/BT module and integrated antenna.


Pin Use Description

Functional Interface Mapping

Some signals of the AM335x are connected to a fixed device on the EVM where it cannot be changed. Some of the signals of the AM335x, however, are connected to devices on the EVM based on the profile setting.

Since AM335x processor has up to 8 different mux options for each signal, options have to exist on the EVM for allowing the supported subsets of these signals. The pinuse document shows only the signals which are used on the expansion daughterboard.

In the schematics, the AM335x pin names are used for the net names up to the specific mux that connects the signal to the particular function. This is to allow easy knowledge of a single pin's connection to multiple functions through the muxes without burdening the net name to tell all the various functions.

See the additional columns in the pinmux document as there are preset profiles which define what peripherals on the hardware boards are connected and able to be used at a given time.

Pin Use Assignment - Assignment list of pin functions


GPIO Definitions

See the updated pinmux documents which show use case columns for GPIO's. Developer can select and enable pins based on the selective peripheral pins as output or input. For the GP EVM, each single pin is muxed based on the CPLD profile number that is active. (The CPLD profile number is selected by a DIP switch.)


Board Connectors

Expansion Connectors

The expansion connector details are listed in the tables below.

Pin No Signal Description
1 V1_8D Power 1.8V supply
2 V5_0D Power 5.0V rail
3 GPMC_AD7 GPMC Address & Data
4 RMII1_RXD3 RMII Receive Data bit 3
5 GPMC_AD6 GPMC Address & Data
6 RMII1_TXCLK RMII Transmit Clock
7 GPMC_AD5 GPMC Address & Data
8 RMII1_RXCLK RMII Receive Clock
9 GPMC_AD4 GPMC Address & Data
10 RMII1_RXD2 RMII Receive Data bit 2
11 GPMC_AD3 GPMC Address & Data
12 RMII1_TXD2 RMII Transmit Data bit 2
13 GPMC_AD2 GPMC Address & Data
14 RMII1_RXDV RMII Receive Data Valid
15 GPMC_AD1 GPMC Address & Data
16 RMII1_TXD3 RMII Transmit Data bit 3
17 GPMC_AD0 GPMC Address & Data
18 RMII1_TXD1 RMII Transmit Data bit 1
19 GPMC_CS2n GPMC Chip Select
20 RMII1_TXD0 RMII Transmit Data bit 0
21 GPMC_CS1n GPMC Chip Select
22 RMII1_RXD1 RMII Receive Data bit 1
23 SPI0_D1 SPI Data
24 SPI0_CS0 SPI Chip Select
25 PMIC_PWR_EN
26 SYS_RESETn System reset
27 DGND Ground
28 DGND Ground


Table 21: AM335x EXP0 Connector



Pin No Signal Description
1 NOT USED
2 NOT USED
3 NOT USED
4 NOT USED
5 NOT USED
6 NOT USED
7 DGND Ground
8 DGND Ground
9 NOT USED
10 NOT USED
11 SYS_WARMRESETn System warm reset
12 EXP_PB_POWERON Power ON
13 NOT USED
14 NOT USED
15 NOT USED
16 NOT USED
17 NOT USED
18 NOT USED
19 GPMC_WAIT GPMC Wait
20 NOT USED
21 GPMC_WPn GPMC Write Protect
22 NOT USED
23 GPMC_CLK GPMC Clock
24 NOT USED
25 GPMC_CS0n GPMC Chip Select
26 GPMC_ADVn_ALE GPMC Address Valid / Address Latch Enable
27 NOT USED
28 GPMC_BE0n_CLE GPMC Byte Enable 0 / Command Latch Enable


Table 22: AM335x EXP1 Connector


Pin No Signal Description
1 DGND Ground
2 GPMC_BE1n GPMC Byte Enable 1
3 RMII1_REFCLK RMII Reference Clock
4 GPMC_CS3n GPMC Chip Select
5 RMII1_RXD0 RMII Receive Data bit 0
6 GPMC_OEn_REn GPMC Output / Read Enable
7 MDIO_DATA MDIO Data
8 GPMC_WEn GPMC Write Enable
9 MDIO_CLK MDIO Clk
10 DGND Ground
11 DGND Ground
12 MMC0_CLK MMC Clock
13 SPI0_CLK SPI Clock
14 MMC0_CMD MMC Command
15 SPI0_D0 SPI Data
16 MMC0_DAT0 MMC Data Bus
17 SPI0_CS1 SPI Chip Select
18 WAKEUP
19 ECAP0_IN_PWM0_OUT enhanced capture 0 input or Auxiliary PWM0 out
20 DGND Ground
21 UART0_CTSn UART Clear to Send
22 MMC0_DAT1 MMC Data Bus
23 UART0_RTSn UART Request to Send
24 MMC0_DAT2 MMC Data Bus
25 UART0_RXD UART Receive Data
26 MMC0_DAT3 MMC Data Bus
27 UART0_TXD UART Transmit Data
28 XDMA_EVENT_INTR0 External DMA Event or Interrupt 0
29 UART1_CTSn UART Clear to Send
30 DGND Ground
31 UART1_RTSn UART Request to Send
32 XDMA_EVENT_INTR1 External DMA Event or Interrupt 1
33 UART1_RXD UART Receive Data
34 RMII1_COL RMII Colision
35 UART1_TXD UART Transmit Data
36 RMII1_CRS RMII Carrier Sense
37 DGND Ground
38 RMII1_RXERR RMII Receive Data Error
39 V3_3D Power 3.3V supply
40 RMII1_TXEN RMII Transmit Enable


Table 23: AM335x EXP2 Connector


Pin No Signal Description
1 MCASP0_ACLKX McASP0 Transmit Bit Clock
2 GPMC_A0 GPMC Address
3 DGND Ground
4 GPMC_A1 GPMC Address
5 MCASP0_FSX McASP0 Transmit Frame Sync
6 GPMC_A2 GPMC Address
7 MCASP0_AXR0 McASP0 Serial Data (IN/OUT)
8 GPMC_A3 GPMC Address
9 EXP3_P9
10 GPMC_A4 GPMC Address
11 VDDSHV2 Power supply for SDMMC cards
12 GPMC_A5 GPMC Address
13 MCASP0_AHCLKR McASP0 Receive Master Clock
14 DGND Ground
15 V3_3D Power 3.3V supply
16 GPMC_A6 GPMC Address
17 MCASP0_ACLKR McASP0 Receive Bit Clock
18 GPMC_A7 GPMC Address
19 VEXPD VBAT spower
20 DGND Ground
21 MCASP0_FSR McASP0 Receive Frame Sync
22 GPMC_A8 GPMC Address
23 MCASP0_AXR1 McASP0 Serial Data (IN/OUT)
24 GPMC_A9 GPMC Address
25 DGND Ground
26 GPMC_A10 GPMC Address
27 MCASP0_AHCLKX McASP0 Transmit Master Clock
28 GPMC_A11 GPMC Address


Table 24: AM335x EXP3 Connector

LCD Connectors

     The connector details of LCD are described below.
Pin No Signal Description
1 V5_0D Power 5.0V rail
2 V5_0D Power 5.0V rail
3 LCD_DATA1 LCD data bus
4 LCD_DATA0 LCD data bus
5 LCD_DATA3 LCD data bus
6 LCD_DATA2 LCD data bus
7 LCD_DATA5 LCD data bus
8 LCD_DATA4 LCD data bus
9 LCD_DATA12 LCD data bus
10 LCD_DATA10 LCD data bus
11 LCD_DATA23 LCD data bus
12 LCD_DATA14 LCD data bus
13 LCD_DATA19 LCD data bus
14 LCD_DATA22 LCD data bus
15 I2C0_SDA I2C0 Data
16 LCD_DATA11 LCD data bus
17 LCD_VSYNC LCD Vertical Sync
18 DGND Ground
19 DGND Ground
20 DGND Ground


Table 25: AM335x LCD Connector 1



Pin No Signal Description
1 VEXPD Power variable supply
2 V1_8D Power 1.8V supply
3 LCD_DATA20 LCD data bus
4 LCD_DATA21 LCD data bus
5 LCD_DATA17 LCD data bus
6 LCD_DATA18 LCD data bus
7 LCD_DATA15 LCD data bus
8 LCD_DATA16 LCD data bus
9 LCD_DATA7 LCD data bus
10 LCD_DATA13 LCD data bus
11 LCD_DATA8 LCD data bus
12 V5_0D Power 5.0V rail
13 LCD_DATA9 LCD data bus
14 I2C0_SCL I2C0 Clock
15 LCD_DATA6 LCD data bus
16 LCD_PCLK LCD pixel clock
17 LCD_DEN
18 LCD_HSYNC LCD Horizontal Sync
19 DGND Ground
20 DGND Ground


Table 26: AM335x LCD Connector 2


     This is the touchscreen connector.
Pin No Signal Description
1 TSC_GIO0 GIO0
2 V3_3D Power 3.3V supply
3 TSC_GIO1 GIO1
4 TSC_I2CSCL I2C SCLK for touchscreen
5 TSC_CLK Source clock for touchscreen controller
6 TSC_I2CSDA I2C SDATA for touchscreen
7 TSC_RSV0 Reserved
8 TSC_GIO2 GIO2
9 TSC_RSV1_VREF Reserved power pin
10 DGND Ground
11 GNDA_TSC Analog ground
12 GNDA_TSC Analog ground
13 TSC_AIN4 ADC4 input
14 TSC_AIN0 ADC0 input
15 TSC_AIN5 ADC5 input
16 TSC_AIN1 ADC1 input
17 TSC_AIN6 ADC6 input
18 TSC_AIN2 ADC2 input
19 TSC_AIN7 ADC7 input
20 TSC_AIN3 ADC3 input


Table 27: AM335x Touchscreen Connector


JTAG Connector

TI 20 pin connector... other JTAG adaptors are available on TI e-store and can be purchased from here

EVM Important Notice

NoteNote: The Standard Terms And Conditions for TI Evaluation Modules can be downloaded from here:http://www.ti.com/lit/pdf/sszz027

ANNEX

This HUG is prepared by using the following documents as references.

  1. AM335x Sitara ARM Microprocessors TRM (SPRUH73)