AM335x Industrial Communication Engine EVM Rev2 1 HW User Guide

From Texas Instruments Wiki
Jump to: navigation, search
AM335x Industrial Communication Engine (ICE) EVM Rev. 2.1 Hardware User Guide


Introduction

This document provides the design information on the AM335x processor based ICE EVM (TMDSICE3359) to the users. ICE stands for Industrial Communications Engine. This EVM can be used to evaluate industrial communication protocols based on AM335x.

Description

The low-cost ICE EVM can be used for evaluation and development of industrial communication type applications. It has been equipped with a TI AM3359 processor and a defined set of features to allow the user to experience specifically industrial communication solutions using serial or Ethernet based interfaces. It is not intended as a generic development platform as some of the features and interfaces supplied by the AM335x are not accessible from the ICE board. Using standard interfaces, the ICE board may interface to other processors or systems and act as a communication gateway in this case. In addition it can directly operate as a standard remote I/O system or simple sensor connected to an industrial communication network. The embedded emulation logic allows emulation and debug using standard development tools such as TI’s Code Composer Studio by just using the supplied USB cable.

It is not intended for use in end products. All of the design information is freely available and can be used as the basis for the development of an AM335x based product.

EVM System View

The ICE EVM board has dimensions of 3.09” x 4.10 “". The Top Side and the Iso views of the AM335x ICE 2.0 EVM are shown in the pictures provided below.

Top view


ICE_Rev2_1production-0.jpg


Figure 1: AM3359 ICE 2.1 EVM Top view

Isometric view


ICE_Rev2_1production-1.jpg


Figure 2: AM3359 ICE 2.1 EVM Iso View


Component Positions


ICE_Rev2_1production-1.jpg


Figure 3: AM3359 ICE 2.1 EVM Connector and Jumper Loactions


Schematics/Design Files

Functional Block Diagram of AM335x ICE 2.0 EVM

AM335x ICE Rev. 2.1 EVM Functional Block Descriptions

This section describes about the major functional blocks of the AM335x ICE V2.0 EVM System. The Functional block diagram of the AM335x ICE 2.0 EVM is shown below.


ICE_V2_Block_Diagram1.JPG


Figure 4: AM335x ICE Rev. 2.1 EVM Block Diagram

Processor

The AM3359ZCZ processor is the central processor for this EVM. All the resources on the board surround the AM3359 processor to provide development capabilities for hardware and software. See the AM3359 datasheet and TRM for the details about the processor.

There are system configuration signals, SYSBOOT, that can be set on the EVM to define some startup parameters on the AM335x processor. See the Configuration/Setup section later for more details.

Clocks

The main clock for the processor is derived from a 24MHz crystal. An on-board oscillator in the AM3359 generates the base clock and subsequent module clocks as needed within the AM3359 processor. A 32kHz clock for the RTC section on the AM3359 processor is derived from a 32kHz crystal on board.

Reset Signals

SYS_RESETn is a signal running to several peripherals and AM335x which performs a reset on those peripherals. SYS_WARMRESETn is asserted by a pushbutton on the board and is used to force a reset of the AM3359. AM3359 can also pulldown on the RESET_INOUTn signal to cause the SYS_RESETn line to go active. The RTC_PORZ reset signal for the RTC section is derived using from an RC delay of the main power supply through VRTC power rail. An AND gate sharpens the edge to meet the AM3359 requirements.

Power

The DC power input to the board is from a 24V DC Power Supply. The 24V power input is converted into 5V to provide power input to the Power Manager TPS65910. The power requirements of the processor are taken care of by the Power Manager IC TPS65910A3. The Power ON LED "D16" is ON if the PMIC is active. The power on sequencing requirements of the AM3359 processor (see the AM3359 datasheet) are handled automatically by the TPS65910A3 PMIC.

Note: When powering the TMDSICE3359 EVM, always use the recommended power supply (CUI/V-Infinity Part Number EMSA240075) or equivalent model having output voltage of +24VDC and output current max 0.75 Amps and that complies with applicable regional safety standards such as (by example) UL, CSA, VDE, CCC, PSE, etc.. A power supply is not included with the kit.

Power Management IC

The AM3359 ICE Rev. 2.1 EVM uses the TPS65910A3 power management IC. The I2C0 on AM335x is used to control the TPS65910A3 PMIC. For AM335x, the following power supplies from the TPS65910A are used.


TPS65910A3 Power Supply AM335x Power Rail Voltage
VAUX2 VDDSHV1,3,5,6 3.3V (rails that are 3.3V)
VMMC VDDSHV4 & VDDSHV2 3.3V
VDD2 SMPS VDD_CORE 1.1V
VDD1 SMPS VDD_MPU 1.1V
No supply needed VDD_RTC 1.1V
VRTC VDDS_RTC 1.8V
VIO_SMPS VDDS_DDR 1.8V (or 1.5V for DDR3)
VIO_SMPS DDR_VREF 0.9V
VDAC VDDS 1.8V
VDIG2 VDDS_SRAM_CORE_BG 1.8V
VDIG2 VDDS_SRAM_MPU_BB 1.8V
VDIG2 VDDS_PLL_DDR 1.8V
VDIG2 VDDS_PLL_CORE_LCD 1.8V
VDIG2 VDDS_PLL_MPU 1.8V
VDIG2 VDDS_OSC 1.8V
VAUX1 VDDA1P8V_USB0/1 1.8V
VAUX33 VDDA3P3V_USB0/1 3.3V
VAUX33 USB_VBUS0/1 3.3V
VPLL VDDA_ADC 1.8V
VDD3 SMPS Not Used -
VIO_SMPS DDR3 SDRAM 1.8V

Table 1: AM3359 Power supplies from TPS65910A

Configuration/Setup

Boot Configuration

Various boot configurations can be set using the pull up / down resistor combinations provided on the SYS_BOOT pins (LCD_DATA[15..0]). Boot configuration pins are latched upon de-assertion of PORz pin.

The device supports SPI , MMC/SD and NOR boot mode through ARM ROM Bootloader. Boot mode selection is determined by the state of pins on J5.

NOR Boot
      Pin 1 & 2 shorted  on J5.  
      ROM Bootloader looks for a valid boot image in NOR sector 0 and if found, will execute it from there. If there is no valid image in NOR, SPI boot loader will be executed if present. If SPI bootloader is also not present, SD card  bootloader will be executed.
 

SPI Boot
      Pin 2 & 3 shorted  on J5.
      ROM Bootloader looks for a valid image in SPI flash and if found,loads it to IRAM and executes it. Otherwise, SD card bootloader will be executed if present.
 

MMC/SD Boot

     Pin 2 & 3 shorted  on J5. 
     ROM Bootloader looks for a file named 'MLO' in SD card and if found,loads it to IRAM and executes it. Please note that, SPI bootloader should NOT be present in SPI flash. (See AM335x ICEv2 flash erase )


SYSBOOT(4..0) AM3359 Boot Sequence
11010 XIP (MUX2), UART0, SPI0, MMC0
11000 SPI0, MMC0, USB0, UART0

I2C Port Address Assignments

Information on I2C address assignments are provided below.

AM335x ICE Rev. 2.1A EVM Function AM335x I2C Port Address
ID memory I2C0 0x50
AM65910A PMIC Control I2C0 0x2D
CDCE913 Clock Synthesizer I2C0 0x65
PCA9536DGKR – I2C to IO Expander for Rotary Switch I2C0 0x41
TPIC2810 I2C0 0x60
LCD Display I2C0 0x3C

Table 2:I2C Bus Addresses

ID Memory Contents

Information on the contents of the ID memory is explained below.

Name Size (Bytes) Contents
Header 4 MSB 0xEE3355AA LSB
Version 8 Name for board in ASCII “A335_ICE” = AM335x ICE Board
Version 4 Hardware version code for board in ASCII “2.1A” = rev. 02.1A
Serial Number 12 Serial number of the board. This is a 12 character string which is:

WWYY4P25nnnn where: WW = 2 digit week of the year of production YY = 2 digit year of production nnnn = incrementing board number

Configuration Option 32 Codes to show the configuration setup on this board.

Reserved

Reserved 6 reserved
Reserved 6 reserved
Available 32696 Available space for other non-volatile codes/data

Table 3:ID Memory Contents






JTAG

The ICE Rev. 2.1 EVM supports embedded XDS100V2 USB Emulation through the MicroUSB AB connector. It also has an optional 20 pin TI CJTAG connector to support the Emulation. This CJTAG connector is not installed by default.

Memories Supported

The ICE Rev. 2.1 EVM supports on-board memories like DDR3 SDRAM, SPI Flash, NOR Flash and Board ID EEPROM. It also supports an microSD card socket.

DDR3 SDRAM

The ICE design contains a 2Gbit (128M x16) of DDR3 SDRAM memory. The Part number for the DDR3 SDRAM memory used is MT41J128M16JT-125. The package used is an 84 ball FBGA package. See the AM335x TRM for memory locations for this memory.

SPI Flash

A 64Mbit, W25Q64 SPI Flash is used in this design. SPI Flash Boot is enabled through this Flash. This flash is connected to the SPI0 port of the processor.

NOR Flash

A 16Mbit, M29W160EB NOR Parallel Flash memory is used in this design. This NOR flash is connected to the GPMC interface of the processor and is connected as a halfword (16bit) data width only.

Board Identity Memory

The board contains a 256 Kb serial EEPROM that contains board specific data which allows the processor to automatically detect which board is connected and the version of that board. Other hardware specific data can be stored on this memory device as well. The part number of the memory device is CAT24C256WI-GT3. See the Configuration/Setup section for details on the data in this memory.

SDMMC0

The SDMMC0 connector is a card socket SCHA5B0200 (J16). This is a standard SD/MMC Card type of connector. It is connected to the MMC0 port of the AM335x processor. Check the AM335x data sheet and TRM for supported card types/densities. The Pin assignment is as given below.

Pin No Memory Card PIN No.
uSD#1 DAT2
uSD#2 CD/DAT3
uSD #3 CMD
uSD #4 VCC
uSD #5 CLK
uSD #6 GND
uSD #7 DAT0
uSD #8 DAT1
uSD #9 GND
uSD #10 CD
uSD #11 GND_SD
uSD #12 GND_SD
uSD #13 GND_SD
uSD #14 GND_SD
uSD #15 GND_SD
uSD #16 GND_SD

Table 3: SDMMC0 Connector Pin Details

Ethernet

The ICE Rev. 2.1 EVM has two 10/100 Ethernet transceivers (TLK110) interfaced to connectors J1 & J2 . These Ethernet ports are connected from the Gig Switch and the PRU-ICSS units of the AM335x to the transceivers through a muxing /ORing logic. The reset for the transceivers are driven by the board system reset SYS_RESETn and a GPIO control.The various protocols supported in the design are SERCOS III,SERCOS III S, ETHERNET / IP, POWERLINK, ETHERCAT and PROFINET. The signal MUX_MII_CTL1 is used to switch the muxing logic between the Gb Switch and the PRUSS unit control of the Ethernet PHY's.

The XI clock input pins of both the PHYs are driven from the clock synthesizer CDCE913, (Synthesizer inputs connected to a 25Mhz crystal). The PHYAD pins are left unconnected for setting the PHY's address on the PRU1_MII0 Ethernet so it is by default 0x01. The PHYAD pins on the PRU1_MII1 Ethernet are set to 0x03 using a pull up resistor on the PHYAD1 pin.

Jumpers J18 and J19 need to be set to control the Ethernet ports using CPSW (Gig Switch) or PRU-ICSS mode. For PRU-ICSS mode, connect Pin2 and Pin3. For CPSW mode, connect Pin1 and Pin2. These jumper settings apply in both RTOS and Linux.

Pin No Signal Name Description
1 ETHER0_RDP Ethernet Data Rx Positive
2 ETHER0_RDN Ethernet Data Rx Negative
3 V3_3D_PRUETH0JCK Power
4 V3_3D_PRUETH0JCK Power
5 ETHER0_TDP Ethernet Data Tx Positive
6 ETHER0_TDN Ethernet Data Tx Negative
7 NC No Connect
8 GND Ground
D1 LINK LED Power Power
D2 LINKLED Link LED Signal
D3 Active LED Power Power
D4 ACTLED Active LED Signal

Table 4: Ethernet Jack Pinout

USB

Micro USB-AB connector (J13) is connected to the upstream port of the USB to UART converter IC (FT2232L ) . This is used for USB to JTAG and USB to UART conversion applications. This USB port can also be used for XDS100V2 JTAG emulation .

Pin No Signal Name Description
1 USB_DC USB BUS VOLTAGE
2 USB_DM USB DATA MINUS
3 USB_DP USB DATA PLUS
4 USB_ID USB IDENTIFICATION (NC)
5 DGND Ground

Table 5: USB

CAN/PROFIBUS

The ICE Rev. 2.1 EVM has a DB9 female connector J9 for the PROFI/CAN Bus Interfaces . PR1_UART0 port of AM335x is used for interfacing with the PROFIBUS transceiver ISO1176T & DCAN0 port of the AM335x is used for interfacing with the CAN bus transceiver ISO1050. The Profi signals and CAN signals are on different pins of the connector.

Pin No Signal Name Description
1 Reserved Upgrade Path
2 CAN_L Dominant Low
3 CAN_GND Ground
4 Reserved Upgrade Path
5 PROFI_GND PROFIBUS Ground
6 VPROFI_DB PROFIBUS voltage
7 CAN_H Dominant High
8 Profi BusB PROFIBUS B
9 CAN_V+ Power, Optional

Table 6: CAN/PROFIBUS Connector Pin Details

CAN /PROFIBUS Selection Jumpers

The Jumpers J6,J7,J8 and J10 are used to select between the CAN / PROFI bus. Description of the selection is provided below.

Jumper Selection
J6 Pins 1 & 2 Short for CAN bus Voltage select
J10 Pins 1 & 2 Short for PROFIBUS Voltage select
J8 Pins 1 & 2 Short for PROFIBUSA select,Pins 2 & 3 Short for CAN Ground select
J7 Pins 1 & 2 Short for PROFIBUS Ground select

Industrial Inputs

For industrial 24v digital inputs, a SN65HVS882 serializer is used to accept standard signals in and allow the AM335x to read them. The Serialized output from the serializer is fed to the SPI0 port of the processor.

Ethernet LEDs

The Ethernet Protocol LEDs are used to indicate the status of the various protocols supported in the design like SERCOS III,SERCOS III S, ETHERNET / IP, POWERLINK, ETHERCAT, PROFINET.

Protocol Status Colour of LED
'SERCOS-III S RED, GREEN, YELLOW
'ETHERNET/IP MODULE STATE RED, GREEN
'POWERLINK S/E RED, GREEN
'ETHERCAT ERROR RED
'PROFINET BF RED

Table 7: Tri-Color LED D1 Mapping

Protocol Status Colour of LED
'SERCOS-III SD1 RED, GREEN, YELLOW
'ETHERNET/IP NETWORK RED, GREEN
'ETHERCAT RUN GREEN
'PROFINET SF RED

Table 8: Tri-Color LED D2 Mapping

Industrial Output LEDs

I2C to 8 bit LED driver TPIC2810 is used to drive the eight Industrial output LEDs D6 to D10 AND D12 , D14 and D15. The I2C interface is connected to the I2C0 port of the AM335x processor. By communicating over the I2C bus, these outputs can be set to arbitrary values. The 8 LED driver outputs are also driven to the IO Expansion header. All the LEDs are green in color.

Temperature Sensor

The ICE design has a temperature sensor LM94022 on board which outputs analog ambient temperature data. The output data from the temperature sensor is fed to the Analog input pin AIN0 of the processor.

Rotary Encoded Switch

The EVM has a rotary switch that allows a slave address to be selected. This switch selects a 4bit (hex) value and a I2C converter allows this encoded value to be read by the AM335x through the I2C0 port.


Pin Use Description

GPIO Definitions

See the updated pinmux document TMDX3359_3H0013_Rev2_1A_GPIO_Assignments which shows the use case columns for GPIOs.




Board Expansion Connectors

There are two expansion connectors provided in the ICE board. They are used for HOST and I/O signals Expansion. The J4 ( 15 x2 , Female) and J3 ( 9x2, Female ) connectors are used for HOST expansion is a 25x2 header. The Description of the signals are provided below.

Pin No Signal Description
1 GPMC_A0 Address 0
1 GPMC_AD0 Data 0
3 GPMC_A1 Address 1
4 GPMC_AD1 Data 1
5 GPMC_A2 Address 2
6 GPMC_AD2 Data 2
7 GPMC_A3 Address 3
8 GPMC_AD3 Data 3
9 GPMC_A4 Address 4
10 GPMC_AD4 Data 4
11 GPMC_A5 Address 5
12 GPMC_AD5 Data 5
13 GPMC_A6 Address 6
14 GPMC_AD6 Data 6
15 GPMC_A6 Address 6
16 GPMC_AD7 Data 7
17 GPMC_A8 Address 8
18 GPMC_AD8 Data 8
19 GPMC_A9 Address 9
20 GPMC_AD9 Data 9
21 GPMC_CSn2 Chip Select 2
22 GPMC_AD10 Data 10
23 GPMC_WEn Write Enable
24 GPMC_AD11 Data 11
25 GPMC_OEn_REn Output Enable/ Read Enable
26 GPMC_AD12 Data 12
27 GPMC_ADVn_ALE Address Latch Enable
28 GPMC_AD13 Data 13
29 GPMC_AD15 Data 15
30 GPMC_AD14 Data 14


Table 9: AM335x Host Expansion Connector 1- J4

Pin No Signal Description
1 V3_3D 3.3V Power
2 DGND Ground
3 LATCH0_IN Latch 0 Input
4 I2C0_SDA I2C0 Data
5 LATCH1_IN Latch 1 Input
6 I2C0_SCL I2C0 Clock
7 UART4_RXD_SYNC0_OUT Uart 4 Receive / Sync0 Output
8 UART4_TXD_SYNC1_OUT Uart 4 Transmit / Sync1 Output
9 GPIO3_18 General Purpose IO
10 EMU4 JTAG EMU4
11 GPIO3_19 General Purpose IO
12 SPI1_SCLK SPI1 Port Clock
13 GPIO3_20 General Purpose IO
14 SPI1_D0 SPI1 Data0
15 DGND Ground
16 SPI1_D1 SPI1 Data1
17 V24_IN 24V Power
18 SPI1_CS0 SPI1 Chip Select 0


Table 10: AM335x Host Expansion Connector 2- J3


Pin No Signal Description
1 INDUS INPUT0 Digital Input 0
2 V24_0HVS 24V Power
3 INDUS INPUT1 Digital Input 1
4 V24_0HVS 24V Power
5 INDUS INPUT2 Digital Input 2
6 V24_0HVS 24V Power
7 INDUS INPUT3 Digital Input 3
8 V24_0HVS 24V Power
9 INDUS INPUT4 Digital Input 4
10 V24_0HVS 24V Power
11 INDUS INPUT5 Digital Input 5
12 V24_0HVS 24V Power
13 INDUS INPUT6 Digital Input 6
14 V24_0HVS 24V Power
15 INDUS INPUT7 Digital Input 7
16 V24_0HVS 24V Power
17 DGND Ground
18 DGND Ground
19 DRAIN0 Digital Output 0
20 DRAIN1 Digital Output 1
21 DRAIN2 Digital Output 2
22 DRAIN3 Digital Output 3
23 DRAIN4 Digital Output 4
24 DRAIN5 Digital Output 5
25 DRAIN6 Digital Output 6
26 DRAIN7 Digital Output 7
27 V5_0D 5V Power
28 V5_0D 5V Power
29 DGND Ground
30 DGND Ground
31 AIN1 Analog Input 1
32 AIN5 Analog Input 1
33 AIN2 Analog Input 2
34 AIN6 Analog Input 6
35 AIN3 Analog Input 3
36 AIN7 Analog Input7
37 AIN4 Analog Input 4
38 GNDA_ADC Analog Ground
39 GNDA_ADC Analog Ground
40 GNDA_ADC Analog Ground


Table 11: AM335x I/O Expansion Connector – J14

LCD

The LCD used in this design is a Passive Matrix , Monochrome (light blue) display with 96 × 16 pixels and has a panel size of 29.10 × 9.20 × 1.60 mm. The J17 connector is provided on board to connect with the LCD assembly. The 13V required for the LCD is generated on board using the TPS61041 Boost converter with power input from the 5V power available in the board.

Pin No Signal Description
1 V13 Power 13.0V rail
2 VCOMH Voltage output High
3 IRREF Current Reference
4 I2C0_SDA I2C0 Data
5 I2C0_SCL I2C0 Clock
6 RESn Power Reset
7 VDD_3V3 Power Supply 3.3V
8 DGND Ground
9 VBREF Voltage Reference
10 VBAT_LCD Power Supply for DC-DC converter
11 C1N Charge Pump Capacitor1 negative
12 C1P Charge Pump Capacitor1 positive
13 C2N Charge Pump Capacitor2 negative
14 C2P Charge Pump Capacitor2 positive


Table 12:LCD Connector

EVM Important Notices

NoteNote: The Standard Terms And Conditions for TI Evaluation Modules can be downloaded from here:http://www.ti.com/lit/pdf/sszz027

ANNEX

This Hardware User's Guide is prepared by using the following documents as references.

  1. AM335x Sitara ARM Microprocessors TRM (SPRUH73)