Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

AM335x Linux Power Management User Guide

From Texas Instruments Wiki
Jump to: navigation, search


TIBanner.png
AM335x Power Management User's Guide
Linux PSP

Introduction

AM335x processors support a rich set of power management techniques

  1. Clock gating
  2. Clock domain transitions
  3. Power domain transitions
  4. Dynamic Voltage and Frequency scaling
  5. DeepSleep modes

These techniques are leveraged in the different power management frameworks within the Linux kernel.

PM features in the kernel

PM features in Linux kernel relevant to AM335x are

  1. CPU Freq is available in kernel since release 04.06.00.04 onward.
  2. CPU Idle is available in kernel since release 04.06.00.03 onward.
  3. Suspend-to-RAM is available in kernel since release 04.06.00.07 onward.
  4. Runtime PM is supported in most of the drivers. The usage will be made more aggressive in the upcoming releases.

cpufreq

Cpufreq framework provides support to change frequency of processor on the run. This helps to save processor power, when the load is less (processor power is proportional to frequency and square of the voltage). cpufreq framework works in conjunction with driver & governor.

  • cpufreq driver provides link for framework to achieve frequency change at the hardware level.
  • cpufreq governor decides frequency at which processor should run. Various governors like ondemand, userspace, performance (self descriptive names) exist in Linux Kernel.

Changing voltage is also achieved in cpufreq driver by dealing with voltage regulator. Linux OPP infrastructure is made use to achieve it.

Supported OPPs

OPP (Operating Performance Points) - voltage frequency pair that defines a specific power state that the SoC supports running at. Refer SoC Technical Reference Manual for more details. cpufreq implementation controls OPP only with respect to the processor, i.e VDD_MPU (voltage fed to ARM Cortex-A8) and ARM Cortex-A8 frequency.

Usage

ondemand and userspace governors are enabled in Kernel, default governor is userspace.

To view available governers,

target# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_governors
ondemand userspace
target#

To view current governer,

target# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
userspace
target#

To set a governer,

target# echo ondemand > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
target#

To view current OPP (frequency in KHz)

target# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_cur_freq
720000
target#

To view supported OPP's (frequency in KHz),

target# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_frequencies
275000 500000 600000 720000
target#

To change OPP (can be done only for userspace governor. If governors like ondemand is used, OPP change happens automatically based on the system load)

target# echo 275000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed
target#

To view current processor voltage on AM335X EVM,

target# cat /sys/class/regulator/regulator.3/microvolts
1262500
target#

Kernel configuration

Start the Linux Kernel Configuration tool.

$ make menuconfig 

Select CPU Power Management from the main menu.

    ...
    ...
    Boot options --->
    CPU Power Management --->
    Floating point emulation --->
    ...

Select CPU Frequency Scaling as shown here:

    ...
    ...
        CPU Frequency Scaling --->
    [*] CPU idle PM support
    ...

Select CPU Frequency scaling and required governers as shown here:


    [*] CPU Frequency scaling
    <*> CPU frequency translation statistics
    [ ] CPU frequency translation statistics details
        Default CPUFreq governor (userspace)  --->
    < >   'performance' governor
    < >   'powersave' governor
    -*-   'userspace' governor for userspace frequency scaling
    <*>   'ondemand' cpufreq policy governor
    < >   'conservative' cpufreq governor
    ...
NOTE

CPUFreq is enabled by default in the am335x_evm_defconfig.


cpuidle

The cpuidle framework consists of two key components:

  • A governor that decides the target C-state of the system.
  • A driver that implements the functions to transition to target C-state.

The idle loop is executed when the Linux scheduler has no thread to run. When the idle loop is executed, current 'governor' is called to decide the target C-state. Governor decides whether to continue in current state/ transition to a different state. Current 'driver' is called to transition to the selected state.

C-states

A C-state is used to identify the power state supported through the cpu idle loop. Each C-state is characterized by its:

  • Power consumption
  • Wakeup latency
  • Preservation of processor state while in 'the' state.

Currently these C-states have been defined:

C-states in AM335x
State Description
C1 MPU WFI
C2 MPU Clock Off


CPU Idle Governor

The current implementation supports 'menu' and 'ladder' governors to decide the target C-state of the system.

CPU Idle Driver

The cpuidle driver registers itself with the framework during boot-up and populates the C-sates with exit latency, target residency (minimum period for which the state should be maintained for it to be useful).

Once the governor has decided the target C-state, the control reaches the function am33xx_enter_idle(). Here, the C-state is adjusted based on the value of valid flag corresponding to the chosen state.

Supported C-states

[root@arago /]# ls -l /sys/devices/system/cpu/cpu0/cpuidle/state0/						
-r--r--r--    1 root     root         4096 Jan  1 00:02 desc						
-r--r--r--    1 root     root         4096 Jan  1 00:02 latency						
-r--r--r--    1 root     root         4096 Jan  1 00:02 name						
-r--r--r--    1 root     root         4096 Jan  1 00:02 power						
-r--r--r--    1 root     root         4096 Jan  1 00:02 time						
-r--r--r--    1 root     root         4096 Jan  1 00:02 usage						
[root@arago /]# ls -l /sys/devices/system/cpu/cpu0/cpuidle/state1/						
-r--r--r--    1 root     root         4096 Jan  1 00:05 desc						
-r--r--r--    1 root     root         4096 Jan  1 00:05 latency						
-r--r--r--    1 root     root         4096 Jan  1 00:03 name						
-r--r--r--    1 root     root         4096 Jan  1 00:05 power						
-r--r--r--    1 root     root         4096 Jan  1 00:05 time						
-r--r--r--    1 root     root         4096 Jan  1 00:02 usage

Kernel configuration

Start the Linux Kernel Configuration tool.

$ make menuconfig 

Select CPU Power Management from the main menu.

    ...
    ...
    Boot options --->
    CPU Power Management --->
    Floating point emulation --->
    ...

Select CPU idle PM support to enable the cpuidle driver.

    ...
    ...
        CPU Frequency Scaling --->
    [*] CPU idle PM support
    ...
NOTE

cpuidle is enabled by default in the am335x_evm_defconfig.

Suspend & Resume

The suspend operation results in the system transitioning to the lowest power state being supported. On AM335x, this maps to DeepSleep0 state. For more info on this refer to the AM335x TRM available @ www.ti.com/am335x

The drivers implement the suspend() function defined in the LDM. When the suspend for the system is asserted, the suspend() function is called for all drivers. The drivers quiesce the peripherals and release the clocks to reach the desired low power state. The actual transition to suspend is implemented in the function am33xx_pm_suspend().

Usage

Once a kernel image with the PM firmware has been compiled and booted up, the following messages are displayed during the bootup

Uncompressing Linux... done, booting the kernel.
[    0.000000] Linux version 3.2.0-...
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
...
...
[    2.118896] Power Management for AM33XX family
[    2.127075] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[    2.137084] Copied the M3 firmware to UMEM
...
...

The suspend for device can now be asserted as follows:

$ echo mem > /sys/power/state

Successful suspend-resume cycle

[root@arago /]# echo mem > /sys/power/state
[    8.774536] PM: Syncing filesystems ... done.
[    8.804199] Freezing user space processes ... (elapsed 0.01 seconds) done.
[    8.827575] Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.
[    8.847717] Suspending console(s) (use no_console_suspend to debug)
[    8.868530] PM: suspend of devices complete after 12.542 msecs <-- Wake event using console (UART0)
[    8.870147] PM: late suspend of devices complete after 1.556 msecs
[   10.840209] GFX domain entered low power state
[   11.044891] PM: early resume of devices complete after 204.184 msecs
[   11.284027] PM: resume of devices complete after 238.709 msecs
[   11.317382] Successfully transitioned all domains to low power state
[   11.325012] Restarting tasks ... done
[root@arago /]#
NOTE

In order to avoid data loss, it is recommended that the users issue a "sync" command before suspending the system
[root@arago /]# sync; echo mem > /sys/power/state

Lower standby power via optimum pad configuration during suspend-resume

Under Construction

WORK IN PROGRESS

This article is work-in-progress. Until completed, the contents are expected to change quite frequently. Quality and accuracy is not guaranteed until this message has been removed. Please bookmark the page and visit soon...

Latest PSP release (Version : TBD) supports configuring IO pad during Suspend for Optimum Power Saving. The feature is available through debugfs entries.

A new debugfs directory are available for utilizing these features

<debugfs-mount-dir>/omap_mux/suspend_io_pad_conf

<debugfs-mount-dir> --> Directory where "debugfs" file system is mounted

enable_suspend_io_pad_conf - enable io pad configuration during suspend.

suspend_pad_conf - takes the name of pin-mux that is to be setup during suspend with value. Pin-mux name should be in "mode0_name.function_name" format. Internally the pin-mux offset is calculated from the pin-mux name.

If "enable_suspend_io_pad_conf" is set, then the entire pin-mux is saved. The user setup pin-mux registers are setup with the value provided by the user. During resume, the original values saved are restored back.

Usage

  • Create Mount point for debugfs
mkdir -p /debugfs
  • Mount "debugfs"
mount -t debugfs debugfs /debugfs
  • Go to directory
cd /debugfs/omap_mux/board/suspend_io_pad_conf/
  • Enable io pad configuration during suspend.
echo 1 > enable_suspend_io_pad_conf
  • Specify the Pin-mux name & the value to set for the pin during suspend.
echo mcasp0_aclkx.gpio3_14=0x27 > suspend_pad_conf

Note

NOTE

* Any number of the Pin-Mux can be configured using above steps. Repeat step 5 with different pin-mux names and value
  • Pin-mux name passed to "suspend_pad_conf" should be in "mode0_name.function_name" format.
  • NO spaces anywhere in the input to the "suspend_pad_conf" or it will be ignored.
  • To view the current io pad configuration, read the "suspend_pad_conf" entry.
cat suspend_pad_conf
  • To Disable io pad configuration reset to 0.
echo 0 > enable_suspend_io_pad_conf
  • The value that the user sets are only copied to physical registers during suspend if and only if "enable_suspend_io_pad_conf" is set.

Caution

CAUTION * User should make sure that the mux mode being setup exists for the selected pin-mux.

  • User should make sure that the Read-Only pin-muxs (like DDR, Analog-input pins) are not configured.
  • When the Features is disabled and enabled again using "echo 0/1 > enable_suspend_io_pad_conf", previously set io-pad configuration is retained. Therefore user needs to setup the appropriate pin-mux across disable/enable.

Example

 root@arago-armv7:~# mkdir -p /debugfs
 root@arago-armv7:~# mount -t debugfs debugfs /debugfs
 root@arago-armv7:~# cd /debugfs/omap_mux/board/suspend_io_pad_conf/
 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# cat enable_suspend_io_pad_conf
 0

 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# cat suspend_pad_conf
 [  102.750732] susp_io_pad_status_show: IO PAD Configuration is not enabled

 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# echo 1 > enable_suspend_io_pad_conf
 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# cat enable_suspend_io_pad_conf
 1

 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# cat suspend_pad_conf

 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# echo gpmc_ad0.gpio1_0=0x27 > suspend_pad_conf

 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# cat suspend_pad_conf
 gpmc_ad0.gpio1_0 (0x44e10800 = 0x27)

 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# echo gpmc_ad1.gpio1_1=0x27 > suspend_pad_conf
 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# echo gpmc_ad2.gpio1_2=0x27 > suspend_pad_conf
 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# echo gpmc_ad3.gpio1_3=0x27 > suspend_pad_conf

 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# cat suspend_pad_conf
 gpmc_ad0.gpio1_0 (0x44e10800 = 0x27)
 gpmc_ad1.gpio1_1 (0x44e10804 = 0x27)
 gpmc_ad2.gpio1_2 (0x44e10808 = 0x27)
 gpmc_ad3.gpio1_3 (0x44e1080c = 0x27)

 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# echo 0 > enable_suspend_io_pad_conf

 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# cat suspend_pad_conf
 [  427.960754] susp_io_pad_status_show: IO PAD Configuration is not enabled


 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# echo 1 > enable_suspend_io_pad_conf
 root@arago-armv7:/debugfs/omap_mux/board/suspend_io_pad_conf# cat suspend_pad_conf
 gpmc_ad0.gpio1_0 (0x44e10800 = 0x27)
 gpmc_ad1.gpio1_1 (0x44e10804 = 0x27)
 gpmc_ad2.gpio1_2 (0x44e10808 = 0x27)
 gpmc_ad3.gpio1_3 (0x44e1080c = 0x27)

Wakeup sources

In the default configuration wakeup from suspend using the following interfaces are supported:

  • UART0 (console)
  • GPIO0
  • Touchscreen:

To disable wakeup from touchscreen interface the following command can be used:

[root@arago /]# echo disabled > /sys/devices/platform/omap/ti_tscadc/power/wakeup

To re-enable wake from touchscreen, use:

[root@arago /]# echo enabled > /sys/devices/platform/omap/ti_tscadc/power/wakeup
NOTE

By using this wake disable feature, ADC used for touchscreen is stopped, hence the power consumption is further reduced. This feature is available from PSP release 04.06.00.07 onwards


Configuration

Enable/Disable suspend-resume support

To enable/ disable suspend-resume support start the Linux Kernel Configuration tool.

$ make menuconfig

Select Power management options from the main menu.

...
...
Kernel Features  --->
Boot options  --->
CPU Power Management  --->
Floating point emulation  --->
Userspace binary formats  --->
Power management options  --->
[*] Networking support  --->
Device Drivers  --->
...
...

Select Suspend to RAM and standby to toggle the power management support.

[*] Suspend to RAM and standby
-*- Run-time PM core functionality
... 
< > Advanced Power Management Emulation

Cortex-M3 binary blob for suspend-resume

On AM335x, suspend-resume involves loading a binary to the Cortex-M3 core during the boot process. For this the binary named am335x-pm-firmware.bin needs to be kept in the firmware/ folder on the kernel sources before the build process is started.

For more information on how to obtain the above mentioned binary, refer to the accompanying Release Notes for the PSP package.

The pre-built kernel image in the PSP package has the binary blob compiled into the kernel image.

To manually compile a kernel image with the PM firmware start the Linux Kernel Configuration tool.

$ make menuconfig

Select Device Drivers from the main menu.

...
...
Kernel Features  --->
Boot options  --->
CPU Power Management  --->
Floating point emulation  --->
Userspace binary formats  --->
Power management options  --->
[*] Networking support  --->
Device Drivers  --->
...
...

Select Generic Driver Options

Generic Driver Options
CBUS support
...
...

Configure the name of the PM firmware and the location as shown below

...
-*- Userspace firmware loading support
[*] Include in-kernel firmware blobs in the kernel binary
(am335x-pm-firmware.bin) External firmware blobs to build into the kernel binary
(firmware) Firmware blobs root directory
NOTE

  • The above changes are enabled by default in the am335x_evm_defconfig.
  • The above configuration assumes that the PM firmware named am335x-pm-firmware.bin has been placed under firmware folder of the kernel sources.

Standby Mode

For details about AM335x Power Management Standby low power mode support please refer to AM335x Power Management Standby User's Guide.