Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

AM335x NAND Driver's Guide

From Texas Instruments Wiki
Jump to: navigation, search
TIBanner.png
AM335x NAND Driver's Guide
Linux PSP

Introduction

The general-purpose memory controller (GPMC) is an unified memory controller dedicated to interfacing external memory devices:

  • Asynchronous SRAM-like memories and application-specific integrated circuit (ASIC) devices
  • Asynchronous, synchronous, and page mode (only available in non-multiplexed mode) burst NOR flash devices
  • NAND Flash
  • Pseudo-SRAM devices


Features

Hardware Features

The GPMC can access various external devices through the L3 Slow Interconnect. The flexible programming model allows a wide range of attached device types and access schemes.

The GPMC consists of six blocks:

  • Interconnect port interface
  • Address decoder, GPMC configuration, and chip-select configuration register file
  • Access engine
  • Prefetch and write-posting engine
  • Error correction code engine (ECC)
  • External device/memory port interface

AM335x Memory subsystem.jpg


Software Features

  • Access 8-bit NAND
  • BCH8 ECC scheme with 8-bit error correction. BCH8 ECC Scheme used to make compatible with all other components (RBL, U-Boot..)
  • Polled Prefetch Mode


AM335x NAND Device Layout

Layout for NAND flash device is described here.


ECC schemes usage table

ECC scheme used by different components is described in the table


Driver Configuration

To enable/disable NAND support, start the Linux Kernel Configuration tool:


host$ make menuconfig 


Select Device Drivers from the main menu.

    ...
    ...
    [ ] Networking support --->
    Device Drivers --->
    File systems --->
    ...
    ...
  • Enable below Configs to enable MTD Support along with MTD nand driver support
Device Drivers  ---> 
  <*> Memory Technology Device (MTD) support  --->
            [*]   Command line partition table parsing
            <*>   Direct char device access to MTD devices
            <*>   Caching block device access to MTD devices
            <*>   NAND Device Support  --->
                        <*>    NAND Flash device on OMAP2 and OMAP3
            <*>   Enable UBI - Unsorted block images  --->

Module Build

Module build for the NAND driver is supported. To do this, make the changes as below

Device Drivers  ---> 
  <*> Memory Technology Device (MTD) support  --->
            [*]   Command line partition table parsing
            <*>   Direct char device access to MTD devices
            <*>   Caching block device access to MTD devices
            <M>   NAND Device Support  --->
                        <M>    NAND Flash device on OMAP2 and OMAP3
            <*>   Enable UBI - Unsorted block images  --->

For loading modules follow the steps below

      target$ insmod drivers/mtd/nand/nand_ecc.ko 
      target$ insmod drivers/mtd/nand/nand_ids.ko
      target$ insmod drivers/mtd/nand/nand.ko
      target$ insmod drivers/mtd/devices/omap2_elm.ko
      target$ insmod drivers/mtd/nand/omap2.ko

Device Interface

You always need a pair mtdx/mtdblockx of device nodes to access your flash file system. The mtdx is used to access the raw flash device, the mtdblockx is used to access the disk/block established in the raw flash.

Use MTD-Utils user space tools to access NAND partition from Linux console

Below are some of the examples for accessing NAND partitions

  • Erase the nand partition (assume partition 3)
    target$ flash_eraseall /dev/mtd3
  • write a file to nand partition (assume partition 4)
    target$ nandwrite -p /dev/mtd4 u-boot.img
  • Mount nand partition from U-Boot as Root file system partition for Linux
    u-boot> setenv bootargs 'console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=<partion_id>,2048 noinitrd rootfstype=ubifs mem=256M rootwait=1'


The value of PARTITION_ID depends on MTD device which holds the root filesystem. The below example assumes UBIFS file system is flashed on MTD partition 7 and respective device is enabled on the board.

    u-boot> setenv bootargs 'console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=7,2048 noinitrd rootfstype=ubifs mem=256M rootwait=1'



Proc Interface

The /proc/mtd kernel interface is a status interface. A lot of useful information about the nand system can be found in the /proc/mtd file.

  • Use /proc/mtd to get information on how many partitions are currently configured by the kernels flash driver.
    target$ cat /proc/mtd

You should see output similar to:

    target$ cat /proc/mtd
   dev:    size   erasesize  name
   mtd0: 00020000 00020000 "SPL"
   mtd1: 00020000 00020000 "SPL.backup1"
   mtd2: 00020000 00020000 "SPL.backup2"
   mtd3: 00020000 00020000 "SPL.backup3"
   mtd4: 001e0000 00020000 "U-Boot"
   mtd5: 00020000 00020000 "U-Boot Env"
   mtd6: 00500000 00020000 "Kernel"
   mtd7: 0f880000 00020000 "File System"


AM335x NAND File system support

On AM335x, JFFS2 support has been super-seeded by UBIFS. JFFS2 support is disabled in default config.

For more information of UBIFS refer UBIFS Support Guide

To enable JFFS2, Refer AM335x JFFS2 Support Guide