AM335x PRU Read Latencies

From Texas Instruments Wiki
Jump to: navigation, search

Introduction

The AM335x PRU-ICSS is a master initiator with access to all SoC resources, in addition to the local subsystem resources. This wiki article documents best-case access latencies for the AM335x PRU reading various SoC resources.

The PRU write instruction is a fire-and-forget command that executes in ~1 cycle. The PRU read instruction executes in ~2 cycles, plus additional latencies due to traversing through interconnect layers and variable processing loads. In general, MMRs that are "closer" to the PRU (i.e. within the PRU subsystem) will have lower access latencies.

The read latency values provided in this article are considered "best-case," accounting for the 2 cycle instruction and interconnect introduced latency. Note memory accesses outside of the PRU subsystem are not deterministic.

PRU Read Latencies

The following are considered "best-case" read latency values for the PRU on AM335x.

Table 1. AM335x PRU Read Latencies - Local PRU Subsystem Resources
MMRs Read Latency (PRU cycles @ 200MHz)
PRU CTRL 4
PRU CFG 3
PRU INTC 3
PRU DRAM 3
PRU Shared DRAM 3
PRU ECAP 4
PRU UART 14
PRU IEP 12
PRU R31 (GPI) 1


Table 2. AM335x PRU Read Latencies - Global SoC Resources
MMRs Read Latency (PRU cycles @ 200MHz)
L3F Interconnect
EMIF 36
TPTC0-2 (EDMA3TC0-2) 34
TPCC (EDMA3CC) 41
OCMC RAM 27
L3S Interconnect
GPMC 38
McASP0-1 38
ADC/TSC 42
L4_PER Interconnect
DCAN0-1 40
DMTIMER2-7 38
PWMSS 38
ELM 34
GPIO1-3 34
I2C1-2 34
LCDC 38
Mailbox 38
MMCSD0-1 34
McSPI0-1 34
Spinlock 38
UART1-5 34
L4_FAST Interconnect
CPSW/GEMAC 41
L4_WKUP Interconnect
ADC/TSC 41
Control Module 41
DMTIMER0 38
DMTIMER1_1MS 38
GPIO0 38
I2C0 38
UART0 38
WDT1 38
PRCM 88
RTC 62


PRU Data Transfer Latencies

The following are considered "best-case" data transfer latencies for the AM335x PRU.

Table 3. PRU Data Transfer Latencies
Source Destination Size (bytes) Latency (PRU cycles @ 200MHz)
PRU Shared RAM DDR 4 5
32 19
128 65
DDR PRU Shared RAM 4 47
32 62
128 107