Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

AM335x PWM Driver's Guide

From Texas Instruments Wiki
Jump to: navigation, search
TIBanner.png
AM335X PWMSS Driver's Guide
Linux PSP

Introduction

The Pulse-Width Modulation Subsystem (PWMSS) consists of an instance of Enhanced High Resolution Pulse Width Modulator (eHRPWM), Enhanced Capture (eCAP), and Enhanced Quadrature Encoded Pulse (eQEP) modules. AM335x has 3-instances of PWMSS.

eHRPWM

The eHRPWM is an effective PWM peripheral, able to generate complex pulse width waveforms with minimal CPU overhead or intervention. The ePWM module represents one complete PWM channel composed of two PWM outputs: EPWMA and EPWMB.

  1. Dedicated 16 bit time-base with Period / Frequency control
  2. Two PWM outputs (EPWMA and EPWMB) that can be used in the following configurations
    1. Two independent PWM outputs with single-edge operation
    2. Two independent PWM outputs with dual-edge symmetric operation
    3. One independent PWM output with dual-edge asymmetric operation
  3. Programmable event prescaling minimizes CPU overhead on interrupts.


eCAP

The eCAP module can function either in PWM mode or Capture mode.

  1. Dedicated external pin
  2. 32 bit Time Base counter
  3. 4 x 32 bit Time-stamp Capture registers (CAP1-CAP4)
  4. Input Capture signal pre-scaling
  5. Interrupt capabilities on any of the 4 capture events


Current PWM Driver only supports below Features

  1. only eHRPWM & eCAP is supported
  2. only PWM mode is supported for eCAP.

PWMSS software architecture

AM335X PWM-SS arch.JPG

Driver Configuration

Procedure to build eHRPWM driver

         Device Drivers --->
                 <*> PWM Support --->
                    <*> Davinci eHRPWM support   

Procedure to build eCAP driver

         Device Drivers --->
                 <*> PWM Support --->
                    <*> eCAP PWM support   


Driver Usage


IMPORTANT

*Due to heavy pin-muxing, few instances have pin-outs available on selected AM335x EVMs & profiles. Details about the availability of the peripherals can be found from the EVM reference manual.


eHRPWM

eHRPWM can be controlled from the user space through SYSFS interface. SYSFS interface for eHRPWM is available at

/sys/class/pwm/ehrpwm.i:j

Where,

‘i’ is the eHRPWM instance
‘j’ is the eHRPWM ouptut 0 or 1[Each instance of eHRPWM has 2 channel outputs] 

Various SYSFS Attributes

2 types of SYSFS attributes are available

  1. Request and Control attributes
  2. Configuration attributes

Note

  • Below examples uses eHRPWM instance 2 and output channel 0 (i = 2, j = 0).

Type 1 attributes

  • request Attribute.

Request PWM-SS for permission to use the module. Writing 1 to the request attribute Acquires the device and writing 0 to the request attribute Frees/Releases the device. Before performing any operations, device has to be requested first.

Example

  • Request the Device:
target$ echo 1 > /sys/class/pwm/ehrpwm.2:0/request
  • free the device:
target$ echo 0 > /sys/class/pwm/ehrpwm.2:0/request
  • run Attribute

Start or Stop the PWM Module. 0 – Stop Module, 1 – Start module.

Example

  • Start the PWM
target$ echo 1 > /sys/class/pwm/ehrpwm.2:0/run
  • Stop the PWM
target$ echo 0 > /sys/class/pwm/ehrpwm.2:0/run

CAUTION
Before enabling the module, the module needs to be configured using below configuration attributes. Else proper operation is not assured.

Type 2 attributes

i.Setting the Period
Following attributes set the period of the PWM waveform.

  • frequency Attribute

Enter the period in HZ. Once the frequency is configured, make sure to set the duty cycle value.

Example
Setup PWM to generate a pwm signal of 100 HZ with 50% duty cycle.

target$ echo 100 > /sys/class/pwm/ehrpwm.2:0/period_freq
target$ echo 50 > /sys/class/pwm/ehrpwm.2:0/duty_percent
  • period_ns Attribute

Enter the period in nano seconds value.

Example
if the period is 1 sec , enter

target$ echo 1000000000 > /sys /class/pwm/ehrpwm.2:0/period_ns

ii.Setting the Duty
Following attributes set the duty of the PWM waveform.

  • duty_percent Attribute

Enter the Duty cycle value in percentage.

Example
To configure for 50% duty cycle, enter

target$ echo 50 > /sys/class/pwm/ehrpwm.2:0/duty_percent
  • duty_ns Attribute

duty_ns takes the duty cycle value in nano seconds.

Example
To configure for 0.5s, enter

target$ echo 500000000 > /sys /class/pwm/ehrpwm.2:0/duty_ns

iii.Setting the Polarity

  • Polarity Attribute.

Setup Signal Polarity

Example
To set the polarity to Active High, Enter

target$ echo 1 > /sys /class/pwm/ehrpwm.2:0/polarity

Example
To set the polarity to Active Low, Enter

target$ echo 0 > /sys /class/pwm/ehrpwm.2:0/polarity

Example Configuration:
Following example shows steps to configure the PWM for 100 HZ with 50% duty cycle.

target$ echo 1 >  /sys/class/pwm/ehrpwm.2:0/request
target$ echo 100 > /sys/class/pwm/ehrpwm.2:0/period_freq
target$ echo 50 > /sys/class/pwm/ehrpwm.2:0/duty_percent
target$ echo 1 > /sys/class/pwm/ehrpwm.2:0/run

Issuing above commands will generate PWM wave. This can be verified by probing to eHRPWM pin.

IMPORTANT

  1. To change the frequency, first stop the PWM waveform, reset the duty to zero and then follow the last 3 steps in the above Example Configuration.
  2. eHRPWM 2 instance channel 1 pwm pin is hooked to Haptics AM335x EVM. Changing the duty percentage/frequency will affect the speed of the Haptics.


Controlling haptics

Haptics on Evaluation Module can be controlled through eHRPWM sysfs interface.

IMPORTANT

In order to run Haptics using eHRPWM interface, the Evaluation Module needs to be in Profile 4.
target$ echo 1 > /sys/class/pwm/ehrpwm.2:1/request
target$ echo 250 > /sys/class/pwm/ehrpwm.2:1/period_freq
target$ echo 50 > /sys/class/pwm/ehrpwm.2:1/duty_percent
target$ echo 1 > /sys/class/pwm/ehrpwm.2:1/run

eCAP

The current release of the driver supports only PWM mode. eCAP can be controlled from the user space through SYSFS interface. SYSFS interface for eCAP is available at

target$ cat /sys/class/pwm/ecap.i

Where,

‘i’ is the eCAP instance. 

Various SYSFS Attributes

2 types of SYSFS attributes are available

  1. Request and Control attributes
  2. Configuration attributes

Note

  • Below examples uses eCAP instance 0 (i = 0).

Type 1 attributes

  • request Attribute.

Request PWM-SS for permission to use the module. Writing 1 to the request attribute Acquires the device and writing 0 to the request attribute Frees/Releases the device. Before performing any operations, device has to be requested first.


Example

  • Request the Device:
target$ echo 1 > /sys/class/pwm/ecap.0/request
  • free the device:
target$ echo 0 > /sys/class/pwm/ecap.0/request
  • run Attribute

Start or Stop the PWM Module. 0 – Stop Module, 1 – Start module.

Example

  • Start the PWM
target$ echo 1 > /sys/class/pwm/ecap.0/run
  • Stop the PWM
target$ echo 0 > /sys/class/pwm/ecap.0/run

CAUTION
Before enabling the module, the module needs to be configured using below configuration attributes. Else proper operation is not assured.


Type 2 attributes

i.Setting the Period
Following attributes set the period of the PWM waveform.

  • frequency Attribute

Enter the period in HZ. Once the frequency is configured, make sure to set the duty cycle value.

Example
Setup PWM to generate a pwm signal of 100 HZ with 50% duty cycle.

target$ echo 100 > /sys/class/pwm/ecap.0/period_freq
target$ echo 50 > /sys/class/pwm/ecap.0/duty_percent 
  • period_ns Attribute

Enter the period in nano seconds value.

Example
if the period is 1 sec , enter

target$ echo 1000000000 > /sys /class/pwm/ecap.0/period_ns 

ii.Setting the Duty
Following attributes set the duty of the PWM waveform.

  • duty_percent Attribute

Enter the Duty cycle value in percentage.

Example
To configure for 50% duty cycle, enter

target$ echo 50 > /sys/class/pwm/ecap.0/duty_percent
  • duty_ns Attribute

duty_ns takes the duty cycle value in nano seconds.

Example
To configure for 0.5s, enter

target$ echo 500000000 > /sys /class/pwm/ecap.0/duty_ns

iii.Setting the Polarity

  • Polarity Attribute.

Setup Signal Polarity

Example
To set the polarity to Active High, Enter

target$ echo 1 > /sys /class/pwm/ecap.0/polarity


Example
To set the polarity to Active Low, Enter

target$ echo 0 > /sys /class/pwm/ecap.0/polarity

Example Configuration:
Following example shows steps to configure the PWM for 100 HZ with 50% duty cycle.

target$ echo 1 > /sys/class/pwm/ecap.0/request
target$ echo 100 > /sys/class/pwm/ecap.0/period_freq
target$ echo 50 > /sys/class/pwm/ecap.0/duty_percent
target$ echo 1 > /sys/class/pwm/ecap.0/run

Issuing above commands will generate PWM wave. This can be verified by probing to eCAP pin.

IMPORTANT

  1. To change the frequency, first stop the PWM waveform, reset the duty to zero and then follow the last 3 steps in the above Example Configuration.
  2. In this EVM, eCAP instance 0 pin is hooked to backlight of the LCD. Changing the duty percentage will affect the brightness of the LCD screen.


Controlling backlight

Following are the 2 procedures to vary brightness of the LCD screen.

i. Setting duty percentage of pwm wave from eCAP sysfs files

target$ echo val > /sys/class/pwm/ecap.0/duty_percent

'val' can range from 0 to 100.
ii. Setting brightness from backlight sysfs files

target$ echo val > /sys/class/backlight/pwm-backlight/brightness
'val' can range from 0 to 100.