Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

AM335x Power Consumption Summary

From Texas Instruments Wiki
Jump to: navigation, search

CAUTION Data presented in this wiki was collected on an unsupported version of the SDK, and is provided for legacy purposes. For most recent data, please refer to the TI Processor SDK Kernel Performance Guide, Power Management section

TIBanner.png
AM335x Power Consumption Summary

Overview

CAUTION Data presented in this wiki was collected on an unsupported version of the SDK, and is provided for legacy purposes. For most recent data, please refer to the TI Processor SDK Kernel Performance Guide, Power Management section

Note: the power consumption data in this Wiki was last collected on May 15, 2013

The AM335x Power Consumption Summary discusses the power consumption for common system application usage scenarios for the AM335x ARM® Cortex™-A8 Microprocessors (MPUs). The metrics contained in this document serve to give users a better understanding of AM335x active power behaviors -- making it easier to determine a suitable configuration to meet a given power budget. Power consumption is highly dependent on the individual user’s application; however, this document focuses on providing several AM335x application-usage case scenarios and the environment settings that were used to perform such power measurements. This collection of real power measurements was measured on an AM335x GP EVM with a high-precision digital multimeter.

For additional details about the AM335x processor, please visit the TI.com product page.

Power Measurement Setup

The power measurements have been performed on the following platform:

  • Texas Instruments AM335x 15x15 GP EVM
    • Base Board Revision : 1.2A ("DDR2")
    • Base Board Revision : 1.5A ("DDR3")
    • General Purpose Daughterboard Revision : 1.2B
    • LCD Board Revision : 1.3A


Base Board SW3 settings

Switch
1 2 3 4 5 6 7 8
State
OFF ON ON ON ON ON ON ON


Base Board SW4 settings

Switch
1 2 3 4 5 6 7 8
State
ON ON ON ON ON ON OFF ON


  • Keithley 2701 DMM with a 7702 40-channel mux module.
  • All tests were not conducted in a controlled environment. The ambient room temperature was ~25C.


AM335x Power Supplies

The following table describes the power supplies for AM335x:

AM335x Power Supply rails
SIGNAL DESCRIPTION VALUE
VDD_CORE Core domain 0.95V - 1.1V
VDD_MPU * MPU domain 0.95V - 1.325V
VDDS_RTC RTC domain 1.8V
VDDS_DDR DDR IO domain (DDR2 / DDR3) 1.8V / 1.5V
VDDS Dual voltage IO domains 1.8V
VDDS_SRAM_CORE_BG Core SRAM LDOs, Analog 1.8V
VDDS_SRAM_MPU_BB MPU SRAM LDOs, Analog 1.8V
VDDS_PLL_DDR DPLL DDR, Analog 1.8V
VDDS_PLL_CORE_LCD DPLL Core and LCD, Analog 1.8V
VDDS_PLL_MPU DPLL MPU, Analog 1.8V
VDDS_OSC System oscillator IOs, Analog 1.8V
VDDA1P8V_USB0/1 USB PHY, Analog, 1.8V 1.8V
VDDA3P3V_USB0/1 USB PHY, Analog, 3.3V 3.3V
VDDA_ADC ADC, Analog 1.8V
VDDSHV1 Dual Voltage IO domain 1.8/3.3V
VDDSHV2 * Dual Voltage IO domain 1.8/3.3V
VDDSHV3 * Dual Voltage IO domain 1.8/3.3V
VDDSHV4 Dual Voltage IO domain 1.8/3.3V
VDDSHV5 Dual Voltage IO domain 1.8/3.3V
VDDSHV6 Dual Voltage IO domain 1.8/3.3V

* Note: These voltage rails are not available in the 13x13 package.

The "DDR3" measurements have an additional "VDDSDDRMEM" supply, which is brought up on the Rev1.5A GP EVM. This is not an AM335x voltage rail. It is used to measure the power consumption of the dual-loaded DDR3 + VTT.

High-level Summary

The following tables contain a high-level summary of the total device power (measured in milliwatts) for each application use case and/or configuration. For a detailed breakdown of the total device power over all 20 supplies, click on the corresponding link in the table cells.

An Excel spreadsheet of the data can be downloaded here: Media:AM335x_PowerConsumptionSummary_20130515.zip

Low Power Modes

Implemented in StarterWare. "Max" accounts for additional leakage power due to worst-case silicon process variation, at room temperature.

  Typical (mW) Max (mW)
RTC-Only 0.04 0.05
DS0 3.00 4.30
DS1 6.00 10.00
Standby 16.50 22.00


Active Power

CAUTION Data presented in this wiki was collected on an unsupported version of the SDK, and is provided for legacy purposes. For most recent data, please refer to the TI Processor SDK Kernel Performance Guide, Power Management section

Selected demo applications from the AM335x EVM SDK 05.07

  • VDD_CORE and VDD_MPU at OPP100 (ARM 600 MHz, L3 200 MHz, L4 100 MHz)
  • "DDR3" refers to AM335x Rev. 1.5A GP EVM, which has dual-loaded DDR3 with VTT termination at running 303 MHz
  • "DDR2" refers to AM335x Rev. 1.2A GP EVM, which has dual-loaded DDR2 running at 266 MHz
Application DDR3 (mW) DDR2 (mW)
Linux PSP 553.99 395.29
OS Idle 605.33 449.33
Dhrystone 721.07 554.23
DDR Bandwidth 631.04 471.53
USB Bonnie 687.27 528.57
AAC Decode 572.59 414.21
H.264 Decode 746.00 612.49
Mpeg4 + AAC Decode 750.60 613.10
3D Chameleon Man 823.21 700.96


MPU DVFS

CAUTION Data presented in this wiki was collected on an unsupported version of the SDK, and is provided for legacy purposes. For most recent data, please refer to the TI Processor SDK Kernel Performance Guide, Power Management section

Dynamic Voltage Frequency Scaling (DVFS) for the MPU voltage domain. VDD_CORE is maintained at OPP100.

  DDR3 DDR2
  OS Idle (mW) Dhrystone (mW) OS Idle (mW) Dhrystone (mW)
OPP50 527.81 533.26 380.53 385.51
OPP100 605.95 721.07 454.82 556.88
OPP120 658.72 852.76 506.00 677.59
Turbo 700.30 953.03 544.25 771.31
Nitro 780.54 1142.02 622.31 949.37


VDD_MPU Power vs. Total Device Power Consumption (DDR3 EVM)

    OS Idle Dhrystone
MPU OPP Frequency (MHz) VDD_MPU Power (mW) Total Power (mW) VDD_MPU Power (mW) Total Power (mW)
OPP50 300 45.26 527.81 109.29 533.26
OPP100 600 120.43 605.95 290.38 721.07
OPP120 720 172.32 658.72 420.67 852.76
Turbo 800 212.90 700.30 518.05 953.03
Nitro 1000 290.59 780.54 703.67 1142.02


CORE OPP

CORE OPP for the VDD_CORE voltage domain.

  DDR3 DDR2
  OS Idle (mW) Dhrystone (mW) OS Idle (mW) Dhrystone (mW)
CORE OPP50, MPU OPP50 N/A N/A 253.59 257.24
CORE OPP50, MPU OPP100 N/A N/A 327.19 429.24
CORE OPP100, MPU OPP100 605.33 721.07 449.33 554.23


Low Power Modes

  • As implemented in Starterware
  • Rev1.5A GP EVM
  • "Typical" refers to nominal PG2.x silicon, at room temperature
  • "Max" accounts for additional leakage power due to worst-case silicon process variation, at room temperature
  • This version of DS1 does not include USB remote wakeup

RTC-Only

RTC-Only   Typical       Maximum      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0000005 0.000 0.01 0.00 0.0000022 0.000 0.04 0.00
VDD_MPU 0.05 0.0000028 0.000 0.06 0.00 0.0000073 0.000 0.15 0.00
VDDS_RTC 2 0.0000404 1.800 0.02 0.04 0.0000511 1.800 0.03 0.05
VDDS_DDR 0.24 0.0000021 0.000 0.01 0.00 0.0000017 0.000 0.01 0.00
VDDS 0.24 0.0000018 0.320 0.01 0.00 0.0000010 0.346 0.00 0.00
VDDS_SRAM_CORE_BG 2 0.0000022 0.025 0.00 0.00 0.0000025 0.025 0.00 0.00
VDDS_SRAM_MPU_BB 2 0.0000018 0.025 0.00 0.00 0.0000020 0.025 0.00 0.00
VDDS_PLL_DDR 2 0.0000017 0.025 0.00 0.00 0.0000005 0.025 0.00 0.00
VDDS_PLL_CORE_LCD 2 0.0000019 0.025 0.00 0.00 0.0000013 0.025 0.00 0.00
VDDS_PLL_MPU 2 0.0000021 0.025 0.00 0.00 0.0000013 0.025 0.00 0.00
VDDS_OSC 2 0.0000024 0.024 0.00 0.00 0.0000022 0.025 0.00 0.00
VDDA1P8V_USB0/1 1 0.0000021 0.024 0.00 0.00 0.0000012 0.025 0.00 0.00
VDDA3P3V_USB0/1 2 0.0000018 0.061 0.00 0.00 0.0000017 0.061 0.00 0.00
VDDA_ADC 1 0.0000011 0.347 0.00 0.00 0.0000011 0.232 0.00 0.00
VDDSHV1 0.24 0.0000000 0.000 0.00 0.00 0.0000784 0.000 0.33 0.00
VDDSHV2 0.24 0.0000019 0.026 0.01 0.00 0.0000016 0.027 0.01 0.00
VDDSHV3 0.24 0.0000000 0.000 0.00 0.00 0.0009411 0.000 3.92 0.00
VDDSHV4 0.24 0.0000016 0.026 0.01 0.00 0.0000016 0.027 0.01 0.00
VDDSHV5 0.24 0.0000000 0.000 0.00 0.00 0.0021680 0.000 9.03 0.00
VDDSHV6 0.24 0.0000000 0.000 0.00 0.00 0.0030291 0.000 12.62 0.00
        Total 0.0398     Total 0.0482
                   
VDDSDDRMEM 0.24 0.0000000 0.000 0.00 0.00 0.0000000 0.000 0.00 0.00

DS0

DS0   Typical       Maximum      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0000498 0.956 1.00 0.95 0.0001143 0.956 2.29 2.18
VDD_MPU 0.05 0.0000152 0.961 0.30 0.29 0.0000285 0.961 0.57 0.55
VDDS_RTC 2 0.0000432 1.800 0.02 0.04 0.0000526 1.800 0.03 0.05
VDDS_DDR 0.24 0.0000049 1.498 0.02 0.03 0.0000064 1.498 0.03 0.04
VDDS 0.24 0.0000235 1.811 0.10 0.18 0.0000231 1.810 0.10 0.17
VDDS_SRAM_CORE_BG 2 0.0003279 1.823 0.16 0.30 0.0003419 1.822 0.17 0.31
VDDS_SRAM_MPU_BB 2 0.0000139 1.823 0.01 0.01 0.0000137 1.822 0.01 0.01
VDDS_PLL_DDR 2 0.0000016 1.823 0.00 0.00 0.0000011 1.823 0.00 0.00
VDDS_PLL_CORE_LCD 2 0.0000020 1.823 0.00 0.00 0.0000023 1.823 0.00 0.00
VDDS_PLL_MPU 2 0.0000019 1.823 0.00 0.00 0.0000015 1.822 0.00 0.00
VDDS_OSC 2 0.0000024 1.823 0.00 0.00 0.0000024 1.822 0.00 0.00
VDDA1P8V_USB0/1 1 0.0000024 1.820 0.00 0.00 0.0000024 1.820 0.00 0.00
VDDA3P3V_USB0/1 2 0.0000422 3.342 0.02 0.07 0.0000464 3.341 0.02 0.08
VDDA_ADC 1 0.0000021 1.829 0.00 0.00 0.0000014 1.829 0.00 0.00
VDDSHV1 0.24 0.0000057 3.312 0.02 0.08 0.0000054 3.311 0.02 0.07
VDDSHV2 0.24 0.0000058 3.324 0.02 0.08 0.0000061 3.322 0.03 0.08
VDDSHV3 0.24 0.0000071 3.312 0.03 0.10 0.0000076 3.311 0.03 0.11
VDDSHV4 0.24 0.0000047 3.324 0.02 0.06 0.0000048 3.322 0.02 0.07
VDDSHV5 0.24 0.0000054 3.312 0.02 0.07 0.0000056 3.311 0.02 0.08
VDDSHV6 0.24 0.0000327 3.312 0.14 0.45 0.0000329 3.311 0.14 0.45
        Total 2.74     Total 4.27
                   
VDDSDDRMEM 0.24 0.0028000 1.493 11.67 17.42 0.0028000 1.493 11.67 17.42

DS1

DS1   Typical       Maximum      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0001994 0.956 3.99 3.81 0.0004040 0.956 8.08 7.72
VDD_MPU 0.05 0.0000155 0.961 0.31 0.30 0.0000272 0.961 0.54 0.52
VDDS_RTC 2 0.0000420 1.800 0.02 0.04 0.0000519 1.800 0.03 0.05
VDDS_DDR 0.24 0.0000049 1.498 0.02 0.03 0.0000068 1.498 0.03 0.04
VDDS 0.24 0.0000237 1.811 0.10 0.18 0.0000236 1.810 0.10 0.18
VDDS_SRAM_CORE_BG 2 0.0003283 1.823 0.16 0.30 0.0003413 1.822 0.17 0.31
VDDS_SRAM_MPU_BB 2 0.0000135 1.823 0.01 0.01 0.0000140 1.823 0.01 0.01
VDDS_PLL_DDR 2 0.0000021 1.823 0.00 0.00 0.0000014 1.823 0.00 0.00
VDDS_PLL_CORE_LCD 2 0.0000016 1.823 0.00 0.00 0.0000023 1.822 0.00 0.00
VDDS_PLL_MPU 2 0.0000014 1.823 0.00 0.00 0.0000016 1.822 0.00 0.00
VDDS_OSC 2 0.0000025 1.823 0.00 0.00 0.0000020 1.822 0.00 0.00
VDDA1P8V_USB0/1 1 0.0000028 1.820 0.00 0.01 0.0000016 1.820 0.00 0.00
VDDA3P3V_USB0/1 2 0.0000426 3.342 0.02 0.07 0.0000457 3.341 0.02 0.08
VDDA_ADC 1 0.0000014 1.829 0.00 0.00 0.0000019 1.829 0.00 0.00
VDDSHV1 0.24 0.0000056 3.312 0.02 0.08 0.0000060 3.311 0.02 0.08
VDDSHV2 0.24 0.0000059 3.324 0.02 0.08 0.0000061 3.323 0.03 0.08
VDDSHV3 0.24 0.0000070 3.312 0.03 0.10 0.0000067 3.311 0.03 0.09
VDDSHV4 0.24 0.0000046 3.324 0.02 0.06 0.0000045 3.323 0.02 0.06
VDDSHV5 0.24 0.0000055 3.312 0.02 0.08 0.0000047 3.311 0.02 0.07
VDDSHV6 0.24 0.0000326 3.312 0.14 0.45 0.0000329 3.311 0.14 0.45
        Total 5.60     Total 9.77
                   
VDDSDDRMEM 0.24 0.0028000 1.493 11.67 17.42 0.0028000 1.493 11.67 17.42

Standby

Standby   Typical       Maximum      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0005892 0.956 11.78 11.26 0.0007874 0.955 15.75 15.04
VDD_MPU 0.05 0.0000174 0.961 0.35 0.34 0.0000303 0.961 0.61 0.58
VDDS_RTC 2 0.0001373 1.799 0.07 0.12 0.0001492 1.799 0.07 0.13
VDDS_DDR 0.24 0.0000047 1.498 0.02 0.03 0.0000063 1.498 0.03 0.04
VDDS 0.24 0.0000237 1.811 0.10 0.18 0.0000236 1.810 0.10 0.18
VDDS_SRAM_CORE_BG 2 0.0024246 1.823 1.21 2.21 0.0039976 1.822 2.00 3.64
VDDS_SRAM_MPU_BB 2 0.0000132 1.823 0.01 0.01 0.0000143 1.822 0.01 0.01
VDDS_PLL_DDR 2 0.0000013 1.823 0.00 0.00 0.0000016 1.822 0.00 0.00
VDDS_PLL_CORE_LCD 2 0.0000022 1.823 0.00 0.00 0.0000026 1.822 0.00 0.00
VDDS_PLL_MPU 2 0.0000015 1.823 0.00 0.00 0.0000021 1.822 0.00 0.00
VDDS_OSC 2 0.0013934 1.823 0.70 1.27 0.0013752 1.822 0.69 1.25
VDDA1P8V_USB0/1 1 0.0000022 1.820 0.00 0.00 0.0000023 1.820 0.00 0.00
VDDA3P3V_USB0/1 2 0.0000432 3.342 0.02 0.07 0.0000464 3.341 0.02 0.08
VDDA_ADC 1 0.0000024 1.829 0.00 0.00 0.0000031 1.829 0.00 0.01
VDDSHV1 0.24 0.0000058 3.312 0.02 0.08 0.0000064 3.311 0.03 0.09
VDDSHV2 0.24 0.0000060 3.324 0.03 0.08 0.0000062 3.323 0.03 0.09
VDDSHV3 0.24 0.0000076 3.312 0.03 0.11 0.0000076 3.311 0.03 0.10
VDDSHV4 0.24 0.0000044 3.324 0.02 0.06 0.0000054 3.323 0.02 0.07
VDDSHV5 0.24 0.0000057 3.312 0.02 0.08 0.0000049 3.311 0.02 0.07
VDDSHV6 0.24 0.0000331 3.312 0.14 0.46 0.0000327 3.311 0.14 0.45
        Total 16.37     Total 21.84
                   
VDDSDDRMEM 0.24 0.0028000 1.493 11.67 17.42 0.0028000 1.493 11.67 17.42


Active Power

  • Selected demo applications from the AM335x EVM SDK 05.07
  • VDD_CORE and VDD_MPU at OPP100 (ARM 600 MHz, DDR3 303 MHz, L3 200 MHz, L4 100 MHz)
  • Optimized IO pad configuration
  • SmartReflex disabled
  • Matrix GUI is shutdown (except for "OS Idle")
  • LCDC is disabled (except for "OS Idle", "H.264 Decode", "Mpeg4 + AAC Decode", "3D Chameleon Man")

Linux PSP

Use Case: Command prompt after login, no application running

Linux PSP   DDR3       DDR2      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0092644 1.143 185.29 211.85 0.0077265 1.128 154.53 174.27
VDD_MPU 0.05 0.0054017 1.111 108.03 120.00 0.0052665 1.096 105.33 115.42
VDDS_RTC 2 0.0008652 1.798 0.43 0.78 0.0009008 1.797 0.45 0.81
VDDS_DDR 0.24 0.0240616 1.495 100.26 149.89 0.0043077 1.756 17.95 31.52
VDDS 0.24 0.0000415 1.810 0.17 0.31 0.0000481 1.801 0.20 0.36
VDDS_SRAM_CORE_BG 2 0.0027236 1.820 1.36 2.48 0.0026791 1.818 1.34 2.44
VDDS_SRAM_MPU_BB 2 0.0032137 1.820 1.61 2.92 0.0031413 1.818 1.57 2.86
VDDS_PLL_DDR 2 0.0021812 1.820 1.09 1.99 0.0020869 1.818 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0149135 1.820 7.46 13.57 0.0147957 1.818 7.40 13.45
VDDS_PLL_MPU 2 0.0040831 1.820 2.04 3.72 0.0040701 1.818 2.04 3.70
VDDS_OSC 2 0.0013886 1.820 0.69 1.26 0.0013568 1.818 0.68 1.23
VDDA1P8V_USB0/1 1 0.0162042 1.815 16.20 29.41 0.0162293 1.824 16.23 29.60
VDDA3P3V_USB0/1 2 0.0070970 3.339 3.55 11.85 0.0066446 3.323 3.32 11.04
VDDA_ADC 1 0.0004581 1.828 0.46 0.84 0.0004581 1.827 0.46 0.84
VDDSHV1 0.24 0.0000342 3.310 0.14 0.47 0.0000271 3.316 0.11 0.37
VDDSHV2 0.24 0.0000061 3.321 0.03 0.08 0.0000054 3.325 0.02 0.07
VDDSHV3 0.24 0.0000090 3.310 0.04 0.12 0.0000098 3.319 0.04 0.14
VDDSHV4 0.24 0.0000072 3.322 0.03 0.10 0.0000070 3.325 0.03 0.10
VDDSHV5 0.24 0.0000071 3.310 0.03 0.10 0.0001886 3.319 0.79 2.61
VDDSHV6 0.24 0.0001624 3.310 0.68 2.24 0.0001871 3.314 0.78 2.58
        Total 553.99     Total 395.2924
                   
VDDSDDRMEM 0.24 0.0140000 1.500 58.33 87.50        


OS Idle

Use Case: Matrix Qt GUI

OS Idle (Matrix)   DDR3       DDR2      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0093595 1.143 187.19 213.98 0.0080373 1.129 160.75 181.52
VDD_MPU 0.05 0.0054176 1.111 108.35 120.33 0.0052680 1.096 105.36 115.48
VDDS_RTC 2 0.0008660 1.798 0.43 0.78 0.0008992 1.797 0.45 0.81
VDDS_DDR 0.24 0.0251420 1.494 104.76 156.48 0.0051808 1.757 21.59 37.92
VDDS 0.24 0.0001431 1.810 0.60 1.08 0.0001468 1.801 0.61 1.10
VDDS_SRAM_CORE_BG 2 0.0028104 1.820 1.41 2.56 0.0026061 1.819 1.30 2.37
VDDS_SRAM_MPU_BB 2 0.0033125 1.820 1.66 3.01 0.0030585 1.819 1.53 2.78
VDDS_PLL_DDR 2 0.0021828 1.820 1.09 1.99 0.0020846 1.819 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0147823 1.820 7.39 13.45 0.0147780 1.819 7.39 13.44
VDDS_PLL_MPU 2 0.0040859 1.820 2.04 3.72 0.0040656 1.818 2.03 3.70
VDDS_OSC 2 0.0013842 1.820 0.69 1.26 0.0013594 1.819 0.68 1.24
VDDA1P8V_USB0/1 1 0.0162018 1.815 16.20 29.40 0.0162061 1.824 16.21 29.56
VDDA3P3V_USB0/1 2 0.0066459 3.338 3.32 11.09 0.0066482 3.324 3.32 11.05
VDDA_ADC 1 0.0004581 1.828 0.46 0.84 0.0004590 1.828 0.46 0.84
VDDSHV1 0.24 0.0000337 3.307 0.14 0.46 0.0000273 3.315 0.11 0.38
VDDSHV2 0.24 0.0007357 3.320 3.07 10.18 0.0005006 3.325 2.09 6.94
VDDSHV3 0.24 0.0000101 3.309 0.04 0.14 0.0000112 3.318 0.05 0.16
VDDSHV4 0.24 0.0000077 3.320 0.03 0.11 0.0000067 3.325 0.03 0.09
VDDSHV5 0.24 0.0000078 3.309 0.03 0.11 0.0001908 3.318 0.80 2.64
VDDSHV6 0.24 0.0024931 3.307 10.39 34.35 0.0025674 3.312 10.70 35.43
        Total 605.33     Total 449.331
                   
VDDSDDRMEM 0.24 0.0170000 1.500 70.83 106.25        


Dhrystone

  • Measured DMIPS/MHz : 1.8 ~ 1.9 DMIPS/MHz
Dhrystone   DDR3       DDR2      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0092576 1.144 185.15 211.73 0.0077025 1.128 154.05 173.74
VDD_MPU 0.05 0.0131109 1.107 262.22 290.38 0.0123149 1.094 246.30 269.34
VDDS_RTC 2 0.0008667 1.798 0.43 0.78 0.0008988 1.797 0.45 0.81
VDDS_DDR 0.24 0.0227718 1.495 94.88 141.88 0.0042967 1.756 17.90 31.44
VDDS 0.24 0.0000412 1.810 0.17 0.31 0.0000484 1.801 0.20 0.36
VDDS_SRAM_CORE_BG 2 0.0027687 1.819 1.38 2.52 0.0027166 1.818 1.36 2.47
VDDS_SRAM_MPU_BB 2 0.0094873 1.819 4.74 8.63 0.0093426 1.818 4.67 8.49
VDDS_PLL_DDR 2 0.0021790 1.820 1.09 1.98 0.0020848 1.818 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0147669 1.820 7.38 13.44 0.0147721 1.818 7.39 13.43
VDDS_PLL_MPU 2 0.0040814 1.819 2.04 3.71 0.0040650 1.818 2.03 3.69
VDDS_OSC 2 0.0013888 1.820 0.69 1.26 0.0013505 1.818 0.68 1.23
VDDA1P8V_USB0/1 1 0.0161796 1.815 16.18 29.37 0.0162206 1.824 16.22 29.58
VDDA3P3V_USB0/1 2 0.0066463 3.339 3.32 11.10 0.0066404 3.324 3.32 11.03
VDDA_ADC 1 0.0004578 1.828 0.46 0.84 0.0004576 1.827 0.46 0.84
VDDSHV1 0.24 0.0000357 3.309 0.15 0.49 0.0000272 3.317 0.11 0.38
VDDSHV2 0.24 0.0000058 3.321 0.02 0.08 0.0000051 3.325 0.02 0.07
VDDSHV3 0.24 0.0000094 3.310 0.04 0.13 0.0000092 3.320 0.04 0.13
VDDSHV4 0.24 0.0000079 3.321 0.03 0.11 0.0000077 3.325 0.03 0.11
VDDSHV5 0.24 0.0000082 3.310 0.03 0.11 0.0001891 3.319 0.79 2.62
VDDSHV6 0.24 0.0001616 3.309 0.67 2.23 0.0001867 3.314 0.78 2.58
        Total 721.07     Total 554.23
                   
VDDSDDRMEM 0.24 0.0171000 1.500 71.25 106.88        


DDR Bandwidth

DDR Bandwidth   DDR3       DDR2      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0092733 1.143 185.47 212.03 0.0077094 1.128 154.19 173.91
VDD_MPU 0.05 0.0088350 1.109 176.70 196.02 0.0085640 1.095 171.28 187.54
VDDS_RTC 2 0.0008657 1.798 0.43 0.78 0.0008991 1.797 0.45 0.81
VDDS_DDR 0.24 0.0240999 1.495 100.42 150.12 0.0043295 1.756 18.04 31.68
VDDS 0.24 0.0000414 1.810 0.17 0.31 0.0000811 1.801 0.34 0.61
VDDS_SRAM_CORE_BG 2 0.0027665 1.820 1.38 2.52 0.0026895 1.818 1.34 2.45
VDDS_SRAM_MPU_BB 2 0.0046273 1.820 2.31 4.21 0.0038408 1.818 1.92 3.49
VDDS_PLL_DDR 2 0.0021808 1.820 1.09 1.98 0.0020848 1.818 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0149132 1.820 7.46 13.57 0.0147828 1.818 7.39 13.44
VDDS_PLL_MPU 2 0.0040843 1.819 2.04 3.72 0.0040676 1.818 2.03 3.70
VDDS_OSC 2 0.0013874 1.820 0.69 1.26 0.0013543 1.819 0.68 1.23
VDDA1P8V_USB0/1 1 0.0162240 1.815 16.22 29.45 0.0162125 1.824 16.21 29.57
VDDA3P3V_USB0/1 2 0.0066487 3.339 3.32 11.10 0.0066423 3.324 3.32 11.04
VDDA_ADC 1 0.0004583 1.828 0.46 0.84 0.0004583 1.827 0.46 0.84
VDDSHV1 0.24 0.0000340 3.309 0.14 0.47 0.0000270 3.317 0.11 0.37
VDDSHV2 0.24 0.0000066 3.321 0.03 0.09 0.0000049 3.325 0.02 0.07
VDDSHV3 0.24 0.0000091 3.310 0.04 0.13 0.0000092 3.320 0.04 0.13
VDDSHV4 0.24 0.0000076 3.321 0.03 0.10 0.0000067 3.325 0.03 0.09
VDDSHV5 0.24 0.0000072 3.310 0.03 0.10 0.0004407 3.320 1.84 6.10
VDDSHV6 0.24 0.0001623 3.309 0.68 2.24 0.0001867 3.315 0.78 2.58
        Total 631.04     Total 471.53
               
VDDSDDRMEM 0.24 0.0260000 1.500 108.33 162.50        


USB Bonnie

USB Bonnie   DDR3       DDR2      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0092641 1.143 185.28 211.85 0.0078401 1.128 156.80 176.89
VDD_MPU 0.05 0.0110872 1.107 221.74 245.49 0.0106669 1.095 213.34 233.55
VDDS_RTC 2 0.0008653 1.798 0.43 0.78 0.0008997 1.797 0.45 0.81
VDDS_DDR 0.24 0.0245889 1.495 102.45 153.15 0.0048278 1.756 20.12 35.33
VDDS 0.24 0.0000420 1.810 0.18 0.32 0.0000816 1.801 0.34 0.61
VDDS_SRAM_CORE_BG 2 0.0027820 1.819 1.39 2.53 0.0027129 1.818 1.36 2.47
VDDS_SRAM_MPU_BB 2 0.0076701 1.820 3.84 6.98 0.0070746 1.818 3.54 6.43
VDDS_PLL_DDR 2 0.0021805 1.820 1.09 1.98 0.0020851 1.818 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0147742 1.820 7.39 13.45 0.0147746 1.818 7.39 13.43
VDDS_PLL_MPU 2 0.0040834 1.820 2.04 3.72 0.0040673 1.818 2.03 3.70
VDDS_OSC 2 0.0013892 1.820 0.69 1.26 0.0013525 1.818 0.68 1.23
VDDA1P8V_USB0/1 1 0.0181203 1.815 18.12 32.88 0.0181985 1.823 18.20 33.18
VDDA3P3V_USB0/1 2 0.0053435 3.339 2.67 8.92 0.0053366 3.324 2.67 8.87
VDDA_ADC 1 0.0004580 1.828 0.46 0.84 0.0004587 1.827 0.46 0.84
VDDSHV1 0.24 0.0000346 3.309 0.14 0.48 0.0000272 3.317 0.11 0.38
VDDSHV2 0.24 0.0000060 3.321 0.03 0.08 0.0000056 3.325 0.02 0.08
VDDSHV3 0.24 0.0000096 3.310 0.04 0.13 0.0000090 3.320 0.04 0.12
VDDSHV4 0.24 0.0000078 3.321 0.03 0.11 0.0000073 3.325 0.03 0.10
VDDSHV5 0.24 0.0000070 3.310 0.03 0.10 0.0004402 3.320 1.83 6.09
VDDSHV6 0.24 0.0001621 3.309 0.68 2.24 0.0001863 3.315 0.78 2.57
        Total 687.27     Total 528.57
               
VDDSDDRMEM 0.24 0.0150000 1.500 62.50 93.75        


AAC Decode

AAC Decode   DDR3       DDR2      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0091971 1.143 183.94 210.33 0.0077432 1.128 154.86 174.67
VDD_MPU 0.05 0.0059143 1.111 118.29 131.36 0.0057297 1.096 114.59 125.56
VDDS_RTC 2 0.0008655 1.798 0.43 0.78 0.0009008 1.797 0.45 0.81
VDDS_DDR 0.24 0.0255236 1.494 106.35 158.91 0.0043994 1.756 18.33 32.19
VDDS 0.24 0.0000412 1.810 0.17 0.31 0.0000813 1.801 0.34 0.61
VDDS_SRAM_CORE_BG 2 0.0027484 1.820 1.37 2.50 0.0026792 1.818 1.34 2.44
VDDS_SRAM_MPU_BB 2 0.0034700 1.820 1.73 3.16 0.0033579 1.818 1.68 3.05
VDDS_PLL_DDR 2 0.0021816 1.820 1.09 1.99 0.0020867 1.819 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0149157 1.820 7.46 13.58 0.0147918 1.819 7.40 13.45
VDDS_PLL_MPU 2 0.0040849 1.820 2.04 3.72 0.0040705 1.818 2.04 3.70
VDDS_OSC 2 0.0013886 1.820 0.69 1.26 0.0013564 1.819 0.68 1.23
VDDA1P8V_USB0/1 1 0.0162332 1.815 16.23 29.46 0.0162343 1.824 16.23 29.61
VDDA3P3V_USB0/1 2 0.0066526 3.339 3.33 11.11 0.0066443 3.324 3.32 11.04
VDDA_ADC 1 0.0004587 1.828 0.46 0.84 0.0004586 1.827 0.46 0.84
VDDSHV1 0.24 0.0000347 3.309 0.14 0.48 0.0000277 3.316 0.12 0.38
VDDSHV2 0.24 0.0000060 3.321 0.02 0.08 0.0000056 3.325 0.02 0.08
VDDSHV3 0.24 0.0000092 3.310 0.04 0.13 0.0000098 3.318 0.04 0.14
VDDSHV4 0.24 0.0000082 3.321 0.03 0.11 0.0000070 3.325 0.03 0.10
VDDSHV5 0.24 0.0000178 3.310 0.07 0.25 0.0007124 3.318 2.97 9.85
VDDSHV6 0.24 0.0001629 3.309 0.68 2.25 0.0001868 3.314 0.78 2.58
        Total 572.595     Total 414.2132
                   
VDDSDDRMEM 0.24 0.0125000 1.500 52.08 78.13        


H.264 Decode

H.264 Decode   DDR3       DDR2      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0099085 1.144 198.17 226.65 0.0085588 1.128 171.18 193.17
VDD_MPU 0.05 0.0094418 1.108 188.84 209.32 0.0091769 1.096 183.54 201.07
VDDS_RTC 2 0.0008658 1.798 0.43 0.78 0.0008996 1.797 0.45 0.81
VDDS_DDR 0.24 0.0254633 1.492 106.10 158.28 0.0083682 1.755 34.87 61.19
VDDS 0.24 0.0001543 1.809 0.64 1.16 0.0001977 1.801 0.82 1.48
VDDS_SRAM_CORE_BG 2 0.0028304 1.820 1.42 2.58 0.0027286 1.818 1.36 2.48
VDDS_SRAM_MPU_BB 2 0.0056576 1.820 2.83 5.15 0.0056739 1.818 2.84 5.16
VDDS_PLL_DDR 2 0.0021825 1.820 1.09 1.99 0.0020847 1.818 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0149203 1.820 7.46 13.58 0.0147740 1.819 7.39 13.43
VDDS_PLL_MPU 2 0.0040848 1.819 2.04 3.72 0.0040663 1.818 2.03 3.70
VDDS_OSC 2 0.0013846 1.820 0.69 1.26 0.0013504 1.818 0.68 1.23
VDDA1P8V_USB0/1 1 0.0162216 1.815 16.22 29.44 0.0181442 1.823 18.14 33.08
VDDA3P3V_USB0/1 2 0.0066447 3.339 3.32 11.09 0.0053360 3.324 2.67 8.87
VDDA_ADC 1 0.0004574 1.828 0.46 0.84 0.0004580 1.827 0.46 0.84
VDDSHV1 0.24 0.0000340 3.307 0.14 0.47 0.0000265 3.313 0.11 0.37
VDDSHV2 0.24 0.0019268 3.318 8.03 26.64 0.0015042 3.323 6.27 20.83
VDDSHV3 0.24 0.0000094 3.308 0.04 0.13 0.0000085 3.317 0.04 0.12
VDDSHV4 0.24 0.0000081 3.318 0.03 0.11 0.0000071 3.324 0.03 0.10
VDDSHV5 0.24 0.0000068 3.308 0.03 0.09 0.0004367 3.317 1.82 6.03
VDDSHV6 0.24 0.0038282 3.306 15.95 52.73 0.0041077 3.310 17.12 56.65
        Total 746.00     Total 612.49
                   
VDDSDDRMEM 0.24 0.0240000 1.500 100.00 150.00        


Mpeg4 + AAC Decode

MPEG-4 + AAC Decode   DDR3       DDR2      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0099605 1.144 199.21 227.85 0.0085667 1.128 171.33 193.28
VDD_MPU 0.05 0.0093620 1.108 187.24 207.56 0.0088928 1.095 177.86 194.79
VDDS_RTC 2 0.0008662 1.798 0.43 0.78 0.0008994 1.797 0.45 0.81
VDDS_DDR 0.24 0.0254475 1.492 106.03 158.18 0.0087538 1.755 36.47 64.01
VDDS 0.24 0.0001485 1.809 0.62 1.12 0.0002011 1.801 0.84 1.51
VDDS_SRAM_CORE_BG 2 0.0028292 1.820 1.41 2.57 0.0027683 1.818 1.38 2.52
VDDS_SRAM_MPU_BB 2 0.0055558 1.820 2.78 5.05 0.0054227 1.818 2.71 4.93
VDDS_PLL_DDR 2 0.0021818 1.820 1.09 1.99 0.0020859 1.818 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0149184 1.820 7.46 13.58 0.0147790 1.818 7.39 13.44
VDDS_PLL_MPU 2 0.0040851 1.819 2.04 3.72 0.0040661 1.818 2.03 3.70
VDDS_OSC 2 0.0013851 1.820 0.69 1.26 0.0013474 1.818 0.67 1.22
VDDA1P8V_USB0/1 1 0.0162379 1.815 16.24 29.47 0.0181931 1.823 18.19 33.16
VDDA3P3V_USB0/1 2 0.0066445 3.338 3.32 11.09 0.0053333 3.323 2.67 8.86
VDDA_ADC 1 0.0004579 1.828 0.46 0.84 0.0004570 1.827 0.46 0.84
VDDSHV1 0.24 0.0000332 3.306 0.14 0.46 0.0000264 3.311 0.11 0.36
VDDSHV2 0.24 0.0024338 3.318 10.14 33.64 0.0012473 3.323 5.20 17.27
VDDSHV3 0.24 0.0000095 3.308 0.04 0.13 0.0000083 3.314 0.03 0.12
VDDSHV4 0.24 0.0000071 3.319 0.03 0.10 0.0000066 3.323 0.03 0.09
VDDSHV5 0.24 0.0000157 3.308 0.07 0.22 0.0005059 3.314 2.11 6.99
VDDSHV6 0.24 0.0037025 3.306 15.43 51.00 0.0045931 3.308 19.14 63.31
        Total 750.60     Total 613.10
                   
VDDSDDRMEM 0.24 0.0260000 1.500 108.33 162.50        


3D Chameleon Man

3D Chameleon Man   DDR3       DDR2      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0142116 1.141 284.23 324.37 0.0127182 1.126 254.36 286.39
VDD_MPU 0.05 0.0067084 1.110 134.17 148.91 0.0065003 1.095 130.01 142.42
VDDS_RTC 2 0.0008668 1.798 0.43 0.78 0.0008997 1.797 0.45 0.81
VDDS_DDR 0.24 0.0284022 1.489 118.34 176.22 0.0144338 1.753 60.14 105.43
VDDS 0.24 0.0002512 1.809 1.05 1.89 0.0002890 1.800 1.20 2.17
VDDS_SRAM_CORE_BG 2 0.0032439 1.820 1.62 2.95 0.0031668 1.818 1.58 2.88
VDDS_SRAM_MPU_BB 2 0.0041402 1.820 2.07 3.77 0.0040281 1.818 2.01 3.66
VDDS_PLL_DDR 2 0.0021825 1.820 1.09 1.99 0.0020859 1.818 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0149238 1.820 7.46 13.58 0.0147811 1.818 7.39 13.44
VDDS_PLL_MPU 2 0.0040866 1.819 2.04 3.72 0.0040660 1.818 2.03 3.70
VDDS_OSC 2 0.0013842 1.820 0.69 1.26 0.0013471 1.818 0.67 1.22
VDDA1P8V_USB0/1 1 0.0162014 1.815 16.20 29.40 0.0181554 1.823 18.16 33.10
VDDA3P3V_USB0/1 2 0.0066429 3.338 3.32 11.09 0.0053325 3.323 2.67 8.86
VDDA_ADC 1 0.0004572 1.828 0.46 0.84 0.0004572 1.827 0.46 0.84
VDDSHV1 0.24 0.0000329 3.306 0.14 0.45 0.0000256 3.311 0.11 0.35
VDDSHV2 0.24 0.0030549 3.316 12.73 42.21 0.0019922 3.322 8.30 27.58
VDDSHV3 0.24 0.0000087 3.308 0.04 0.12 0.0000080 3.316 0.03 0.11
VDDSHV4 0.24 0.0000076 3.317 0.03 0.11 0.0000067 3.323 0.03 0.09
VDDSHV5 0.24 0.0000075 3.308 0.03 0.10 0.0004362 3.316 1.82 6.03
VDDSHV6 0.24 0.0043170 3.305 17.99 59.46 0.0043533 3.308 18.14 60.01
        Total 823.21     Total 700.96
                   
VDDSDDRMEM 0.24 0.0330000 1.500 137.50 206.25        

MPU DVFS

  • Updated OPP voltage/frequency table for PG2.x
  • VDD_CORE kept at OPP100
  • Optimized IO pad configuration
  • SmartReflex disabled
  • Matrix GUI is shutdown (except for "OS Idle")
  • LCDC is disabled (except for "OS Idle", "H.264 Decode", "Mpeg4 + AAC Decode", "3D Chameleon Man")

OPP50

    DDR3               DDR2              
OPP50   OS Idle       Dhrystone       OS Idle       Dhrystone      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0093102 1.143 186.20 212.87 0.0092293 1.143 184.59 211.00 0.0080328 1.129 160.66 181.30 0.0076838 1.128 153.68 173.31
VDD_MPU 0.05 0.0023722 0.954 47.44 45.26 0.0057051 0.958 114.10 109.29 0.0022979 0.939 45.96 43.17 0.0053746 0.945 107.49 101.58
VDDS_RTC 2 0.0008676 1.798 0.43 0.78 0.0008665 1.798 0.43 0.78 0.0009014 1.797 0.45 0.81 0.0009004 1.797 0.45 0.81
VDDS_DDR 0.24 0.0252374 1.494 105.16 157.08 0.0225466 1.495 93.94 140.49 0.0051706 1.756 21.54 37.83 0.0043228 1.756 18.01 31.63
VDDS 0.24 0.0001440 1.810 0.60 1.09 0.0000415 1.810 0.17 0.31 0.0001805 1.801 0.75 1.35 0.0000814 1.801 0.34 0.61
VDDS_SRAM_CORE_BG 2 0.0027444 1.820 1.37 2.50 0.0027177 1.820 1.36 2.47 0.0027362 1.818 1.37 2.49 0.0026673 1.818 1.33 2.42
VDDS_SRAM_MPU_BB 2 0.0032226 1.820 1.61 2.93 0.0062828 1.820 3.14 5.72 0.0031978 1.818 1.60 2.91 0.0061835 1.818 3.09 5.62
VDDS_PLL_DDR 2 0.0021815 1.820 1.09 1.99 0.0021800 1.820 1.09 1.98 0.0020884 1.818 1.04 1.90 0.0020864 1.818 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0147782 1.820 7.39 13.45 0.0147725 1.820 7.39 13.45 0.0148063 1.818 7.40 13.46 0.0147851 1.818 7.39 13.44
VDDS_PLL_MPU 2 0.0022381 1.820 1.12 2.04 0.0022368 1.820 1.12 2.04 0.0022313 1.818 1.12 2.03 0.0022298 1.818 1.11 2.03
VDDS_OSC 2 0.0013909 1.820 0.70 1.27 0.0013910 1.820 0.70 1.27 0.0013550 1.818 0.68 1.23 0.0013560 1.819 0.68 1.23
VDDA1P8V_USB0/1 1 0.0162115 1.815 16.21 29.42 0.0161813 1.815 16.18 29.37 0.0182332 1.823 18.23 33.24 0.0162174 1.824 16.22 29.58
VDDA3P3V_USB0/1 2 0.0066516 3.339 3.33 11.10 0.0066512 3.339 3.33 11.10 0.0053368 3.323 2.67 8.87 0.0066426 3.323 3.32 11.04
VDDA_ADC 1 0.0004587 1.828 0.46 0.84 0.0004586 1.828 0.46 0.84 0.0004583 1.827 0.46 0.84 0.0004581 1.827 0.46 0.84
VDDSHV1 0.24 0.0000349 3.307 0.15 0.48 0.0000357 3.309 0.15 0.49 0.0000267 3.314 0.11 0.37 0.0000276 3.317 0.12 0.38
VDDSHV2 0.24 0.0007353 3.320 3.06 10.17 0.0000057 3.322 0.02 0.08 0.0005010 3.324 2.09 6.94 0.0000052 3.325 0.02 0.07
VDDSHV3 0.24 0.0000091 3.309 0.04 0.12 0.0000090 3.310 0.04 0.12 0.0000080 3.318 0.03 0.11 0.0000105 3.320 0.04 0.15
VDDSHV4 0.24 0.0000079 3.320 0.03 0.11 0.0000082 3.321 0.03 0.11 0.0000067 3.324 0.03 0.09 0.0000083 3.325 0.03 0.12
VDDSHV5 0.24 0.0000082 3.309 0.03 0.11 0.0000082 3.310 0.03 0.11 0.0004385 3.318 1.83 6.06 0.0004451 3.320 1.85 6.16
VDDSHV6 0.24 0.0024820 3.307 10.34 34.20 0.0001623 3.310 0.68 2.24 0.0025748 3.311 10.73 35.52 0.0001880 3.315 0.78 2.60
        Total 527.81     Total 533.26     Total 380.53     Total 385.51
                                   
VDDSDDRMEM 0.24 0.0168000 1.500 70.00 105.00 0.0172000 1.500 71.67 107.50                


OPP100

    DDR3               DDR2              
OPP100   OS Idle       Dhrystone       OS Idle       Dhrystone      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0093440 1.144 186.88 213.72 0.0092576 1.144 185.15 211.73 0.0080349 1.128 160.70 181.35 0.0076964 1.128 153.93 173.65
VDD_MPU 0.05 0.0054215 1.111 108.43 120.43 0.0131109 1.107 262.22 290.38 0.0052756 1.096 105.51 115.62 0.0122661 1.094 245.32 268.32
VDDS_RTC 2 0.0008667 1.798 0.43 0.78 0.0008667 1.798 0.43 0.78 0.0009001 1.797 0.45 0.81 0.0008994 1.797 0.45 0.81
VDDS_DDR 0.24 0.0253053 1.494 105.44 157.51 0.0227718 1.495 94.88 141.88 0.0051762 1.756 21.57 37.87 0.0042918 1.756 17.88 31.40
VDDS 0.24 0.0001435 1.810 0.60 1.08 0.0000412 1.810 0.17 0.31 0.0001795 1.801 0.75 1.35 0.0000818 1.801 0.34 0.61
VDDS_SRAM_CORE_BG 2 0.0027684 1.820 1.38 2.52 0.0027687 1.819 1.38 2.52 0.0027375 1.818 1.37 2.49 0.0027071 1.818 1.35 2.46
VDDS_SRAM_MPU_BB 2 0.0032579 1.820 1.63 2.96 0.0094873 1.819 4.74 8.63 0.0032028 1.818 1.60 2.91 0.0093236 1.818 4.66 8.47
VDDS_PLL_DDR 2 0.0021819 1.820 1.09 1.99 0.0021790 1.820 1.09 1.98 0.0020870 1.818 1.04 1.90 0.0020831 1.818 1.04 1.89
VDDS_PLL_CORE_LCD 2 0.0147772 1.820 7.39 13.45 0.0147669 1.820 7.38 13.44 0.0147949 1.818 7.40 13.45 0.0147650 1.818 7.38 13.42
VDDS_PLL_MPU 2 0.0040849 1.820 2.04 3.72 0.0040814 1.819 2.04 3.71 0.0040709 1.818 2.04 3.70 0.0040645 1.818 2.03 3.69
VDDS_OSC 2 0.0013896 1.820 0.69 1.26 0.0013888 1.820 0.69 1.26 0.0013529 1.818 0.68 1.23 0.0013504 1.818 0.68 1.23
VDDA1P8V_USB0/1 1 0.0162055 1.815 16.21 29.41 0.0161796 1.815 16.18 29.37 0.0181827 1.823 18.18 33.15 0.0162176 1.824 16.22 29.58
VDDA3P3V_USB0/1 2 0.0066491 3.339 3.32 11.10 0.0066463 3.339 3.32 11.10 0.0053349 3.323 2.67 8.87 0.0066372 3.324 3.32 11.03
VDDA_ADC 1 0.0004582 1.828 0.46 0.84 0.0004578 1.828 0.46 0.84 0.0004582 1.827 0.46 0.84 0.0004585 1.827 0.46 0.84
VDDSHV1 0.24 0.0000343 3.307 0.14 0.47 0.0000357 3.309 0.15 0.49 0.0000267 3.314 0.11 0.37 0.0000277 3.317 0.12 0.38
VDDSHV2 0.24 0.0007348 3.320 3.06 10.17 0.0000058 3.321 0.02 0.08 0.0004833 3.324 2.01 6.69 0.0000060 3.325 0.02 0.08
VDDSHV3 0.24 0.0000090 3.309 0.04 0.12 0.0000094 3.310 0.04 0.13 0.0000083 3.318 0.03 0.11 0.0000114 3.320 0.05 0.16
VDDSHV4 0.24 0.0000083 3.320 0.03 0.11 0.0000079 3.321 0.03 0.11 0.0000067 3.324 0.03 0.09 0.0000084 3.325 0.04 0.12
VDDSHV5 0.24 0.0000082 3.309 0.03 0.11 0.0000082 3.310 0.03 0.11 0.0004387 3.318 1.83 6.06 0.0004440 3.320 1.85 6.14
VDDSHV6 0.24 0.0024813 3.307 10.34 34.19 0.0001616 3.309 0.67 2.23 0.0026059 3.311 10.86 35.96 0.0001873 3.315 0.78 2.59
        Total 605.95     Total 721.07     Total 454.82     Total 556.88
                                   
VDDSDDRMEM 0.24 0.0168000 1.500 70.00 105.00 0.0171000 1.500 71.25 106.88                


OPP120

    DDR3               DDR2              
OPP120   OS Idle       Dhrystone       OS Idle       Dhrystone      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0093508 1.144 187.02 213.86 0.0092962 1.144 185.92 212.64 0.0080451 1.129 160.90 181.62 0.0077067 1.128 154.13 173.85
VDD_MPU 0.05 0.0071129 1.211 142.26 172.32 0.0174224 1.207 348.45 420.67 0.0069283 1.198 138.57 165.98 0.0161996 1.194 323.99 386.91
VDDS_RTC 2 0.0008672 1.798 0.43 0.78 0.0008672 1.798 0.43 0.78 0.0009001 1.797 0.45 0.81 0.0008985 1.797 0.45 0.81
VDDS_DDR 0.24 0.0252120 1.494 105.05 156.92 0.0225454 1.495 93.94 140.46 0.0051622 1.756 21.51 37.77 0.0043031 1.756 17.93 31.49
VDDS 0.24 0.0001434 1.810 0.60 1.08 0.0000413 1.810 0.17 0.31 0.0001799 1.801 0.75 1.35 0.0000815 1.801 0.34 0.61
VDDS_SRAM_CORE_BG 2 0.0027699 1.820 1.38 2.52 0.0028189 1.819 1.41 2.56 0.0027486 1.818 1.37 2.50 0.0027595 1.818 1.38 2.51
VDDS_SRAM_MPU_BB 2 0.0032718 1.820 1.64 2.98 0.0108705 1.819 5.44 9.89 0.0032285 1.818 1.61 2.93 0.0106892 1.818 5.34 9.72
VDDS_PLL_DDR 2 0.0021801 1.820 1.09 1.98 0.0021787 1.820 1.09 1.98 0.0020876 1.818 1.04 1.90 0.0020828 1.818 1.04 1.89
VDDS_PLL_CORE_LCD 2 0.0147750 1.820 7.39 13.45 0.0147691 1.820 7.38 13.44 0.0147895 1.818 7.39 13.45 0.0147552 1.818 7.38 13.41
VDDS_PLL_MPU 2 0.0047650 1.820 2.38 4.34 0.0047610 1.819 2.38 4.33 0.0047485 1.818 2.37 4.32 0.0047384 1.818 2.37 4.31
VDDS_OSC 2 0.0013891 1.820 0.69 1.26 0.0013871 1.820 0.69 1.26 0.0013516 1.818 0.68 1.23 0.0013460 1.818 0.67 1.22
VDDA1P8V_USB0/1 1 0.0161996 1.815 16.20 29.40 0.0161871 1.815 16.19 29.38 0.0181567 1.823 18.16 33.10 0.0162121 1.824 16.21 29.57
VDDA3P3V_USB0/1 2 0.0066484 3.339 3.32 11.10 0.0066408 3.339 3.32 11.09 0.0053332 3.323 2.67 8.86 0.0066333 3.324 3.32 11.02
VDDA_ADC 1 0.0004579 1.828 0.46 0.84 0.0004574 1.828 0.46 0.84 0.0004580 1.827 0.46 0.84 0.0004574 1.827 0.46 0.84
VDDSHV1 0.24 0.0000340 3.307 0.14 0.47 0.0000349 3.309 0.15 0.48 0.0000267 3.314 0.11 0.37 0.0000272 3.317 0.11 0.38
VDDSHV2 0.24 0.0007330 3.320 3.05 10.14 0.0000058 3.321 0.02 0.08 0.0005107 3.324 2.13 7.07 0.0000056 3.325 0.02 0.08
VDDSHV3 0.24 0.0000084 3.309 0.04 0.12 0.0000096 3.310 0.04 0.13 0.0000080 3.318 0.03 0.11 0.0000107 3.320 0.04 0.15
VDDSHV4 0.24 0.0000071 3.320 0.03 0.10 0.0000077 3.321 0.03 0.11 0.0000070 3.324 0.03 0.10 0.0000089 3.325 0.04 0.12
VDDSHV5 0.24 0.0000079 3.309 0.03 0.11 0.0000077 3.310 0.03 0.11 0.0004386 3.318 1.83 6.06 0.0004447 3.320 1.85 6.15
VDDSHV6 0.24 0.0025371 3.307 10.57 34.96 0.0001615 3.309 0.67 2.23 0.0025825 3.311 10.76 35.63 0.0001860 3.315 0.78 2.57
        Total 658.72     Total 852.76     Total 506.00     Total 677.59
                                   
VDDSDDRMEM 0.24 0.0168000 1.500 70.00 105.00 0.0170000 1.500 70.83 106.25                


Turbo

    DDR3               DDR2              
OPP Turbo   OS Idle       Dhrystone       OS Idle       Dhrystone      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0093692 1.144 187.38 214.33 0.0092923 1.144 185.85 212.57 0.0080535 1.129 161.07 181.77 0.0077223 1.128 154.45 174.20
VDD_MPU 0.05 0.0083439 1.276 166.88 212.90 0.0204167 1.269 408.33 518.05 0.0081135 1.260 162.27 204.42 0.0190630 1.257 381.26 479.28
VDDS_RTC 2 0.0008674 1.798 0.43 0.78 0.0008673 1.798 0.43 0.78 0.0008995 1.797 0.45 0.81 0.0008984 1.797 0.45 0.81
VDDS_DDR 0.24 0.0252026 1.494 105.01 156.85 0.0228224 1.495 95.09 142.17 0.0051599 1.756 21.50 37.76 0.0042926 1.756 17.89 31.41
VDDS 0.24 0.0001460 1.810 0.61 1.10 0.0000415 1.810 0.17 0.31 0.0001786 1.801 0.74 1.34 0.0000813 1.801 0.34 0.61
VDDS_SRAM_CORE_BG 2 0.0027944 1.820 1.40 2.54 0.0028784 1.819 1.44 2.62 0.0027607 1.818 1.38 2.51 0.0028274 1.818 1.41 2.57
VDDS_SRAM_MPU_BB 2 0.0038138 1.820 1.91 3.47 0.0119621 1.819 5.98 10.88 0.0034480 1.818 1.72 3.13 0.0116531 1.818 5.83 10.59
VDDS_PLL_DDR 2 0.0021810 1.820 1.09 1.98 0.0021797 1.819 1.09 1.98 0.0020867 1.818 1.04 1.90 0.0020827 1.818 1.04 1.89
VDDS_PLL_CORE_LCD 2 0.0147777 1.820 7.39 13.45 0.0147706 1.820 7.39 13.44 0.0147872 1.818 7.39 13.44 0.0147531 1.818 7.38 13.41
VDDS_PLL_MPU 2 0.0050134 1.820 2.51 4.56 0.0050078 1.819 2.50 4.55 0.0049932 1.818 2.50 4.54 0.0049823 1.818 2.49 4.53
VDDS_OSC 2 0.0013883 1.820 0.69 1.26 0.0013852 1.820 0.69 1.26 0.0013506 1.818 0.68 1.23 0.0013419 1.818 0.67 1.22
VDDA1P8V_USB0/1 1 0.0162181 1.815 16.22 29.44 0.0161772 1.815 16.18 29.36 0.0181803 1.823 18.18 33.14 0.0161874 1.824 16.19 29.52
VDDA3P3V_USB0/1 2 0.0066480 3.338 3.32 11.10 0.0066379 3.339 3.32 11.08 0.0053331 3.323 2.67 8.86 0.0066315 3.324 3.32 11.02
VDDA_ADC 1 0.0004577 1.828 0.46 0.84 0.0004576 1.828 0.46 0.84 0.0004577 1.827 0.46 0.84 0.0004569 1.827 0.46 0.83
VDDSHV1 0.24 0.0000350 3.307 0.15 0.48 0.0000350 3.309 0.15 0.48 0.0000270 3.314 0.11 0.37 0.0000269 3.317 0.11 0.37
VDDSHV2 0.24 0.0007582 3.320 3.16 10.49 0.0000059 3.321 0.02 0.08 0.0004817 3.324 2.01 6.67 0.0000052 3.325 0.02 0.07
VDDSHV3 0.24 0.0000092 3.309 0.04 0.13 0.0000092 3.309 0.04 0.13 0.0000076 3.318 0.03 0.11 0.0000106 3.320 0.04 0.15
VDDSHV4 0.24 0.0000072 3.320 0.03 0.10 0.0000075 3.321 0.03 0.10 0.0000073 3.324 0.03 0.10 0.0000080 3.325 0.03 0.11
VDDSHV5 0.24 0.0000084 3.309 0.03 0.12 0.0000083 3.309 0.03 0.11 0.0004389 3.318 1.83 6.07 0.0004440 3.320 1.85 6.14
VDDSHV6 0.24 0.0024947 3.307 10.39 34.38 0.0001610 3.309 0.67 2.22 0.0025536 3.311 10.64 35.23 0.0001855 3.315 0.77 2.56
        Total 700.30     Total 953.03     Total 544.25     Total 771.31
                                   
VDDSDDRMEM 0.24 0.0168000 1.500 70.00 105.00 0.0173000 1.500 72.08 108.13                


Nitro

    DDR3               DDR2              
OPP Nitro   OS Idle       Dhrystone       OS Idle       Dhrystone      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0093909 1.144 187.82 214.84 0.0093198 1.144 186.40 213.22 0.0080751 1.129 161.50 182.29 0.0077236 1.128 154.47 174.25
VDD_MPU 0.05 0.0108813 1.335 217.63 290.59 0.0265022 1.328 530.04 703.67 0.0105964 1.323 211.93 280.32 0.0248164 1.318 496.33 654.16
VDDS_RTC 2 0.0008673 1.798 0.43 0.78 0.0008682 1.798 0.43 0.78 0.0008993 1.797 0.45 0.81 0.0008970 1.797 0.45 0.81
VDDS_DDR 0.24 0.0252216 1.494 105.09 156.98 0.0226178 1.495 94.24 140.88 0.0051553 1.756 21.48 37.72 0.0042830 1.756 17.85 31.34
VDDS 0.24 0.0001450 1.810 0.60 1.09 0.0000412 1.810 0.17 0.31 0.0001780 1.801 0.74 1.34 0.0000810 1.801 0.34 0.61
VDDS_SRAM_CORE_BG 2 0.0028314 1.820 1.42 2.58 0.0029712 1.818 1.49 2.70 0.0027853 1.818 1.39 2.53 0.0028626 1.818 1.43 2.60
VDDS_SRAM_MPU_BB 2 0.0045669 1.820 2.28 4.15 0.0151347 1.819 7.57 13.76 0.0041249 1.818 2.06 3.75 0.0140857 1.818 7.04 12.80
VDDS_PLL_DDR 2 0.0021813 1.820 1.09 1.98 0.0021806 1.819 1.09 1.98 0.0020862 1.818 1.04 1.90 0.0020811 1.818 1.04 1.89
VDDS_PLL_CORE_LCD 2 0.0147762 1.820 7.39 13.45 0.0147722 1.820 7.39 13.44 0.0147791 1.818 7.39 13.44 0.0147365 1.818 7.37 13.40
VDDS_PLL_MPU 2 0.0061765 1.819 3.09 5.62 0.0061685 1.818 3.08 5.61 0.0061470 1.818 3.07 5.59 0.0061280 1.817 3.06 5.57
VDDS_OSC 2 0.0013873 1.820 0.69 1.26 0.0013828 1.819 0.69 1.26 0.0013484 1.818 0.67 1.23 0.0013366 1.818 0.67 1.22
VDDA1P8V_USB0/1 1 0.0161816 1.815 16.18 29.37 0.0161992 1.815 16.20 29.40 0.0181376 1.823 18.14 33.07 0.0161835 1.824 16.18 29.52
VDDA3P3V_USB0/1 2 0.0066431 3.339 3.32 11.09 0.0066301 3.338 3.32 11.07 0.0053313 3.323 2.67 8.86 0.0066238 3.324 3.31 11.01
VDDA_ADC 1 0.0004576 1.828 0.46 0.84 0.0004571 1.828 0.46 0.84 0.0004571 1.827 0.46 0.84 0.0004554 1.828 0.46 0.83
VDDSHV1 0.24 0.0000347 3.307 0.14 0.48 0.0000350 3.309 0.15 0.48 0.0000268 3.314 0.11 0.37 0.0000270 3.317 0.11 0.37
VDDSHV2 0.24 0.0007771 3.320 3.24 10.75 0.0000052 3.321 0.02 0.07 0.0004818 3.324 2.01 6.67 0.0000049 3.325 0.02 0.07
VDDSHV3 0.24 0.0000093 3.308 0.04 0.13 0.0000090 3.309 0.04 0.12 0.0000081 3.318 0.03 0.11 0.0000101 3.320 0.04 0.14
VDDSHV4 0.24 0.0000074 3.320 0.03 0.10 0.0000073 3.321 0.03 0.10 0.0000073 3.324 0.03 0.10 0.0000081 3.326 0.03 0.11
VDDSHV5 0.24 0.0000076 3.309 0.03 0.10 0.0000080 3.309 0.03 0.11 0.0004383 3.318 1.83 6.06 0.0004432 3.320 1.85 6.13
VDDSHV6 0.24 0.0024922 3.307 10.38 34.34 0.0001606 3.309 0.67 2.21 0.0025603 3.312 10.67 35.33 0.0001846 3.315 0.77 2.55
        Total 780.54     Total 1142.0     Total 622.31     Total 949.37
                                   
VDDSDDRMEM 0.24 0.0168000 1.500 70.00 105.00 0.0170000 1.500 70.83 106.25                

CORE OPP

CAUTION Data presented in this wiki was collected on an unsupported version of the SDK, and is provided for legacy purposes. For most recent data, please refer to the TI Processor SDK Kernel Performance Guide, Power Management section

  • Please be aware of the limitations and advisories for using OPP50, as specified in the Datasheet and Silicon Errata.
  • CORE OPP50 configured in uboot
  • Optimized IO pad configuration
  • SmartReflex disabled
  • Matrix GUI is shutdown (except for "OS Idle")
  • LCDC is disabled (except for "OS Idle", "H.264 Decode", "Mpeg4 + AAC Decode", "3D Chameleon Man")

CORE OPP50/50

    DDR2              
CORE OPP50, MPU OPP50   OS Idle       Dhrystone      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0037363 0.939 74.73 70.13 0.0034243 0.937 68.49 64.17
VDD_MPU 0.05 0.0022964 0.940 45.93 43.16 0.0053885 0.945 107.77 101.84
VDDS_RTC 2 0.0004936 1.797 0.25 0.44 0.0004933 1.797 0.25 0.44
VDDS_DDR 0.24 0.0053132 1.757 22.14 38.90 0.0037520 1.757 15.63 27.46
VDDS 0.24 0.0001460 1.801 0.61 1.10 0.0000464 1.801 0.19 0.35
VDDS_SRAM_CORE_BG 2 0.0026041 1.819 1.30 2.37 0.0026137 1.819 1.31 2.38
VDDS_SRAM_MPU_BB 2 0.0030421 1.819 1.52 2.77 0.0061184 1.819 3.06 5.56
VDDS_PLL_DDR 2 0.0016289 1.819 0.81 1.48 0.0016285 1.819 0.81 1.48
VDDS_PLL_CORE_LCD 2 0.0039718 1.819 1.99 3.61 0.0039727 1.819 1.99 3.61
VDDS_PLL_MPU 2 0.0022320 1.819 1.12 2.03 0.0022319 1.819 1.12 2.03
VDDS_OSC 2 0.0013638 1.819 0.68 1.24 0.0013623 1.819 0.68 1.24
VDDA1P8V_USB0/1 1 0.0162071 1.824 16.21 29.56 0.0162124 1.824 16.21 29.57
VDDA3P3V_USB0/1 2 0.0066494 3.324 3.32 11.05 0.0066500 3.324 3.33 11.05
VDDA_ADC 1 0.0004582 1.828 0.46 0.84 0.0004576 1.827 0.46 0.84
VDDSHV1 0.24 0.0000272 3.314 0.11 0.38 0.0000274 3.317 0.11 0.38
VDDSHV2 0.24 0.0005150 3.325 2.15 7.13 0.0000045 3.325 0.02 0.06
VDDSHV3 0.24 0.0000116 3.318 0.05 0.16 0.0000112 3.320 0.05 0.16
VDDSHV4 0.24 0.0000082 3.325 0.03 0.11 0.0000084 3.325 0.03 0.12
VDDSHV5 0.24 0.0001382 3.318 0.58 1.91 0.0001381 3.320 0.58 1.91
VDDSHV6 0.24 0.0025521 3.312 10.63 35.22 0.0001875 3.315 0.78 2.59
        Total 253.59     Total 257.24


CORE OPP50

    DDR2              
CORE OPP50   OS Idle       Dhrystone      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0037484 0.939 74.97 70.36 0.0034345 0.937 68.69 64.33
VDD_MPU 0.05 0.0052706 1.096 105.41 115.53 0.0123115 1.094 246.23 269.29
VDDS_RTC 2 0.0004928 1.797 0.25 0.44 0.0004929 1.797 0.25 0.44
VDDS_DDR 0.24 0.0053102 1.757 22.13 38.88 0.0037296 1.756 15.54 27.29
VDDS 0.24 0.0001449 1.801 0.60 1.09 0.0000462 1.801 0.19 0.35
VDDS_SRAM_CORE_BG 2 0.0025661 1.819 1.28 2.33 0.0026559 1.818 1.33 2.41
VDDS_SRAM_MPU_BB 2 0.0029987 1.819 1.50 2.73 0.0092503 1.818 4.63 8.41
VDDS_PLL_DDR 2 0.0016273 1.819 0.81 1.48 0.0016280 1.819 0.81 1.48
VDDS_PLL_CORE_LCD 2 0.0039651 1.819 1.98 3.61 0.0039673 1.819 1.98 3.61
VDDS_PLL_MPU 2 0.0040697 1.819 2.03 3.70 0.0040670 1.818 2.03 3.70
VDDS_OSC 2 0.0013633 1.819 0.68 1.24 0.0013557 1.819 0.68 1.23
VDDA1P8V_USB0/1 1 0.0161281 1.824 16.13 29.42 0.0162159 1.824 16.22 29.57
VDDA3P3V_USB0/1 2 0.0066483 3.324 3.32 11.05 0.0066442 3.324 3.32 11.04
VDDA_ADC 1 0.0004588 1.828 0.46 0.84 0.0004571 1.827 0.46 0.84
VDDSHV1 0.24 0.0000274 3.315 0.11 0.38 0.0000278 3.317 0.12 0.38
VDDSHV2 0.24 0.0004892 3.325 2.04 6.78 0.0000058 3.325 0.02 0.08
VDDSHV3 0.24 0.0000114 3.318 0.05 0.16 0.0000112 3.320 0.05 0.15
VDDSHV4 0.24 0.0000079 3.325 0.03 0.11 0.0000082 3.325 0.03 0.11
VDDSHV5 0.24 0.0001388 3.318 0.58 1.92 0.0001386 3.320 0.58 1.92
VDDSHV6 0.24 0.0025473 3.312 10.61 35.15 0.0001874 3.315 0.78 2.59
        Total 327.19     Total 429.24


CORE OPP100

    DDR3               DDR2              
CORE OPP100   OS Idle       Dhrystone       OS Idle       Dhrystone      
Power Supply Shunt [Ohm] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW] Voltage Drop [V] Voltage [V] Current [mA] Power [mW]
VDD_CORE 0.05 0.0093595 1.143 187.19 213.98 0.0092576 1.144 185.15 211.73 0.0080373 1.129 160.75 181.52 0.0077025 1.128 154.05 173.74
VDD_MPU 0.05 0.0054176 1.111 108.35 120.33 0.0131109 1.107 262.22 290.38 0.0052680 1.096 105.36 115.48 0.0123149 1.094 246.30 269.34
VDDS_RTC 2 0.0008660 1.798 0.43 0.78 0.0008667 1.798 0.43 0.78 0.0008992 1.797 0.45 0.81 0.0008988 1.797 0.45 0.81
VDDS_DDR 0.24 0.0251420 1.494 104.76 156.48 0.0227718 1.495 94.88 141.88 0.0051808 1.757 21.59 37.92 0.0042967 1.756 17.90 31.44
VDDS 0.24 0.0001431 1.810 0.60 1.08 0.0000412 1.810 0.17 0.31 0.0001468 1.801 0.61 1.10 0.0000484 1.801 0.20 0.36
VDDS_SRAM_CORE_BG 2 0.0028104 1.820 1.41 2.56 0.0027687 1.819 1.38 2.52 0.0026061 1.819 1.30 2.37 0.0027166 1.818 1.36 2.47
VDDS_SRAM_MPU_BB 2 0.0033125 1.820 1.66 3.01 0.0094873 1.819 4.74 8.63 0.0030585 1.819 1.53 2.78 0.0093426 1.818 4.67 8.49
VDDS_PLL_DDR 2 0.0021828 1.820 1.09 1.99 0.0021790 1.820 1.09 1.98 0.0020846 1.819 1.04 1.90 0.0020848 1.818 1.04 1.90
VDDS_PLL_CORE_LCD 2 0.0147823 1.820 7.39 13.45 0.0147669 1.820 7.38 13.44 0.0147780 1.819 7.39 13.44 0.0147721 1.818 7.39 13.43
VDDS_PLL_MPU 2 0.0040859 1.820 2.04 3.72 0.0040814 1.819 2.04 3.71 0.0040656 1.818 2.03 3.70 0.0040650 1.818 2.03 3.69
VDDS_OSC 2 0.0013842 1.820 0.69 1.26 0.0013888 1.820 0.69 1.26 0.0013594 1.819 0.68 1.24 0.0013505 1.818 0.68 1.23
VDDA1P8V_USB0/1 1 0.0162018 1.815 16.20 29.40 0.0161796 1.815 16.18 29.37 0.0162061 1.824 16.21 29.56 0.0162206 1.824 16.22 29.58
VDDA3P3V_USB0/1 2 0.0066459 3.338 3.32 11.09 0.0066463 3.339 3.32 11.10 0.0066482 3.324 3.32 11.05 0.0066404 3.324 3.32 11.03
VDDA_ADC 1 0.0004581 1.828 0.46 0.84 0.0004578 1.828 0.46 0.84 0.0004590 1.828 0.46 0.84 0.0004576 1.827 0.46 0.84
VDDSHV1 0.24 0.0000337 3.307 0.14 0.46 0.0000357 3.309 0.15 0.49 0.0000273 3.315 0.11 0.38 0.0000272 3.317 0.11 0.38
VDDSHV2 0.24 0.0007357 3.320 3.07 10.18 0.0000058 3.321 0.02 0.08 0.0005006 3.325 2.09 6.94 0.0000051 3.325 0.02 0.07
VDDSHV3 0.24 0.0000101 3.309 0.04 0.14 0.0000094 3.310 0.04 0.13 0.0000112 3.318 0.05 0.16 0.0000092 3.320 0.04 0.13
VDDSHV4 0.24 0.0000077 3.320 0.03 0.11 0.0000079 3.321 0.03 0.11 0.0000067 3.325 0.03 0.09 0.0000077 3.325 0.03 0.11
VDDSHV5 0.24 0.0000078 3.309 0.03 0.11 0.0000082 3.310 0.03 0.11 0.0001908 3.318 0.80 2.64 0.0001891 3.319 0.79 2.62
VDDSHV6 0.24 0.0024931 3.307 10.39 34.35 0.0001616 3.309 0.67 2.23 0.0025674 3.312 10.70 35.43 0.0001867 3.314 0.78 2.58
        Total 605.33     Total 721.07     Total 449.33     Total 554.23
                                   
VDDSDDRMEM 0.24 0.0170000 1.500 70.83 106.25 0.0171000 1.500 71.25 106.88                


Additional Power Savings

  • Disabling unused modules (USB, Ethernet, etc.)
  • Minimizing frequencies (MPU, interconnect, DDR)

References