Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

AM335x SYSBIOS Industrial SDK 01.01.00.01 Release Notes

From Texas Instruments Wiki
Jump to: navigation, search

Content is no longer maintained and is being kept for reference only!

TIBanner.png
AM335x SYSBIOS Industrial SDK 01.01.00.01 Release Notes


Sep 02, 2013

Introduction

The SYSBIOS-based software development kit (SDK) for industrial communications is designed for the Sitara AM335x ARM Cortex-A8 microprocessor family to enable customers add real-time industrial communications easily and quickly to their system. By making all the basic system software components immediately available, the Kit allows developers to focus on their application code, where they can add the most differentiation. Optimized to support real-time industrial communications protocols such as EtherCAT, Profibus, Profinet, Ethernet/IP and many others, the SDK includes a real-time, low-footprint SYSBIOS kernel with boot loader and sample industrial applications to get started quickly.


Device Support

The following devices are supported with the current release.

  • SOC's supported
    • AM335x
  • Hardware Platform Supported
    • AM335x IDK (also known as IA EVM)
    • AM335x ICE  V1/V2

Obtaining the Release Package

Documentation

The following documents are provided with this release.


What Is Supported

  • Hardware Platform
    • AM335x IDK (also known as IA EVM)
    • AM335x ICE V1/V2
  • SYSBIOS 6.35.01.29 Real Time Operating System
  • Starterware boot loader
    • Boot from MMC/SD for IDK
    • Boot from SPI flash and NOR flash for ICE
  • Starterware based drivers integrated with SYSBIOS
    • PRUSS
    • Timer
    • UART
    • GPIO
    • I2C
    • Ethernet
  • EtherCAT Slave Controller
    • Beckhoff Slave Stack Version 5.10
    • PRU Firmware load from SPI flash
    • EtherCAT Commands
    • 8 FMMU support in Firmware
    • 8 SM support in Firmware (stack support only 4)
    • 8KB process data RAM
    • Distributed clocks
      • 64-bit DC
      • SYNC0 out generation single shot and cyclic mode support
      • SYNC1 out generation - SYNC1 cycle time multiple of SYNC0 cycle time
      • Latch0 and Latch1 inputs
    • DL Loop Control
      • Using PRU-ICSS MDIO state m/c (slow)
      • Using MII_RX_LINK (fast - depending on PHY link loss detection latency)
      • Enhanced link detection support using TLK105/TLK106/TLK110 PHY RX_ERR threshold counting feature
      • Enhanced link detection in EtherCAT firmware
    • EEPROM Emulation
      • SPI flash non-volatile storage support
      • Provisions to use volatile storage for debug and development
    • Interrupts – AL/ECAT events
    • Watchdog – PDI and SM
    • Error Counters – all key counters
    • LED – Run, Error and Port0/1 activity based on firmware feedback
    • CoE, EoE, FoE and CiA402
    • Management Interface for PHY over EtherCAT
    • PHY address configuration and host side PRU-ICSS MDIO API for PHY programming
    • Redundancy support validated using PG2.x silicon
    • Application upgrade over FoE complying to SEMI TWG guidelines (not resetting PRU-ICSS)
  • PROFIBUS DP Slave Controller
    • Evaluation PROFIBUS DP slave stack library file from TMG
    • Baud rates 12M, 6M, 3M, 1.5M, 500k, 187.5k, 93.75k, 45.45k 19.2k, 9.6k
    • Telegram size Up to 244 bytes
    • DPv0 support Cyclic exchange of data and diagnosis
    • DPv1 support Acyclic/cyclic data exchange and alarm handling
    • Response time 11-bit minimum TSDR response time
    • Watchdog 10ms time base
    • Get diagnostics and extended diagnostics
  • Powerlink Slave
    • openPOWERLINK Stack Version V1.7.1.
    • Data link layer and NMT state machine for controlled nodes.
    • SDO via EPL ASND frames.
    • openMAC and openHUB
    • API for PHY programming.
    • Interoperable with B&R X20BC slaves.
    • Interoperable with openPOWERLINK master and B&R PLC (Power Panel 500)
    • Run LED
    • Cycle time till 400 us
  • EtherNet/IP
    • EtherNet/IP adapter implementation on low latency ICSS cut-thru switch as well as on Gigabit hardware switch (CPSW)
    • Integrated with Molex Ethernet/IP adapter stack Version 3.1.2 supporting the following features
      • Ethernet/IP Capabilities
        • Explicit Messaging and Implicit Messaging
        • UCMM
        • Class 1 and Class 3 Connection
      • Supported CIP Objects
        • Identity
        • Message Router
        • Assembly
        • Connection Manager
        • Ethernet Link
        • TCP/IP Interface
    • Compliant with ODVA EtherNet/IP Protocol Conformance Test Tool (Rev CT-10)
  • Sample Applications
    • HTTP Server
    • UART Echo
    • LED Control
    • EtherCAT slave
    • EtherNet/IP Adapter
    • Profibus DP Slave
    • Powerlink Slave
  • Host Development Platform And Toolchain


What Is Not Supported

  • In general, peripherals or features not mentioned as part of "What is Supported" section are not supported in this release.
  • For EtherCAT Slave Controller, the following features are not supported in this release. These are planned to be supported in upcoming releases
    • Distributed Clocks (DC)
      • System Time difference filter depth (0x934) other than 0,2,4 and 8
      • Speed Counter filter depth (0x935)- Not used by EtherCAT firmware
    • ECAT side register protection when using LRD command
    • APRW/FPRW/BRW for SM mapped area
  • For Powerlink Slave, following features are not supported in this release
    • SDO over UDP.
    • Shared Buffer functionality
    • OpenMAC doesn't have Collision detection functionality implemented yet.
  • For PROFIBUS DP Slave, the following features are not supported in this release
    • DP-V2 support for asynchronous mode and data exchange
    • PA support
    • Set_Slave_Add (SAP 55) support
  • For EtherNet/IP Adapter application
    • DLR feature
    • IEEE 1588/PTP feature
    • 10Mbps and half duplex on ICSS Switch

New In This Release

  • SDK
    • MMU configuration structure has been changed. Logical address has been removed and page attributes are combined to a single variable. 
    • Support for ICE Version 2 (V2)
    • NDK driver for CPSW and ICSS
    • Supported on CCS 5.4 with TI Tool chain.
    • New SPI Flasher which can be executed from SD card.
  • EtherNet/IP Adapter implementation using Molex stack over both ICSS cut-through switch and CPSW
  • EtherCAT
    • Bug fixes (see below)

Fixed In This Release

Issue Identifier Issue Description Status
SDOCM00103151 EtherCAT: DL status enhanced link status bit set incorrectly Fixed
SDOCM00103158 EtherCAT: Process data handling in firmware assumes SM directions instead of using direction bit in SM Control register Fixed
SDOCM00103162 EtherCAT: bsp_get_process_data_address often returns zero Fixed
SDOCM00103192 EtherCAT: Mailbox enable/disable from PDI causes incosistent mailbox state in firmware rarely Fixed
SDOCM00103295 EtherCAT: Mailbox interrupts generated for process data access in PREOP State Fixed
SDOCM00103296 EtherCAT: PDI IRQs generated on some frames without access to PD area Fixed
SDOCM00103304 EtherCAT: Shareable attribute is not set to ICSS memory due to bug in MMU config structure Fixed
SDOCM00103505 EtherCAT: Single shot SYNC signal not generated Fixed
SDOCM00103506 EtherCAT: Single shot mode for latch stops upper 32 bits of system time (0x914) after input event is triggered Fixed
SDOCM00103541 EtherCAT - Online firmware upgrade not working on PATCH mode application built with CCS 5.4 Fixed
SDOCM00103542 EtherCAT - Online firmware upgrade not working on LIB mode application when built with CCS 5.4 Fixed
SDOCM00103546 EtherCAT: Last byte not read back correctly in bitwise FMMU access of odd byte length ( > 1 byte) Fixed

Known Issues And Limitations

Issue Identifier Issue Description Workaround
SDOCM00093324 Powerlink: Connection for SDO transfer between master and slave may fail to establish sometimes None
SDOCM00093325 Powerlink: OpenHub fails to forward non-powerlink or large sized frames None
SDOCM00100922 Powerlink: Multiple slaves in a chain will not work for EVMs with PG2.x silicon None
SDOCM00098105 EtherCAT: PDI/PD watchdog counter incremented by 1 whenever PDI/PD watchdog is disabled None
SDOCM00098950 EtherCAT:LRD access on unused registers increment WKC - no register protection while using LRD None
SDOCM00097012 EtherCAT: SYNC0 jitter varies with distance of slave from reference None
SDOCM00092510 EtherCAT: Multiple FMMU access in a single datagram to a slave for process data using LRD/LWR commands Use LRW instead of LRD/LWR
SDOCM00103010 ICSS Switch - Semaphore assertion failure Exception on SYS/BIOS version 6.34.X.X and 6.35.X.X when tested with IXIA None
SDOCM00103421 Ethernet/IP:Four errors found in TCP/IP interface test while running Conformance tool None
SDOCM00103424 CPSW driver does not work in 10Mbps mode None


More details on EtherCAT known issues can be found here

Dependencies

Refer to System Requirements section in AM335x Industrial SDK Getting Started Guide.

Technical Support and Product Updates

For further information or to report any problems, contact http://community.ti.com or http://support.ti.com.