Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

AM335x Touchscreen Driver's Guide

From Texas Instruments Wiki
Jump to: navigation, search
TIBanner.png
AM335x Touchscreen Driver's Guide
Linux PSP

Introduction

Touchscreen controller on AM335x is an 8 channel general purpose ADC, with support for interleaving Touch Screen conversions for a 4-wire resistive panel. A resistive touchscreen operates by applying a voltage across a resistive network and measuring the change in resistance at a given point on the matrix where the screen is touched by an input (stylus or finger). The change in the resistance ratio marks the location on the touchscreen.

Driver Usage

Tslib

Test the working of touchscreen by using the Tslib utility. Tslib is an abstraction layer for touchscreen panel events, as well as a filter stack for the manipulation of those events. Tslib is generally used on embedded devices to provide a common user space interface to touchscreen functionality.

Environment variables

Make sure you have the following settings right.

  • export TSLIB_FBDEVICE=/dev/fb0
This is for the Fbdev device node to be used for display.
  • export TSLIB_TSDEVICE=/dev/input/touchscreen0

Execution

  • First run ts_calibrate to calibrate the touch screen.
  • You can now run ts_test application. This application helps in moving a cross-hair pattern around the LCD touchscreen. The pattern moves with your stylus movements. Also there is a draw option supported. Using your stylus you can write/draw on touchscreen.

Driver Configuration

You can enable touchscreen driver as in the kernel as follows.

Device Drivers  --->
         Input device support  --->
                  [*]  Touchscreens  --->
                           <*>   TI Touchscreen Interface

Building as Loadable Kernel Module

  • Incase if you want to build the drivers as modules, use <M> instead of <*> during menuconfig while selecting the drivers (as shown below). For more information on loadable modules refer Loadable Module HOWTO
Device Drivers  --->
         Input device support  --->
                  [*]  Touchscreens  --->
                           <M>   TI Touchscreen Interface
  • This step applies if the driver is built as module
  1. Do "make modules" to build the Touchscreen driver as module. The module should be present in "drivers/input/touchscreen/ti_tsc.ko".
  2. Load the driver using "ti_tsc.ko".