AM335x Wireless Connectivity Platform
From Texas Instruments Embedded Processors Wiki
Contents |
General Platform Description
The development platform is primarily based on the AM335x EVM kit by Mistral. A COM6M extension card provided by Murata serves as a wireless connectivity add-on.
- Key Properties
- Platform combines a AM335x EVM and a WL1271 connectivity solution
- AM335x is key catalog applications processor platforms, supported worldwide by TI Sales
- Wireless Connectivity Card which incorporates an Open source mac802.11 based module
- Supported Technologies: WLAN and Bluetooth support
- Supported OS: Linux
General Platform Block Diagram
The WL1271 connectivity solution is available in the form of a COM6M module. This board connects to the EVM main board using COM6 connector.
Because this board draws power from the Main EVM board via two sources; 1.8V VIO supply and Vbat (battery supply), no additional power source is needed to power this board.
Figure: Block diagram showing the functional interconnection between WLAN connectivity board and the OMAP EVM board.
Following table describes the AM335x Host side connection to the COM6M module
| Board Revision | Entity | AM335x Host related |
| Alpha | WLAN Enable | GPIO1_30 |
| Alpha | BT Enable | GPIO1_31 |
| Alpha | WLAN SDIO | MMC2 |
| Alpha | BT UART | ttyO1 |
| Beta | WLAN Enable | GPIO1_16 |
| Beta | BT Enable | GPIO1_21 |
| Beta | WLAN SDIO | MMC2 |
| Beta | BT UART | ttyO1 |
Connectivity Expansion Card Description & COM6M Connector Pin assignment
This daughter board contains an Murata module which is based on a WL1271 Wireless LAN and a Bluetooth combo chip.
The wireless LAN and Bluetooth share one antenna which is mounted directly on the connectivity board.
The following table shows the pin assignment from the connectivity COM6M card to the Main EVM: <COM6M Connector Pin assignment>
Getting Started Guide
Follow this link to access the Getting Started Guide that describes the HW setting, WLAN and BT drivers installation and basic connection to the WLAN AP: Getting Started Guide
See Also
Links
- AM335x Evaluation Module - page
- Com6M card - Murata web site
- Com6 Connector description
- AM335 PSP Users Guide
- AM335 U-Boot Users Guide
- Am335x Flash Programming Guide
Comments
Comments on AM335x Wireless Connectivity Platform


Is the WIFI Module included in this?
--Elkhatib 05:23, 23 December 2011 (CST)