AM35x-OMAP35x-PSP 03.00.00.04 Release Notes
From Texas Instruments Embedded Processors Wiki
Important
AM/DM37x support is included for internal development only.
AM35x-OMAP35x PSP 03.00.00.04 -
Release Notes
January 28, 2010
Document License
This work is licensed under the Creative Commons Attribution-Share Alike 3.0 United States License. To view a copy of this license, visit http://creativecommons.org/licenses/by-sa/3.0/us/ or send a letter to Creative Commons, 171 Second Street, Suite 300, San Francisco, California, 94105, USA.
Introduction
This is Release 03.00.00.04 of OMAP PSP Software Development Kit (SDK). The SDK serves to provide a fundamental software platform for development, deployment and execution of Linux based applications on Texas Instruments AM3517EVM and OMAP3EVM(OMAP35x, AM/DM37x). The Linux kernel and U-Boot software in this release are based on the following open source repositories:
| Component | Version | Base Repository | Base Tag (or commit id) |
|---|---|---|---|
| OMAP Linux Kernel | 2.6.32(Linux kernel version) | The baseline was chosen from "pm" branch of http://git.kernel.org/?p=linux/kernel/git/tmlind/linux-omap-2.6.git;a=shortlog;h=refs/heads/pm | 3fd5969a81a9324b58a1c19cf510c0da97c99565. History on "pm" branch gets rewritten and hence the commit may not be valid always. |
| U-Boot | 2009.11 | http://git.denx.de/?p=u-boot.git;a=summary | v2009.11 |
The File system is based on the Arago, version 2009.11-rc2.
The codebase for Linux kernel and U-Boot included in this release is also hosted at the following repositories:
| Component | Repository (Branch) | Baseline Tag | Release Tag |
|---|---|---|---|
| OMAP Linux Kernel | http://arago-project.org/git/people/?p=sriram/ti-psp-omap.git;a=summary (OMAPPSP_03.00.00.04) | OMAPPSP_03.00.00.04_baseline | v2.6.32_OMAPPSP_03.00.00.04 |
For detailed information on the various software components included in the release and how to use them, please refer to the User's Guide.
The kernel and U-Boot have been compiled with CodeSourcery GNU Toolchain for ARM Processors 2009-q1-203 based on GCC 4.3.3
Documentation
The User Guide provides instructions on how to use the PSP SDK package. A copy of the User Guide is included in the docs folder of the SDK package.
The datasheet included in the docs folder of the SDK package provides performance benchmarks on drivers included with the PSP SDK package.
What's Supported
SDK package includes support for AM3517 platform(AM3517EVM), OMAP35x platforms(OMAP3EVM). Support for AM/DM37x(Early adopter) has been added as part of this release.
The SDK package supports the following components:
- U-Boot supporting NAND, MMC boot modes
- X-loader supporting NAND, MMC boot modes
- Linux Kernel and device drivers.
- Audio (McBSP)
- Video Display (V4L2 and Fbdev)
- Video Capture (BT656 mode)
- Video Resizer (Only on OMAP35x, AM/DM37x)
- Ethernet
- MUSB host supporting MSC, HID and USB Audio/Video
- MUSB gadget supporting File-storage and CDC/RNDIS
- MUSB OTG supporting HNP/SRP
- EHCI host supporting MSC, HID(via a HS hub) and USB Audio/Video
- NAND
- MMC/SD/SDIO
- UART
- I2C
- TouchScreen
- SPI
- RTC
- WDT
- Keypad
- CAN - SocketCAN implementation (on AM3517)
- Power Management ICs (TPS65023 on AM3517, TPS65950 on OMAP35x, AM/DM37x)
- Audio and video examples.
- Pre-built binaries for X-loader, U-Boot, Linux kernel and filesystem.
What's Not Supported
- Following are not supported:
- U-boot (Unified binary supporting Nand/OneNand on OMAP35x platform)
- NOR support (on AM3517EVM)
Fixed in this Release
| Issue Identifier | Issue headline |
|---|---|
| SDOCM00064575 | Audio capture gives overrun error, when running in background, with suspend/resume |
Fixed in this Release - OMAP35x
| Issue Identifier | Issue headline |
|---|---|
| SDOCM00065473 | OMAP35x:Resizer: highlight document for Memory to Memory Resizer: buffer size alignment |
| SDOCM00065206 | OMAP35x:Resizer: Multi-channel operation is failing |
| SDOCM00056428 | For usecases which have audio and video decode and playback: Noise level in Display on TV increases after audio stops playing |
| SDOCM00065771 | Keypad entries changed with respect to previous version. (The S7 and S13 keys have been swapped). |
| SDOCM00065203 | MUSB (OMAP35x): MSC data read corruption when USB LAN devices interface is up |
Fixed in this Release - AM3517
| Issue Identifier | Issue headline |
|---|---|
| SDOCM00065139 | AM3517 Capture : CPU consumption is going as high as 95% in MMAP mode |
| SDOCM00062552 | AM3517 Capture : Capture is giving Greenish output [Please refer to the Sample application (saMmapLoopback.c or SaUserPtrLoopback.c) for reference] |
| SDOCM00065111 | MUSB: MUSB port is unusable with CONFIG_PM=y |
| SDOCM00062832 | MUSB: RNDIS: iperf fails to work |
| SDOCM00065129 | EHCI: Port becomes unusable when EHCI module is inserted 2nd time onward. |
New in this Release
Since version 03.00.00.03, the following features have been added:
- U-boot updated to version 2009.11
- Linux kernel updated to version 2.6.32(off /pm branch)
- Support for AM/DM37x platform (EA)
New in this Release - OMAP35x
- RTC Driver
New in this Release - AM3517
- I2C GPIO Expander Driver (TCA6416)
- WDT Driver
- KeyPad Driver
Known Issues
| Issue Identifier | Issue headline | Known Workaround(s) |
|---|---|---|
| SDOCM00065224 | Video Display: Rotation with 720P DVI output doesn't work | None |
| SDOCM00034288 | Video Display: Mirroring of RGB888 images fails | Hardware issue |
| SDOCM00034465 | Video Display: switching back and forth between ntsc and pal standard results into display corruption. | Avoid disabling display when output is on TV. |
| SDOCM00034492 | Video Capture: Interlacing artifacts observed in video sample loopback application when displayed on LCD | None |
| SDOCM00053357 | Video Display: Flicker and color corruption observed on TV Display | None |
| SDOCM00053359 | Video Display: Sharpness is reduced when image is up-scaled. | Hardware behavior: Fine tuning the scaling coeff. may give better result |
| SDOCM00053361 | Video Display: Directing any of the pipeline to TV cuts image on top left corner by few pixels. | None |
| SDOCM00053362 | Video Display: Frame rate may fall below 60Hz when rotation enabled for V4L2 driver under heavy system load. | Requires custom fine tuning of application |
| SDOCM00059300 | Video Display: Suspend/Resume is not supported when any of output is on TV (VENC). | Avoid suspend/resume when output is on TV. This issue is related to SDOCM00034465, where Venv goes out of order after multiple on-off sequence. |
| SDOCM00053412 | Standalone Resizer: Blockiness and feathering effect (at edges) are observed with 4x scaling. | Hardware behavior: Fine tuning the scaling coeff. may give better result |
| SDOCM00055541 | MUSB: Rx throughput is low when CPUIDLE is enabled | none |
| SDOCM00053644 | OTG : OPT failure for MUSB as A-devcie | Use custom patch as per details in IR |
| SDOCM00053934 | OMAP35x-Linux:USB RNDIS : Pings fail beyond packet size of 64000 bytes | none |
| SDOCM00034419 | USB-CDC/RNDIS : Device frame work and NDIS 6.0 failures are observed during DTM test execution | none |
| SDOCM00054860 | MUSB Video capture : USB capture for image size 640*480 not working with LogitechPro5000 | Use EHCI host |
| SDOCM00055317 | OMAP35x, AM/DM37x: USB ISO- Stress tests are failing(video capture, audio playback stop after a days run) | none |
| SDOCM00062599 | USB RNDIS: NFS retry observed when RNDIS module is inserted | Use built-in CDC/RNDIS driver untill issue gets fixed in Arago filesystem. |
| SDOCM00064573 | Audio capture gives overrun errors when tried using NFS | Use MMC card or ramdisk to store the captured audio files |
| SDOCM00066233 | Audio loopback sometimes fails to resume after system comes out of suspend state | Kill the loopback application and restart it. |
| SDOCM00064808 | TestBench : Capture application fails in S_FMT ioctl on both AM3517/OMAP35x | None |
| SDOCM00066405 | Build fails when CONFIG_PM is disabled in omap3_evm_defconfig | None |
Known Issues - OMAP35x
| Issue Identifier | Issue headline | Known Workaround(s) |
|---|---|---|
| SDOCM00053374 | Video Capture: Video quality issues observed with video test patterns | None |
| SDOCM00053360 | Video Display: On some EVMs that have a Micron Nand part, display quality is bad. | None |
| SDOCM00064663 | Video Display: Display doesn't work after suspending the system with "enable_off_mode=1" | None |
| SDOCM00062661 | pm: high cpu usage after 'failed' suspend | None. The issue is being tracked here with Arago Project. |
| SDOCM00066078 | MUSB: USB reset messages observed when MSC read/write and Audio loopback performed | None |
| SDOCM00066080 | OMAP35x, AM/DM37x: MUSB: System hangs while resuming with core_off enabled | None |
Known Issues - AM/DM37x
| Issue Identifier | Issue headline | Known Workaround(s) |
|---|---|---|
| SDOCM00066195 | Video Display: Issues related to DPLL4 Configuration to Video Display output | None |
| SDOCM00066196 | Video Capture: Capture fram-rate is 10-15 FPS | None |
| SDOCM00064663 | Video Display: Display doesn't work after suspending the system with "enable_off_mode=1" | None |
| SDOCM00066228 | Video Display: With enable_off_mode and Sleep_while_idle flag enabled, display goes off on every console timeout | None |
| SDOCM00066081 | AM/DM37x: MUSB: CDC: Ping beyond packet size 1470 fails | None |
Known Issues - AM3517
| Issue Identifier | Issue headline | Known Workaround(s) |
|---|---|---|
| SDOCM00066330 | Video Display: 480P DVI output mode is not working | Modify modedb.c file for hsw/vsw, should be less that 64. |
| SDOCM00066290 | Video Capture: Quality issues due to reverse A-Law table work-around in application | Hardware issue |
| SDOCM00066230 | RTC : RTC interrupt is not supported | None |
| SDOCM00065165 | MUSB (AM3517) : SRP from device is not detected by host | Start session from host side where mini-A plug is inserted. |
| SDOCM00064809 | TestBench : fbdev application fails on AM3517 due to wrong resolution configuration | None |
Installation and Usage
Please look for detailed installation and usage instructions in the User's Guide
Upgrade and Compatibility Information
To upgrade to new PSP release, simply delete the old release and extract the new release in its place.
Dependencies
Device Support
This release supports the Texas Instruments AM3517(on AM3517EVM) and OMAP35x, AM/DM37x (on OMAP3EVM Rev.G) platforms
Validation Information
Please use the Linux Functional Test Bench (LFTB) included in the release package for validating the release. Documentation on using LFTB is included in the LFTB package itself.
Versioning
This is Release 03.00.00.04 of OMAP PSP SDK product.
Technical Support and Product Updates
For further information or to report any problems, contact http://community.ti.com or http://support.ti.com.
OMAP Linux Mailing List: http://vger.kernel.org/vger-lists.html#linux-omap