AM35x Getting Started Guide
From Texas Instruments Embedded Processors Wiki
This Getting Started Guide (GSG) walks you through setting up a development system for the AM35x. You should proceed through this guide in the order listed on this page for best results. By the end of this Getting Started Guide you will have the AM35x EVM hardware set up, a Linux host development environment configured, and a Linux target booting to run some provided demonstration software. You will also have the Graphics SDK installed as well as run the provided Graphics SDK demonstration software. You should also bookmark the OMAP35x category since new articles will continue to appear here.
Contents |
AM35x EVM overview
GSG: AM35x EVM Overview provides an overview of the AM35x EVM kits.
The AM35x EVM SDK consists the following packages
- AM35x Linux Platform Support Package (PSP)
- AM35x Graphics Software Development Kit (SDK)
- AM35x Graphics Demonstration Software
Follow the sequence below to get started with the AM35x EVM
- If you do not already have a Linux host setup you might wish to refer to the following:
- Setup the AM35x Linux PSP
- For Graphics SDK setup, refer to OMAP35x_Graphics_SDK_Getting_Started_Guide
- For getting started on the graphics demos, refer to OpenGLES_Texture_Streaming_-_bc-cat_User_Guide
Reference BSP for TI Sitara AM35x MPUs - Overview
The Windows Embedded CE 6.0 R3 BSP based on the Texas Instruments Sitara™ AM35x ARM® Cortex™ A8 microprocessors (MPUs) family is designed for industrial computing applications such as industrial automation, electronic point-of-service, portable data terminals or single board computers. It also is a unified support of both AM35x and OMAP35x platform ensuring embedded device makers a smooth transition between the two architectures.
Hardware setup
GSG: AM35x EVM Hardware Setup steps you through setting up the AM35x EVM hardware.
Software setup
GSG: AM35x EVM Software Setup covers how to install the Linux tools, SDK software, and Linux Support Package for the AM35x EVM.
Additional procedures
GSG: AM35x EVM Additional Procedures covers the following useful procedures that are not necessarily part of the getting started process.
- Updating/Restoring the Flash Image provides information on Updating/Restoring the Flash Image on AM35x EVM board.
- AM35x EVM Boot from SD/MMC card provides information on creating AM35x EVM Linux boot from SD/MMC card.
- Booting the New Linux Kernel provides information on booting the AM35x EVM board.
- Alternate Boot Methods provides information on updating or restoring the kernel image on the AM35x EVM.
The following pages provide additional procedures that apply to a variety of platforms, including the AM35x:
- Setting up a TFTP Server explains how to set up a TFTP server.
Additional information
The following pages provide additional information that applies to a variety of platforms, including the OMAP35x:
- AM35x PSP Known Issues and Limitations lists issues related to the AM35x PSP.
- Texas Instruments Sitara AM35x/OMAP35x unified BSP by Adeneo Embedded