AM572x General Purpose EVM HW User Guide

From Texas Instruments Wiki
Jump to: navigation, search

Contents


Introduction

This document describes the hardware architecture of the AM572x Evaluation Module (EVM) (Part # TMDSEVM572X) which is based on the Texas Instruments AM572x processor. This EVM is also commonly known as the AM572x General Purpose (GP) EVM.


Description

The AM572x General Purpose EVM is a standalone test, development, and evaluation module system that enables developers to write software and develop hardware around an AM572x processor subsystem. The main elements of the AM572x subsystem are already available on the base board of the EVM which gives developers the basic resources needed for most general purpose type projects that encompass the AM572x as the main processor. Furthermore, additional, "typical" type peripherals are built into the EVM such as memory, sensors, LCD, Ethernet PHY, etc. so that prospective systems can be modeled quickly without significant additional hardware resources.

The following sections give more details regarding the EVM.


EVM System View

The System View of the AM572x General Purpose EVM consists the Processor Module and LCD Module stacked together and connected through SMT connectors (Camera Module, TMDSCM572x, is optional and it must be purchased separately). See the pictures below of the EVM.

EVM modules.png


Figure 1: AM572x General Purpose EVM



Schematics/Design/Errata Files

  • HW Documentation - Schematics, Design Files, and other related HW Documentation
Be sure to view the Errata document for important notes


Other Useful Links


Important Usage Notes

Isolated Power Supply

An isolated Power Supply (GND sleeve of DC barrel not shorted to earth GND) must be used. Refer to "Power Source" section of this wiki for additional Power Supply requirements.


Powering On EVM

If the PMIC needs to be on for more than 7 sec without SD boot image (i.e. connecting with CCS), a zero ohm shunt can be installed in J5.

CAUTION: Do not leave the board on without first either:
  • Booting using the Linux SDK boot image, or
  • Booting using the RTOS SDK boot image (using SBL), or
  • Connecting to CCS and running the AM572x GEL file (using fast JTAG connection such as XDS560)
This is required because the AM57x device has limited Power-On-Hours without releasing eMMC contention after reset. Refer to the Device Silicon Errata (i863) for more details.


A boot option was added to silicon revision 2.0 which allows the user to disable internal pull-down resistors on the eMMC signals and avoid the issue. However, this option was not implemented on the earlier AM572x GP EVMs even though they contain silicon revision 2.0 devices with this option. All TMDXEVM5728 and TMDSEVM572X revisions earlier than A3a, have the SYSBOOT[15] input pulled low which doesn’t disable the internal pull-down resistors on the MMC2 terminals. To disable the internal pull-down resistors without software intervention, remove R432 and install R197 which pulls SYSBOOT[15] high, and install external 47k ohm resistors into positions R250, R251, R252, R253, R254, R255, R256, R257, R258, and R259. This should be done if you plan to have power applied to the AM572x GP EVM for long periods of time without software properly initializing the internal pull resistors.


There is one additional concern with adding a shunt to J5. The Linux image for the AM572x GP EVM contains thermal management code that will automatically turn off power to the AM572x GP EVM if it detects a dangerous junction temperature. When a shunt is installed in J5, software will not be able to power off the EVM and you run the risk of damaging the processor if you are not providing an alternate thermal management solution.



Powering Off EVM

Do NOT remove the DC power jack to turn off the board, as it may cause damage.
The proper procedure to power down the board is as follows:
  1. Use software to gracefully power off (e.g., in Linux, use the "poweroff" command).
  2. If unable to use software (e.g., software has crashed or does not have a shut down command), press the power button for at least 15 seconds until the power LED (D3) turns off.
If you need to remove the DC power jack:
  1. Follow above steps to gracefully power down the board.
  2. Disconnect AC power cord from the power brick.
  3. Wait several seconds until the DC LED (D41) turns off (the power brick discharges its voltage).
  4. Disconnect DC barrel of power brick from the board's DC jack.


Removing Processor and LCD Module Boards

Frequent removal and reattaching of the LCD Module should be avoided. The LCD Module connectors are spec'ed an insertion/extraction lifetime of 500 times.
The proper procedure for removing the LCD Module is as follows:
  1. Unplug from power
  2. Lift straight up at arrows on the LCD Module
  3. "Unzip" connectors lengthwise, not back and forth. Removing the LCD Module with a back and forth motion (i.e. perpendicular to long edge of connectors), may damage the connectors.
The proper procedure for reattaching the LCD Module is as follows:
  1. Unplug from power
  2. Place LCD Module face down on a flat surface
  3. Align connectors on Processor Module with those on LCD Module
  4. Push down on all four connectors evenly to attach Processor Module


Removing Camera Module Board

The proper procedure for removing the Camera Module is as follows:
  1. Unplug from power
  2. Either "unzip" along long edge or pull straight up at connector ends. Removing the Camera Module with a back and forth motion (i.e. perpendicular to long edge of connectors), may damage the connector.


Caution: Hot Surface

The Processor Module can get extremely hot. Observe the caution hot icon in silk screen next to processor, and never touch the heatsink without feeling if its hot first.

Hot Icon.png


Figure 2: Caution Hot Icon on Processor Module board



System Description

System Board Diagram

The complete AM572x General Purpose EVM is partitioned across three different boards for modularity.

The GP EVM consists of the Processor Module (processor and peripherals), LCD Module (LCD, touchscreen, and peripherals), and the Camera Module (CM).

AM572X GP EVM Overview.png


Figure 3: AM572x GP EVM Key Components


Processor

The AM5728FCBGA processor is the central processor to this EVM. All the resources on the board surround the AM5728 processor to provide development capabilities for hardware and software. See the AM5728 datasheet and TRM for the details about the processor.

There are system configuration signals, SYSBOOT, that can be set on the EVM to define some startup parameters on the AM572x processor. See the Configuration/Setup section later for more details.


Clocks

The EVM has several clocks to support the AM5728 processor.

The main clock for the processor is derived from a 20MHz crystal. An on-board oscillator in the AM5728 generates the base clock and subsequent module clocks as needed within the AM5728 processor. An Auxiliary Oscillator in the AM5728 generates 22.5792MHZ (evenly divides to 44.1KHz and 180.6336MHz).


Reset Signals

RSTOUTn is a warm reset generated by AM572x (RSTOUTN signal). Whenever driven low, it generates a PORZ pulse causing a power-on-reset.

CPU_POR_RESETn is asserted by the reset pushbutton (S2) and is used to force a reset of the AM572x.

PMIC_RESET_OUT is controlled by the PMIC and is used to hold the AM572x in PORZ until all power supplies are ramped and/or stable.



Power System

This section describes how the power supply will be implemented.

Power Source

A power supply with the following specs is included with the AM572x Evaluation Module:

  • 5A output
  • Positive inner and negative outer terminals
  • Female barrel with 2.5mm tuning fork inner contact and 5.5mm outer diameter contact
  • Isolated power supply


CUI Isolated Power Supply.png


Figure 4: Isolated Power Supply


The push button S1 near to the power cable is used for power ON/OFF. The main power is off until the push button is pressed. After pressing the S1 push button, the main power stays on for 7 seconds then powers off. To keep the power on, see the "Important Usage Notes" section of this wiki. Holding the push button for 15 seconds will forcably turn the main power off.


NOTE

:* Do not remove the DC power jack to turn off the board, as it may cause damage.
  • The proper power down procedure is documented in the "Important Usage Notes" section of this wiki.



Power adapter plugged in.JPG


Figure 5: AM572x GP EVM DC Power Jack



The AM572x Processor Module also includes a connector for a Lithium CR1220 non-rechargeable battery for powering a battery back external Real Time Clock (RTC) MCP79410.

  • The CR1220 battery is NOT included with the AM572x Evaluation Module and needs to be purchased separately, if the MCP79410 is required.
  • This battery should only be replaced by a trained technician.
  • If the battery is installed, R416 must first be removed to avoid shorting the battery.



Power Nets

The power nets used in the AM572x Processor Module schematics are listed in the below tables.

Net Description
12V Main board supply voltage. Supplies all other voltages including LCD module. There is a 5A fuse from DC jack to board. Powered when DC jack connected. Note that the DC LED (D41) indicates power.
LDO_VRTC Always on PMIC voltage for control signals (boot0/1), AM572x RTC bias and RTC oscillator analog power supply. Supplied by PMIC LDOVRTC_OUT. Powered when DC jack connected.
5V0 5V supply to the PMIC (LDO7USB_IN1, LDOUSB_IN2, LDO12_IN), LEDS, HDMI, and the expansion headers. Powered when DC jack connected. TPS54531 switching regulator supply rated at 4A.
USB_5V Dedicated supply for USB3.0 ports. Supplied by 12V. TPS54531 switching regulator rated at 4A. Ramps during PMIC power sequence.
PS_3V3 Supplies PMIC LDOs & SMPS rails (LDO34_IN, LDO9_IN, LDOLN_IN, SMPS1-9 rails), also supplies VDD_3V3. Powered when DC jack connected. TPS54531 switching regulator supply rated at 4A.
VDD_3V3 Main I/O rail for the board and the expansion headers. Ramps during PMIC power sequence (with regen1). Load switch from PS_3V3. Supplies AM572x VDDSHV1, VDDSHV2, VDDSHV3, VDDSHV4, VDDSHV6, VDDSHV7, VDDSHV9, VDDSHV10, VDDSHV11 rails.
VDDA_1V8_PHYA Supplies AM572x PHYs (VDDA_SATA, VDDA_USB3). Supplied by PMIC LDO3_OUT. Ramps during PMIC power sequence.
VDDA_1V8_PHYB Supplies AM572x PHYs (VDDA_HDMI, VDDA_PCIE0, VDDA_PCIE1, VDDA_PCIE). Supplied by PMIC LDO4_OUT. Ramps during PMIC power sequence.
VDD_SHV5 Supplies AM572x RTC Power Group. Supplied by PMIC LDO2_OUT.
VDD_SD Supplies AM572x SD card IOs, pull-ups for SD card. Supplied by PMIC LDO1_OUT.
VUSB_3V3 Supplies AM572x USB 3.3V analog power supplies. Supplied by PMIC LDOUSB_OUT.
VDD_RTC Supplies AM572x RTC domain. Supplied by PMIC LDO9_OUT.
VDDA_1V8_PLL Analog supply for GPU, DEBUG, DDR, VIDEO, IVA, DSP, GMAC_CORE, MPU, ABE_PER. Supplied by PMIC LDOLN_OUT.
VDD_MPU Supplies AM572x VDD_MPU rails. Supplied by PMIC SMPS1 & SMPS2, AVS voltage.
VDD_DDR Supplies AM572x VDDS_DDR rails & DDR3L DRAMs. Supplied by PMIC SMPS3, PMIC boot1 pin selects 1.5V or 1.35V (default).
VDD_DSP Supplies AM572x VDD_DSP, VDD_IVA, VDD_GPU. Supplied by PMIC SMPS4 & SMPS5, AVS votage.
VDD_CORE AM572x core supply voltage. Supplied by PMIC SMPS, AVS voltage.
VDD_1V8 Supplies AM572x vdds18v rails. Supplied by PMIC SMPS8.

Table 1: AM572x Processor Module Power Nets



Net Description
12V From by PM board expansion connectors.
5V Supplies 5V0 through load switch. From by PM board expansion connectors.
VDD_3V3 Main I/O rail for the board. From by PM board expansion connectors, camera, push buttons, SATA redriver, touchscreen controller, board ID EEPROM, control signals, signal buffers & level shifters.
PS_3V3 Supplies mSATA & mPCIe connectors Supplied by 12V.
5V0 Source supply for LCD voltages, LCD backlight boost converter, load switch from 5V. Enabled with VDD_3V3. Ramps during PMIC power sequence.
PCI_1.5V PCIe 1.5V supply. Supplied by PS_3V3.
Thin film transistor (TFT) LCD display voltages sourced by TPS65105:
VCOM LCD Common voltage, 3.96V
VDD LCD DVDD P Power for Digital Circuit, 3.3V
VGH LCD Gate ON Voltage, 17.75V
VGL LCD -8.5V supplied by negative charge pump of TPS65105
AVDD LCD Power for Analog Circuit, 9.64V
VLED+ LCD LED backlight power (Anode), 9.6V (9.9max)
VLED- LCD LED backlight power (Cathode)

Table 2: AM572x LCD Module Power Nets


Net Description
VDD_3V3 Main I/O rail for the board. Supplied by LM board (from expansion connectors).
VDD_2V8 Analog and IO voltage for MT9T111 image sensor. From 3.3V level shifter. Supplied by VDD_3V3, 2.8V
VDD_1V8 Digital voltage for MT9T111 image sensor. From 3.3V level shifter. Supplied by VDD_3V3.

Table 3: AM572x Camera Module Power Nets


The power sequencing requirements of the AM572x processor (see the AM572x datasheet) are handled automatically by the TPS659037 PMIC.


Power Management IC Power Supplies

The AM572x Processor Module uses the TPS659037 power management IC with the following power supply configuration.


TPS659037 Power Supply AM572x Power Rail Schematic Net Name Voltage
SMPS1/2 VDD_MPU VDD_MPU 1.10V at reset
SMPS3 VDDS_DDR1/2 VDD_DDR 1.35V for DDR3L
SMPS4/5 VDD_DSPEVE,
VDD_GPU,
VDD_IVA
VDD_DSP 1.06V at reset
SMPS6 VDD VDD_CORE 1.06V at reset
SMPS7 SW configuration after boot
SMPS8 VDDS18V,
VDDS18V_DDR1/2
VDD_1V8 1.8V
SMPS9 SW configuration after boot
LDOUSB_OUT VDDA33V_USB1/2 VUSB_3V3 3.3V I/O
LDOVRTC_OUT VDDA_RTC LDO_VRTC 1.8V
LDOVANA_OUT Ground GND
LDO1_OUT VDDSHV8 VDD_SD 3.3V
LDO2_OUT VDDSHV5 VDD_SHV5 3.3V
LDO3_OUT VDDA_USB1/2/3,
VDDA_SATA
VDDA_1V8_PHYA 1.8V
LDO4_OUT VDDA_HDMI,
VDDA_PCIE,
VDDA_PCIE0/1
VDDA_1V8_PHYB 1.8V
LDO9_OUT VDD_RTC VDD_RTC 1.0V
LDOLN_OUT VDDA_ABE_PER,
VDDA_DDR,
VDDA_DEBUG,
VDDA_DSP_EVE,
VDDA_GMAC_CORE,
VDDA_GPU,
VDDA_IVA,
VDDA_VIDEO,
VDDA_MPU,
VDDA_OSC
VDDA_1V8_PLL 1.8V
LDO7USB_IN1/2 - 5V0 5.0V
LDO12_IN - 5.0V 5.0V
LDO32_IN/_1 - PS_3V3 3.3V
LDO9_IN - PS_3V3 3.3V
LDOLN_IN - PS_3V3 3.3V

Table 4: AM572x Power supplies from TPS659037



APM Sense Resistors

The AM572x Processor Module has the following sub-systems with current sense resistors. These resistors allow the power to be monitored on each supply rail to check AM572x power requirements during real time software execution. All supply rails with sense resistors have their test points located on headers P2 and P3 so that they can be read easily by a multimeter or connected to a TI INA226 current and power monitor. The value of the resistors are selected to provide the best dynamic range when using a TI INA226 EVM.


Board Resistor Voltage Net Sense Resistor Value
R34 VDD_MPU 0.01ohm
R35 VDD_DSP 0.01ohm
R36 VDD_CORE 0.02ohm
R1 PS_3V3 0.01ohm
R7 5V0 0.01ohm

Table 5: AM572x Baseboard APM Sense Resistors



Configuration/Setup

Boot and emulation setup

The AM572x boot mode sequence is selected via three jumpers on the board (J3, J4, J6).

There are three boot mode options (described below) supported by this board.

OPTION 1 Boot Order:
  1. SD Boot. This mode will boot from the microSD slot. It can be used to override what is on the eMMC device or to program the eMMC when used in the manufacturing process or for field updates.
  2. eMMC Boot. This is the default boot mode, if the microSD is NOT inserted, and will allow for the fastest boot time.
OPTION 2 Boot Order:
  1. UART Boot. The EVM is hardwired to boot from UART3 in this mode. Note the Linux debug serial boot also uses this same UART port and pinmuxing.
OPTION 3 Boot Order:
  1. SATA Boot. This mode will boot from the eSATA connector. This mode can be used to override what is on the microSD.
  2. SD Boot. This mode will boot from the microSD slot.


The table below summarizes the jumper configuration for the three bode mode sequence options supported by the board.

Option Header Jumper on Pin 1-2 Jumper on Pin 2-3
Option1 J3 X
J4 X
J6 X
Option2 J3 X
J4 X
J6 X
Option3 J3 X
J4 X
J6 X

Table 6: Jumper Configuration for Boot Mode Selection

Emulation and Hardware setup

For complete list of supported emulators and hardware configuration required to connect to the GP EVM using CCS refer to the Hardware setup guide here: AM572x GP EVM Hardware Setup


I2C Address Assignments

In the AM572x GP EVM boards, each separate board has an I2C ID memory that contains the details of the identity of that board such as it's configuration, etc. (see sections below for more details on the memories' contents).


AM572x Processor Module Function AM572x I2C Port Address
Processor Module ID memory I2C1 0x50
AM572x PMIC Control I2C1 0x58 (Power registers),
0x59 (Interfaces and auxiliaries),
0x5A (Trimming and test),
0x5B (OTP),
0x12 (DVS)
Temperature Sensor I2C1 0x48
AIC3104 Audio codec I2C1 0x18
Real Time Clock I2C3 0x6F (SRAM & RTCC access),
0x57 (EEPROM access)
USB 3.0 Hub I2C3 0x50

Table 7: AM572x Processor Module I2C Bus Addresses


AM572x LCD Module Function AM572x I2C Port Address
LCD Module ID memory I2C5 0x50
Touchscreen Connector for OSD Display I2C5 0x5C


Table 8: AM572x LCD Module I2C Bus Addresses

AM572x Camera Module Function AM572x I2C Port Address
Camera I2C3 0x3C

Table 9: AM572x Camera Module I2C Bus Addresses


I2C ID Memory

The Processor Module and LCD Module boards each have a dedicated I2C EEPROM which contains specific identity/configuration information for that board. In addition, there is available space in each memory for user specific configuration information.

The part number of the memory device is pn#CAT24C256WI-G.

Name Size (bytes) Contents
Header 4 MSB 0xEE3355AA LSB
Board Name 8 Name for board in ASCII "AM572PM_" = AM572x GP EVM Processor Board
Version 4 Hardware version code for board in ASCII "A.20" = rev. A2
Serial Number 12 Serial number of the board. This is a 12 character string which is:

WWYY4P55nnnn where: WW = 2 digit week of the year of production YY = 2 digit year of production nnnn = incrementing board number

Configuration 32 Codes to show the configuration setup on this board. Reserved.
Reserved 6 Reserved
Reserved 6 Reserved
Available 32696 Available space for other non-volatile codes/data

Table 10: AM572x Processor Module EEPROM Data


Name Size (bytes) Contents
Header 4 MSB 0xEE3355AA LSB
Board Name 8 Name for board in ASCII "AM572LM_" = AM572x GP EVM LCD Board
Version 4 Hardware version code for board in ASCII "A.20" = rev. A2
Serial Number 12 Serial number of the board. This is a 12 character string which is:

WWYY4P57nnnn where: WW = 2 digit week of the year of production YY = 2 digit year of production nnnn = incrementing board number

Configuration 32 Codes to show the configuration setup on this board. Reserved.
Reserved 6 Reserved
Reserved 6 Reserved
Available 32696 Available space for other non-volatile codes/data

Table 11: AM572x LCD Module EEPROM Data




Processor Module Functional Block Descriptions

This section describes major functional blocks of the AM572x EVM Processor Module System.


Memory

Described in the following sections are the four memory devices found on the board.

4KB EEPROM (Board Identity Memory)

The Processor Module and LCD Module boards each contain a single 4KB EEPROM provided on I2C1 that contains the board specific information and allows the processor to automatically detect which board is connected and the version of that board. Other hardware specific data can be stored on this memory device as well. The WP pin on the EEPPROM device should be pulled to GND before writing to the device. Note that over writing the pre-programmed data in the EEPROM will inhibit TI software from running as-is.

The part number of the memory device is pn#CAT24C256WI-G. See the Configuration/Setup section for details on the data in this memory.


2GB DDR3L

The Processor Module contains four 4 Gb (256M x16) of DDR3L SDRAM memories from Kingston. The part number for the DDR3L SDRAM memory used is D2516EC4BXGGB. The AM572x has two 32 bit memory buses with two DDR3L devices on each bus.

A regulator is implemented on the Processor Module that handles the VTT voltage rail. The regulator creates the voltage for the termination circuits and the DDR_VREF level as well. This regulator supplies the required functions for both of the DDR3L banks on the Processor Module. Termination resistors are used.


eMMC Flash Memory

A single Kingston 4GB eMMC Flash Memory is on the Processor Module and can be used for booting and non-volatile storage. The eMMC device connects to the MMC2 port of the processor, allowing for 8-bit wide access.


MicroSD (MMC1) Connector

The MMC1 connector on the Processor Module is an ALPS card socket #SCHA5B0200. This is a standard SD/MMC Card type of connector. It is connected to the MMC1 port of the AM572x processor. Check the AM572x data sheet and TRM for supported card types/densities.



Temperature Sensor

A TI TMP102A temperature sensor on the Processor Module is used to report ambient temperature near the processor. It is controlled by I2C and is configured for an I2C slave address of 0x48.

The sensor is connected to the I2C1 bus on the processor. The alert pin that indicates that the temperature has exceeded the configurable limit is connected to GPIO7_16 on the processor.



Real Time Clock

A battery back external Real Time Clock (RTC) MCP79410 is provided to keep the current clock active while the board is powered down. It can be used in conjunction with the internal Real Time Clock of the processor which will reset when power is removed from the board.

In addition to the typical RTC functions, the MCP79410 device has 64 bytes of battery backed RAM and 1Kb of EEPROM.


The MCP79410 RTC IC will only keep time when RTC coin battery is installed. The AM572x GP EVM does not ship with a coin battery. However, the Processor Module includes connections for a CR1220 non-rechargeable battery that is capable of supplying 35mAh of backup power and is sufficient to keep the RTC active for a couple of years.

The CR1220 battery must be installed by a trained technician. When installing the CR1220, make sure to remove R416 that shorts across the battery. R416 is needed for MCP79410 to operate without a battery. After the battery is installed, make sure to not short the battery by placing the board on a conductive surface when not in use, as the RTC time will be lost.



10/100/1000 Ethernet

The AM572x GP EVM has two 10/100/1000 Ethernet transceiver from Micrel(KSZ9031RN) that is connected to a dual RJ45 (P5) connector. The two Ethernet interfaces are connected to the switch inside the AM572x processor.

The reset on the transceivers are driven by the board system reset signal ENET0/1_PORZ. A 25MHz crystal drives the clock input of the KSZ9031RN Ethernet PHY.

The PHY address on the MDIO bus is set to 0x00h.



USB

The Processor Module connects the AM572x USB1/USB2 ports as follows:

  • AM572x USB1 port (capable of USB 3.0 SuperSpeed) --> USB 3.0 hub w/ 3 downstream ports
  • AM572x USB2 port (limited to USB 2.0 High-Speed) --> microUSB B connector (Client mode only)

The AM572x USB1 port has its USB_ID pin (GPIO7_25) pulled low for host mode. The three downstream ports of the USB 3.0 hub attached to the AM572x USB1 port are connected to a single port USB 3.0 A connector and a stacked, two port USB 3.0 A connector.

The AM572x USB2 port has its USB_ID pin (GPIO7_24) pulled high for client, or device, mode. By default, the USB2 port is routed to a microUSB client port (P7) on the Processor Module. Alternatively, the AM572x USB2 signals are also available on the expansion connectors for use with an expansion board. To route the USB2 port to a custom daughter board on the expansion connector, remove R210 & R211 and populate R314 & R315 with 0-ohm resistors. To support host mode or OTG, VBUS 5V must be supplied by the custom daughter board.



Audio

There are two sources of audio on the Processor Module:

  1. the HDMI interface, or
  2. via two stereo jacks on the board that are connected to the AIC3104 CODEC

This section covers the stereo CODEC. The HDMI interface is covered in the following section.


The AIC3104 CODEC is controlled from AM572x by I2C which is at address 0x18 and is connected to the McASP3 I2S interface on the AM572x processor. The AIC3104 requires a master clock (MCLK) that is supplied by the processor using the AM572x CLKOOUT2 pin. Depending on the requirements, this clock can be any range from 512KHz to 50MHz. The most likely frequencies to be used are 12MHZ, 13MHZ, 16MHz, 19.2MHZ or 19.68MHZ. Additionally, the RSTOUTn signal provides a reset to the AIC3014 whenever the system is reset.



HDMI

A single HDMI interface is provided direct from the processor. The Processor Module supports level translation from 3.3V to 5V for the HDMI interface.

A standard (not mini) HDMI connector is implemented on the Processor Module.



eSATA

A switch is used to direct the SATA signals to the onboard eSATA connector or to the expansion header, where they are routed to the mSATA connector on the LCD Module. If the signal on the expansion header, P19-4, is left open, the signals go to the eSATA onboard connector. If the pin is grounded via the SATA_SEL jumper (J1) on the LCD Module, the switch is activated and the signals are routed to the expansion headers.

The eSATA interface on the Processor Module is a combination of two separate interfaces, SATA and USB. The eSATA port can be used as an eSATA or a USB 2.0 port. The USB signals originate from the USB 3.0 HUB. The SATA interfaces originate from the AM57xx processor via the switch.

Power for the eSATA is from the USB power pins, 5V. Power is routed to the eSATA connector via the TPS2560 FET switch. It is capable of providing the 500mA required by the eSATA connector. Only 5V is supplied.

NOTE that when J1 on the LCD Module is installed (for mSATA), the eSATA on the Processor Module will no longer function. However, the connector can still function as a USB 2.0 port.



Serial Debug Header

The Processor Module has a 6-pin Serial Debug Header that enables the AM572x UART3 to be used as a serial debug port. It provides TX, RX, and ground signals. An isolation buffer (SN74LVC2G241) is located between the SoC and header to prevent the signals from being fed back into the processor when the board is powered off.

The UART TX and RX signals provided to this header are 3.3V level. In order to connect them to a PC, a USB to serial converter is required. A common converter is the FTDI USB to TTL cable (TTL-232R-3V3). However, make sure to use the 3.3V version and not the 5V version.



AM572x EVM LCD Module Functional Block Descriptions

This section describes major functional blocks of the AM572x EVM LCD Module System.


LCD Screen

The LCD is a OSD 7in WVGA (800x480) RGB LCD panel part number #OSD070T1718-19TS v1 3. It is a 24bit RGB TFT LCD with 21 white LED's for backlight (controlled by one power regulator). The connector is FPC 50pin pn #XF3M-5015-1B.

The LED backlight on the LCD is controlled by a TPS61080 PWM controlled LED driver.



Capacitive Touch Screen

The Pixcir Tango C48 touchscreen is integrated into the OSD070T1718-19TS v1 3. It supports multi-touch for 5 fingers using the I2C interface.



mSATA

There is a single mSATA connector on the backside of the LCD Module for use with SSD drives.

Only one SATA interface exists on the Processor Module. In order to use this interface on the LCD Module, SATA_SEL jumper (located on the LCD Module) must be installed. This switches the SATA mux on the Processor Module to the expansion connectors. When the SATA_SEL jumper (J1) is installed, the eSATA on the Processor Module will no longer function. However, the connector can still function as a USB 2.0 port.



miniPCIe

The miniPCIe (single lane) connector is identical to the mSATA connector. However, different pins are used.

miniPCIe can support several different functions such as WLAN/WIFI, Ethernet, Video, Analog, GPS, and Memory.



COM8 Interface – Mobile Connectivity Expansion Connector

A single COM8 connector and interface is provided on the LCD Module. This connector is intended to facilitate the plugging in of TI WiLink8 type devices for the addition of a Wi-Fi interface. The COM8 connector is a Samtec card edge type connector pn# MEC. This connector thus supports TI WiLink8 types of boards, and more details about this connector can be found in the TI WiLink8 board documents.

The COM connector requires on 3.6V on the power supply. Thus a TPS74801 LDO regulator is used to provide this voltage supply from the base 5.0V supply. The signals on the COM board are all 1.8V voltage level. Thus voltage translators are placed to convert to/from 3.3V of the AM572x rail for a particular signal which is running at 3.3V.

The TI WiLink8 evaluation modules have a built-in antennae. However, the LCD Module has holes cut to accommodate a custom board with antennae if needed.



AM572x EVM Camera Module Functional Block Descriptions

This section describes major functional blocks of the AM572x EVM Camera Module System.


Camera

The Camera Module uses the Leopard Imaging LI-3M02CM 3MP imager. The imager uses the Aptina MT9T11 sensor module.

Level shifters and buffers are provided on the Camera Module to interface to the 3.3V of the expansion headers.

Control signals from the Processor Module controls the module. These include I2C, oscillator, and power down. A dedicated 32MHz oscillator is provided to the CMOS Imager.



Board Connectors

The pinout details of all the connectors used in the GP EVM are provided below.

Gigabit Ethernet - P5 (Processor Module)

Pin No Signal Name Description
1 P1_TRD[0]P Data 0 +ve
2 P1_TRD[0]N Data 0 -ve
3 P1_TRD[1]P Data 1 +ve
4 P1_TRD[1]N Data 1 -ve
5 P1_TRD[2]P Data 2 +ve
6 P1_TRD[2]N Data 2 -ve
7 P1_TRD[3]P Data 3 +ve
8 P1_TRD[3]N Data 3 -ve
9 NC No Connect
10 GND Ground
11 P0_TRD[0]P Data 0 +ve
12 P0_TRD[0]N Data 0 -ve
13 P0_TRD[1]P Data 1 +ve
14 P0_TRD[1]N Data 1 -ve
15 P0_TRD[2]P Data 2 +ve
16 P0_TRD[2]N Data 2 -ve
17 P0_TRD[3]P Data 3 +ve
18 P0_TRD[3]N Data 3 -ve
19 NC No Connect
20 GND Ground
D1 E1_GRN Cathode of LINK LED
D2 VDD_3V3 Anode of LINK LED
D3 E1_YEL Anode of ACT LED
D4 VDD_3V3 Cathode of ACT LED
D5 E0_GRN Cathode of LINK LED
D6 VDD_3V3 Anode of LINK LED
D7 E0_YEL Anode of ACT LED
D8 VDD_3V3 Cathode of ACT LED
M1 NC No Connect
M2 NC No Connect
SHLD1 DGND Ground
SHLD2 DGND Ground
SHLD3 DGND Ground
SHLD4 DGND Ground

Table 12: AM572x Gbit Ethernet Pin Details


eSATA / USB - P6 (Processor Module)

The 4th port of the Processor Module's USB 3.0 hub is connected to P6 and is limited to USB 2.0 (High-speed).

Pin No Signal Description
1 USB4VBUS USB Hub Port 4 5V Supply
2 USB_DM3 USB Hub Port 4 High-speed Transceiver (Negative)
3 USB_DP3 USB Hub Port 4 High-speed Transceiver (Positive)
4 GND1 Ground
5 GND2 Ground
6 eSATA_T+ eSATA Data Transmit (Positive)
7 eSATA_T- eSATA Data Transmit (Negative)
8 GND3 Ground
9 eSATA_R- eSATA Data Receive (Negative)
10 eSATA_R+ eSATA Data Receive (Positive)
11 GND4 Ground
M1 NC No Connect
M2 NC No Connect

Table 13: eSATA Connector Pin Details


USB

AM572x USB2 (USB 2.0 Client) - P7 (Processor Module)

Pin No Signal Name Description
1 USB2_5V AM572x USB2 5V Supply
2 USBSP_DM AM572x USB2 High-Speed Transceiver (Negative)
3 USBSP_DP AM572x USB2 High-Speed Transceiver (Positive)
4 ID Not connected (USB device/client mode only)
5 DGND Ground

Table 14: AM572x USB2 (USB 2.0 Client)


AM572x USB1 (USB 3.0 Host) - P13, P15 (Processor Module)

The AM572x USB1 port supports USB 3.0 speeds and is connected to a 4-port USB 3.0 hub. Three are accessible on the USB 3.0 Host ports while the fourth is located in the eSATA/USB combination port and is therefore limited to USB 2.0.

Pin No Signal Name Description
1 USBxVBUS USB Hub Port 0 5V Supply
2 USB_DM0 USB Hub Port 0 High-speed Transceiver (Negative)
3 USB_DP0 USB Hub Port 0 High-speed Transceiver (Positive)
4 GND Ground
5 USB_RXM0 USB Hub Port 0 SuperSpeed Receiver (Negative)
6 USB_RXP0 USB Hub Port 0 SuperSpeed Receiver (Positive)
7 GND Ground
8 USB_TXM0 USB Hub Port 0 SuperSpeed Transmitter (Negative)
9 USB_TXP0 USB Hub Port 0 SuperSpeed Transmitter (Positive)
10 P13P15_SHLD Shield
11 P13P15_SHLD Shield

Table 15: USB 3.0 Hub Port 1 (AM572x USB1 Port) - P13


Pin No Signal Name Description
1 USBxVBUS USB Hub Port 1 5V Supply
2 USB_DM1 USB Hub Port 1 High-speed Transceiver (Negative)
3 USB_DP1 USB 3.0 Hub USB2 High-speed Transceiver (Positive)
4 GND Ground
5 USB_RXM1 USB Hub Port 1 SuperSpeed Receiver (Negative)
6 USB_RXP1 USB Hub Port 1 SuperSpeed Receiver (Positive)
7 GND Ground
8 USB_TXM1 USB Hub Port 1 SuperSpeed Transmitter (Negative)
9 USB_TXP1 USB Hub Port 1 SuperSpeed Transmitter (Positive)
10 USB3VBUS USB Hub Port 2 Bus Voltage
11 USB_DM2 USB Hub Port 2 High-speed Transceiver (Negative)
12 USB_DP2 USB Hub Port 2 High-speed Transceiver (Positive)
13 GND Ground
14 USB_RXM2 USB Hub Port 2 SuperSpeed Receiver (Negative)
15 USB_RXP2 USB Hub Port 2 SuperSpeed Receiver (Positive)
16 GND Ground
17 USB_TXM2 USB Hub Port 2 SuperSpeed Transmitter (Negative)
18 USB_TXP2 USB Hub Port 2 SuperSpeed Transmitter (Positive)
19 P13P15_SHLD Shield
20 P13P15_SHLD Shield
21 P13P15_SHLD Shield
22 P13P15_SHLD Shield

Table 16: USB 3.0 Hub Port 2/3 (AM572x USB1 Port) - P15


Serial Debug Header - P10 (Processor Module)

Pin No Signal Description
1 GND Ground
2 NC No Connect
3 NC No Connect
4 UART3_RX UART3 Receive Data
5 UART3_TX UART3 Transmit Data
6 NC No Connect

Table 17: Serial Debug Header Pin Details


HDMI - P11 (Processor Module)

Pin No Signal Description
1 HDMI_TX2+ HDMI Data 2 Differential Pair (Y)
2 GND HDMI Data 2 Shield
3 HDMI_TX2- HDMI Data 2 Differential Pair (X)
4 HDMI_TX1+ HDMI Data 1 Differential Pair (Y)
5 GND HDMI Data 2 Shield
6 HDMI_TX1- HDMI Data 1 Differential Pair (X)
7 HDMI_TX0+ HDMI Data 0 Differential Pair (Y)
8 GND HDMI Data 0 Shield
9 HDMI_TX0- HDMI Data 0 Differential Pair (X)
10 HDMI_TXC+ HDMI Clock Differential Pair (Y)
11 GND HDMI Clock Shield
12 HDMI_TXC- HDMI Clock Differential Pair (X)
13 HDMI_CEC_B HDMI Consumer Electronics Control (CEC) Interface
14 NC No connect
15 HDMI_SCL_B HDMI Display Data Channel (DDC) I2C Clock
16 HDMI_SDA_B HDMI Display Data Channel (DDC) I2C Data
17 GND Ground
18 HDMI_5VOUT HDMI 5V Supply (55mA max)
19 HDMI_HPD_B HDMI Hot Plug Detect (HPD)
MTG1 P11_ESD
MTG2 P11_ESD
MTG3 P11_ESD
MTG4 P11_ESD

Table 18: HDMI Connector Pin Details


MicroSD - P12 (Processor Module)

Pin No Signal Description
1 DAT2 MMC1 Data 2
2 DAT3/CD MMC1 Data 3
3 CMD MMC1 Command
4 VDD VDD_SD (3.3V)
5 CLK MMC1 Clock
6 VSS Ground
7 DAT0 MMC1 Data 0
8 DAT1 MMC1 Data 1
10 CD MMC1 Card Detect

Table 19: AM572x MMC1 Connector Pin Details


Expansion Connectors

The expansion connector details are listed in the tables below.

Processor Module P16 / LCD Module P1

Pin No Processor Module LCD Module
Signal Description Signal Description
A1 NC No Connect not connected
A2 GND Ground same as PM
A3 VDD_3V3 3.3V Power Supply same as PM
A4 NC No Connect not connected
B1 12V 12V Power Supply (always-on) same as PM
B2 5V0 5V Power Supply (always-on) same as PM
1 GND Ground same as PM
2 GND Ground same as PM
3 GPIO4_17 GPIO4[17] same as PM
4 GPIO5_11 GPIO5[11] same as PM
5 MCASP7_AXR0 McASP7 Audio Transmit/Receive (Pin 0) PCM_DOUT COM Port Bluetooth Audio Out (to AM57xx)
6 VIN3A_D22 Video Input 3 Port A Data Input same as PM
7 GPIO2_3 GPIO2[3] not connected
8 GPIO2_8 GPIO2[8] PCIe_RESET PCI-Express Mini Card RESET (active high)
9 VIN3A_HSYNC Video Input 3 Port A Horizontal Sync Input same as PM
10 VIN3A_D20 Video Input 3 Port A Data Input same as PM
11 DMA_EVT3 System DMA Event Input 3 not connected
12 VIN3A_D18 Video Input 3 Port A Data Input same as PM
13 VIN3A_D21 Video Input 3 Port A Data Input same as PM
14 VIN3A_DEO Video Input 3 Port A Data Enable Input same as PM
15 VIN3A_D4 Video Input 3 Port A Data Input same as PM
16 VIN3A_D2 Video Input 3 Port A Data Input same as PM
17 DMA_EVT4 System DMA Event Input 4 not connected
18 VIN3A_D5 Video Input 3 Port A Data Input same as PM
19 GPIO2_25 GPIO2[25] PB2 LCD Module Push Button 2
20 GPIO2_28 GPIO2[28] PB3 LCD Module Push Button 3
21 GPIO2_23 GPIO2[23] PB1 LCD Module Push Button 1
22 VIN3A_D3 Video Input 3 Port A Data Input same as PM
23 VIN3A_D8 Video Input 3 Port A Data Input same as PM
24 VIN3A_D12 Video Input 3 Port A Data Input same as PM
25 VIN3A_D15 Video Input 3 Port A Data Input same as PM
26 VIN3A_D13 Video Input 3 Port A Data Input same as PM
27 VIN3A_D14 Video Input 3 Port A Data Input same as PM
28 GND Ground not connected
29 USB2_DMEX USB2 USB 2.0 Data (Negative) not connected
30 GND Ground not connected
31 GND Ground same as PM
32 GND Ground same as PM
33 GPIO5_12 GPIO5[12] same as PM
34 GPIO5_10 GPIO5[10] same as PM
35 DMA_EVT1 System DMA Event Input 1 not connected
36 VIN3A_D16 Video Input 3 Port A Data Input same as PM
37 VIN3A_VSYNC Video Input 3 Port A Vertical Sync Input same as PM
38 GPIO2_5 GPIO2[5] LCDPWR LCD Power Supply Enable (active-high)
39 GPIO2_6 GPIO2[6] CAP_RST Touch Controller Reset
40 GPIO2_4 GPIO2[4] CAP_INT Touch Controller Interrupt
41 GPIO2_19 GPIO2[19] not connected
42 VIN3A_D19 Video Input 3 Port A Data Input same as PM
43 VIN3A_D17 Video Input 3 Port A Data Input same as PM
44 VIN3A_FLD Video Input 3 Port A Field ID Input same as PM
45 VIN3A_D23 Video Input 3 Port A Data Input same as PM
46 GPIO2_2 GPIO2[2] LCD_RSTn LCD Reset (may not be connected)
47 GPIO2_24 GPIO2[24] PB4 LCD Module Push Button 4
48 GPIO2_17 GPIO2[17] not connected
49 GPIO2_20 GPIO2[20] PB5 LCD Module Push Button 5
50 VIN3A_CLK0 Video Input 3 Port A Clock same as PM
51 VIN3A_D0 Video Input 3 Port A Data Input same as PM
52 VIN3A_D1 Video Input 3 Port A Data Input same as PM
53 VIN3A_D6 Video Input 3 Port A Data Input same as PM
54 VIN3A_D7 Video Input 3 Port A Data Input same as PM
55 VIN3A_D11 Video Input 3 Port A Data Input same as PM
56 VIN3A_D10 Video Input 3 Port A Data Input same as PM
57 VIN3A_D9 Video Input 3 Port A Data Input same as PM
58 GND Ground not connected
59 USB2_DPEX USB2 USB 2.0 Data (Positive) not connected
60 GND Ground not connected

Table 20: AM572x P16 Expansion Connector



Processor Module P17 / LCD Module P3

Pin No Processor Module LCD Module
Signal Description Signal Description
A1 NC No Connect not connected
A2 GND Ground same as PM
A3 VDD_3V3 3.3V Power Supply same as PM
A4 NC No Connect not connected
B1 12V 12V Power Supply (always-on) same as PM
B2 5V0 5V Power Supply (always-on) same as PM
1 GND Ground same as PM
2 GND Ground same as PM
3 GPIO6_11 GPIO6[11] CAM_ENn Camera Module Enable (active-low)
4 MMC3_CMD MMC3 Command COMQ_MMC0_CMD COM Port WLAN SDIO CMD
5 EHRPWM2A Enhanced High-Resolution PWM Module 2 Output A BLPWM LCD Module Brightness Control (PWM)
6 MMC3_DAT7 MMC3 Data (Bit 7) not connected
7 MMC3_DAT0 MMC3 Data (Bit 0) COMQ_MMC0_DAT0 COM Port WLAN SDIO Data
8 MMC3_DAT2 MMC3 Data (Bit 2) COMQ_MMC0_DAT2 COM Port WLAN SDIO Data
9 UART9_TXD UART9 Data Transmit (Output) not connected
10 UART9_RXD UART9 Data Receive (Input) not connected
11 UART8_CTS UART8 Clear to Send BT_UART_RTS COM Port Bluetooth Request to Send
12 TIMER3 PWM output/event trigger input not connected
13 TIMER2 PWM output/event trigger input not connected
14 UART8_RTS UART8 Request to Send BT_UART_CTS COM Port Bluetooth Clear to Send
15 GPIO5_7 GPIO5[7] WLAN_IRQ COM Port WLAN IRQ
16 MCASP2_AXR4 McASP2 Audio Transmit/Receive (Pin 4) not connected
17 GPIO5_5 GPIO5[5] GPS_PPS_OUT COM Port GPS Pulse Per Second
18 MCASP2_AXR2 MCASP22 Audio Transmit/Receive (Pin 2) not connected
19 MCASP7_FSX MCASP7 Audio Transmit Frame Sync I/O PCM_FSYNC COM Port Bluetooth Audio Frame Sync
20 DCAN1_RX DCAN1 Data Receive Pin not connected
21 MCASP2_CLKX MCASP2 Audio Transmit Clock I/O not connected
22 MCASP2_AXR3 MCASP2 Audio Transmit/Receive (Pin 3) not connected
23 MCASP2_AXR1 MCASP2 Audio Transmit/Receive (Pin 1) not connected
24 MCASP2_AXR5 MCASP2 Audio Transmit/Receive (Pin 5) not connected
25 GPIO5_9 GPIO5[9] not connected
26 MCASP2_AXR6 MCASP2 Audio Transmit/Receive (Pin 6) not connected
27 UART8_TXD UART8 Data Transmit (Output) BT_UART_RX COM Port Bluetooth Data Recieve
28 GPIO6_19 GPIO6[19] not connected
29 USB2_OC GPIO7[17] not connected
30 USB2_ID GPIO7[24] (pulled up - 10k ohms) not connected
31 GND Ground same as PM
32 GND Ground same as PM
33 MMC3_DAT3 MMC3 Data (Bit 3) COMQ_MMC0_DAT3 COM Port WLAN SDIO Data
34 MMC3_CLK MMC3 Clock COMQ_MMC0_CLK COM Port WLAN SDIO Clock
35 MMC3_DAT5 MMC3 Data (Bit 5) not connected
36 MMC3_DAT1 MMC3 Data (Bit 1) COMQ_MMC0_DAT1 COM Port WLAN SDIO Data
37 MMC3_DAT4 MMC3 Data (Bit 4) not connected
38 MMC3_DAT6 MMC3 Data (Bit 6) not connected
39 UART9_RTSN UART9 Request to Send active low not connected
40 UART9_CTSN UART9 Clear to Send active low not connected
41 CLKOUT3 Device Clock Output 3 not connected
42 TIMER1 PWM output/event trigger input not connected
43 UART8_RXD UART8 Receive Data (Input) BT_UART_TXD COM Port Bluetooth Data Transmit
44 MCASP2_ACLKR McASP2 Audio Receive Clock I/O not connected
45 GPIO5_6 GPIO5[6] GPS_TIME_STAMP COM Port GPS Time Stamp
46 I2C4_SCL I2C Port 4 Serial Clock same as PM
47 GPIO5_4 GPIO5[4] BT_EN COM Port Bluetooth Enable
48 MCASP7_ACLKX McASP7 Audio Transmit Bit Clock I/O PCM_CLK COM Port Bluetooth Audio Clock
49 MCASP7_AXR1 McASP7 Audio Transmit/Receive (Pin 1) PCM_DIN COM Port Bluetooth Audio In (from AM57xx)
50 DCAN1_TX DCAN1 Data Transmit Pin not connected
51 GPIO7_7 GPIO7[7] not connected
52 MCASP2_FSX McASP2 Audio Transmit Frame Sync I/O not connected
53 I2C4_SDA I2C Port 4 Serial Data same as PM
54 MCASP2_AXR0 McASP2 Audio Transmit/Receive (Pin 0) not connected
55 GPIO5_8 GPIO5[8] WL_EN COM Port WLAN Enable
56 MCASP2_AXR7 McASP2 Audio Transmit/Receive (Pin 7) not connected
57 MCASP2_FSR McASP2 Audio Receive Frame Sync I/O not connected
58 GPIO6_18 GPIO6[18] not connected
59 USB2_DRVBUS USB2 Host VBUS Signal output not connected
60 USB2VBUS_EXP USB2 Client VBUS Signal input (depends on resistor configuration) not connected

Table 21: AM572x P17 Expansion Connector


Processor Module P18 / LCD Module P4

Pin No Processor Module LCD Module
Signal Description Signal Description
A1 NC No Connect not connected
A2 GND Ground same as PM
A3 VDD_3V3 3.3V Power Supply same as PM
A4 NC No Connect not connected
B1 12V 12V Power Supply (always-on) same as PM
B2 5V0 5V Power Supply (always-on) same as PM
1 GND Ground same as PM
2 GND Ground same as PM
3 I2C5_SDA I2C Port 5 Serial Data 1V8_I2C5_SDA COM Port I2C Serial Data
4 I2C5_SCL I2C Port 5 Serial Clock 1V8_I2C5_SCL COM Port I2C Serial Clock
5 PWRON Power On Signal (active-low) same as PM
6 EHRPWM2_TRIPZONE_INPUT Enhanced High-Resolution PWM Port 2 Trip Zone Input not connected
7 GPIO4_10 GPIO4[10] not connected
8 UART10_RTSn UART10 Request to Send (active low) not connected
9 GPIO3_29 GPIO3[29] not connected
10 PR1_UART0_TXD PRU-ICSS1 UART Data Transmit not connected
11 GPIO3_28 GPIO3[28] not connected
12 UART10_RXD UART10 Data Receive (Input) not connected
13 UART10_CTSn UART10 Clear to Send (active low) not connected
14 VOUT1_D15 Video Output 1 Data Output same as PM
15 VOUT1_D13 Video Output 1 Data Output same as PM
16 VOUT1_D10 Video Output 1 Data Output same as PM
17 VOUT1_D14 Video Output 1 Data Output same as PM
18 VOUT1_D11 Video Output 1 Data Output same as PM
19 VOUT1_D20 Video Output 1 Data Output same as PM
20 VOUT1_D12 Video Output 1 Data Output same as PM
21 VOUT1_D18 Video Output 1 Data Output same as PM
22 VOUT1_D19 Video Output 1 Data Output same as PM
23 VOUT1_D21 Video Output 1 Data Output same as PM
24 VOUT1_D23 Video Output 1 Data Output same as PM
25 VOUT1_D0 Video Output 1 Data Output same as PM
26 VOUT1_D3 Video Output 1 Data Output same as PM
27 VOUT1_HSYNC Video Output 1 Horizontal Sync Output same as PM
28 VOUT1_VSYNC Video Output 1 Vertical Sync Output same as PM
29 GPIO5_19 GPIO5[19] not connected
30 UART1_TXD UART1 Data Transmit (Output) not connected
31 GND Ground same as PM
32 GND Ground same as PM
33 RSTOUTn Reset Out (active-low) not connected
34 RESETIN Reset Signal (active-low) same as PM
35 EXT_WAKE not connected
36 GPIO3_30 GPIO3[30] not connected
37 PR1_UART0_RTSn PRU-ICSS1 UART Request to Send (active low) not connected
38 GPIO4_9 GPIO4[9] not connected
39 GPIO4_8 GPIO4[8] not connected
40 PR1_UART0_CTSn PRU-ICSS1 UART Clear to Send (active low) not connected
41 PR1_UART0_RXD PRU-ICSS1 UART Data Receive not connected
42 UART10_TXD UART10 Data Transmit (Output) not connected
43 GPIO4_7 GPIO4[7] not connected
44 EHRPWM2B Enhanced High-Resolution PWM Port 2 Output B not connected
45 VOUT1_D6 Video Output 1 Data Output same as PM
46 VOUT1_D7 Video Output 1 Data Output same as PM
47 VOUT1_D8 Video Output 1 Data Output same as PM
48 VOUT1_D4 Video Output 1 Data Output same as PM
49 VOUT1_D5 Video Output 1 Data Output same as PM
50 VOUT1_D16 Video Output 1 Data Output same as PM
51 VOUT1_D17 Video Output 1 Data Output same as PM
52 VOUT1_D22 Video Output 1 Data Output same as PM
53 VOUT1_DE Video Output 1 Data Enable Output same as PM
54 VOUT1_D2 Video Output 1 Data Output same as PM
55 VOUT1_D1 Video Output 1 Data Output same as PM
56 VOUT1_D9 Video Output 1 Data Output same as PM
57 VOUT1_CLK Video Output 1 Clock Output same as PM
58 NC No Connect same as PM
59 GPIO5_18 GPIO5[18] not connected
60 UART1_RXD UART1 Data Receive (Input) not connected

Table 22: AM572x P18 Expansion Connector


Processor Module P19 / LCD Module P2

Pin No Processor Module LCD Module
Signal Description Signal Description
A1 NC No Connect not connected
A2 GND Ground same as PM
A3 VDD_3V3 3.3V Power Supply same as PM
A4 NC No Connect not connected
B1 12V 12V Power Supply (always-on) same as PM
B2 5V0 5V Power Supply (always-on) same as PM
1 GND Ground same as PM
2 NC No Connect GND Ground (does not conflict with PM)
3 NC No Connect not connected
4 GND Ground not connected
5 GND Ground same as PM
6 SATA_SEL Ground to enable SATA on P19 SATA_SEL Ground to enable mSATA card slot
7 EXP_SATA_RXN SATA Data Receive (Negative) same as PM
8 EXP_SATA_RXP SATA Data Receive (Positive) same as PM
9 GND Ground same as PM
10 GND Ground same as PM
11 GPIO3_20 GPIO3[20] same as PM
12 GPIO3_24 GPIO3[24] same as PM
13 GND Ground same as PM
14 GPIO3_11 GPIO3[11] same as PM
15 GPIO3_12 GPIO3[12] same as PM
16 GND Ground same as PM
17 CON.PCIE_RXP1 PCI-Express Lane 1 Receive (Positive) not connected
18 CON.PCIE_RXN1 PCI-Express Lane 1 Receive (Negative) not connected
19 GND Ground same as PM
20 CON.PCIE_TXP1 PCI-Express Lane 1 Transmit (Positive) not connected
21 CON.PCIE_TXN1 PCI-Express Lane 1 Transmit (Negative) not connected
22 GND Ground not connected
23 GND Ground same as PM
24 CON.PCIE_RXP0 PCI-Express Lane 0 Receive (Positive) same as PM
25 CON.PCIE_RXN0 PCI-Express Lane 0 Receive (Negative) same as PM
26 GND Ground same as PM
27 CON.PCIE_TXP0 PCI-Express Lane 0 Transmit (Positive) same as PM
28 CON.PCIE_TXN0 PCI-Express Lane 0 Transmit (Negative) same as PM
29 GND Ground not connected
30 NC

E| No Connect

not connected
31 GND Ground same as PM
32 GND Ground same as PM
33 NC No Connect not connected
34 GND Ground same as PM
35 EXP_SATA_TXP SATA Data Transmit (Positive) same as PM
36 EXP_SATA_TXN SATA Data Transmit (Negative) same as PM
37 GND Ground same as PM
38 GND Ground same as PM
39 GPIO3_23 GPIO3[23] same as PM
40 GPIO3_26 GPIO3[26] same as PM
41 GND Ground same as PM
42 GPIO3_16 GPIO3[16] same as PM
43 GPIO3_18 GPIO3[18] same as PM
44 GND Ground same as PM
45 GPIO3_8 GPIO3[8] same as PM
46 GPIO3_14 GPIO3[14] same as PM
47 GND Ground same as PM
48 GPIO3_9 GPIO3[9] same as PM
49 GPIO3_15 GPIO3[15] same as PM
50 GND Ground same as PM
51 GND Ground same as PM
52 GPIO3_7 GPIO3[7] same as PM
53 GPIO3_10 GPIO3[10] same as PM
54 GND Ground same as PM
55 GPIO2_31 GPIO2[31] same as PM
56 GPIO3_6 GPIO3[6] same as PM
57 GND Ground same as PM
58 PCI_CONN_REFN PCI-Express Reference Signal (Negative) same as PM
59 PCI_CONN_REFP PCI-Express Reference Signal (Positive) same as PM
60 GND Ground same as PM

Table 23: AM572x P19 Expansion Connector



JTAG Connector

TI 20 pin connector... other JTAG adaptors are available on TI e-store and can be purchased from here


LCD Connector - P5 (LCD Module)

The LCD Module's backlight supply comes from a TPS61080 LED Driver / Boost-Converter. It outputs 9.9V max and is controlled by PWM (See: EHRPWM2A on Pin 5 of P17 Processor Module).

Pin No Signal Description
1 VLED+ LED Backlight Supply+
2 VLED+ LED Backlight Supply+
3 VLED- LED Backlight Supply-
4 VLED- LED Backlight Supply-
5 GND Ground
6 VCOM LCD COM Voltage
7 VDD LCD Main Voltage
8 MODE Not Connected
9 DE Data Enable
10 VS Vertical Sync
11 HS Horizontal Sync
12-19 B7-B0 Pixel's Blue Data
20-27 G7-G0 Pixel's Green Data
28-35 R7-R0 Pixel's Red Data
36 GND Ground
37 PCLK Pixel Clock
38 GND Ground
39 L/R Not Connected
40 U/D Not Connected
41 VGH LCD Bias Voltage
42 VGL LCD Bias Voltage
43 AVDD LCD Main Analog Voltage
44 LCDRSTn LCD Reset Signal (always-high)
45 NC Not Connected
46 VCOM LCD COM Voltage
47 DITHB Not Connected
48 GND Ground
49 NC Not Connected
50 NC Not Connected

Table 24: LCD Connector Pin Details


Touchscreen Connector - P15 (LCD Module)

Pin No Signal Description
1 NC Not Connected
2 NC Not Connected
3 CAP_INT Touch Controller Interrupt (GPIO2_4)
4 I2C5_SDA I2C Port 5 Serial Data
5 I2C5_SCL I2C Port 5 Serial Clock
6 CAP_RST Touch Controller RESET (GPIO2_6)
7 GND Ground
8 VDD_3V3 3.3V Supply

Table 25: LCD Module Capacitive Touch Screen Pin Details


PCI-Express Mini Card Slot - P7 (LCD Module)

PCI-Express Mini Card Slot supports x1 speeds. 3.3V Supply 1.5A max. 1.5V Supply 0.5A max.

Pin No Signal Description
1 WAKEn Not Connected
2 PS_3V3 3.3V Supply
3 COEX1 Not Connected
4 GND Ground
5 COEX2 Not Connected
6 PCI_1.5V 1.5V Supply
7 CLKREQn Not Connected
8 UIM_PWR Not Connected
9 GND Ground
10 UIM_DATA Not Connected
11 REFCLK- PCI-Express Reference Clock Differential Pair (Negative)
12 UIM_CLK Not Connected
13 REFCLK+ PCI-Express Reference Clock Differential Pair (Positive)
14 UIM_RESET Not Connected
15 GND Ground
16 UIM_VPP Not Connected
17 RSVD1 Not Connected
18 GND Ground
19 RSVD2 Not Connected
20 W_DISABLEn Not Connected
21 GND Ground
22 PERSTn Not Connected
23 PERn0 PCI-Express Lane 0 Receive Differential Pair (Negative)
24 VDD_3V3 3.3V Supply
25 PERp0 PCI-Express Lane 0 Receive Differential Pair (Positive)
26 GND Ground
27 GND Ground
28 PCI_1.5V 1.5V Supply
29 GND Ground
30 SMBus_CLK AM57xx I2C Port 4 Serial Clock
31 PETn0 PCI-Express Lane 0 Transmit Differential Pair (Negative)
32 SMBus_DATA AM57xx I2C Port 4 Serial Data
33 PETp0 PCI-Express Lane 0 Transmit Differential Pair (Positive)
34 GND Ground
35 GND Ground
36 USB_D- Not Connected
37 GND Ground
38 USB_D+ Not Connected
39 PS_3V3 3.3V Supply
40 GND Ground
41 PS_3V3 3.3V Supply
42 LED_WWANn Not Connected
43 GND Ground
44 LED_WLANn Not Connected
45 RSVD3 Not Connected
46 LED_WPANn Not Connected
47 RSVD4 Not Connected
48 PCI_1.5V 1.5V Supply
49 RSVD5 Not Connected
50 GND Ground
51 RSVD6 Not Connected
52 PS_3V3 3.3V Supply

Table 26: PCIe Mini Card Connector Pin Details


mSATA Connector - P8 (LCD Module)

The mSATA slot is intended to support SATA based Solid State Drives compatible with the PCI-Express Mini Card slot physical specification but carry SATA signals instead of PCI-E. There is a remote LED indicator at Pin 49 called “Device Activity Signal”. The mSATA card should sink current on Pin 49 to allow the LED to flash to indicate an ACTIVITY.

Pin No Signal Description
1 NC Not Connected
2 PS_3V3 3.3V Supply
3 NC Not Connected
4 GND Ground
5 NC Not Connected
6 NC Not Connected
7 NC Not Connected
8 NC Not Connected
9 GND Ground
10 NC Not Connected
11 NC Not Connected
12 NC Not Connected
13 NC Not Connected
14 NC Not Connected
15 GND Ground
16 NC Not Connected
17 NC Not Connected
18 GND Ground
19 NC Not Connected
20 NC Not Connected
21 GND Ground
22 NC Not Connected
23 RXP SATA Receive (Positive)
24 VDD_3V3 3.3V Supply
25 RXN SATA Receive (Negative)
26 GND Ground
27 GND Ground
28 NC Not Connected
29 GND Ground
30 NC Not Connected
31 TXN SATA Transmit (Negative)
32 NC Not Connected
33 TXP SATA Transmit (Positive)
34 GND Ground
35 GND Ground
36 NC Not Connected
37 GND Ground
38 NC Not Connected
39 PS_3V3 3.3V Supply
40 GND Ground
41 PS_3V3 3.3V Supply
42 NC Not Connected
43 NC Not Connected
44 NC Not Connected
45 NC Not Connected
46 NC Not Connected
47 NC Not Connected
48 NC Not Connected
49 DA/DSS Device Activity Signal
50 GND Ground
51 RSVD6 Not Connected
52 PS_3V3 3.3V Supply

Table 27: mSATA Connector Pin Details


Camera Connector - P9 (LCD Module), P9 (Camera Module)

Pin No Signal Description
A1 NC No Connect
A2 GND Ground
A3 VDD_3V3 3.3V Power Supply
A4 NC No Connect
B1 12V 12V Power Supply (always-on)
B2 5V0 5V Power Supply (always-on)
1 GND Ground
2 GPIO3_20 GPIO3[20]
3 GPIO3_24 GPIO3[24]
4 GND Ground
5 GPIO3_11 GPIO3[11]
6 GPIO3_12 GPIO3[12]
7 GND Ground
8 GPIO3_15 GPIO3[15]
9 GPIO3_9 GPIO3[9]
10 GND Ground
11 GPIO2_31 GPIO2[31]
12 GPIO3_6 GPIO3[6]
13 GND Ground
14 VIN3A_D0 Video Input Port 3A Data
15 VIN3A_D2 Video Input Port 3A Data
16 VIN3A_D4 Video Input Port 3A Data
17 VIN3A_D6 Video Input Port 3A Data
18 VIN3A_D8 Video Input Port 3A Data
19 VIN3A_D10 Video Input Port 3A Data
20 VIN3A_D12 Video Input Port 3A Data
21 VIN3A_D14 Video Input Port 3A Data
22 VIN3A_D16 Video Input Port 3A Data
23 VIN3A_D18 Video Input Port 3A Data
24 VIN3A_D20 Video Input Port 3A Data
25 VIN3A_D22 Video Input Port 3A Data
26 VIN3A_HSYNC Video Input Port 3A HSYNC
27 VIN3A_VSYNC Video Input Port 3A VSYNC
28 VIN3A_CLK Video Input Port 3A CLK
29 I2C5_SCL AM572x I2C Port 5 Serial Clock
30 I2C5_SDA AM572x I2C Port 5 Serial Data
31 GPIO3_23 GPIO3[23]
32 GPIO3_26 GPIO3[26]
33 GND Ground
34 GPIO3_16 GPIO3[16]
35 GPIO3_18 GPIO3[18]
36 GND Ground
37 GPIO3_8 GPIO3[8]
38 GPIO3_14 GPIO3[14]
39 GND Ground
40 GPIO3_10 GPIO3[10]
41 GPIO3_7 GPIO3[7]
42 GND Ground
43 VIN3A_D1 Video Input Port 3A Data
44 VIN3A_D3 Video Input Port 3A Data
45 VIN3A_D5 Video Input Port 3A Data
46 VIN3A_D7 Video Input Port 3A Data
47 VIN3A_D9 Video Input Port 3A Data
48 VIN3A_D11 Video Input Port 3A Data
49 VIN3A_D13 Video Input Port 3A Data
50 VIN3A_D15 Video Input Port 3A Data
51 VIN3A_D17 Video Input Port 3A Data
52 VIN3A_D19 Video Input Port 3A Data
53 VIN3A_D21 Video Input Port 3A Data
54 VIN3A_D23 Video Input Port 3A Data
55 VIN3A_DE0 Video Input Port 3A DE0
56 VIN3A_FLD Video Input Port 3A FLD
57 GPIO5_10 GPIO5[10]
58 GPIO5_11 GPIO5[11]
59 GPIO5_12 GPIO5[12]
60 GPIO4_17 GPIO4[17]

Table 28: Camera Connector Pin Details


Communications Connector - P12 (LCD Module)

The Communications Connector (P12) on the LCD module is intended for use with WiLink boards. All I/O operates at 1.8V logic levels behind level shifters that limit some GPIO signal directions. The 3.6V and 1.8V rails are supplied by separate LDOs capable of 1.5A max each.

Pin No Signal Description
1 SLEEP_CLK 32.768 kHz low power clock (TC32M5I32K7680)
2 GND Ground
3 GND Ground
4 WL_EN WLAN Enable (GPIO5_8 output)
5 COM_3V6 3.6V Power Supply (1.5A max)
6 GND Ground
7 COM_3V6 3.6V Power Supply (1.5A max)
8 COM_1V8 1.8V Power Supply (1.5A max)
9 GND Ground
10 NC Not Connected
11 NC Not Connected
12 NC Not Connected
13 NC Not Connected
14 NC Not Connected
15 NC Not Connected
16 NC Not Connected
17 NC Not Connected
18 GND Ground
19 GND Ground
20 COMQ_MMC0_CLK AM572x SDIO Clock
21 NC Not Connected
22 GND Ground
23 NC Not Connected
24 COMQ_MMC0_CMD AM572x SDIO Command
25 NC Not Connected
26 COMQ_MMC0_DAT0 AM572x SDIO Data
27 NC Not Connected
28 COMQ_MMC0_DAT1 AM572x SDIO Data
29 NC Not Connected
30 COMQ_MMC0_DAT2 AM572x SDIO Data
31 1V8_I2C5_SCL AM572x I2C Port 5 Serial Clock (at 1.8V)
32 COMQ_MMC0_DAT3 AM572x SDIO Data
33 1V8_I2C5_SDA AM572x I2C Port 5 Serial Data (at 1.8V)
34 WLAN_IRQ WLAN Interrupt Request (GPIO5_7 input)
35 NC Not Connected
36 NC Not Connected
37 GND Ground
38 NC Not Connected
39 NC Not Connected
40 NC Not Connected
41 NC Not Connected
42 GND Ground
43 NC Not Connected
44 NC Not Connected
45 NC Not Connected
46 NC Not Connected
47 GND Ground
48 GPS_TIME_STAMP GPS Time Stamp (GPIO5_6 output)
49 NC Not Connected
50 GPS_PPS_OUT GPS Pulse Per Second (GPIO5_5 input)
51 NC Not Connected
52 PCM_CLK Bluetooth's PCM Clock
53 NC Not Connected
54 PCM_FSYNC Bluetooth's PCM Frame Sync
55 NC Not Connected
56 PCM_DIN Bluetooth's PCM Audio In
57 NC Not Connected
58 PCM_DOUT Bluetooth's PCM Audio Out
59 NC Not Connected
60 GND Ground
61 NC Not Connected
62 NC Not Connected
63 GND Ground
64 GND Ground
65 NC Not Connected
66 BT_UART_RX Bluetooth's UART Data Transmit
67 NC Not Connected
68 BT_UART_RX Bluetooth's UART Data Receive
69 NC Not Connected
70 BT_UART_CTS Bluetooth's UART Clear to Send
71 NC Not Connected
72 BT_UART_RTS Bluetooth's UART Request to Send
73 NC Not Connected
74 NC Not Connected
75 NC Not Connected
76 NC Not Connected
77 GND Ground
78 NC Not Connected
79 NC Not Connected
80 NC Not Connected
81 NC Not Connected
82 NC Not Connected
83 GND Ground
84 NC Not Connected
85 NC Not Connected
86 NC Not Connected
87 GND Ground
88 NC Not Connected
89 BT_EN WPAN Bluetooth Enable (GPIO5_4 output)
90 NC Not Connected
91 NC Not Connected
92 GND Ground
93 NC Not Connected
94 NC Not Connected
95 GND Ground
96 NC Not Connected
97 GND Ground
98 NC Not Connected
99 NC Not Connected
100 NC Not Connected

Table 29: COM Connector Pin Details


EVM Important Notice

NoteNote: The Standard Terms And Conditions for TI Evaluation Modules can be downloaded from here:http://www.ti.com/lit/pdf/sszz027

ANNEX

This HUG is prepared by using the following documents as references.

  1. AM572x Sitara ARM Microprocessors TRM (SPRUHZ6)