Accessing c int00
From Texas Instruments Embedded Processors Wiki
Contents |
Introduction
_c_int00 is the name of the symbol of the C environment entry point. Sometimes it is necessary to obtain this address (e.g., to reset the software) or even to set c_int00 address to a fixed location (so that the host that is booting the processor can make it jump to that location). This page describes how to achieve that.
Retrieving the c_int00 Address
If you need to retrieve the address of c_int00 at run time, use the code below as an example:
extern void c_int00(void);
void main( void )
{
void (*x)(void) = c_int00;
}
Setting the c_int00 Address to a Fixed Location
When using an external host to boot the DSP, it might need the c_int00 address to be always the same. The procedures below describe how to achieve that.
Using DSP/BIOS
If you are using DSP/BIOS, the symbol _c_int00 is placed in a section named .sysinit.
You can create a new memory section and put .sysinit in it.
To do that, go to your DSP/BIOS Configuration file (.tcf). At System, right click on MEM – Memory Section Manager and select Insert MEM to create a new section. Adjust the properties of the new section: base, len. You can look in your map file to see the size of the .sysinit section to determine the minimum length that you need to fit it in this memory section that you created. Do not forget to adjust the other memory sections to make sure that they do not overlap each other. So, for example, if you are going to put sysinit in internal memory, reduce the base and len of IRAM if necessary. You can remove the heap in this section by unchecking the option create a heap in this memory. At the bottom of the Properties window, select space: code.
After that, right click on MEM – Memory Section Manager and select Properties. In the BIOS Code tab select your new memory section for Startup Code Section (.sysinit).
Thus, the linker will always put the c_int00 entry point in the same location.
If you not only need the address of c_int00 to be always in the same location, but want to specify that location, you may need to create a custom linker command (.cmd) file that references the DSP/BIOS generated file.
To do that, in the tcf file, create a new memory region (for example called RAM4CINT00). Then create your own custom .cmd file containing (example for C5000):
-l configcfg.cmd /* name of your original .cmd */
SECTIONS {
.bootcode: {
-lbios.a55L<boot.o55L>(.sysinit)
} > RAM4CINT00
}
This should only put the code for _c_int00 into the new section .bootcode. Don't forget to put the normal .sysinit back to your original memory location.
Here's an example for 64x+ core:
SECTIONS
{
boot > 0x00800000
{
-l bios.a64P<boot.o64P>(.sysinit)
}
}
In the above example we are pulling in only the code for c_int00 and hard-coding it to a specific address, 0x00800000. This might be helpful on a device such as TMS320C6455 for doing HPI boot which begins executing from address 0x00800000 after the host sends the interrupt to the DSP to begin execution.
NOTE: If you you are using a C674x DSP, use a674 and o674. If you are using huge memory model for C5000, use a55H and o55H.
Using SYS/BIOS
If you are using SYS/BIOS, system start up and initialization is handled by XDCtools, which places the symbol _c_int00 in the .text section. RTSC puts each function into its own section (using the compiler's "-mo flag).
To place the .text symbol at an explicit address, add a custom linker command (.cmd) file to your project with a directive similar to:
SECTIONS {
.text:_c_int00 > 0xc3000000
}
Not using DSP/BIOS
If you are not using DSP/BIOS, you should be able to specify the address using the linker command file. The general idea is to put the boot module (where _c_int00 is defined) into an output section of its own, then allocate that output section to a specific memory address. For example for C5000:
boot > 0x1234
{
-l rts55.lib<boot.obj>(.text)
}
You can change the address 0x1234 to be whatever address that you want to put the code. Probably the start of your RAM would be a good place so that the linker doesn’t have problems allocating other objects around it.
NOTE: If you are using a C64x+ DSP, replace rts55.lib with rts64plus.lib. If you you are using a C674x DSP, use rts6740.lib. If you are using huge memory model for C5000, use rts55h.lib.
Related information and forum posts
How to specify an exact address for c_int00?
Comments
Comments on Accessing c int00

For C6748 I tried with rts6740.lib (and later with rts6740_elf_eh.lib) but I receive a warning 10068-D: no matching section. The resulted map file doesn't seem to change. Any idea?
--Davidluca3000 09:46, 28 February 2012 (CST)