Adding an ETB Node to the CCSv5 Target Configuration
From Texas Instruments Embedded Processors Wiki
Overview
If you are using a C66x Device, you have the ability to use System Trace (STM), either through an XDS560v2 Generation emulator or through the device's Embedded Trace Buffer (ETB). However, if you're using an early version of CCSv5, the default CCSv5 target configuration might not have the ETBnode available. This document will walk you through adding that node if you need it. This article won't discuss how to use the Embedded Trace Buffer, only how to add the ETB node that will be needed. There are other articles on this wiki that will discuss how to use System Trace, such as this one.
Identifying whether you need to take these steps
It's pretty simple to tell whether you need to add the ETB node to your CCS configuration, or whether you already have it. Open your target configuration in Code Composer Studio 5, and click the "Advanced" tab, as shown in the image. Be sure that DAP node of the target configuration is totally expanded. If it is totally expanded, and you do not see a node that says TETB_STM, then the ETB node is not present and will need to be added. This is the case in Figure 1. Figure 1 shows a C6678 device, but the C6670 will look identical at the DAP node and below.
If your device shows a TETB_STM node (It might also be called CS_ETB) somewhere below the CS_DAP_DebugSS node, then you do have the correct node. You can go through the rest of this page and ensure that the value settings are correct, but you shouldn't have to add anything.
Adding the TETB_STM Node
If you need to add the TETB_STM node in order to use ETB, follow these instructions.
- Open the Target Configuration in CCS and click on the Advanced Tab. You should see something similar to what we see in Figure 1.
- DAP Node
- Click on the DAP node (You should see some Subpath Properties. Ensure that the properties are set as marked below.
- DAP Properties
- Port Number = 0x9
- Initial Configuration = Unchecked
- Custom Configuration = Unchecked
- Force Configuration = Checked
- Pseudo Address = Unchecked
- Type = Debug
- Click on the DAP node (You should see some Subpath Properties. Ensure that the properties are set as marked below.
- CS_DAP_DebugSS Node
- Click on the CS_DAP_DebugSS node. Ensure that the properties are set as below
- CS_DAP_DebugSS
- Initialization Script = Leave Blank
- DAP TAP ID = 0x4B6B902F
- Click on the CS_DAP_DebugSS node. Ensure that the properties are set as below
- Add a Subpath
- Right Click on the CS_DAP_DebugSS node and select "Add"
- A Dialog box will open and you'll only have one choice. Choose Subpath. You can leave the name blank (or name it whatever you want so long as it doesn't conflict with other names in the structure) and the number of copies as 1. Click "Finish"
- Click on the Subpath you just created and set the properties as noted below.
- Subpath Properties
- Port Number = 0x1
- Initial Configuration = Unchecked
- Custom Configuration = Unchecked
- Type = debug
- Force Configuration = Checked
- Pseudo = Checked
- Add the TETB_STM node
- Right click on the subpath you just created and select "Add"
- In the Dialog box that opens, select the Cpus tab
- From the list of Cpus, find CSETB. You can leave the name blank (or name it whatever you want so long as it doesn't conflict with other names in the structure) and the number of copies as 1. Click "Finish"
- Click on the TETB_STM node you just added and set the properties as below
- TETB_STM Properties
- Bypass = Unchecked
- Initialization Script = <leave blank>
- Slave Processor = Unchecked
- Address = 0x02850000
- TraceDeviceId = 0x0
- Save the target configuration
At this point, your target configuration (Below the DAP) should like like the one in Figure 2.
Leave a Comment