Analog to Digital Converter Type 2 FAQ for C2000
From Texas Instruments Embedded Processors Wiki
Translate this page to
Introduction
This topic is a list of frequently asked questions that users have when using the Analog to Digital Converter of type 2. ADC type 2 is the 3rd generation ADC module released for the C28x devices and is found on 2833x and 2823x devices.
Electrical Specifications
Electrical specifications can change between devices, peripheral types and device families. Always refer to the data manual and errata for a particular device for Electrical Specifications.
ADC Type Summary
The following table summarizes the different type of ADC modules found on C28x devices.
| Type | Description | Devices | Documentation |
|---|---|---|---|
| 0 | Original C28x ADC module | 281x | TMS320x281x Analog-to-Digital Converter (ADC) Reference Guide (spru060) |
| 1 | Added Offset Trim and Reference Select registers | 2801, 2802, 2806, 2808, 2809, 28015, 28016, 28044 | TMS320x280x 2801x, 2804x Analog-to-Digital Converter(ADC) Module Reference Guide (spru716) |
| 2 | Added Internal/External Trim registers Trim by Device_cal() function call | 2833x, 2834x | TMS320x2833x, 2823x Analog-to-Digital Converter (ADC) Module Reference Guide (spru812) |
| 3 | Different control register interface, converts from 0 to 3.3 V fixed scale range, supports ratiometric VREFHI/VREFLO references | 2802x, 2803x 2806x | TMS320x2802x, 2803 Piccolo Analog-to-Digital Converter and Comparator Ref. Guide (spruge5) TMS320x2806x Piccolo Technical Reference Guide (SPRUH18) |
Frequently asked questions for ADC Type 2
Q: I measured ADCREFP and ADCREFM. In the datasheet only a typical value is specified not a min/max. How can I tell if my device is in spec?
- These signals are internally generated voltages for use by the internal ADC only. These are fully tested at by TI at production time and will not be out of spec for the device. The only reason these signals are brought outside the device is for external bulk cap. The Data Manual values are only there to give a ballpark of where the voltages will be and this is why there is no max/min.
Q: Can you explain more about this ADC_Cal() routine that the boot ROM calls?
- The ADC_cal() routine in the ROM of F2833x is just copying a couple of values to the ADCST and ADCOFFTRIM registers. This brings the ADC up to the specs in the datasheet.
Q: Does the ADC_cal() routine require a voltage on an ADC input pin?
- It does not require the use of any ADCINx channels.
Q: Can we still perform manual calibration like on the 280x?
- If you want to further improve the ADC offset and gain you can still do manual calibration AFTER running the ADC_cal() routine. The manual calibration would be the same as for the 280x.