Android Benchmarks DevKit2.3v2.0
From Texas Instruments Embedded Processors Wiki
Contents |
Introduction
This page provides comparison among various TI processors running TI's Android-DevKit. Data published here is for the latest version of released Android-DevKit. Items yet to be measured are marked "TBD" and those that are not applicable to a particular platform are marked "N/A".
Platform Benchmarks
This is a collection of benchmarks comparing mainly CPU speed and other data transfer operations. In below tests, AM389x@1GHz, and AM387x@800MHz.
RowboPerf: ARM
See RowboPERF User Guide for more information about these metrics. The RowboPerf application calls native executables compiled with Android's NDK to perform these tests.
| | AM389x | AM387x |
|---|---|---|
| Dhrystone | 948.59 DMIPS | 569.15 DMIPS |
| Whetstone | 250 MIPS | 166.7 MIPS |
| Linpack | 24524 Kflops | 14610 Kflops |
RowboPERF: 0xBench
See RowboPERF User Guide for more information about these metrics.
| Linpack | AM389x | AM387x |
|---|---|---|
| Mflops/s | 14.97 | 9.09 |
| Scimark2 | AM389x | AM387x |
|---|---|---|
| Composite | 18.45 | 11.02 |
| Fast Fourier Transform | 13.82 | 8.28 |
| Jacobi Successive Over-relaxation | 25.88 | 15.56 |
| Monte Carlo integration | 5.96 | 3.60 |
| Sparse matrix multiply | 16.88 | 10.01 |
| dense LU matrix factorization | 29.72 | 17.64 |
Boot Time
Numbers shown here measure the time from start of loading the kernel image to appearance of Android's Home Screen. These measurements are done using the default (pre-built) images provided with the DevKit. Please note that the very first time you boot your device, the boot time will be significantly higher (approx. 3-4 min).
| Time (secs) | AM389x | AM387x |
|---|---|---|
| SD First Boot Time1 | 60 | 66.2 |
| SD Boot Time | 23 | 27.9 |
1 First boot time refers to first time the system is booted with a freshly created SD card.
EDMA Test
Need to devise this test.
Memory Bandwidth
Need to devise this test.
Quadrant
These metrics were collected using the Quadrant performance benchmark available at http://www.aurorasoftworks.com/products/quadrant. The score for each of the platforms are reflected under the "Your device" bar.
AM389x
AM387x
Browser Performance
Sunspider
These metrics were collected using the well-known Sunspider performance benchmarks available at http://www2.webkit.org/perf/sunspider-0.9/sunspider.html
| Sunspider | AM389x | AM387x |
|---|---|---|
| Total | 6051.6 ms +/- 0.6% | 9734.1 ms +/- 1.3% |
AM389x
AM387x
V8
These metrics were collected using the v8 performance benchmarks available at http://v8.googlecode.com/svn/data/benchmarks/v6/run.html
| V8 | AM389x | AM387x |
|---|---|---|
| Total | 200 | 134 |
AcidTests
These metrics were collected using the acid browser tests available at http://acid3.acidtests.org/ . Additional information about the benchmark can be found at http://www.webstandards.org/action/acid3/
| Acid3 | AM389x | AM387x |
|---|---|---|
| Total | 93/100 | 93/100 |
Flash Player Performance
These metrics represent the frames per second (fps) and revolutions per minute (rpm) observed while using the browser to run FpsMeter.swf, Particules.swf and Donuts.swf from an MMC/SD card.
| Donuts(rpm) | AM389x | AM387x |
|---|---|---|
| 50 sec | 3.5 | 3.5 |
| 100 sec | 3.6 | 3.5 |
| 150 sec | 3.5 | 3.5 |
| FpsMeter(fps) | AM389x | AM387x |
|---|---|---|
| 3 objects | 29.3 to 30.17 | 26.7 to 30.08 |
| 4 objects | 28.67 to 30.08 | 28.4 to 30.01 |
| 5 objects | 28.06 to 30.25 | 26.6 to 30.08 |
| Particules(fps) | AM389x | AM387x |
|---|---|---|
| fps | 24.3 to 26.8 | 16.7 to 18.3 |
File Storage Performance
These tests were performed using the StorageIO application provided in RoboPerf. The application measures the write and read speed of different storage devices using several block sizes. For these tests the file size chosen was 100 MBytes. In order for the application to run the storage device chosen for the test must be mounted in the Android file system and a have read and write access. All the tests were perform on devices with a vfat file system.
1 The performance numbers for AM389x reported by the StorageIO application are not considered to be accurate and the root cause is being investigated.
MMC/SD Performance
| Throughput (MB/s) | AM389x | AM387x |
|---|---|---|
| Write, bs=512 | 6.8171 | 2.623 |
| Write, bs=4096 | 7.7051 | 2.887 |
| Write, bs=16384 | 7.9351 | 3.210 |
| Write, bs=65536 | 8.5851 | 3.044 |
| Write, bs=524288 | 10.0461 | 3.062 |
| Write, bs=1048576 | 12.0471 | 2.926 |
| Read, bs=512 | 39.8841 | 11.684 |
| Read, bs=4096 | 40.0831 | 11.961 |
| Read, bs=16384 | 188.5921 | 11.796 |
| Read, bs=65536 | 288.8631 | 11.016 |
| Read, bs=524288 | 355.4491 | 11.293 |
| Read, bs=1048576 | 350.6941 | 10.073 |
USB Performance
| Throughput (MB/s) | AM389x | AM387x |
|---|---|---|
| Write, bs=512 | 9.3781 | 2.228 |
| Write, bs=4096 | 47.5541 | 3.224 |
| Write, bs=16384 | 23.9511 | 3.089 |
| Write, bs=65536 | 33.3091 | 3.866 |
| Write, bs=524288 | 22.5641 | 4.051 |
| Write, bs=1048576 | 32.4631 | 3.538 |
| Read, bs=512 | 39.8541 | 7.983 |
| Read, bs=4096 | 184.2841 | 8.892 |
| Read, bs=16384 | 278.1361 | 10.770 |
| Read, bs=65536 | 335.0081 | 8.809 |
| Read, bs=524288 | 330.7811 | 9.629 |
| Read, bs=1048576 | 373.1581 | 8.853 |
SATA Hard Drive Performance
The SATA hard drive used for this test is a Hitachi model HTS541680J9SA00.
| Throughput (MB/s) | AM389x | AM387x |
|---|---|---|
| Write, bs=512 | 20.4961 | |
| Write, bs=4096 | 38.9801 | |
| Write, bs=16384 | 38.6351 | |
| Write, bs=65536 | 37.6911 | |
| Write, bs=524288 | 40.3911 | |
| Write, bs=1048576 | 37.3951 | |
| Read, bs=512 | 40.6891 | |
| Read, bs=4096 | 184.9341 | |
| Read, bs=16384 | 165.6511 | |
| Read, bs=65536 | 360.3351 | |
| Read, bs=524288 | 403.2981 | |
| Read, bs=1048576 | 404.8551 |
Connectivity Performance
These tests provide throughput comparison across commonly used transports/mediums.
Ethernet
Measures TCP Throughput between Server (running on Host PC) and Client (Android Platform) using different buffer sizes (bs in bytes) Both Server and client uses the Netperf utility. For more information about Netperf, please see Netperf Home page
| TCP Throughput | AM389x | AM387x |
|---|---|---|
| bs=16 | 136.22 Mb/s | 106.6 Mb/s |
| bs=1024 | 136.49 Mb/s | 101.69 Mb/s |
| bs=4096 | 263.99 Mb/s | 233.56 Mb/s |
| bs=8192 | 373.67 Mb/s | 233.56 Mb/s |
ADB
Measure Android Debug Bridge (ADB) throughput between Host PC and Android device by pushing and pulling a 20MB file with random content 10 times. TX and RX numbers are from the Host PC point of view, so TX is measured by doing "adb push" on the Host PC.
Ethernet
| ADB USB Throughput | AM389x | AM387x |
|---|---|---|
| TX | 4853.80 KB/s | 3905.40 KB/s |
| RX | 5050.20 KB/s | 5016.40 KB/s |
Graphics Performance
The display resolution for AM389x and AM387x is 1920x1080 pixels.
RowboPERF: 0xBench 2D
See RowboPERF User Guide for more information about these metrics.
| 2D | AM389x | AM387x |
|---|---|---|
| Draw Canvas (fps) | 30.87 | 21.88 |
| Draw Circle (fps) | 23.60 | 16.44 |
| Draw Circle2 (fps) | 14.11 | 10.44 |
| Draw Rect (fps) | 6.77 | 4.15 |
| Draw Arc (fps) | 14.58 | 9.58 |
| Draw Image (fps) | 7.90 | 5.51 |
| Draw Text (fps) | 38.40 | 24.57 |
RowboPERF: 0xBench 3D
See RowboPERF User Guide for more information about these metrics.
| 3D | AM389x | AM387x |
|---|---|---|
| OpenGL Cube (fps) | 30.90 | 23.59 |
| OpenGL Blending (fps) | 30.89 | 22.11 |
| OpenGL Fog (fps) | 30.83 | 22.92 |
| OpenGL Teapot (fps) | 30.30 | 22.60 |
Versioning
This is Release DevKit-V2.3 v2.0. The release is available from http://software-dl.ti.com/dsps/dsps_public_sw/sdo_tii/TI_Android_DevKit/TI_Android_GingerBread_2_3_DevKit_2_0/index_FDS.html