Android am389x build procedure
From Texas Instruments Embedded Processors Wiki
Build procedure document for Android on AM389x
Android on AM389xEVM Guide - Nov 10, 2010
Requirements
This section describes the list of Software and Hardware requirements to set-up Android on AM389x.
- Hardware Requirements:
This build set-up is verified is evaluated on the below given list of platforms. This package should be easily portable on other platforms on similar TI devices.
| TI Device | Platform Supported | Version | Other Accessories |
|---|---|---|---|
| AM389x | AM389x EVM | Rev B | TV/Monitor with HD component capability, USB Keyboard, USB Mouse, Ethernet, UART Cable, Audio Speakers, MMC/SD Card (2GB min), am389xevm processor fan |
- Software Requirements:
If you are a Android application developer or would like to use Android SDK Tools then refer to http://developer.android.com/sdk/requirements.html for Host PC requirements.
To evaluate this release we recommend you to have a Linux "Ubuntu 8.04 or above" Host machine, See Ubuntu Linux installation notes
Build requirements at HOST machine
- Refer to arowboat.org for software requirements at host side
- Installing the repo tool:
$ curl http://android.git.kernel.org/repo > ~/bin/repo $ chmod a+x ~/bin/repo
Hardware Setup
- AM389xEVM with a processor fan and a 12V/5.0A Power Supply.
- BOOT/CFG(SW3 switch), configured for MMC booting as shown below:
| Switch | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 |
| State | ON | ON | ON | OFF | ON | OFF | OFF | OFF | OFF | OFF |
- A network cable and working ethernet connection for NFS mount and/or for tftpboot.
- A USB mouse and keyboard for input.
- TV with HD component output capability connected to AM389xEVM board through component out and Audio output(3.5mm jack) device connected to HP out(P2).
Software versions used in this release
- Android 2.2 Froyo release from arowboat.org
- AM389xEVM u-boot and kernel-2.6.34 from PSP v04.00.00.07 release and then kernel backported to Android-2.6.32 kernel
- SysLink v02.00.00.56_alpha2 release
- IPC v1.22.00.10 release
Configuring the HOST build environment
- Exporting top level Android root directory where Rowboat-Froyo sources are cloned.
$ export ANDROID_ROOT=~/rowboat-android
- Adding Android and code-sourcery toolchain in the default PATH.
Note: code-sourcery arm-2010q1 toolchain is used to build u-boot.bin and MLO.
$ export PATH=$ANDROID_ROOT/prebuilt/linux-x86/toolchain/arm-eabi-4.4.0/bin:<code_sourcery_toolchain_installed_path>/arm-2010q1/bin:$PATH
- Exporting SysLink and IPC directories.
$ export SYSLINK_ROOT=$ANDROID_ROOT/hardware/ti/am389x/syslink/syslink_02_00_00_56_alpha2/
$ export IPCDIR=$ANDROID_ROOT/hardware/ti/am389x/syslink/ipc_1_22_00_10_eng/packages
- Exporting the Rootfs directory which can be used as a NFS share as well.
$ export NFS_ROOT=$ANDROID_ROOT/out/target/product/am389xevm/android_rootfs
- Exporting the u-boot source directory.
$ export UBOOT=~/u-boot-04.00.00.07
Downloading the AM389xEVM Android Froyo(Rowboat) sources
$ mkdir $ANDROID_ROOT $ cd $ANDROID_ROOT $ ~/bin/repo init -u git://gitorious.org/rowboat/manifest.git -m rowboat-froyo-am389x.xml $ ~/bin/repo sync
Building AM389xEVM Android Froyo(Rowboat) rootfs
$ cd $ANDROID_ROOT $ make TARGET_PRODUCT=am389xevm
$ mkdir $NFS_ROOT $ cp -rf $ANDROID_ROOT/out/target/product/am389xevm/root/* $NFS_ROOT $ cp -rf $ANDROID_ROOT/out/target/product/am389xevm/system $NFS_ROOT $ cp -rf $ANDROID_ROOT/device/ti/am389xevm/syslink $NFS_ROOT/system/bin
Building MLO and u-boot with MMC/SD support
- Building MLO:
$ cd $UBOOT $ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm distclean $ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm ti8168_evm_min_sd $ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm u-boot.ti $ cp u-boot.min.sd MLO
- Building u-boot:
$ cd $UBOOT $ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm distclean $ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm ti8168_evm_config $ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm u-boot.ti
Building AM389xEVM kernel
$ cd $ANDROID_ROOT/kernel $ make ARCH=arm CROSS_COMPILE=arm-eabi- clean $ make ARCH=arm CROSS_COMPILE=arm-eabi- ti8168_evm_android_defconfig $ make ARCH=arm CROSS_COMPILE=arm-eabi- uImage
Building and installing the SysLink
- Building the SysLink module:
$ cd $ANDROID_ROOT/hardware/ti/am389x $ tar xjf syslink_vpss.tar.bz2 $ cd $SYSLINK_ROOT/ti/syslink/utils/hlos/knl/Linux $ make ARCH=arm CROSS_COMPILE=arm-eabi- SYSLINK_PLATFORM=TI81XX clean $ make ARCH=arm CROSS_COMPILE=arm-eabi- SYSLINK_PLATFORM=TI81XX
- Building the SysLink user library:
$ cd $SYSLINK_ROOT/ti/syslink/utils/hlos/usr/Linux $ make ARCH=arm CROSS_COMPILE=arm-eabi- SYSLINK_PLATFORM=TI81XX clean $ make ARCH=arm CROSS_COMPILE=arm-eabi- SYSLINK_PLATFORM=TI81XX
- Building the ProcMgr binary:
$ cd $SYSLINK_ROOT/ti/syslink/samples/hlos/procMgr/usr/Linux $ make ARCH=arm CROSS_COMPILE=arm-eabi- SYSLINK_PLATFORM=TI81XX clean $ make ARCH=arm CROSS_COMPILE=arm-eabi- SYSLINK_PLATFORM=TI81XX
- Installing the SysLink module, ProcMgr and M3 firware to the Rootfs:
$ cp $SYSLINK_ROOT/ti/syslink/utils/hlos/knl/Linux/syslink.ko $SYSLINK_ROOT/ti/syslink/lib/samples/procmgrapp.exe \
$ANDROID_ROOT/hardware/ti/am389x/ti816x_hdvpss/ti816x_hdvpss.xem3 $NFS_ROOT/system/bin/syslink/
Building and installing VPSS/TI816xFB
- Building VPSS/TI816xFB and other kernel modules:
$ cd $ANDROID_ROOT/kernel $ make ARCH=arm CROSS_COMPILE=arm-eabi- KBUILD_EXTRA_SYMBOLS=$SYSLINK_ROOT/ti/syslink/utils/hlos/knl/Linux/Module.symvers modules
- Installing vpss/ti816xfb modules to the Rootfs:
$ make ARCH=arm CROSS_COMPILE=arm-eabi- INSTALL_MOD_PATH=$NFS_ROOT/system/ \
KBUILD_EXTRA_SYMBOLS=$SYSLINK_ROOT/ti/syslink/utils/hlos/knl/Linux/Module.symvers modules_install
- Default output channel for fb0 is HDMI. To change it to HDCOMP set 'hdcomp_out=1' in $NFSROOT/system/bin/syslink/rc.syslink
Install the Android Graphics SGX SDK on Host Machine
Untar AM389x_Android_SGX_SDK.tar.gz to some suitable location.
After extracting following directory structure should be seen.
root@android-pc:~/AM389x_Android_SGX_SDK# ls ANDROID_RN_3_01_00_03.pdf GFX_Linux_SDK gfx_rel_es5.x_android Makefile.KM.Android ANDROID_RN_3_01_00_03.txt gfx_rel_es2.x_android initrc.patch Rules.make GFX_Linux_KM gfx_rel_es3.x_android Makefile uninstall::
Edit Rules.make to configure the SGX source build
1) #set home area HOME (relative location for all SDK operations) HOME=INVALIDVAL
2) #Current Directory where Graphics SDK is installed GRAPHICS_INSTALL_DIR=$(HOME)/AM389x_Android_SGX_SDK
3) #Path of Android Root FS ANDROID_ROOT=$(HOME)/INVALIDVAL
4) #set toolchain root path for arm-eabi CSTOOL_DIR=INVALIDVAL
5) #set the kernel installation path KERNEL_INSTALL_DIR=$(HOME)/INVALIDVAL
Example:
HOME=/home/user GRAPHICS_INSTALL_DIR=$(HOME)/AM389x_Android_SGX_SDK ANDROID_ROOT=$(HOME)/rowboat-android/out/target/product/am389xevm/android_rootfs CSTOOL_DIR=$(HOME)/rowboat-android/prebuilt/linux-x86/toolchain/arm-eabi-4.4.0/ KERNEL_INSTALL_DIR=$(HOME)/rowboat-android/kernel
Build the Kernel Module sources
Execute the make command in the sources directory
root@android-pc:~/AM389x_Android_SGX_SDK# make
Will display:
copying the sgx kernel modules to appropriate folder...
Install the SGX drivers in Target filesystem
Install the SGX drivers in the root filesystem built
root@android-pc:~/AM389x_Android_SGX_SDK# make install OMAPES=5.x
Packaging the rootfs
$ cd $ANDROID_ROOT/out/target/product/am389xevm $ sudo ../../../../build/tools/mktarball.sh ../../../host/linux-x86/bin/fs_get_stats android_rootfs . rootfs rootfs.tar.bz2
Preparing the MMC card
Use the mk-mmc utility provided in TI_Android_DevKit 02_00_00 release to populate the SD Card. This utility helps users create a MMC/SD Card with required Images to boot Android on any given TI platform.
- Execute the following command:
Example:
$ ./mkmmc-android /dev/sdc $UBOOT/MLO $UBOOT/u-boot.bin $ANDROID_ROOT/kernel/arch/arm/boot/uImage boot.scr $NFS_ROOT/../rootfs.tar.bz2
This populates the SD/MMC card with all the images.
NOTE:
To create the boot.scr boot script use the mkbootscr tool found in the same package. You can set the bootargs as mentioned in the next section.
YAFFS2 rootfs image on NAND
Do not try this at the moment, Use MMC/NFS boot instead
- Copy the rootfs.tar.bz2 file-system created above to the rootfs partition of MMC/SD card.
host$ sudo cp $NFS_ROOT/../rootfs.tar.bz2 <mount_point>/rootfs
- Now boot the device from MMC by setting the MMC/SD bootargs from the next section.
- Run the following commands from target board
- Determine the MTD device for the file system partition of you Flash device
target# cat /proc/mtd
You should see output similar to:
target# cat /proc/mtd dev: size erasesize name mtd0: 00260000 00020000 "U-Boot" mtd1: 00020000 00020000 "U-Boot Env" mtd2: 00440000 00020000 "Kernel" mtd3: 0c820000 00020000 "File System" mtd4: 03120000 00020000 "Reserved"
The file system partition of the flash device is /dev/mtd/mtd3
- Erase the file system partition
target# flash_eraseall /dev/mtd/mtd3
You should see output similar to:
target# flash_eraseall /dev/mtd/mtd3 Erasing 16 Kibyte @ 3b9c000 -- 99 % complete.
- Mount the Flash file system partition using the block device node on a temporary directory /tempd.
target# mkdir /tempd
NOTE: For small block NAND devices (i.e. DM6446) you must mount the file system as a YAFFS file system. For large block NAND devices (i.e. DM355/AM389X) the file system should be mounted as YAFFS2. Using the wrong version of YAFFS will result in error messages similar to:
target# mount -t yaffs2 /dev/block/mtdblock3 /tempd
yaffs: dev is 32505859 name is "mtdblock3"
yaffs: Attempting MTD mount on 31.3, "mtdblock3"
yaffs: MTD device does not support have the right page sizes
mount: wrong fs type, bad option, bad superblock on /dev/mtdblock3,
or too many mounted file systems
- Untar the contents of the tarball file system image to the Flash device
target# cd /tempd target# date MMDDhhmmCCYY (this is month,day,hour,minute,century,year format. i.e. for May 22 10:15 2008 this would be "date 052210152008") target# busybox tar xjf /rootfs.tar.gz
NOTE: The date command is used to avoid warnings about time differences
- Unmount the Flash file system partition
target# cd / target# umount /tempd
- Now the target is ready to mount the rootfs from NAND.
Setting the Bootargs
- For NFS boot:
$ setenv bootargs 'mem=166M@0x80000000 mem=768M@0x90000000 console=ttyS2,115200n8 androidboot.console=ttyS2 noinitrd init=/init rw vram=50M ip=dhcp root=/dev/nfs nfsroot=<nfs_root_ip_address>:<nfs_root_path>,nolock'
- For MMC boot:
$ setenv bootargs 'mem=166M@0x80000000 mem=768M@0x90000000 console=ttyS2,115200n8 androidboot.console=ttyS2 noinitrd init=/init rw vram=50M ip=dhcp root=/dev/mmcblk0p2 rootfstype=ext3'
- For NAND boot:
$ setenv bootargs 'mem=166M@0x80000000 mem=768M@0x90000000 console=ttyS2,115200n8 noinitrd rw root=/dev/mtdblock3 rootfstype=yaffs2 rootwait ip=dhcp init=/init androidboot.console=ttyS2'
Known Issues
- Video overlays are not supported in this release.
- Audio recording is working but playback from Audio Recorder application is not working. Recordings can be played from Music application.
- USB Mouse/Keyboard have hot-plug issues. *Sometimes* they don't work on hot-plug.
- USB OTG is not supported.
- Composite, SVideo and RGB display output is not supported in this release.