Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

BIN2TDF

From Texas Instruments Wiki
Jump to: navigation, search

Introduction

This page describes usage of BIN2TDF utility. BIN2TDF utility is delivered as part of Code Composer Studio (CCS) and used to convert field captured hardware trace data into a format (.tdf) that can be imported in standalone CCS Trace Visualizer.

Location

This utility gets installed in CCS_DIR/ccsv5/ccs_base/emulation/analysis/bin directory as part of Code Composer Studio installation. To use this utility, open a command line shell and change directory to CCS_DIR/ccsv5/ccs_base/emulation/analysis/bin.

Parameters

Required

-bin <Full path to binary file>
This parameter is used to specify the trace binary file.


-app <Full path to out file>
This parameter is used to specify full path of the application location. Trace decoders use application information to decompress and output the trace information.
If using software messages from STM, this parameter needs to be specified with CPU qualification (i.e. CPU=file). More than one of such entries can be specified with comma(,) seperations e.g. CPU0=file0,cpu1=file1,...

It is sufficient to give just the name after the slash (e.g., C66XX_0) as CPU name, it is not required to use full CPU name as formed in CCS (e.g., Blackhawk XDS560v2-USB Mexxanine Emulator_0/C66XX_0).

If there is only one processor generating STM SW messages, CPU qualification could be skipped

Note: If you are using CCSv4, this parameter name would be -outfile.  


-procid <proc>
This parameter is used to specify processor or trace type.  Valid options - 64x, 64x+, 66x, 55x, 55x+, arm7, arm9, arm11, cortexa8, and stm.

Note: If you are using CCSv4, this parameter name would be -cpuid.


-rcvr <receiver name>

This parameter is used to specify receiver type used for trace collection. Valid options - ETB, 560T, 560V2, and Pro


Required for STM (Optional for DSP and ARM/Cortex trace)

-devicekey DeviceID
This parameter is used to define the device ID or device key for identifying STM topology in the device. This is a unique ID (TAP ID) and can be read via R0 of ICEPICK or retreived from the device TRM.

Examples:

Device id for

     OMAP4430 ES2      -- 0x1B85202F

     OMAP4430 ES2.1   -- 0x3B95C02F

     OMAP4460              --  0x0B94E02F

     OMAP4470              -- 0x0B97502F

     C6678                     -- 0x0009E02F

     C6670                     -- 0x0009D02F

Turbo-C6670/TCI6618     -- 0x0b94102F

     TCI6614/2                -- 0x0B96202F

     C6657/5/4                -- 0xB97A02F

     AM335x                  -- 0x0B94402F

     AM386x                   -- 0x0B96802F

     AM387x                   -- 0x0B8F202F

     DM816x                   -- 0x0B81E02F 

 

Note: If you are using CCSv4, this parameter name would be -deviceid.


-dcmfile <Full path to the metadata file>
This parameter is used to pass additional metadata to help decode. Default is none.
For STM ETB, you could create a foo.dcm configuration file by copying the text in the box below into a text file and saving it with a name like foo.dcm or whatever you prefer.

STM_data_flip=1
STM_Buffer_Wrapped=0
HEAD_Present_0=0
HEAD_Pointer_0=
HEAD_Present_1=1
HEAD_Pointer_1=4


STM_data_flip=1 --> This field tells decoder that the data is flipped in receiver packing. This is 1 if using ET. Otherwise, its 0. 

STM_Buffer_Wrapped=0 --> This field tells decoder that the buffer is wrapped or not. 1 is wrapped, 0 for buffer not wrapped. 

HEAD_Present_0=0  --> STM ETB pointer references to efficiently detect start of the buffer (if buffer wrapped). Default to 0 unless you know the HEAD information.

HEAD_Pointer_0=0 --> STM ETB pointer references to efficiently detect start of the buffer (if buffer wrapped). Default to 0 unless you know the HEAD information.

HEAD_Present_1=0 --> STM ETB pointer references to efficiently detect start of the buffer (if buffer wrapped). Default to 0 unless you know the HEAD information.

HEAD_Pointer_1=0 --> STM ETB pointer references to efficiently detect start of the buffer (if buffer wrapped). Default to 0 unless you know the HEAD information.

Optional

-output <TDFFileName>

This parameter is used to specify output TDF file name. Defaul is <BinaryFileName>.tdf.

Note: If you are using CCSv4, this parameter name would be -tdf.

 

-sourcepaths <"Source paths">
This parameter is used to specify source path location to help Trace Visualizer locate the source files. Multiple paths can be specified with comma seperated string. The Trace Visualizer automatically searches in the sub-directories. Default is empty source path string.

 

 

Examples

DSP Trace

bin2tdf -bin C:/temp/etbdata.bin -app C:/Examples/bin/csetbexample.tci6488.out -procid 64x+ -rcvr ETB -output C:/Examples/bin/mytrace.tdf


ARM Trace

bin2tdf.exe -bin c:/temp/ETM_etbdata.bin -app C:/Examples/bin/etm_csetb_A8.c6a816x.out -procid cortexa8 -rcvr ETB -dcmfile c:/temp/ETM_etbdata.dcm -output C:/Examples/bin/etm_csetb_A8.c6a816x.tdf

Note: If the device has more than one ARM core, the -cpuname parameter will need to be specified.

bin2tdf.exe -bin c:/temp/ETM_etbdata.bin -app C:/Examples/bin/ptm_tietb_d_A15.c66ak2hxx.out -procid cortexa15 -rcvr ETB -dcmfile c:/temp/ETM_etbdata.dcm -output C:/temp/ptm_tietb_d_A15.c66ak2hxx.tdf -cpuname CortexA15_0


System Trace

bin2tdf -bin C:/temp/etbdata.bin -app C66X_0=C:/Examples/bin/tietbexample_d.c66xxstm.out -procid stm -rcvr ETB -devicekey 0x0009D02F -dcmfile C:/temp/foo.dcm -output C:/Examples/bin/mytrace.tdf


bin2tdf -bin C:/temp/etbdata.bin -app CortexA8_0=C:/Examples/bin/csetbexample_d.ti816xstma8.out -procid stm -rcvr ETB -devicekey 0x0B81E02F -dcmfile C:/temp/foo.dcm -output C:/Examples/bin/mytrace.tdf



Related