BeagleBone-Android-DevKit Guide
From Texas Instruments Embedded Processors Wiki
Contents
|
What is BeagleBone
The BeagleBone is the low-cost, high-expansion hardware-hacker focused BeagleBoard. It is a bare-bones BeagleBoard that acts as a USB or Ethernet connected expansion companion for your current BeagleBoard and BeagleBoard-xM or works stand-alone. The BeagleBone is small even by BeagleBoard standards and with the high-performance ARM capabilities you expect from a BeagleBoard, the BeagleBone brings full-featured Linux to places it has never gone before.
BeagleBone Features
| | Feature |
| Processor | 720MHZ AM3359 15x15 |
| Memory | 256MB DDR2 200MHz (128MB Optional) |
| PMIC TPS65217 | Power Regulators LiION Single cell battery charger (via expansion) 20mA LED Backlight driver, 39V, PWM (via expansion) |
| Debug Support | USB to Serial Adapter, On Board JTAG via USB, miniUSB connector, 4 USER LEDs Optional 20-pin CTI JTAG |
| Power | 5VDC External jack USB |
| PCB | |
| Indicators | Power 4-User Controllable LEDs |
| HS USB 2.0 Client Port | Access to the USB1 Client mode |
| HS USB 2.0 Host Port | USB Type A Socket, 500mA LS/FS/HS |
| Ethernet | 10/100, RJ45 |
| SD/MMC Connector | microSD , 3.3V |
| User Interface | 1-Reset Button |
| Overvolatage Protection | Shutdown @ 5.6V MAX |
| Expansion Connectors | Power 5V, 3.3V , VDD_ADC 3.3V I/O on all signals McASP0, SPI1, I2C, GPIO(65), LCD, GPMC, MMC1, MMC2, 7 AIN(1.8V MAX), 4 Timers, PRI_MII0, 3 Serial Ports, CAN0, EHRPWM(0,2),XDMA Interrupt, Power button, Battery Charger, LED Backlight, Expansion Board ID (Up to 3 can be stacked) |
BeagleBone Unique Characteristics
Open Low Cost High Performance Board
BeagleBone has ARM CortexA8 720MHz + 3D graphics acceleration with SGX and priced at a very low $89 with Open community support from beagleboard.org and arowboat.org
Single Cable to provide Power, Debug and Serial
Mini USB Cable from BeagleBone to the Host Machine can provide Power, Debug and Serial connections at the same time.
BeagleBone offers an easy replacement for underpowered micro-controller-based controller boards
BeagleBone offers extensive expansion, on-chip Ethernet, analog-to-digital data conversion and a lower cost. Much more applications are supported on BeagleBone since High level OS like Android and Linux is supported
Android on BeagleBone
BeagleBone is a very low cost EVM, equiped with ARM Cortex A8 processor and SGX.
This platform is well suited as a development platform for low-end and mid-end android solutions.
Moreover the Android solution on BeagleBone can be used as an Open Accessory Kit for connecting to other Android Devices.
Objective of this wiki page
This wiki page has mainly two objectives
- Quickly evaluate Android GingerBread using pre-built images
- Start develop using sources
A newer release of TI Android DevKit for BeagleBone is available. See TI-Android-ICS-4.0.3-DevKit-3.0.1 ReleaseNotes for more details.
Installation and Usage
This section explains how to prepare a micro-sd card for booting android on the BeagleBone. The details on booting the BeagleBone and evaluating Android is also explained.
Getting Prebuilt Images
BeagleBone Prebuilt SD card image from TI Android DevKit download page
Prepartion of SD card
Connect a Micro SD card (Atleast 2GB size and Class 4) via a USB card reader on an Ubuntu Machine
From a terminal, type the below commands,
$ tar -xzvf BeagleBone.tar.gz $ cd BeagleBone $ sudo ./mkmmc-android.sh /dev/sd<device>
The above step prepares the SD Card with three partitions.
- boot - Boot Images (Boot Loaders, Boot Script and Kernel)
- rootfs - Filesystem (Android GingerBread 2.3.4)
- data - Media Clips (Audio, Video and Images)
Now this card can be used to boot the BeagleBone
Hardware setup
Connect MiniB USB Cable, Ethernet Cable and 5V DC Power to the BeagleBone and have it powered. Windows or Linux Host can be used to connect and evaluate BeagleBone. We prefer to use Ubuntu 10.04 as the host to connect to BeagleBone.
Getting serial console
Serial console is provided via MiniB USB connection between the BeagleBone and the Host.
In Windows
Side note: it may be possible to download BONE_DRV.exe for 32-bit Windows or BONE_D64.exe for 64-bit Windows to avoid needing to manually edit the driver entries, but this has not yet been validated.
For Windows XP, Download FTDI driver from http://www.ftdichip.com/Drivers/CDM/CDM20814_WHQL_Certified.zip
Extract the contents and edit the ftdibus.inf file
Replace the section between
[FtdiHw]
and
[FtdiHw.NTamd64]
with the following content
%USB\VID_0403&PID_A6D0.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_A6D0 %USB\VID_0403&PID_A6D0&MI_00.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_A6D0&MI_00 %USB\VID_0403&PID_A6D0&MI_01.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_A6D0&MI_01 %USB\VID_0403&PID_A6D0&MI_00.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_A6D0&MI_00 %USB\VID_0403&PID_A6D0&MI_01.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_A6D0&MI_01 %USB\VID_0403&PID_A6D0&MI_02.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_A6D0&MI_02 %USB\VID_0403&PID_A6D0&MI_03.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_A6D0&MI_03 %USB\VID_0403&PID_A6D0.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_A6D0
Also
Replace the section between
DriversDisk="FTDI USB Drivers Disk"
and
SvcDesc="USB Serial Converter Driver"
with the following content
USB\VID_0403&PID_A6D0.DeviceDesc="USB Serial Converter" USB\VID_0403&PID_A6D0&MI_00.DeviceDesc="USB Serial Converter A" USB\VID_0403&PID_A6D0&MI_01.DeviceDesc="USB Serial Converter B" USB\VID_0403&PID_A6D0&MI_00.DeviceDesc="USB Serial Converter A" USB\VID_0403&PID_A6D0&MI_01.DeviceDesc="USB Serial Converter B" USB\VID_0403&PID_A6D0&MI_02.DeviceDesc="USB Serial Converter C" USB\VID_0403&PID_A6D0&MI_03.DeviceDesc="USB Serial Converter D" USB\VID_0403&PID_A6D0DeviceDesc="USB Serial Converter"
Then follow these steps
- Boot the board
- Connect Mini B USB cable between board and Windows PC.
- If it is proceeding as planned, Windows will tell you it found a new hardware asks you to install the driver. Install driver that was downloaded as described in the above step
- Answer "No, not this time" to the question about running Windows Update to search for software.
- Choose "Install the hardware that I manually select from a list (Advanced)" this is the 2nd option, then click "Next"
- Select "Show All Devices", then click "Next"
- You are going to see a grayed-out text box with "(Retrieving a list of all devices)", click the "Have Disk..." button
- Browse" to your driver folder (c:\...\_driver). It will be looking of a .inf file so select "ftdibus.inf" and click "Open" then "OK".
- Select "USB Serial Port" then click the "Next" button.
- A warning will appear, answer "Yes" but read the warning anyway.
- Click the "Close" when the wizard is completed.
- Disconnect and reconnect Mini B USB cable from Board(probably reboot it as well).
- Serial COM port will be listed on the Terminal Utility menu
- Adjust the baudrate to 115200 to connect to the BeagleBone serial.
In Linux
To get serial console output on ubuntu follow these steps:
$ sudo modprobe ftdi_sio vendor=0x0403 product=0xa6d0
$ minicom -D /dev/`dmesg | grep FTDI | grep "now attached to" | tail -n 1 | awk '{ print $NF }'`
- You might need to make sure minicom's serial port setup is for 115200n8 with hardware flow control. You can get into the minicom configuration menu by invoking 'minicom -s' and selecting serial port setup -> Serial Device (option A).
- You may have to run minicom with sudo in case sufficient permission is not available for the USB serial node
Verifying Serial Connection
Once you finish setting up serial console, you can test the connection via the below steps
- Push the small black reset button beside ethernet port
- If your serial connection is proper, you can see the sequnce 'CCCC' getting popped up on the serial console.
Powering on to Android Terminal
Put the Micro SD card to the slot on the BeagleBone. Press the reset button again. See X-loader and Uboot loading. Allow the boot loader to run the boot script uEve.txt to run.Kernel boots up and Android shell is activated. Wait till Android init to start the zygote thread.
See the below message appearing on the shell.
warning: `zygote' uses 32-bit capabilities (legacy support in use)
Android Display through VNC
Since the BeagleBone currently does not have a display output, we rely on VNC connection from the Host to the BeagleBone. Here are the steps to establish VNC connection between the BeagleBone to the Host PC
Setup Ethernet and VNC server
Make sure Ethernet port on board and host machine are connected to the network. Check Ethernet configuration for the board
# netcfg lo UP 127.0.0.1 255.0.0.0 0x00000049 eth0 DOWN 0.0.0.0 0.0.0.0 0x00001002
If Ethernet was not configured, configure Ethernet of the board using ifconfig/netcfg as shown below.
# netcfg eth0 up # netcfg eth0 dhcp
Wait for the Ethernet configuration to complete. If you see the above command taking too much time the Ethernet cable may be loose. Attach the Ethernet cable once again on the port and type the command again. You can check the Configuration again via type netcfg command to se Ethernet is configured.
# netcfg lo UP 127.0.0.1 255.0.0.0 0x00000049 eth0 UP 172.24.191.37 255.255.252.0 0x00001043
Now VNC server can be started in the background.
# androidvncserver &
Connecting to target from Host
Using VNC Viewer application user can connect to the Beaglebone at the target address [say 172.24.191.37] port 5901.
USB Debugging
Android Debug Bridge (adb) is a versatile tool lets you manage the state of the Android-powered device. For more information about what is possible with adb, see Android Debug Bridge page at http://developer.android.com/guide/developing/tools/adb.html. The ADB tool can be used to
- Download an application from a host machine, install & run it on the target board.
- Start a remote shell in the target instance.
- Debug applications running on the device using the debugging tool DDMS ( Dalvik Debug Monitor Server) which runs on top of adb connection.
- Copy files to and from the board to host machine
Please visit http://processors.wiki.ti.com/index.php/Android_ADB_Setup for setting up ADB on BeagleBone
Running Android Applications
Keypad mappings
The below table lists the keypad and USB Keyboard mappings to Android UI functionality
| Functionality | USB Keyboard/Mouse |
| Home Screen | Home |
| Left | Left Arrow |
| Right | Right Arrow |
| Up | Up Arrow |
| Down | Down Arrow |
| Volume Up | Volume Up |
| Volume Down | Volume Down |
| Contacts | F3 |
| Power | |
| Select | Enter |
| Back / Previous screen | Mouse right |
| Menu | F1 |
Android Home Screen
After the first boot, the user will see an unlocked Android home screen. On subsequent boot, a locked screen will be displayed. User need to unlock the screen via Mouse/ Keyboard [Either HOST or TARGET]. YOu can easily unloack the screen via Pressing the F1 key on the keyboard. Once the screen is unlocked, the user can navigate to Google Search, Tips, Browser or Application Launcher. Click the Application Launcher to see all pre-built applications.
Gallery Application
In Gallery, the user can view the images and play videos.
Rowboperf and 3D graphics applications
RowboPERF is comprehensive set of banchmarks and Demos.
Select the rowboperf icon and get into the app directory. For more information on RowboPERF, please check RowboPERF User Guide
Browser Configuration
To browse web pages user should configure the Internet connection as given below.
# netcfg eth0 up # netcfg eth0 dhcp # getprop net.eth0.dns1
This prints the dns for the ethernet port, do the following to configure the DNS entries on board.
# setprop net.dns1 <your_dns_server_ip>
If the platform is behind proxy, then following command should be executed to set the proxy settings
# setprop net.gprs.http-proxy http://proxyurl:80
USB Mouse/Keyboard
Then connect USB Mouse/Keyboard to USB HOST port . The keyboard/mouse will be functional if it was plugged in while booting.
Otherwise type the below command to make it functional
# echo F > /proc/driver/musb_hdrc.1
Developing with source code
This section show the steps to obtain the complete source code for the android images(Boot loader, Kernel and Filesystem) and to build the same.
Host (PC) setup requirements
The host development environment for Android is based on Ubuntu, please install Ubuntu version 10.04 or later http://www.ubuntu.com/desktop/get-ubuntu/download. The host installation would need few more Android specific dependencies, these can be installed dynamically over network using below commands.
For Ubuntu on 32-bit machines
$ sudo add-apt-repository "deb http://archive.canonical.com/ lucid partner" $ sudo add-apt-repository "deb-src http://archive.canonical.com/ubuntu lucid partner" $ sudo apt-get update $ sudo apt-get install git-core gnupg sun-java6-jdk flex bison gperf libsdl-dev libesd0-dev libwxgtk2.6-dev build-essential zip curl libncurses5-dev zlib1g-dev minicom tftpd uboot-mkimage expect $ sudo update-java-alternatives -s java-6-sun
NOTE: Android Gingerbread (2.3.4) needs Java 6 on ubuntu, whereas the previous version FroYo (2.2) was using Java 5.
Getting Source Code
Developers can download the sources from the gitorious.org/rowboat repository.
A tool called 'Repo' helps to fetch the android sources from gitorious.org/rowboat. Repo is a tool that makes it easier to work with Git in the context of Android.
For more information about Repo, see the link http://source.android.com/source/version-control.html.
To install, initialize, and configure Repo, follow these steps:
Make sure you have a bin/ directory in your home directory, and that it is included in your path:
$ mkdir ~/bin $ PATH=~/bin:$PATH
Download the Repo script and ensure it is executable:
$ curl https://dl-ssl.google.com/dl/googlesource/git-repo/repo > ~/bin/repo $ chmod a+x ~/bin/repo
The following commands help developers to clone sources from www.gitorious.org/rowboat repository
$ mkdir $HOME/rowboat-android $ cd $HOME/rowboat-android $ repo init -u git://gitorious.org/rowboat/manifest.git -m rowboat-gingerbread-am335x.xml $ repo sync
Building Source Code
Tool chain setup
Setup the tool-chain path to point to arm-eabi- tools in prebuilt/linux-x86/toolchain/arm-eabi-4.4.3/bin
$ export PATH=$HOME/rowboat-android/prebuilt/linux-x86/toolchain/arm-eabi-4.4.3/bin:$PATH
Compilation procedure
To build MLO and boot loader (u-boot)
- Change directory to u-boot
$ cd u-boot
- Execute the following commands
$ make CROSS_COMPILE=arm-eabi- distclean $ make CROSS_COMPILE=arm-eabi- am335x_evm_config $ make CROSS_COMPILE=arm-eabi-
- This command will generate the MLO and the u-boot Image "u-boot.img"
NOTE: Copy the "mkimage" from "tools" folder to /usr/bin folder on your host machine, this is needed for kernel uImage generation
To build Linux kernel
- Change directory to kernel
$ cd kernel
- Do the following to build kernel sources for BeagleBone
$ make ARCH=arm CROSS_COMPILE=arm-eabi- distclean $ make ARCH=arm CROSS_COMPILE=arm-eabi- beaglebone_android_defconfig $ make ARCH=arm CROSS_COMPILE=arm-eabi- uImage
- This will generate uImage (kernel image) in kernel/arch/arm/boot folder
To build Android filesystem
- RowboPERF Integration
- Download the sources from rowboat
$ git clone -b rowboat-gingerbread git://gitorious.org/rowboat/rowboperf.git $ cd rowboperf
NOTE: Clone RowboPERF sources inside the rowboat-android tree.
- Have Android SDK in the PATH of the host machine
- Android filesystem build will take care of the integration of rowboperf applications
- Android VNC Server Integration
- Download the sources from rowboat
$ git clone -b rowboat-gingerbread git://gitorious.org/rowboat/droid-vnc-server.git
NOTE: Clone droid-vnc-server sources inside the rowboat-android tree.
- Android filesystem build will take care of the integration of android vnc server application
To Build the root file system for begleBone, from android source top directory, type the following command
$ make TARGET_PRODUCT=beaglebone OMAPES=4.x
The above command will build Android FS, kernel, SGX drivers. After successful build, the kernel image can be found at kernel/arch/arm/uImage. Android rootfs components (root and system folders) will be located in out/target/product/beaglebone. SGX drivers and libraries are installed in Android rootfs components.
Create root filesystem tarball
Prepare the root filesystem as follows:
$ cd out/target/product/beaglebone $ mkdir android_rootfs $ cp -r root/* android_rootfs $ cp -r system android_rootfs $ sudo ../../../../build/tools/mktarball.sh ../../../host/linux-x86/bin/fs_get_stats android_rootfs . rootfs rootfs.tar.bz2
The rootfs.tar.bz2 is the android filesystem, it can be put on a SD/MMC Card or used our NFS.
To generate SD/MMC card to boot Android
These compiled Images can be copied to a SD / MMC card to boot Android on the BeagleBone.
The text file uEnv.txt is required to provide the boot commands and boot arguments.
Generate a text file uEnv.txt with the following contents
bootargs=console=ttyO0,115200n8 androidboot.console=ttyO0 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait init=/init ip=off bootcmd=mmc rescan ; fatload mmc 0 81000000 uImage ; bootm 81000000 uenvcmd=boot
Copy all the images to one folder
$ mkdir image_folder $ cp kernel/arch/arm/boot/uImage image_folder $ cp u-boot/u-boot.img image_folder $ cp u-boot/MLO image_folder $ cp out/target/product/beaglebone/rootfs.tar.bz2 image_folder $ cp Media_clips image_folder
NOTE: Get the Media_clips folder from the SD card prebuilt image
$ cp mkmmc-android.sh image_folder
NOTE: Get the mkmmc-android.sh script from the SD card prebuilt image
Connect an SD card to the Host machine
Invoke the mkmmc-android.sh script to prepare the card for booting
$ cd image_folder $ sudo ./mkmmc-android.sh <sd card mounted dev folder example:/dev/sdc> MLO u-boot.img uImage uEnv.txt rootfs.tar.bz2 Media_Clips
Wait for the script to complete.
Safely remove the SD card and put it on the BeagleBone for Booting.
References
- More about the AM3358/9 device used on the BeagleBone at http://www.ti.com/am335x.
- AM335x Technical Reference Manual at http://www.ti.com/lit/ug/spruh73/spruh73.pdf
- Android Sources for BeagleBone is hosted at www.gitorious.org/rowboat with manifest rowboat-gingerbread-am335x.xml
- Android on BeagleBone community support at arowboat.org
- BeagleBoard.org design materials, including BeagleBone
- BeagleBone Rev A3 System Reference Manual
- BeagleBone Rev A3 Schematic
- BeagleBone Rev A3 Bill Of Materials
Observations
- Ethernet is now limited to 10Mbits, So the display resolution is lowerd to get more refresh rate on the VNC screen.
- Host Mouse/Keyboard event responses will be slower compared to target side Mouse/Keyboard events
- Serial Connection sometimes not established properly. But it is relable on Linux host.
- If target side mouse-keyboard is connected the board after bootup, the command "echo F > /proc/driver/musb_hdrc.1" to be issued to detect them.
- External Power is required as USB connection power supply sometimes goes off unexpectedly
Comments
Comments on BeagleBone-Android-DevKit Guide
Contents |
Bobrecny said ...
Bobrecny said ...
OK - the formatting isn't showing correctly (line breaks missing), but the information itself is correct.
--Bobrecny 02:47, 29 November 2011 (CST)
Xxiao said ...
could not get rowboperf compiled:
make[1]: Entering directory `/home/xxiao/devel/android/rowboat/rowboperf/3D/SDKPackage_OGLES2/Demos/ChameleonMan/OGLES2/Build/Android' ../../../../../Builds/OGLES2/AndroidGeneric/make_shared_lib.mak:16: default.properties: No such file or directory Makefile:24: warning: overriding commands for target `clean' ../../../../../Builds/OGLES2/AndroidGeneric/make_shared_lib.mak:149: warning: ignoring old commands for target `clean' make[1]: *** No rule to make target `default.properties'. Stop. make[1]: Leaving directory `/home/xxiao/devel/android/rowboat/rowboperf/3D/SDKPackage_OGLES2/Demos/ChameleonMan/OGLES2/Build/Android' make: *** [rowboperf/3D/SDKPackage_OGLES2/Demos/ChameleonMan/OGLES2/Build/Android/libs/armeabi/libPVRShell.so] Error 2
--Xxiao 12:20, 4 December 2011 (CST)
Eric.fort said ...
notes on:
Ubuntu 12.04 LTS
http://processors.wiki.ti.com/index.php/BeagleBone-Android-DevKit_Guide#Installation_and_Usage
card install went flawlessly, however the following did not go as expected.
$ sudo modprobe ftdi_sio vendor=0x0403 product=0xa6d0
1. rather than using this, much better to simply add a udev rule. https://help.ubuntu.com/community/AndroidSDK is a pretty good guide for setting up a development environment for android on ubuntu. 2. Failed initially with device busy, no explaination of why that may be or how to find and remedy the issue
$ minicom -D /dev/`dmesg | grep FTDI | grep "now attached to" | tail -n 1 | awk '{ print $NF }'`
1. Had to run this command with sudo as aparently I have no rights to access the port as a mortal user. 2. Failed initially with device busy, no explaination of why that may be or how to find and remedy the issue.
Powering on to Android Terminal
Put the Micro SD card to the slot on the BeagleBone. Press the reset button again. See X-loader and Uboot loading. Allow the boot loader to run the boot script uEve.txt to run.Kernel boots up and Android shell is activated. Wait till Android init to start the zygote thread. See the below message appearing on the shell.
warning: `zygote' uses 32-bit capabilities (legacy support in use)
1. above message never displays 2. gives what looks like a brief # prompt that never echos anything back 3. after above "false prompt" goes on to start adb server.
Finally got shell prompt after getting the basic sdk installed and figured out how to use adb -s <serial-number> <adb-command> with the proper incantation being 'adb -s 0123456789ABCDEF shell'
keyboard and mouse on the host failed to "unloak" the home screen. plugging in a usb hub to the bone (target) and then attaching a usb keyboard and mouse got me a display on the host and working keyboard and mouse directly connected to the target (bone)
found later that it's just really sloooow over vnc. need to light up hdmi at a res the display likes....
yea, after a week to 2 weeks of steadily chipping away at this project I can almost start building my android beaglebone based cellular communicator and smartphone.
usefull reference webpages that made this possible:
https://help.ubuntu.com/community/AndroidSDK http://processors.wiki.ti.com/index.php/BeagleBone-Android-DevKit_Guide#Installation_and_Usage http://processors.wiki.ti.com/index.php/Android_ADB_Setup http://developer.android.com/guide/developing/tools/adb.html http://en.wikipedia.org/wiki/Android_%28operating_system%29 http://<address-of-your-beaglebone>:5801
--Eric.fort 16:43, 23 May 2012 (CDT)

The FTDI ftdibus.inf file only needs the following lines below for [FtdiHw], [FtdiHw.NTamd64] and [Strings]. The other lines should be deleted as they are for other FTDI chips and not the FT2232H that's on the BeagleBone.
...
[FtdiHw] %USB\VID_0403&PID_A6D0&MI_00.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_A6D0&MI_00 %USB\VID_0403&PID_A6D0&MI_01.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_A6D0&MI_01
[FtdiHw.NTamd64] %USB\VID_0403&PID_A6D0&MI_00.DeviceDesc%=FtdiBus.NTamd64,USB\VID_0403&PID_A6D0&MI_00 %USB\VID_0403&PID_A6D0&MI_01.DeviceDesc%=FtdiBus.NTamd64,USB\VID_0403&PID_A6D0&MI_01
...
[Strings] Ftdi="BeagleBone" DESC="CDM Driver Package - Bus/D2XX Driver" DriversDisk="FTDI USB Drivers Disk" USB\VID_0403&PID_A6D0&MI_00.DeviceDesc=" XDS100v2 compatible USB Serial Converter A" USB\VID_0403&PID_A6D0&MI_01.DeviceDesc="XDS100v2 compatible USB Serial Converter B" SvcDesc="USB Serial Converter Driver" ClassName="USB"
Note that this will break the signature. 64-bit Windows 7 and Vista will need to boot with the <F8> menu and disable the driver signature requirement until the ftdibus.cat file can be regenerated.
--Bobrecny 02:44, 29 November 2011 (CST)