Beagle Board Challenge: Beagle Phone

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Google Code Wiki

Main Wiki and Code Repository is on Google Code

http://code.google.com/p/beaglephone/

Pre-Launch Questions

Group J LO

<insert picture of jennifer lopez here at later date> http://en.wikipedia.org/wiki/File:JenniferLopez.jpg

surprisingly, that picture is under public domain because it was shot by a service man... you learn something new everyday


Describe Your Group

Describe your group. What are the interests and skills of your group members. Give a small bio here to help people get to know you.

What do you hope to gain by participating in this challenge?

Enhancing our understanding of Linux, and testing our own abilities while hopefully learning something along the way

IRC

irc.freeenode.net #beagle oliverz(Oliver), jyen(Jack), larryz(Larry)

Where are you located, and what hours do you tend to work?

We are all located in North/Northwest Campus area, and love to work odd hours Larry, Oliver, and Jack are all also working/co-op in some capacity, so may have time blocked off because of that as well

What is your project?

The BeaglePhone

Project Description

Short 10-20 sentence description that tells readers:

Leopard1.jpg

Basic Premise - Load Angstrom on TI Beagleboard Set up SIP server details etc to connect a GV account to the board, and then connect a hardware phone/headset in order to use it as a VOIP phone

Goals

  1. get a call thru
  2. get a phone hooked up via USB or other method
  3. switch from ethernet connectivity to wifi
  4. attach monitor to create a visual gui
  5. webcam integration if possible
  6. bluetooth capabilities
  7. additional functionality (ie previous call lists) to be accessed via a button

Project Scope

We have planned out several stages, and after just stage 3, we feel like this project will have been a success.

We are all EE or CE students in the 3rd or 4th years of our studies at UT Austin, and have a wide range of experiences among the 3 of us.

What license(s) does your project use?

For code written for this project, we will use GPLv2. When the project is based on an existing open source package, the license of that package will be used.

Existing code is primarily GPLv2 and all kernel code should be so. Some developers use other FOSS licenses, such as MIT, LGPL, etc. There are some TI codecs available for use on the platform that are provided under publicly-available binary-only licenses as well as other binary firmware builds distributed as part of the Linux kernel, but these are discouraged from being used as part of any student project.

Generally you should avoid using the GPLv3 license if possible.

Authors

Features

Pictures & Videos

Video your design working and upload to YouTube with link here:

Videos can be embedded directly into the wiki using the EmbedVideoPlus extension. For documentation on this extension, please see http://www.mediawiki.org/wiki/Extension:EmbedVideoPlus

Usage Instructions

Include any instructions that a user will need if they try to reproduce your project. This might include instructions on installing some piece of software, compiling something, or hardware assembly.

Source Code

Schematics

E2e.jpg For technical support on MSP430 please post your questions on The MSP430 Forum. Please post only comments about the article Beagle Board Challenge: Beagle Phone here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox