Bios MCSDK 2.0 API Documentation Locations
From Texas Instruments Embedded Processors Wiki
Translate this page to
Overview
The Bios MCSDK comes with a host of libraries that implement software APIs that can be called by the user's code. The documentation for the APIs is not in the MCSDK User's Guide nor is it in the Getting Started Guide. These APIs are typically documented with via Doxygen markup contained within the source code header files, and then Doxygen is used to create the actual documentation in a .html (and in some cases a Windows Help (.chm) or Latex) format which is provided with the libraries. The location of this documentation is not yet standardized across all of the components of the MCSDK. So, this page is provided as a reference to where each library's documentation can be found within the MCSDK file structure.
Note the following:
- The "variable" MCSDK_INSTALL_DIR will be used in each of the following sections. This translates to the location where the MCSDK installer was pointed when the install occurred. Replace this with your install location to resolve the location on your system
- Directories with a revision number (Example: dsplib_c66x_3_0_0_8) may differ slightly based on the revision of each component.
- Directories with a device number in the name (Example: pdk_C6678_1_0_0_14) may differ slightly based on the device number.
Documentation Locations
Bit Coprocessor LLD (BCP)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-drv
|
|-bcp
|
|-docs
|
|-doxygen
|
|-html
|
|-index.html
Chip Support Library (CSL)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-csl
|
|-docs
|
|-doxygen
|
|-html
|
|-index.html
Communications Port Programming Interface Low Level Driver (CPPI LLD/Packet DMA)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-drv
|
|-cppi
|
|-docs
|
|-doxygen
|
|-html
|
|-index.html
DSP Library (DSPLIB)
<MCSDK_INSTALL_DIR>
|
|- dsplib_c66x_3_0_0_8
|
|-doxygen
|
|-html
|
|-dsplib_html
|
|-index.html
EDMA3 Low Level Driver (EDMA3 LLD)
<MCSDK_INSTALL_DIR>
|
|-edma3_lld_02_11_02_04
|
|-packages
|
|-ti
|
|-sdo
|
|-edma3
|
|-drv
|
|-docs
|
|-html
|
|-index.html
FFT Accelerator Coprocessor Low Level Driver (FFTC LLD)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-drv
|
|-fftc
|
|-docs
|
|-doxygen
|
|-html
|
|-index.html
Hyperlink Low Level Driver (Hyplnk LLD)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-drv
|
|-hyplnk
|
|-docs
|
|-doxygen
|
|-html
|
|-index.html
Imaging Library (IMGLIB)
<MCSDK_INSTALL_DIR>
|
|-imglib_c66x_3_0_1_0
|
|-docs
|
|-doxygen
|
|-html
|
|-imglib_html
|
|-index.html
Interprocessor Communication (IPC)
<MCSDK_INSTALL_DIR>
|
|-ipc_1_22_03_23
|
|-docs
|
|-doxygen
|
|-html
|
|index.html
Math Library (MATHLIB)
<MCSDK_INSTALL_DIR>
|
|-mathlib_c66x_3_0_0_0
|
|-docs
|
|-doxygen
|
|-html
|
|-mathlib_html
|
|-index.html
Network Developers Kit (NDK)
<MCSDK_INSTALL_DIR>
|
|-ndk_2_20_04_26
|
|-docs
|
|-cdoc
|
|-index.html
Packet Accelerator Low Level Driver (PA LLD)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-drv
|
|-pa
|
|-docs
|
|-doxygen
|
|-html
|
|-index.html
PCI Express Low Level Driver (PCIe LLD)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-drv
|
|-pcie
|
|-docs
|
|-doxygen
|
|-html
|
|-index.html
Queue Manager Subsystem Low Level Driver (PA LLD)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-drv
|
|-qmss
|
|-docs
|
|-doxygen
|
|-html
|
|-index.html
Serial RapidIO Low Level Driver (SRIO LLD)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-drv
|
|-srio
|
|-docs
|
|-doxygen
|
|-html
|
|-index.html
TCP3 Decoder Low Level Driver (TCP3D LLD)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-drv
|
|-tc3pd
|
|-docs
|
|-doxy
|
|-html
|
|-index.html
TCP3 Decoder Low Level Driver (TCP3D LLD)
<MCSDK_INSTALL_DIR>
|
|-pdk_C6678_1_0_0_14
|
|-packages
|
|-ti
|
|-drv
|
|-tcp3e
|
|-docs
|
|-doxy
|
|-html
|
|-index.html
Leave a Comment