Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Build OpenSSL for Sitara

From Texas Instruments Wiki
Jump to: navigation, search


Introduction

This is the third of three articles written as a how-to guide for enabling hardware accelerated cryptographic functions for OpenSSL version 1.0.0d.

The first and second articles describe how to patch the Linux kernel with Open Crypto Framework (OCF-Linux) and how to build and use the crypto module which accesses the hardware accelerators.

This article describes how to build and run OpenSSL version 1.0.0d with support for the hardware accelerated cryptographic functions available on the 37xx and 35xx general purpose (GP) device family.

Assumptions

  • Linux host development system.  Ubuntu 10.04 running in a VMWare machine is used in the examples here
  • Sitara SDK for the AM37xx or AM35xx (this includes the kernel source code, root file system and the cross-compiler tools)
  • Shiva EVM (AM3517) or OMAP3 Rev G EVM (AM37x).  For examples here the board uses the AM3703 processor module
  • Source tarball from openssl.org (openssl-1.0.0d.tar.gz)


For the rest of this article it is assumed that the Sitara SDK has been installed on the Linux host development system.  The root file system for the EVM lies in a sub-directory of the SDK called targetNFS and the board performs a NFS mount of this directory. 



Procedure to Build/Test OpenSSL

Install OpenSSL 1.0.0d in the Host Development System

Place the OpenSSL tarball a convenient directory on the Linux host and extract it in place. 

Configure OpenSSL

There is a README file and INSTALL file under the openssl-1.0.0d directory.  The instructions under the INSTALL file do NOT apply to the situation for cross-compiling with an ARM target.  Do NOT run the ./configure or ./Configure scripts.  Skip the instructions in the INSTALL file and just do the following:

Edit the Makefile and make the following changes:

INSTALL_PREFIX=[path to NFS]

CFLAG= -O -DHAVE_CRYPTODEV -DUSE_CRYPTODEV_DIGESTS
CC= arm-arago-linux-gnueabi-gcc
AR= arm-arago-linux-gnueabi-ar $(ARFLAGS) r
RANLIB= arm-arago-linux-gnueabi-ranlib
NM= arm-arago-linux-gnueabi-nm

The path in the INSTALL_PREFIX parameter should match the path in the host dev system for the root of the NFS mount to be used by the EVM target.


Patch OpenSSL

OpenSSL needs a small modification to make SHA and MD5 operations work with large files when using the AM3x HW accelerators.

File:0002-Modify-eng cryptodev.c-to-make-SHA1-and-MD5-work-wit.patch

Compile and Install into target

To ensure that the OpenSSL Makefile will find the cross-compile tools from the SDK, source the environment setup script from the SDK.  The prompt will change to indicate that the tools are now in the current path.

user@usergt-laptop:~/OpenSSL/openssl-1.0.0d$
user@usergt-laptop:~/OpenSSL/openssl-1.0.0d$ source ~/ti-sdk-am37x-evm-05.04.00.00/linux-devkit/environment-setup
[linux-devkit]:~/OpenSSL/openssl-1.0.0d>

Now just run make and then make install.  The make install command will place OpenSSL in the usr/local/ssl sub-directory of the NFS mount.  This will then be the /usr/local/ssl sub-directory of the target system after the target boots up.

When the target boots and mounts this NFS, the openssl app and collateral will be under /usr/local/ssl.  From the target perspective this will look like the following:


root@arago:/usr/local/ssl# ls -l
drwxr-xr-x 2 1000 1000 4096 Jun 23 2010 bin
drwxr-xr-x 2 1000 1000 4096 Jun 23 2010 certs
drwxr-xr-x 3 1000 1000 4096 Jun 23 2010 include
drwxr-xr-x 4 1000 1000 4096 Jun 23 2010 lib
drwxr-xr-x 6 1000 1000 4096 Jun 23 2010 man
drwxr-xr-x 2 1000 1000 4096 Jun 23 2010 misc
-rw-r--r-- 1 1000 1000 10819 Jun 23 2010 openssl.cnf
drwxr-xr-x 2 1000 1000 4096 Jun 23 2010 private
root@arago:/usr/local/ssl#


And the openssl app will be in the bin sub-directory:

root@arago:/usr/local/ssl# cd bin/
root@arago:/usr/local/ssl/bin# ls -l
-rwxr-xr-x 1 1000 1000 4261 Jun 23 2010 c_rehash
-rwxr-xr-x 1 1000 1000 2142934 Jun 23 2010 openssl
root@arago:/usr/local/ssl/bin#

Modify path to OpenSSL

The Sitara SDK contains an OpenSSL executable at the location /usr/bin/openssl in the root filesystem.  So in the Linux host this is at /home/[user]/ti-[SDK]/targetNFS/usr/bin/openssl.  This needs to be changed so that calls to OpenSSL go to the new executable in /usr/local/bin/openssl.

First save the existing openssl executable.  Then make a soft link to the new new version.

[linux-devkit]:~/ti-sdk-am37x-evm-05.04.00.00/targetNFS/usr/bin> mv openssl openssl.old
[linux-devkit]:~/ti-sdk-am37x-evm-05.04.00.00/targetNFS/usr/bin> ln -s /usr/local/ssl/bin/openssl openssl
[linux-devkit]:~/ti-sdk-am37x-evm-05.04.00.00/targetNFS/usr/bin>
[linux-devkit]:~/ti-sdk-am37x-evm-05.04.00.00/targetNFS/usr/bin> ls -l openssl
lrwxrwxrwx 1 root root 26 2012-03-07 15:34 openssl -> /usr/local/ssl/bin/openssl
[linux-devkit]:~/ti-sdk-am37x-evm-05.04.00.00/targetNFS/usr/bin>

Now when the board boots up any calls to the executable openssl will go to the newly compiled version instead of the one included in the SDK.

Testing

Speed Tests

Now it is possible to run speed tests on the target EVM.  The log below shows the speed test executed without the ocf driver loaded and then again after installing the module.  So the first speed test below shows the performance without the hardware acceleration.  The command is the same because OpenSSL simply reverts to a pure SW implementation if the hardware accelerators are not available.  The time function is used to wrap the openssl application and measure time and bandwidth for the application


root@arago:/usr/local/ssl/bin# time -v openssl speed -evp aes-128-cbc -engine cryptodev
engine "cryptodev" set.
Doing aes-128-cbc for 3s on 16 size blocks: 111841 aes-128-cbc's in 2.60s
Doing aes-128-cbc for 3s on 64 size blocks: 107004 aes-128-cbc's in 2.56s
Doing aes-128-cbc for 3s on 256 size blocks: 15170 aes-128-cbc's in 0.46s
Doing aes-128-cbc for 3s on 1024 size blocks: 14993 aes-128-cbc's in 0.45s
Doing aes-128-cbc for 3s on 8192 size blocks: 4706 aes-128-cbc's in 0.28s
OpenSSL 1.0.0a 1 Jun 2010
built on: Tue Sep 14 14:22:46 CDT 2010
options:bn(32,32) rc4(ptr,int) des(idx,cisc,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -O -DHAVE_CRYPTODEV -DUSE_CRYPTODEV_DIGESTS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
aes-128-cbc 596.49k 2282.75k 1294.51k 5117.61k 12850.52k
Command being timed: "openssl speed -evp aes-128-cbc -engine cryptodev"
User time (seconds): 0.28
System time (seconds): 6.15
Percent of CPU this job got: 41%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 15.44s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 5440
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 30
Minor (reclaiming a frame) page faults: 326
Voluntary context switches: 34919
Involuntary context switches: 219132
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:/usr/local/ssl/bin#

root@arago:/usr/local/ssl/bin# time -v openssl speed -evp aes-192-cbc -engine cryptodev
engine "cryptodev" set.
Doing aes-192-cbc for 3s on 16 size blocks: 111771 aes-192-cbc's in 2.60s
Doing aes-192-cbc for 3s on 64 size blocks: 102088 aes-192-cbc's in 2.55s
Doing aes-192-cbc for 3s on 256 size blocks: 14859 aes-192-cbc's in 0.45s
Doing aes-192-cbc for 3s on 1024 size blocks: 15148 aes-192-cbc's in 0.45s
Doing aes-192-cbc for 3s on 8192 size blocks: 4511 aes-192-cbc's in 0.27s
OpenSSL 1.0.0a 1 Jun 2010
built on: Tue Sep 14 14:22:46 CDT 2010
options:bn(32,32) rc4(ptr,int) des(idx,cisc,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -O -DHAVE_CRYPTODEV -DUSE_CRYPTODEV_DIGESTS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
aes-192-cbc 596.11k 2177.88k 1267.97k 5170.52k 12318.04k
Command being timed: "openssl speed -evp aes-192-cbc -engine cryptodev"
User time (seconds): 0.24
System time (seconds): 6.10
Percent of CPU this job got: 42%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 15.04s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 5440
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 356
Voluntary context switches: 34528
Involuntary context switches: 214123
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:/usr/local/ssl/bin#

root@arago:/usr/local/ssl/bin# time -v openssl speed -evp aes-256-cbc -engine cryptodev
engine "cryptodev" set.
Doing aes-256-cbc for 3s on 16 size blocks: 112338 aes-256-cbc's in 2.60s
Doing aes-256-cbc for 3s on 64 size blocks: 100421 aes-256-cbc's in 2.39s
Doing aes-256-cbc for 3s on 256 size blocks: 14423 aes-256-cbc's in 0.42s
Doing aes-256-cbc for 3s on 1024 size blocks: 16441 aes-256-cbc's in 0.50s
Doing aes-256-cbc for 3s on 8192 size blocks: 3982 aes-256-cbc's in 0.23s
OpenSSL 1.0.0a 1 Jun 2010
built on: Tue Sep 14 14:22:46 CDT 2010
options:bn(32,32) rc4(ptr,int) des(idx,cisc,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -O -DHAVE_CRYPTODEV -DUSE_CRYPTODEV_DIGESTS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
aes-256-cbc 599.14k 2142.31k 1230.76k 5611.86k 10873.51k
Command being timed: "openssl speed -evp aes-256-cbc -engine cryptodev"
User time (seconds): 0.32
System time (seconds): 5.85
Percent of CPU this job got: 41%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 15.05s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 5440
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 356
Voluntary context switches: 46666
Involuntary context switches: 201214
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:/usr/local/ssl/bin#

root@arago:/usr/local/ssl/bin# time -v openssl speed -evp des-cbc -engine cryptodev
engine "cryptodev" set.
Doing des-cbc for 3s on 16 size blocks: 111207 des-cbc's in 2.59s
Doing des-cbc for 3s on 64 size blocks: 106106 des-cbc's in 2.52s
Doing des-cbc for 3s on 256 size blocks: 15585 des-cbc's in 0.46s
Doing des-cbc for 3s on 1024 size blocks: 15965 des-cbc's in 0.48s
Doing des-cbc for 3s on 8192 size blocks: 4809 des-cbc's in 0.29s
OpenSSL 1.0.0a 1 Jun 2010
built on: Tue Sep 14 14:22:46 CDT 2010
options:bn(32,32) rc4(ptr,int) des(idx,cisc,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -O -DHAVE_CRYPTODEV -DUSE_CRYPTODEV_DIGESTS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
des-cbc 593.10k 2263.59k 1329.92k 5449.39k 13131.78k
Command being timed: "openssl speed -evp des-cbc -engine cryptodev"
User time (seconds): 0.25
System time (seconds): 6.10
Percent of CPU this job got: 42%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 15.04s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 5440
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 356
Voluntary context switches: 40137
Involuntary context switches: 213806
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:/usr/local/ssl/bin#

root@arago:/usr/local/ssl/bin# time -v openssl speed -evp des3 -engine cryptodev
engine "cryptodev" set.
Doing des-ede3-cbc for 3s on 16 size blocks: 112762 des-ede3-cbc's in 2.62s
Doing des-ede3-cbc for 3s on 64 size blocks: 101369 des-ede3-cbc's in 1.69s
Doing des-ede3-cbc for 3s on 256 size blocks: 14209 des-ede3-cbc's in 0.42s
Doing des-ede3-cbc for 3s on 1024 size blocks: 15949 des-ede3-cbc's in 0.48s
Doing des-ede3-cbc for 3s on 8192 size blocks: 3973 des-ede3-cbc's in 0.24s
OpenSSL 1.0.0a 1 Jun 2010
built on: Tue Sep 14 14:22:46 CDT 2010
options:bn(32,32) rc4(ptr,int) des(idx,cisc,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -O -DHAVE_CRYPTODEV -DUSE_CRYPTODEV_DIGESTS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
des-ede3-cbc 601.40k 2162.54k 1212.50k 5443.93k 10848.94k
Command being timed: "openssl speed -evp des3 -engine cryptodev"
User time (seconds): 0.29
System time (seconds): 5.17
Percent of CPU this job got: 36%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 15.05s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 5440
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 356
Voluntary context switches: 135308
Involuntary context switches: 113232
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:/usr/local/ssl/bin#

Encryt/Decryt Tests

To test encryption/decryption some data files must be created.  In the following example four random files are created with the dd command.  The sizes of these files are 1k, 10k, 1M, and 100M.  The performance of crypto varies greatly with file size.


root@arago:~# dd if=/dev/urandom of=smallrnddata bs=1024 count=1
root@arago:~# dd if=/dev/urandom of=medrnddata bs=1024 count=10
root@arago:~# dd if=/dev/urandom of=bigrnddata bs=1024 count=1024
root@arago:~# dd if=/dev/urandom of=hugernddata bs=1048576 count=100


Now each file is encrypted and then decrypted and compared to the original file.  The encrypted file ends in .enc.  The decrypted files end in dec.


root@arago:~# time -v openssl enc -aes-128-cbc -engine cryptodev -in smallrnddata -out smallrnddata.enc -pass pass:password
engine "cryptodev" set.
Command being timed: "openssl enc -aes-128-cbc -engine cryptodev -in smallrnddata -out smallrnddata.enc -pass pass:password"
User time (seconds): 0.03
System time (seconds): 0.00
Percent of CPU this job got: 44%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 0.07s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 4480
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 2
Minor (reclaiming a frame) page faults: 294
Voluntary context switches: 24
Involuntary context switches: 3
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:~# time -v openssl enc -aes-128-cbc -engine cryptodev -in medrnddata -out medrnddata.enc -pass pass:password
engine "cryptodev" set.
Command being timed: "openssl enc -aes-128-cbc -engine cryptodev -in medrnddata -out medrnddata.enc -pass pass:password"
User time (seconds): 0.03
System time (seconds): 0.00
Percent of CPU this job got: 59%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 0.05s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 4496
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 297
Voluntary context switches: 15
Involuntary context switches: 2
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:~# time -v openssl enc -aes-128-cbc -engine cryptodev -in bigrnddata -out bigrnddata.enc -pass pass:password
engine "cryptodev" set.
Command being timed: "openssl enc -aes-128-cbc -engine cryptodev -in bigrnddata -out bigrnddata.enc -pass pass:password"
User time (seconds): 0.02
System time (seconds): 0.13
Percent of CPU this job got: 26%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 0.59s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 4496
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 297
Voluntary context switches: 274
Involuntary context switches: 260
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:~# time -v openssl enc -aes-128-cbc -engine cryptodev -in hugernddata -out hugernddata.enc -pass pass:password
engine "cryptodev" set.
Command being timed: "openssl enc -aes-128-cbc -engine cryptodev -in hugernddata -out hugernddata.enc -pass pass:password"
User time (seconds): 0.39
System time (seconds): 6.65
Percent of CPU this job got: 12%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 57.01s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 4496
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 297
Voluntary context switches: 26416
Involuntary context switches: 291
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:~#
root@arago:~# time -v openssl enc -d -aes-128-cbc -engine cryptodev -in smallrnddata.enc -pass pass:password > smallrnddatadec
engine "cryptodev" set.
Command being timed: "openssl enc -d -aes-128-cbc -engine cryptodev -in smallrnddata.enc -pass pass:password"
User time (seconds): 0.03
System time (seconds): 0.00
Percent of CPU this job got: 43%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 0.07s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 4400
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 2
Minor (reclaiming a frame) page faults: 289
Voluntary context switches: 18
Involuntary context switches: 1
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:~# time -v openssl enc -d -aes-128-cbc -engine cryptodev -in medrnddata.enc -pass pass:password > medrnddatadec
engine "cryptodev" set.
Command being timed: "openssl enc -d -aes-128-cbc -engine cryptodev -in medrnddata.enc -pass pass:password"
User time (seconds): 0.01
System time (seconds): 0.01
Percent of CPU this job got: 60%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 0.05s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 4432
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 293
Voluntary context switches: 15
Involuntary context switches: 4
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:~# time -v openssl enc -d -aes-128-cbc -engine cryptodev -in bigrnddata.enc -pass pass:password > bigrnddatadec
engine "cryptodev" set.
Command being timed: "openssl enc -d -aes-128-cbc -engine cryptodev -in bigrnddata.enc -pass pass:password"
User time (seconds): 0.03
System time (seconds): 0.03
Percent of CPU this job got: 16%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 0.41s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 4432
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 293
Voluntary context switches: 389
Involuntary context switches: 8
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:~# time -v openssl enc -d -aes-128-cbc -engine cryptodev -in hugernddata.enc -pass pass:password > hugernddatadec
engine "cryptodev" set.
Command being timed: "openssl enc -d -aes-128-cbc -engine cryptodev -in hugernddata.enc -pass pass:password"
User time (seconds): 0.45
System time (seconds): 6.67
Percent of CPU this job got: 12%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 55.18s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 4432
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 293
Voluntary context switches: 26514
Involuntary context switches: 233
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
root@arago:~#
root@arago:~# time diff smallrnddata smallrnddatadec
real 0m 0.01s
user 0m 0.00s
sys 0m 0.00s
root@arago:~# time diff medrnddata medrnddatadec
real 0m 0.02s
user 0m 0.00s
sys 0m 0.00s
root@arago:~# time diff bigrnddata bigrnddatadec
real 0m 0.50s
user 0m 0.00s
sys 0m 0.02s
root@arago:~# time diff hugernddata hugernddatadec
real 0m 48.92s
user 0m 0.39s
sys 0m 2.30s
root@arago:~# ls -l
drwxrwxrwx 8 1000 1000 4096 Jul 20 2010 Apps
-rw-r--r-- 1 root root 1048576 Aug 13 2010 bigrnddata
-rw-r--r-- 1 root root 1048608 Aug 13 2010 bigrnddata.enc
-rw-r--r-- 1 root root 1048576 Aug 13 2010 bigrnddatadec
drwxr-xr-x 2 1000 1000 4096 Jul 23 2010 crypto-tools
-rw-r--r-- 1 1000 1000 15805 Jun 29 2010 crypto-tools-20100325.tar.gz
-rw-r--r-- 1 root root 104857600 Aug 13 2010 hugernddata
-rw-r--r-- 1 root root 104857632 Aug 13 2010 hugernddata.enc
-rw-r--r-- 1 root root 104857600 Aug 13 2010 hugernddatadec
-rwxrwxrwx 1 1000 1000 611 Aug 3 2010 loop.sh
-rw-r--r-- 1 root root 10240 Aug 13 2010 medrnddata
-rw-r--r-- 1 root root 10272 Aug 13 2010 medrnddata.enc
-rw-r--r-- 1 root root 10240 Aug 13 2010 medrnddatadec
drwxr-xr-x 3 1000 1000 4096 Aug 3 2010 omap3_crypto
-rwxrwxrwx 1 1000 1000 9024 Aug 3 2010 omap3_crypto.tar.gz
drwxrwxr-x 3 1000 1000 4096 Jul 23 2010 omap3_crypto_old
drwxr-xr-x 23 1000 1000 4096 Jul 16 2010 openssl-0.9.8n
drwxr-xr-x 22 1000 1000 4096 Jul 19 2010 openssl-1.0.0a
-rw-r--r-- 1 1000 1000 4015794 Jun 11 2010 openssl-1.0.0a.tar.gz
-rw-r--r-- 1 root root 1024 Aug 13 2010 smallrnddata
-rw-r--r-- 1 root root 1056 Aug 13 2010 smallrnddata.enc
-rw-r--r-- 1 root root 1024 Aug 13 2010 smallrnddatadec
root@arago:~#


The diff function shows that the decrypted file is identical to the original file.