Building TI Android DevKit Filesystem without SGX

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Construction Icon small.png This page is currently under construction. The content of this page is due to change quite frequently and thus the quality and accuracy are not guaranteed until this message has been removed. Please feel free to contribute to this page while construction is in progress.



This page provides instructions on building the TI Android DevKit Filesystem without SGX graphics libraries enabled.

The instructions below refer to omap3evm/AM37xevm. Please modify the target as per your required system.

Contents

Setting up Host

Please refer to the TI Android DevKit Developer Guide for information on ubuntu host setup

Download TI Android DevKit Sources

We shall be using the TI-Android-GingerBread-2.3.4-DevKit-2.1 Android sources for this exercise.

Please refer to TI Android DevKit Developer Guide for instructions on android sources installation

In this guide, it is assumed that the sources are extracted to the following path:

  $ANDROID_DEVKIT_TOP=/home/TI_Android_GingerBread_2_3_4_Sources/

Apply patches

Apply the android patches from here: http://groups.google.com/group/rowboat/browse_thread/thread/906aed7dc5917bde

These patches are required to obtain a smooth display without SGX graphics acceleration.

Build Filesystem

To build the android filesystem run the following command from the top-level android sources directory:

  $ make TARGET_PRODUCT=omap3evm droid -j8

The droid target in the make command causes only the android filesystem to be built. So the SGX graphics acceleration libraries and WLAN/BT drivers and firmwares are not installed in the resulting filesystem

Install WLAN/BT Firmware

This step will install the WLAN/BT drivers and firmware for WL1271 module available on AM37xevm.

  $ make TARGET_PRODUCT=omap3evm wl12xx_compat

Install RowoPERF

Download Performance_Apps.tar.gz from: http://software-dl.ti.com/dsps/dsps_public_sw/sdo_tii/TI_Android_DevKit/TI_Android_GingerBread_2_3_DevKit_1_0/index_FDS.html

From that directory execute:

  $ tar -xvzf ~/Performance_Apps.tar
  $ cd ~/Performance_Apps
  $ ./install_rowboperf.sh <path_to_source>/out/target/product/omap3evm/root

Build Filesystem tarball

First create the unified filesystem:

  $ cd out/target/product/omap3evm
  $ mkdir android_rootfs
  $ cp -vr root/* android_rootfs
  $ cp -vr system android_rootfs

Now create the filesystem tarball:

  $ ../../../../build/tools/mktarball.sh ../../../host/linux-x86/bin/fs_get_stats android_rootfs . rootfs rootfs.tar.bz2

Prepare SD card

Update the pre-built image. > Starting in the <path_to_source> directory, run the following commands.

  $ cp kernel/arch/arm/boot/uImage <path_to_prebuilt>/Boot_Images/uImage
  $ cp out/target/product/am3517evm/rootfs.tar.bz2 <path_to_prebuilt>/Filesystem/rootfs_am35x.tar.bz2

Flash the SD card

Please ensure you follow the SD card guidance available here:
http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3.4-DevKit-2.1_UserGuide#SD_Card_Recommendations

Now, starting in the <path_to_source> directory, run the following command.

  $ sudo ./mkmmc-android /dev/sd<device>

Where <device> is the letter of the SD card device you wish to flash. WARNING: entering the wrong device letter here can result in the loss of data.

Your SD card is ready. Please set up the evm boot switches correctly as per http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3.4-DevKit-2.1_UserGuide#Setting_up_Hardware , insert the SD card and power up the evm.

E2e.jpg For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article Building TI Android DevKit Filesystem without SGX here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox