C2000 32-bit Real-Time MCU Training
From Texas Instruments Embedded Processors Wiki
C2000™ One-Day Workshop
The C2000™ One-Day Workshop is a hands-on technical course facilitated by qualified Texas Instruments instructors. This workshop is based on the Piccolo™ F28069 device, which combines many common features and peripherals of the Piccolo™ and Delfino™ families. Therefore, this workshop would be very useful to anyone interested in the C2000 MCU family of devices. The workshop steps the user through system initialization, peripheral setup and programming an application into flash memory using the CCS on-chip Flash programmer. Every lab exercise builds on the previous lab exercise, running a common application theme through the workshop. The lab exercises are performed using the F28069 ControlSTICK USB Evaluation Tool.
You can attend a live workshop by enrolling at: C2000 Piccolo One-Day Workshop
C2000™ Multi-Day Workshop
The C2000™ Multi-Day Workshop is a hands-on technical course facilitated by qualified Texas Instruments' instructors. This workshop is based on the Piccolo™ F28069 device, which combines many common features and peripherals of the Piccolo™ and Delfino™ families. Therefore, this workshop would be very useful to anyone interested in the C2000 MCU family of devices. The workshop steps the user through system initialization, peripheral setup and programming an application into flash memory using the CCS on-chip Flash programmer. Topics also included are IQmath, DMA, CLA, and DSP/BIOS.
Every lab exercise builds on the previous lab exercise, running a common application theme throughout the workshop. The lab exercises are performed using the F28069 Piccolo Experimenter's Kit. This kit consists of a docking station and an F28069 controlCARD. The docking station features on-board USB JTAG emulation, access to all of the controlCARD signals/peripherals, and breadboard areas. The controlCARD is a complete board level module that utilizes an industry-standard DIMM form factor to provide a single-board controller solution. The docking station is fully powered from the USB connection and no external power supply is needed.
You can attend a live workshop by enrolling at: C2000 Piccolo Multi-Day Workshop
C2000 Archived Workshops
The workshop materials provided at C2000™ Archived Workshops are no longer being updated or maintained. The student guides, labs, and solution files are provided for the following platforms:
- F2407
- F2812
- F2808
- F28335 / Delfino
- C2000 / Piccolo
- C2000 Digital Power Supply
Some workshop labs use their respective eZdsp board or EVM, which may still be available from Spectrum Digital.