C5000 Chip Support Library

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

C5000 Chip Support Library

Dspdspbios.jpg

Download

Documentation

Helpful tips image.jpg

CSL version 2.50.00 and newer include the latest documentation with the software package. This documentation should be used in place of the SPRU433 API reference guide.

Frequently Asked Questions

Q: Is there a CSL GUI?

Q: Where is the USB audio class example in version 2.50.00?

Q: Are there any updates to the CSL API reference guide? (SPRU433)

Q: How can I change the code on CSL_USB_IntExample to send data via pipe 0x01 instead of 0x02 (internal bootloader uses 0x01) so I can boot from USB?

Q: Trouble with the USB comm port example with the 5515 EZDSP

A: TMDX5515EZDSP, CSL_USB_CdcExample_Out - can't open COM port

Q: Where do I specify to the CSL which chip I have?

Q: Are the drivers WHQL Certified?

Q: Does the CSL include USB Mass Storage Class?

Q: Is FAT32 supported?

Q: What kind of performance should I expect using the ATAFS?

Q: Why is ATA Write faster than ATA Read?

Q: Does the CSL include bad block management or load levelling for flash memory?

Q: Does the CSL support USB HID?

Q: Does the CSL support 5532/3/4/5?

Q: The CSL and user guide register names for clock configuration and clock generator registers don't match

Register Address    CSL Name    SPRUFX5A Name
----------------    --------    -------------
1C1Eh            SDRAMCCR    CCR1
1C1Fh            CCR2        CCR2
1C20h            CGCR1        CGCR1
1C21h            CGICR        CGCR2
1C22h            CGCR2        CGCR3
1C23h            CGOCR        CGCR4

Q: Are Video Class drivers supported?

Q: Do I need to get my own USB VID and PID?

Q: Can I use the TI VID and get a unique PID from TI? / Can I get a PID from TI?

Q: What PID doe you use on the 5505?

Q: How do I change the product display name?

Q: What VID/PID does TI use for the bootloader?

Troubleshooting

  1. Please check if you have the latest version of the CSL. The latest version will be available from the download link on this page.
  2. Please check whether you have selected the right device from the CSL. Please look in the csl_general.h file and make sure you have selected the proper device.

Related


Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox