Getting Started with C5505 EVM

From Texas Instruments Embedded Processors Wiki

(Redirected from C5505)
Jump to: navigation, search
Translate this page to   

Contents

Overview

The TMS320C5505 is a member of TI's TMS320C5000™ fixed-point Digital Signal Processor (DSP) product family and is designed for low-power applications.

Some of the C5515 DSP's applications include:

EVM

Overview

C5505 EVM Spectrum Digital support page

Getting Started

Programming the EVM for stand-alone mode

C5515 Boot-Image Programmer

Software Tools Checklist

Frameworks and Applications

eZdsp

Overview

C5505 eZdsp Spectrum Digital support page

C5505 eZdsp TI Product Page/ Order

C5505 eZdsp USB Stick Development Tool.JPG

The TMDX5505eZDSP is a small form factor, very low cost USB-powered DSP development tool which includes all the hardware and software needed to evaluate the industry's lowest power 16-bit DSP: TMS320VC5504 and TMS320VC5505.

This tool has embedded XDS100 emulator for full source level debug capability and supports Code Composer Studio4.0™ integrated development environment (IDE) and eXpressDSP™ software which includes the DSP/BIOS™ kernel. The full contents of the Development Tool include:

Getting Started

Programming the eZdsp for stand-alone mode

Figure 1

First, generate a boot image of your program using the hex55 conversion utility. You can find detailed instructions on how to do that here.

Once a boot image (*.bin) is generated, customers can burn the boot image into the SPI Flash memory of the C5505 eZdsp through a utility called programmer that runs on C5505 using an emulator with Code Composer Studio™ software.

First, load the programmer_USBKey.out using the Code Composer Studio as shown in Figure 5 by selecting “Load Program…” under the Target menu in CCS.

Note: If you don't have the programmer_USBKey.out, you can find it here under C5505 EZDSP Programming Tool.

Next, run the program, when the user will be asked to input the file path and file name for the boot image:

Input your binary file path...

Figure 1 shows how to program led.bin to the C5505 eZdsp using programmer_USBKey.out.

NOTE: There cannot be any white spaces in the file directory path or the program will not run correctly. Programmer will not be able to find the input file as it considers the white space the end of the input.

Software Tools Checklist

Frameworks and Applications

Software


Tool

Code Composer Studio v4


Training and Workshops

FAQ


Related Articles

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox