C5505 EVM FAQ
From Texas Instruments Embedded Processors Wiki
Translate this page to
How do I get my TMS320VC5505 EVM + MDK Analog Front End to mate together? The pin outs don't match.
The J13 connector on the C5515 EVM has an extra pin pair (pins 21 and 22) that are not used by the AFE daugthercards. To install one of the MDK AFEs on the C5515 EVM line up connectors J14 and J10 on the EVM to the mating connector on the AFE. Pins 21 and 22 on the J14 connector will be uncovered if aligned correctly. Push AFE firmly onto the EVM to seat the connectors and you are ready to go.
Related FAQs
- 55x FAQ
- DSP Library FAQ
- C5504/05/14/15 FAQ
- C5505 eZdsp FAQ
- C5505 EVM FAQ
- C5515 eZdsp FAQ
- C5515 EVM FAQ