C6000 Compiler: Recommended Compiler Options

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Introduction

This article discusses the best C/C++ compiler options to use for performance on the C6000, though there are occasional nods to compiling for smaller code size.

Definitely use the following:

By default, the –o switch optimizes for performance. This can increase code size. If code size is an issue, do not reduce the level of optimization. Instead, use the –ms switch to affect the optimization goal (performance versus code size).

When safe, consider using the following:

For example, consider the following function:

selective_copy(int *input, int *output, int n)
{
    int i;
    for (i=0; i<n; i++)
       if (myglobal[i]) output[i] = input[i];
}

–mt is safe when the memory ranges pointed to by "input" and "output" do not overlap.

Be aware of the limitations of -mt. This option applies only to pointer-based function parameters.

To overcome these limitations, use the Restrict Type Qualifier.

In addition, using –mt broadly acts upon the full scope of the code, either file or project wide. Use the Restrict Type Qualifier to handle this problem with more precision.

The software-pipelined loop information in the compiler-generated assembly file notes when adding –mh<num> (or using –mh with a larger value) might improve performance or code size. For example, suppose a (function containing a) loop is compiled without –mh or with –mh<num> where <num> is less than 56. The compiler might output a message similar to:

;*      Minimum required memory pad : 0 bytes
;*
;*      For further improvement on this loop, try option -mh56

This message communicates that currently the compiler is fetching 0 bytes beyond the end (or beginning) of any array. However, if the loop is rebuilt with –mh<num> where <num> is at least 56, there might be better performance and/or smaller code size.

When using this option, ensure that there is a buffer of <num> bytes on both ends of all sections that contain array data. This is the user’s responsibility. Padding can be implemented by shrinking the associated memory region in the linker command file. For example, suppose the original memory region is defined as:

MEMORY {
           myregion: origin = 1000, length = 4000
       }

If the goal is to pad the beginning and end of a region by 56 bytes, the region must be shrunk by 2 * 56. The new origin is 1000+56 and the new length is 4000-2*56 = 3888:

MEMORY {
	   /* pad (reserved):  origin = 1000, length = 56    */
           myregion:           origin = 1056, length = 3888
           /* pad (reserved):  origin = 3944, length = 56    */   
       }

The comments provide a reminder not to put other array data in those regions. Alternatively, one can use other memory areas (code or independent data) as pad regions, provided there is no conflict with EDMA transfers and/or cache-based operations.

If the source code contains many functions that are never executed, consider using:

When using the –mo option, each function is put into its own sub-section; for example, the function dotp() is put into section ".text:_dotp". Because there is only one function per input section, the linker can be more aggressive with respect to the removal of functions that are never executed. This can reduce the memory footprint of the resulting executable and, hence, reduce memory cycles as well.

This benefit comes at a cost. On the C6000, each input section must be aligned on a 32-byte boundary. The more input sections there are, the more space is potentially wasted on alignment. Hence, the benefit of this option depends on the percentage of dead source code and the original grouping of functions into input sections. Thus, this option may improve the performance and/or code size of some applications while hurting others. However, the differences can be significant, so give it a try.

If code size is a concern, consider using the following:

Try –ms0 or –ms1 with performance critical code. Consider –ms2 or –ms3 for seldom-executed code (such as initialization routines). Note that –ms defaults to –ms0.

In CGT >= 6.1 also consider the -mf[0-5] option which provides more granularity on the codesize .v. optimization tradeoff. See -mf_compiler_option for details.

Do not use the following:

Options that reduce tuning time by providing additional analysis information, while having no effect on performance or code size:

Reference

This article is derived from the application note Hand Tuning Loops and Control Code on the TMS320C6000.


CN C6000 Compiler: Recommended Compiler Options

E2e.jpg For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article C6000 Compiler: Recommended Compiler Options here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment

Comments

Comments on C6000 Compiler: Recommended Compiler Options


PeterSteinberg said ...

Shouldn't the optimzation switch be "-O" (upper case). The "-o" (lower case) switch sets the output file name.

--PeterSteinberg 08:42, 6 May 2011 (CDT)

Tthahn said ...

If -o (or -O) is placed before the -z option, it controls the optimization level. If -o is placed after the -z option, it controls the output file name.

--Tthahn 09:30, 6 May 2011 (CDT)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox