C6000 Memory models

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents



C6000 Memory Models & Vendor Libraries

Introduction

This document discusses usage of the C6000 C compiler memory models from the perspective of an object library vendor. It assumes you are using the C6000 compiler v5.1.0 or higher. Note the v5.1.0 compiler comes bundled with Code Composer Studio 3.1.

Background

Review Memory Models

Previous versions of the compiler offered memory models for managing both code and data. The code models were replaced by linker generated trampolines. The compiler always generates near calls, and lets the linker apply trampolines to calls that do not reach. Details on trampolines are in this linker application note.

The data memory models remain the same. But the options for choosing the data memory model, as well as the default, are different from previous releases.

Build Option Means Default
--mem_model:data=near All data near No
--mem_model:data=far_aggregates Aggregate data far; scalar data near Yes
--mem_model:data=far All data far No

Older compilers offered the options –ml[0-3] which controlled both code and data models. Those options are still supported, though deprecated. Please stop using those options as soon as possible. Note the options –ml[1-3] indicate use of the far code model, and thus effectively disable trampolines and all their attendant benefits.

The rest of this document only discusses data memory models.


Terminology

A variable definition tells the compiler everything it needs to know to actually create a given variable …

int global_array[100];          // definition

A variable declaration tells the compiler the type and name of a variable, but typically omits details needed to create it...

extern int global_array[];      // declaration

The keywords near and far can be used on either a variable definition or declaration.

far extern int global_array[];  // far declaration
 
near static int i;              // near definition

Use of near or far overrides any build option.

A variable access is a read or write of the variable …

global_array[i] = 0;            // access

A scalar is a simple variable.

int i;                          // define some
 
float f;                        // scalars
 
int *ptr;                       // pointer is scalar

An aggregate is an array, structure, or union.

int global_array[100];          // define some
 
struct sss global_struct;       // aggregates
 
union  uuu global_union;

Definition & Access, Near & Far

This table shows whether a variable with a given definition can be accessed by the given method.

    Access
    Near Far
Definition Near OK OK
Far Fails OK

The key thing to notice is that a far access of a near variable works, while a near access of a far variable does not work.

Tradeoffs

Drawbacks of near

If near variables work so well, why not use them all the time?

The total size of all the near variables is limited to 32K bytes. That is because such variables are accessed at an offset from the register B14, and that offset is limited to 15-bits.

All the near variables, from the libraries and from user code, must be combined together into a single section named .bss and allocated to memory together. For various system related reasons, that is not always possible.

Costs: near vs. far Accesses

In contrast to software pipelined loops, performance and code size of variable accesses is directly linked. As performance improves, so does code size.

Intuition says that near variable access is cheaper than far variable access. That’s true, but not as often as you might think.

If a variable is accessed indirectly, then the cost is the same. Indirect access obviously includes any access involving a pointer.

*ptr_to_int = ...
 
ptr_to_struct->member = ...

It also includes any other computed memory address.

global_array[i] = ...
 
local_var = ...
 
function_argument = ...

Near access is cheaper only in the case of direct access by name (possibly plus a constant offset).

global_int = ...
 
global_struct.member = ...
 
global_array[10] = ...

Thus, with regard to costs, the importance of the choice of memory model is linked to how often direct accesses occur. If direct accesses are rare, costs will vary little with the choice of memory model. If direct memory access is common, then near memory model will tend to be cheaper than far memory model.

Default: far_aggregates

The default memory model is far_aggregates because, in most code, direct memory access is common only among scalars. Aggregates are nearly always accessed indirectly.

Furthermore, placing only scalars in near memory means the 32K size limit will almost never be exceeded. The largest scalars are 8 bytes big, and it would take 4097 separately named 8-byte scalars to exceed the 32K limit.

Thus, the costs of direct access are minimized while avoiding the 32K size limit of near memory.

Definition and Declaration Must Agree

Variable definitions appear in source files, and variable declarations appear in header files. Declarations influence how accesses are performed. The near or far property of a given variable as written in the definition and the declaration must agree. Agreement, as used here, does not mean identical. It means there will be no error in execution at runtime. Identical use of near or far is one way to get agreement. But it is not the only one. As the table in section 5 indicates, the following would work...

/* header file */
far extern int global_var;   // far declaration
 
/* library source file */
near int global_var;         // near definition

Note the converse is not true. A near declaration cannot access a far definition.

Explicit use of keywords is not the only way to obtain the results in the above example. The same thing happens if the library source file is built with the default far_aggregates data memory model, and the user code that includes the header file is built with far data memory model.

Consistency of Builds

A library is supplied with at least two components: the object files and the header files. The object files are built when the library is released. The header files are included in the user’s source and build. Thus, the header files, and the declarations they contain, are built with the user’s build options.

Some libraries are more sophisticated. They come with configuration tools that auto-generate additional source files. These source files can define variables which are accessed in library object code. The auto-generated source files are built with the user’s build options.

In all these cases, consistency of builds is required so that, as discussed in section 9, the variable definitions and declarations agree. A library vendor has two choices: document build option requirements, or write the header files and auto-generate source files such that they are independent of the user’s build options.

Documenting which build options should or should not be used is a reasonable choice. If the user makes an error, the linker will issue a warning or error message. And correction is straightforward: adopt the build options required by the library.

Rely on Compiler Defaults

This is the first of two sections that make specific recommendations. This section discusses using the compiler default option where scalars are near and aggregates are far.

Advantages

Disadvantages

How User Could Get in Trouble

Force Everything to far

This section discusses a second recommendation. Explicitly define and declare every global variable to be far. Use of the far keyword in this manner overrides any memory model build options chosen by the user.

Advantages

Disadvantages

Discussion

The trade-off here is library costs versus ease of support. It is very easy to support a library where all of the data will always be far. You only need a bit of documentation to tell the user to expect a .far section. This .far section can be allocated anywhere from a correctness perspective. But for that ease of support, you may a price, even a high price, in lost performance and added code size. The only way to know for sure is to take measurements and see.

The compiler RTS library declares all data as far. Most of the RTS data is aggregates that are accessed indirectly. The few scalars that are accessed directly are in seldom used functions.

Note the RTS source actually uses _DATA_ACCESS as the storage class of all variables, and has

#define _DATA_ACCESS far

in the header file linkage.h, which is in turn included by all the source files. Thus, it is easy to change this implementation detail. Note rebuilding the library is required. That is pretty straightforward in the case of the RTS library. It may not be straightforward for other libraries.

Note on Linker Diagnostics

The linker diagnostic emitted when a data memory model mistake occurs is a warning, not an error. Here is an example:

>> warning: Detected a near (.bss section relative) data reference to the symbol
_global defined in section .far.  The reference occurs in
file2.obj, section .text, SPC offset 00000008.  Either make the
symbol near data by placing it in the .bss section, or make the
references to the symbol far.  For C/C++ code use 'far' or 'near'
modifiers on the type definition of the symbol or compile with the
--mem_model:data switch.

This is a warning because the linker cannot be certain it is an error. If the linker could somehow be certain that the error occurred in compiler generated code, it would generate an error instead. It cannot do that. And it is possible, in assembly language, to employ a custom paging scheme that uses B14 as the base register. In such a case, the error message is spurious. Thus, it is categorized as a warning, and not an error.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox