C6747/45/43 Power Consumption Summary

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Overview

This article discusses the power consumption of the Texas Instruments C6747/45/43. Power consumption on the C6747/45/43 device is highly application-dependent, so a spreadsheet is provided to model power consumption for a user's application. To obtain good results from the spreadsheet, realistic usage parameters must be entered. The low-core voltage and other power design optimizations allow these devices to operate with industry-leading performance, while maintaining a low power-to-performance ratio.

The data presented in the accompanying spreadsheet was measured from strong units, representative of devices at the maximum end of power consumption for production units. No production units will have average power consumption that exceeds the spreadsheet values. Therefore, the spreadsheet values may be used for board thermal analysis and power supply design as a maximum long-term average. The power data presented in this document are based on measured data with C6747 silicon revision 2.0 or earlier devices.

The spreadsheet discussed in this application report can be downloaded from the URL listed in the Download Section. Although this spreadsheet was developed for the C6747 device, it can be used to model power consumption on the C6745 and C6743. Features not supported on these devices should not be enabled in the spreadsheet.

Power Consumption Summary


Core Voltage (V) Configuration Device Frequency (Mhz) Junction Temperature (C) Core Power (mW) IO33 Power (mW) Total Power (mW)
1.2 Static 0 25 9.03 50.0 59.03
1.2 Standby 24 25 13.01 50.0 63.01
1.2 Typical 300 25 305.4 161.5 466.94
1.3 Typical 456 25 585.84 161.5 747.39
0 RTC only 0 25 0.02 0 0.02



Model Activity

Activity-Based Models

Power consumption for the C6747/45/43 can vary widely depending on the use of on-chip resources. Thus, power consumption cannot be estimated accurately without an understanding of the components of the SoC in use and the usage patterns for those components. By providing the usage parameters that describe how and what on the SoC is being used, accurate consumption numbers can be obtained for power-supply and thermal analysis.

This model breaks down power consumption into two major components: baseline power and activity power. Using this model, various applications that use the SoC differently can get accurate predictions across the spectrum of possible power consumption on the C6747/45/43.

Baseline Power

Baseline power consumption is power that is independent of chip activity such as static power (leakage), phase-locked loop (PLL), oscillator power and clock tree power to various subsystem components (e.g. SCR) that cannot be turned off via the on-chip power management module. While independent of chip activity, baseline power is dependent on the device operating frequency, voltage, and temperature. Therefore, you can affect baseline power only by changing the PLL(s) output frequency, the core voltage, or the operating temperature.

Activity Power

Activity consumption is power that is consumed by active parts of the SoC: CPU(s), EMIF, peripherals, etc. Activity power is independent of temperature, but dependent on voltage and activity levels. In the spreadsheet, activity power is separated by the major modules within the device. Therefore, the individual module power consumption can be estimated independently; this helps with tailoring power consumption to specific applications. The parameters used to determine the activity level of a module are frequency, utilization, read/write balance, bus size, and switching probability. Note that not all parameters apply to all modules.

Not all modules include all of the parameters.

Modules

The C6747/45/43 power estimation spreadsheet contains the following modules with adjustable parameters:

Although EDMA3 is listed as a separate module, the row essentially provides the power consumption for turning on the clock to the channel controller and the transfer controller(s) for a particular device frequency and voltage. The EDMA3 activity power is included in the module/peripheral serviced by the EDMA3. Therefore, in estimating power for peripherals that typically use EDMA3 for their transfers, the EDMA3 should be kept enabled. For available peripherals and peripheral configurations, please see the device-specific data manual.


Using the Power Estimation Spreadsheet

The power estimation spreadsheet involves entering the appropriate usage parameters as input data in the spreadsheet. Cells that are designed for user input are white in color. The following steps explain how to use the spreasheet:

  1. Select the voltage, junction temperature, PLL configuration and device frequency for the estimated end application
  2. Fill in the appropriate module use parameters

The spreadsheet takes the provided information and displays the details of power consumption for the chosen configuration.

As the spreadsheet is being configured, not all settings are checked for conflicts, e.g. peripheral clock frequency out of allowed range, etc. Consult the device-specific data manual for max frequency limitations. For best results, enter the information from left to right starting at the top and moving downward.

Choosing Appropriate Values

The frequency and bit user values are determined by design and it will be clear what the correct values to enter are. For some modules, the frequency field is used to input the data rates (e.g. UART, EMAC, etc). In order to choose appropriate values, you need a good understanding read/write balance, bit switching required estimation, and utilization of the end application. You should also keep in mind the pin multiplexing configuration for the device to avoid enabling mutually exclusive peripherals/configurations at the same time. For available peripherals and the configuration, see the device-specific data manual.

Utilization

For modules except C674x DSP, utilization is simple the percentage of time the module spend doing something useful, versus being unused or idle. For these peripherals, there are not various degrees of use, so the value is just an average over time. For example, the EMIF performs reads and write one-quarter of the time and has no data to move for the other three-quarters of the time (though it continues to perform background tasks like refresh); this would be 25% utilization.

For peripherals with I/O, utilization can be estimated by comparing used bandwidth with theoretical maximum bandwidth. If, for example, an application must transfer 160 Kb/s via the I2C port, with a theoretical 400 Kb/s maximum, the I2C utilization would be about 40%. In some cases, the max bandwidth allowed may be dependent on the device frequency; factor this while calculating the utilization if doing the estimation at different device frequencies.

System level issues may also reduce utilization. Though the spreadsheet accepts 100% utilization for all peripherals, this is not possible in reality. As concurrency in data movement increases and/or throughput requirements on high bandwidth modules (EDMA, etc) increases, overall peripheral activity is throttled back due to bottlenecks created at various common end points. In such cases, peripherals might not achieve 100% utilization; therefore, you should enter individual module utilization numbers keeping this overall limitation in mind.

 % Writes

Peripherals that transmit as much data as they receive have 50% writes; the spreadsheet assumes the remaining 50% of the time is spend on reads. In some applications, peripherals move data in only one direction, or have a known balance of data movement. In these cases, % writes should be changed to 0%, or 100%, or the known ratio as appropriate for the cases when the SoC is reading all the time, writing all the time, or a combination of the two, respectively. Otherwise, 50% is a typical number that should be used.

 % Switching

Random data has a 50% chance any bit will change from one cycle to the next. Some applications may be able to predict this chance using prior information about the data set. If there is a property of the algorithm that allows prediction of the bit changes, the application-specific probability can be used. All other applications should use the default number of 50%.

Peripheral Enabling and Disabling

As mentioned previously, the C6747/45/43 device provides the capability to disable modules that are not being used via the power sleep controller (PSC). When a peripheral is disabled, its clock is turned off reducing the power consumption of the device.

The spreadsheet accommodates this power saving feature by including fields from which a peripheral can be specified as disable or enabled.

If a module is not used for a given application, then it is recommended to keep it in a disabled state.

It is possible that the module is kept enabled but has no activity. To achieved this, program the % utilization and/or the frequency fields to a value of 0, then the numbers in the module's row will be indicative of the power consumed by clocking the module.

It is also possible for some modules to be disabled but still have activity. For example, EMAC will continue to generate a 50Mhz RMII clock for the PHY even when disabled. To eliminate the RMII clock activity, set the EMAC "Other" paramater to "RMII clk input". Another example is the USB PHYs. Both USB1.1 and USB2.0 PHY can be powered and enabled without having the USB modules enabled. To remove the PHY power consumption, set the USB "Other" parameter to "No Activity".


Using the Results

The results presented by the spreadsheet are based on measured data from C6747 silicon revision 2.0 and earlier devices.

The intent of the power estimation spreadsheet is to provide estimates of the upper bounds in an application-specific loading and peripheral utilization scenario. The measured units were selected to be a strong unit at the maximum end of power consumption for production units. No production units will have average power consumption that exceeds the spreadsheet values. Therefore, the spreadsheet data may be considered maximum average power consumption; the actual observed power may vary. That is, transient currents may cause power to spike above the spreadsheet value for a small amount of time. However, over a long period, the observed average consumption will be below the spreadsheet value. The spreadsheet value may be used for board thermal analysis and power supply design as a maximum long-term average.

Adjusting I/O Power Result

I/O power is dependent not only on the device and activity, but also the load being driven. For loads with CMOS inputs, the power required to drive the trace dominates, and is a better measure of load than the number of inputs of lumped load capacitance. If the target system has very different I/O loading, scale the spreadsheet results either up or down to compensate. For this reason, the spreadsheet allows you to specify the approximate load on the I/O pins for each module by using the trace length field. This parameter is used to adjust the reported I/O power numbers.


Thermal Considerations

As integrated circuit (IC) components become more complex, the challenge of producing an end equipment product with good thermal performance also increases. Thermal performance is a system level concern, impacted by IC packaging as well as printed circuit board (PCB) design, PCB characteristics, PCB layout, ambient temperature, and chassis configuration.

In the device-specific data manual, TI specifies not to exceed the maximum operating junction temperature so the device reliability and/or proper operation can be maintained. To meet this requirement, it is important to understand the contribution of the other system characteristics (mentioned above) and design accordingly. Before finalizing system layout and PCB design, verify that the maximum operating junction temperature documented in the device-specific data manual is met.

The spreadsheet that accompanies this application report includes a worksheet that performs the junction temperature calculations described in section 5.3 of the Thermal Considerations appnote (SPRAAL9). You must enter value from the following fields in the worksheet: package type, core voltage, air flow, case temperature, ambient temperature, total power and static power. All of the remaining fields in the worksheet are calculated based on your inputs.


Example

The following examples demonstrate how to choose appropriate values for a particular application. These values may be imported into the spreadsheet by clicking the appropriate macro button.

The Static macro button reports the static power for the device, when the CLKIN is cut off and voltage is applied to the various core and I/O rails.

The Standby macro button reports the power consumed with the 24Mhz CLKIN. PLL0 is powered down/disabled and the system is operating in bypass mode with the CLKIN as the system clock. The DSP is in the Megamodule Sleep Mode and all peripherals are disabled.

The Typical-300Mhz macro button can be used to quickly visualize the use case scenario as described in the C6747 tech brief. The details of the peripherals and their operating conditions used in this scenario are:

All other modules are not used and disabled.

The Typical-456Mhz macro button is the same as the Typical-300Mhz macro button, except that core voltage is at 1.3 volts, and the device is running at 456Mhz.

The RTC Power Only macro button reports the power consumed with 1.2 volts applied only to RTC CVDD. Core and I/O rails are powered off.


Limitations

The current implementation of the power estimation spreadsheet has the following limitations:


Download


Revision History Date Changes
A May 2010 Initial Release
B Nov 2010 Includes new peripheral


References

E2e.jpg For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article C6747/45/43 Power Consumption Summary here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox