Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

CC13xx CC26xx Tools Overview

From Texas Instruments Wiki
Jump to: navigation, search

This article gives you an overview of the Tools and kits available for developing on the CC13xx and CC26xx family of devices.

Kits

CC1310DK

CC1310 Development Kit
  • Platform for firmware development
  • RF performance reference design
  • 2x CC1310EM-7XD-7793
  • 2x SmartRF06EB

CC1310EMK

CC1310 Evaluation Module Kit
  • RF performance reference design
  • Compatible with SmartRF06EB
  • 2x CC1310EM-7XD-7793
  • 2x Pulse W5017 antennas

CC2640R2 LaunchPad

CC2640R2 LaunchPad for BLE
  • XDS110 debugger included on board
  • RF performance reference design
  • Primary kit for BLE development with the SIMPLELINK-CC2640R2-SDK
  • Bluetooth 5 Ready

CC2650DK

CC2650 Development Kit
  • Platform for firmware development
  • RF performance reference design
  • 2x CC2650EM-7ID
  • 2x SmartRF06EB

CC2650STK

CC2650 SensorTag Kit
  • Sensor kit for app developers
  • iOS and Android apps available
  • Contains CC2650 BLE SensorTag
  • IoT enabled

CC2650 LaunchPad

CC2650 LaunchPad
  • XDS110 debugger included on board
  • RF performance reference design
  • Note: TI recommends CC2640R2F LaunchPadfor BLE development
  • IoT and multi-protocol enabled


CC1350 LaunchPad

CC1350 LaunchPad
  • XDS110 debugger included on board
  • RF performance reference design
  • Dual-band Wireless MCU
  • Supported in the BLE-Stack SDK
  • IoT enabled

CC1310 LaunchPad

CC1310 LaunchPad
  • XDS110 debugger included on board
  • RF performance reference design
  • Sub
  • IoT enabled

  • All LaunchPad and SmartRF06 kits featured above can be used as a standalone JTAG debugger / programmer to custom boards with CC26xx / CC13xx wireless MUCs. Refer to the LaunchPad procedure in Application Note SWRA534.

Software Tools

This section covers the software tools available for the CC13xx/CC26xx device family.

SmartRF Studio 7 Startup Window

SmartRF Studio 7

What is SmartRF Studio?

SmartRF Studio is a PC application that helps designers of radio systems to easily evaluate the RF-IC at an early stage in the design process.

  • Can be used in combination with several development kits for Texas Instruments’ CCxxxx RF-ICs.
  • Test functions for sending and receiving radio packets, continuous wave transmit and receive.
  • Evaluate RF performance on custom boards by wiring it to a supported evaluation board or debugger.
  • Can also be used without any hardware, but then only to generate, edit and export radio configuration settings.


Sensor Controller Studio

Sensor Controller Studio

What is Sensor Controller Studio?

Sensor Controller Studio provides a development environment for the CC26xx/CC13xx Sensor Controller. The Sensor Controller is a proprietary, power-optimized CPU located in the CC26xx/CC13xx AUX domain, which can perform simple background tasks autonomously and independent of the System CPU state.

  • Allows for Sensor Controller task algorithms to be implemented using a C-like programming language
  • Outputs a Sensor Controller Interface driver, which incorporates the generated Sensor Controller machine code and associated definitions
  • Allows for rapid development by using the integrated Sensor Controller task testing and debugging functionality. This allows for live visualization of sensor data and algorithm verification.


SmartRF Flash Programmer 2

SmartRF Flash Programmer 2

What is SmartRF Flash Programmer 2?

SmartRF Flash Programmer 2 is a PC application for JTAG programming TI CC13x0 & CC26x0 ARM devices.

  • Graphical User Interface (GUI) and Command Line Interface (CLI) versions.
  • Features: Edit secondary MAC addresses, program multiple files.
  • Supports cJTAG/JTAG interface and CC13xx/CC26xx serial bootloader
  • Please note JTAG programming of CC13x2 and CC26x2 devices is not supported. Please use Uniflash


CCS Uniflash 3.x

Uniflash

What is Uniflash?

Uniflash is a standalone flash programmer with Windows, Mac and Linux desktop support

  • Graphical User Interface (GUI) and Command Line Interface (CLI) versions.
  • Uniflash 4.x has built-in support for CC13xx/CC26xx devices (for CCS Uniflash 3.1, see here)


IDEs and Compilers

This section covers IDEs and compilers supported for the CC13xx/CC26xx device family. Refer to the SDK documentation for the supported IDE and compiler versions.

Code Composer Studio

Code Composer Studio

  • Integrated development environment with project management tools and editor
  • Code Composer Studio (CCS) 6.1 has built-in support for the CC13xx/CC26xx device family (CCS 6.0.1 support via in-app updates)
  • Best support for XDS debuggers; XDS100v3, XDS110 and XDS200
  • High integration with TI-RTOS with support for TI-RTOS Object View
  • Use CCS for free - A free, unlimited code size license will be generated that supports working with attached low cost XDS100v3/XDS110 equipped debug probes from TI or TI development kits with an on board debug probe.
    This includes the CC2650DK (XDS100v3), CC13xx/CC26xx LaunchPads & the Debugger DevPack (XDS110) for the CC2650 SensorTag. CCS v7 and later can be used for free without the need of an attached TI development kit / probe. See the CCS Licensing Wiki for more details.


IAR Embedded Workbench for ARM

IAR Embedded Workbench for ARM

  • Integrated development environment with project management tools and editor
  • IAR EWARM 7.30.3 and up has built-in support for the CC13xx/CC26xx device family
  • Broad debugger support, supporting XDS100v3, XDS110, XDS200, IAR I-Jet and Segger J-Link
  • Integrated development environment with project management tools and editor
  • RTOS plugin available for TI-RTOS


Using GCC/GDB in Eclipse

GCC/GDB

GNU Compiler Collection (GCC) and GNU Project Debugger (GDB) support is documented in an application note using CGG ARM Embedded.


Debuggers

This section covers the debuggers that support the CC13xx/CC26xx device family.

XDS100v3

XDS100v3 from Spectrum Digital

XDS110

CC26xx or CC13xx LaunchPad
  • Faster download speeds than XDS100v3
  • On board debugger for CC13xx and CC26xx LaunchPads
  • Functions as a standalone debugger for CC26xx/CC13xx custom boards
  • 2-pin cJTAG and 4-pin JTAG
  • SWO trace support
  • Supported in IAR and CCS 6.1+

XDS200

XDS200 from Spectrum Digital
  • Stand-alone version from Spectrum Digital
  • Supported in CCS and IAR
  • 2-pin cJTAG and 4-pin JTAG
  • SWO trace support
  • Faster download speeds than XDS110

IAR I-Jet

IAR I-Jet
  • Supported in IAR
  • 2-pin cJTAG and 4-pin JTAG
  • SWO trace support

Segger J-Link

Segger J-Link
  • Supported in IAR and CCS
  • 4-pin JTAG
  • Requires v6.00g or later of the jLink drivers

CC-DEVPACK-DEBUG

CC-DEVPACK-DEBUG mounted on a CC2650STK
  • Integrated XDS110
  • Debugger DevPack for the CC2650STK SensorTag
  • Not recommended for custom board programming or debugging
  • No Vsense or level shifters
  • Note: ICDI based debuggers, such as found on TM4C LaunchPads, are not compatible with CC13xx/CC26xx devices
  • Note: XDS100v2 is not compatible with CC13xx/CC26xx devices

Production Programmers

There are several production programming solutions available for the CC26xx and CC13xx devices. Please refer to e.g.




Tips & Tricks

XDS100v3

XDS110

CC-DEBUG-DEVPACK + SensorTag 2.0

When using the CC-DEBUG-DEVPACK (XDS110 debugger) with the SensorTag 2.0 (CC2650STK), make sure the SensorTag battery is mounted before attaching USB.

If you power up a CC-DEBUG-DEVPACK (Debugger DevPack) when connected to a SensorTag without battery (or a weak battery), it will boot in "firmware upgrade mode" in the Windows Control Panel. The Debugger DevPack cannot be used to debug or program CC26xx in "firmware upgrade mode." If this mode occurs, disconnect USB, remove & re-insert a fresh battery into the SensorTag, then re-attach USB to the Debugger DevPack. The battery can then be removed once the Debugger DevPack is powered up correctly.

Using IAR 7.40.2 with XDS110 and CC26xx

This section applies to IAR EWARM 7.40.2. EWARM 7.40.3 has built-in support for XDS110 (last updated 2015-08-19).

IAR 7.40.2+ has built-in support for XDS110 debugger that works together with CC13xx/CC26xx devices. To enable XDS110 support, follow the below steps.

  1. Install the included XDS Emulation Software Package on your computer (Important: use "Run as administrator" on Win7)
    1. It is recommended to use the default installation directory
  2. Configure your IAR project to use XDS110 debugger
    1. Project > Options > Debugger: Select "TI XDS" as the Debugger driver
    2. Project > Options > Debugger > TI XDS:
      1. Select "TI XDS110 Emulator" from drop down menu.
    3. Click OK to save settings.
    4. Repeat for each project in the Workspace.
  3. Connect your XDS110 debugger to your CC26xx target and make sure both are powered up.

You should be able to download and debug your CC26xx project using XDS110.

Using CCS v6.1 with XDS110 and CC13xx/CC26xx

CCS v6.1 supports XDS110 when the latest updates are applied. Refer to the Debug_DevPack_User_Guide for the setup procedure.

Using 2-wire / cJTAG with CCS

To use the XDS110 in cJTAG (2-wire) mode, please make sure your XDS110 firmware and CC26xx Device Support in CCS are up-to-date. Most CC26xx/CC13xx SDKs, including BLE-Stack v2.2.0, by default configure CCS to support cJTAG mode. If you are using an older SDK that does not configure XDS110 for cJTAG, you can configure CCS according to the procedure in this E2E post.

Adding device support to CCS Uniflash 3.1

This section applies to CCS Uniflash 3.1. It is recommended to upgrade to Uniflash v3.3 or later (last updated 2015-08-19)

CCS Uniflash 3.1 does not have built-in support for CC13xx and CC26xx devices. Follow the below steps to add device support to CCS Uniflash 3.1.

  1. Open CCS Uniflash
  2. Addding software site
    1. Go to Help > Install New Software ...
    2. Click "Available Software Sites" in the upper right corner
    3. Click Add ...
    4. The actual URL to be filled in the 'location' dialog is dependent on CCS version:
      1. Name: CC2xxx Device Support Updates
      2. Location: http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/smartrf/CCSv6
    5. Click OK twice to get back to the main window of Uniflash
  3. Go to Help > Check for Updates
  4. If updates are available, they will appear in the list of updates.
  5. Follow the Wizard to complete the update

Using CC13xx/CC26xx in MDK-ARM with Segger J-Link

This article describes how: Using Keil MDK-ARM with CC13xx/CC26xx
E2e.jpg For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article CC13xx CC26xx Tools Overview here.
Hyperlink blue.png Links

Amplifiers & Linear
Audio
Broadband RF/IF & Digital Radio
Clocks & Timers
Data Converters

DLP & MEMS
High-Reliability
Interface
Logic
Power Management

Processors

Switches & Multiplexers
Temperature Sensors & Control ICs
Wireless Connectivity