Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

CC254X Overview

From Texas Instruments Wiki
Jump to: navigation, search

Bluetooth Low Energy Main Page

Development Kits and Examples for Texas Instruments CC254X Single Mode Bluetooth 4.0

Development Kits
CC2541 Mini Development Kit CC2541 Sensor Tag (Discontinued) CC254X Development kit CC2541 Advanced Remote
med_cc2541dk-mini_cc2541dk-mini_web.jpg
CC2541 Mini Development Kit
med_cc2541dk-sensor_cc2541sensortag_1.jpg
CC2541 Sensor Tag Development Kit
med_cc2540dk_cc2540dk_web.jpg
CC2540 Development Kit
Med cc2541dk-rc cc2541dk-rc web.jpg
CC2541 Advanced Remote Control Kit
Hardware included with Kit
  • USB Dongle The USB dongle includes a CC2540. The dongle can be plugged into a PC and allow the user to connect to other BLE devices. Use TI's PC tool BTOOL or others to interface the USBDongle with serial commands. The dongle can also be used as a sniffer. Dongle include LEDs, buttons, and GPIOs. 


  • KeyFob - The KeyFob (CC2540 or CC2541) runs stand alone and required a CR2032 coin cell battery. The KeyFob includes a buzzer, 3 axis accellerometer, LEDs, buttons, and GPIO.


  • CC Debugger - Use the CC Debugger to program both the USB dongle or KeyFob.
  • SensorTag - The sensorTag includes a CC2541 and the following sensors.

     - IR temperature Sensor
     - Humidity Sensor
     - Pressure Sensor
     - Accelerometer
     - Gyroscope
     - Magnetometer




  • CC254X EM - Small board with CC254X. Plugs into SmartRF boards.


  • SmartRF Platform - Dev platform which CC254X EM plugs into. Includes: Joystick, LCD, LEDs, GPIO, RS232 connector and level shifter, programming chip (so no need for CC Debugger). Powered by USB cable or AC adapter.


  • USB Dongle - The USB dongle includes a CC2540. The dongle can be plugged into a PC and allow the user to connect to other BLE devices. Use TI's PC tool BTOOL or others to interface the USBDongle with serial commands. The dongle can also be used as a sniffer. Dongle include LEDs, buttons, and GPIOs.


  • RF antennta - Antenna attches to EM module.


  • ARC Remote - Remote with keys, accelerometer, gyro, IR.

Sample Apps Provided by Texas Instruments

(most apps can be ported between dev platforms wih minor modifications using IAR compiler)

KeyFob

  • KeyFobDemo
  • SimpleBlePeripheral
  • HeartRate Sensor
  • Glucose Sensor
  • Bloddpressure Sensor
  • Thermometer
  • HID Keyboard

USB Dongle/PC

  • HostTestApp (Network Processor/Btool)
  • Sniffer
  • HID Dongle
  • Btool
  • MultiTool

IOS /Android

  • Mutitool/OAD

SensorTag

  • SensorTagDemo

IOS/Android

  • SensorTagApp
  • MultiTool/OAD



CC254X EM

  • SimpleBlePeripheral
  • Glucose Collector
  • Bloodpressure Collector
  • HostTestApp (Network Porcessor/Btool/Multitool)
  • Sniffer

USB Dongle/PC

  • HostTestApp(Netork Processor/Btool/Mutltool)
  • Sniffer
  • HID Dongle

ARC Remote

AdvancedRemote

USB

  • HID Dongle
  • HostTestApp (Network Processor/Btool/Multitool
  • Sniffer

IOS/Android

  • MutliTool/OAD