Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

CC256x Downloads

From Texas Instruments Wiki
Jump to: navigation, search

Return to CC256x Main Wiki

CC256x Service Packs - BTS Format

The CC256x Bluetooth Service Packs (SP) are mandatory initialization scripts that contain bug fixes and platform specific configurations. They must be loaded into the corresponding CC256x device after every power cycle. The CC256x SPs are delivered in the form of a Bluetooth Script (BTS) file. A BTS file is a scripted binary file which defines the actions that should be applied to the embedded HCI commands and HCI events within the file itself.

Conversion of Service pack in to ".h" format for TI’s Bluetooth stack

NoteNote: In order to operate the chip, the Main BT init script must be loaded first, followed by either the BLE or AVPR addons.

initscripts-TIInit_VERSION_bt_spec_4.x - Main BT init script
initscripts-TIInit_VERSION_ble_add-on - BLE init script
initscripts-TIInit_VERSION_avpr_add-on - AVPR init script - WBS support and Assisted A2DP add on

You need to convert the Service pack (SP) from “.bts” format to “.h” format using the Bluetooth hardware evaluation tool (BHET), to use it with TI’s Bluetooth stack. The BHET Tool can be downloaded from the following link and how to modify and save it as in the desired format can be found here'. For all the latest TI’s Bluetooth stack versions you need to replace \Bluetopia\btpsvend\CC256XB.h (or \Bluetopia\btpsvend\CC256X.h) files respective (by taking the backup of the original file) depending on your Chip revision.

NoteNote: The sleep mode should be turned off in the Service Packs (SP) since this configuration is done as part of the the TI’s Bluetooth stack initialization. If using the BHET tool, the sleep mode can be turned off in the SP Configurations Panel. This option disables the "Deep sleep enable" parameter in the HCI_VS_Sleep_Mode_Configurations (0xFD0C) command that is inside the SP.

This page holds all the Service Packs (SP) required for proper operation by the different variants of TI Bluetooth device CC256x. As noted previously, the CC256x SP must be loaded first during initialization each time the device boots up.

TI Device Module(s) Module Vendor Filename Version Comments
CC2560 *

* Not recommended for new designs

PAN1315 Panasonic CC2560_BT_SP_BTS.zip v2.44
  • Classic Bluetooth
  • 3Mbps UART baud rate
  • XTAL Support
  • Sleep Enabled
  • AKA TIInit_6.2.31.bts
CC2560A *

* Not recommended for new designs

PAN1315A / PAN1325A Panasonic CC2560A_BT_SP_BTS.zip v2.14
  • Classic Bluetooth
  • 115.2Kbps UART baud rate
  • XTAL Support
  • Sleep Enabled
  • AKA TIInit_6.6.15.bts
CC2564 *

* Not recommended for new designs

PAN1316 / PAN1326, PAN1323 Panasonic CC2564 BT BLE SP BTS.zip v2.14
  • Classic Bluetooth and Bluetooth Low Energy
  • 115.2Kbps UART baud rate
  • XTAL Support
  • Sleep Enabled
  • AKA TIInit_6.6.15.bts
CC2560B CC2560B QFN

PAN1315B / PAN1325B
TI QFN

Panasonic
CC2560B BT 4.0 SP

CC2560B BT 4.1 SP
CC2560B AVPR Add-On

Service Pack Download
  • Classic Bluetooth
  • 115.2Kbps UART baud rate
  • XTAL Support
  • Sleep Enabled
  • AKA TIInit_6.7.16.bts
  • If you are using TI’s Bluetooth stack SDK for MSP430 V1.4 R2 , use initscripts-TIInit_6.7.16_bt_spec_4.1.bts service pack.
    For any other TI’s Bluetooth stack SDK for MSP430 version before V1.4 R2, use initscripts-TIInit_6.7.16_bt_spec_4.0.bts service pack.
  • For Tiva C release V1.1, You would need to use the BHET tool and change the baud rate to 921600 before converting it to array format for the SP to load properly.
CC2564B CC2564B QFN
CC2564MODN

PAN1316B / PAN1326B
TI QFN
TI MODN

Panasonic
CC2564B BT 4.0 SP

CC2564B BT 4.1 SP CC2564B BLE Add-On CC2564B AVPR Add-On

Service Pack Download
  • Classic Bluetooth and Bluetooth Low Energy
  • 115.2Kbps UART baud rate
  • XTAL Support
  • Sleep Enabled
  • AKA TIInit_6.7.16.bts
  • If you are using TI’s Bluetooth stack SDK for MSP430 V1.4 R2, use initscripts-TIInit_6.7.16_bt_spec_4.1.bts service pack.
    For any other TI’s Bluetooth stack SDK version for MSP430 before V1.4 R2, use initscripts-TIInit_6.7.16_bt_spec_4.0.bts service pack.
  • For Tiva C release V1.1, You would need to use the BHET tool and change the baud rate to 921600 before converting it to array format for the SP to load properly.


CC2564C CC2564C QFN
CC256XCQFN-EM
TI CC256XCQFN-EM

CC2564C BT 4.2 SP - Main Script (initscripts-TIInit_6.12.26.bts)

CC2564C BLE Add-On - Audio/Voice processing add-on (initscripts-TIInit_6.12.26_avpr_add-on.bts)

CC2564C AVPR Add-On - BLE add-on (initscripts-TIInit_6.12.26.ble_add-on.bts)

Service Pack Download
  • Classic Bluetooth and Bluetooth Low Energy
  • 115.2Kbps UART baud rate
  • Sleep Enabled


NoteNote: For Linux Users: - The baud rate must be updated to 3000000 in the Main init script: “Send_HCI_VS_UPDATE_Uart_HCI_Baudrate 0xFF36, 115200 to 3000000. Also update Com_SetParams 3000000, 1 instead of Com_SetParams 115200. From here the following steps can be followed to merge the Main init script with either the BLE or AVPR addons.




CC256xB - Updated Fixes in Service Pack 1.6

Subject Description Comments
BLE When there was already one or more BLE connection active for at least 12 hours, connecting another BLE device resulted in a non-optimal BLE connection offset ('d'). This bug caused a lag in BLE data which was sent only after the link supervision timeout.

BLE BLE disconnection might have occurred after several minutes if an already existing BLE connection in parallel with an ACL connection (slave mode) was present.


CC256xB - Updated Fixes in Service Pack 1.5

Subject Description Comments
BT BLE Coex On certain race conditions, the device could lockup while BLE and ACL connections were active, and another BLE connection was being established.

SW Flow Control For hosts working with SW flow control, there could be a missed tx packet during excessive BLE continuous transmission.


CC256xB - Updated Fixes in Service Pack 1.4

Subject Description Comments

Initialization

In certain platforms, there could be a race condition where calibration didn't complete successfully during init, which resulted in device becoming unresponsive



CC256xB - Updated Fixes in Service Pack 1.3


Subject Description Comments

BT BLE Coex

If BLE interval was shorter than 24 frames, A2DP quality was degraded due to using only 3DH1 packets

BT BLE Coex

BLE interval was multiplied (x2 or x3) during BT high throughput scenario without notifying the peer

BLE

In a certain rare/race condition, BLE connection complete event was malformed

BLE

Device could reach a lockup state if BLE Adv interval was very short

BT Connection

BT connection might not have been established successfully if both local and peer started the process at the same time

IOP

If host disabled role switch, connection to iPhone 6 was not set up successfully

Current Consumption

AVPR processor did not go into low power mode. This resulted in higher current consumption

WBS

The PCM clock accuracy had to be less than 10ppm when the CC256XB was the PCM slave during WBS mode. Higher PPM deviation may have lead to high packet loss (“ticks”) at the PCM interface, or device lockup due to the clock drifts between the BT network and PCM bus

A3DP

Device could reach a lockup state when using A3DP SOURCE to 2 SINK devices feature

BLE

Fixed an issue where packets with bad CRC were sent to remote device

BLE

Fixed an issue where device could reach a lockup state if both local and peer devices terminated the BLE connection at the same time

Test Mode

BLE TX start needed to be issued twice if number of packets was set in “HCI_VS_Set_LE_Test_Mode_Parameters” command

Configuration

There was an issue in the HCI_VS_Write_CODEC_Config (0xFD06) command when using “Fsynch Multiplier” field. If the “Frame-sync duty cycle” is set to 0 (50% duty cycle), this value may not have been calculated correctly

HFP/A3DP

No voice was heard when creating NBS after closing the A3DP stream and without disconnecting the ACL

BT SIG

BT4.0 was reported instead of BT4.1 in LMP_VER_RES

BLE A2DP Coex

Device could reach a lockup state if BLE and A2DP were working concurrently

BT Connection

6 sniff connections and 1 active ACL connection resulted in device lockup. Solution is to limit the number of sniff connections to only 5 in the controller, where the rest of the connections (2) would be active

Inquiry Scan

In rare conditions, inquiry scan could have gotten stuck, which lead to device not being discoverable



CC256xB - Updated Fixes in Service Pack 1.2


Subject Description Comments

New Init scripts

New init scripts added divided into three different files:

Main init script - BT file with latest improvements
BLE init script - BLE add on
AVPR init script - WBS support and Assisted A2DP add on

In order to operate chip first use the Main init script and use the relevant add on.

Important Note: Both add on files can't operate at the same time

PCM Clock extension

PCM clock extension support

When CC2564 device is the master of the PCM BUS, allows the system to keep the PCM clock running even when no A3DP channel is open

The new VS command

HCI_VS_Enable_PCM_Clock_Extension 0xfe4c
Receives one parameter (UINT16) which indicates the time to keep the pcm clock on
0 - Keep PCM clock on forever
0xFFFF - Disable PCM clock extension - default value

Sniff

Improved collision handling in Sniff mode

Fixed collision between Sniff sub rate and exit sniff



CC256xB - Updated Fixes in Service Pack 1.1


Subject Description Comments

Assisted A2DP

PCM clock tracking mechanism when Master over the PCM, Improved skew alignment between channels
New features added to Multi Room support

LM

Improved multiple LMP handling simultaneously. Receiving packet type table request during secure simple pairing resulted in unsuccessful connection, this issue is fixed in this version

Clock accuracy

Better clock resolution result received from hci_read_clock
Resolution of 312.5 uS

BLE stability

Improved Interoperability for spec 4.1

Low power support

Better Immunity to hardware noise over the UART lines



CC256xB - Updated Fixes in Service Pack 1.0


Subject Description Comments

BT SIG

BT 4.1 support
No new features were added

Host I/F

Added new event "vs_reject_voice_link_event" upon remote attempting to establish 3rd voice connection (2 voice connections are already active)

ETSI

ETSI 300 328 version 1.8.1 might still have failed despite the fix in service pack 0.2

Stability

Remote name request during A2DP data streaming might have resulted in BT getting stuck

Stability

When running loop of BLE connect-disconnect (with page scan running in background), slave side might get stuck at establishment of BLE connection

Assisted A2DP

Add support for host flow control in assisted A2DP SNK

Assisted A2DP

Fix occasional drop outs in assisted A2DP SNK

BLE

BLE slave ignored "LL terminate" indication if was busy with other peer transaction

Current Consumption

High current draw due to slave exiting latency from reception of “LL channel map” or “LL connection update” until instant

Current Consumption

Device did not enter deep sleep in sniff mode after setting LSTO to 5 seconds



CC256xB - Updated Fixes in Service Pack 0.2


Subject Description Comments

ETSI

ETSI 300 328 version 1.8.1

Assisted A2DP

Assisted A2DP Sink - Audio Dropout Issue

Assisted A2DP

Update Codec Configuration API to support better frequency resolution
processors.wiki.ti.com/index.php/CC256x_VS_HCI_Commands#HCI_VS_Write_CODEC_Config_.280xFD06.29

Host I/F

Added support to host flow control during assisted A2DP
 BLE Fix BLE slave latency behavior during transactions


CC256xB - Updated Fixes in Service Pack 0.1


Subject Description Comments

Current Consumption

Deep Sleep was not enabled after enable and disable advertising mode
Recreated 15% of the time when enable and disable advertising within a 2-3 second period

BLE

Missing BLE disconnection event after sending HCI disconnect command
The command status event was executed


CC2560A/CC2564 - Updated Fixes in Service Pack 2.14

Subject Description Comments

ETSI

ETSI 300 328 version 1.8.1 threshold fine tuning

IOP Improved BLE connection statistics with LPRF 2540 device


CC2560A/CC2564 - Updated Fixes in Service Pack 2.12


Subject Description Comments

ETSI

ETSI 300 328 version 1.8.1

Throughput

Data streaming throughput with peer 1 drops, and stays low after attempting to connect to peer 2, and canceling create connection

Voice

WBS Audio to peer 1 lost upon connection and disconnection with any peer 2 device

Voice

Device connected with WBS to peer 1 and to peer 2. After disconnecting peer 2, when disconnecting and reconnecting to peer 1, there is no audio on peer 1

IOP

When in Master role, response to peer initiated "LMP_Feature_Request" with "LMP_Not_accepted" and reason invalid parameter, peer device crashes and connection drops


Related Documents