Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

CC256x System Design Guide

From Texas Instruments Wiki
Jump to: navigation, search

Return to CC256x Main Wiki

Introduction

Welcome to the CC256x Hardware System Design Guide. This page describes how to use TI's CC256x Bluetooth family of devices and how to interface our CC256x devices and modules from a systems perspective. Among the things discussed is how to interface the host to the CC256x controller, supply the power, provide the clocks, and adding an antenna.  


Power Supply Clocks nSHUTD Host Controller Interface PCM/I2S Interface Bluetooth RF I/O


 

For any discrepencies found on this page, the CC256x datasheet takes precedence over this guide.

Scope

CC256x Functional Diagram.jpg

This guide is intended for customers that are using the CC256x modules and devices. This guide states hardware interfacing requirements and provides several options for implementing custom designs. The following is NOT the objective of this wiki:

Instead the page will provide systems level interfacing techniques that aims to reduce design time and minimize errors.
This page WILL cover interfacing techniques for users incorporating the following CC256x modules in their design:

For the host, we use the MSP430 as an example. The user is free to use any MPU/CPU for the host as long as it meets the required hardware interfaces. For modular based designs, please take into consideration the interfaces that are already incorporated into the module.

Nomenclature

Name Explanation
bps bits per second
HCI Host Controller Interface
RF Radio Frequency
SIG Special Interest Group
BT Bluetooth
VS Vendor Specific

Useful Links

The following links will be frequently referred to in this guide:

Required Interfacing

The following interfaces must be provided to the CC256x:

  • Host Controller Interface through H4 UART
  • Clocks (32KHz & 26 MHz)
  • Power (1.8V & 3.3V)
  • Antenna propagation

Power Supply

The CC256x requires two different power supplies: VDD_IO to power the input/outputs at 1.8V and VDD_IN to power the CC256x Bluetooth core at around 3.6V. If the MCU such as the MSP430 is only 3.3V compatible,

the CC256x can share the 3.3V(range is 2.2 - 4.8 V) power supply for VDD_IN. For VDD_IO,an LDO chip should be provided to drop the 3.3V to 1.8V to supply power to the I/Os. We recommend the  TPS78318 for the LDO.

   CC256x Functional Diagram VIO.PNG

Cc256x powerScheme.PNG
 Figure: VBAT Power Supply Mode

In this power configuration mode, the CL1.5_LDO_IN(Class 1.5 Power Amplifier LDO input) and MLDO_IN(Main LDO input) is connected to the battery (VBAT or VDD_IN). The following table summarizes the specifications for the power inputs:

Power  Pins Nominal Voltage Voltage Range Max Current
VDD_IO 1.8 V 1.62- 1.92 V 1 mA
VDD_IN 3.6 V 2.2 - 4.8 V 150 mA

Refer to the datasheet for further specifications. 

Clocks

Two clocks are required by the device: a fast clock and a slow clock. Note that the Modules already include a fast clock and thus only a 32.768KHz slow clock is required. Otherwise, a 26MHz fast clock and a 32.768KHz slow clock should be provided. For proper start-up, these guidelines must be followed as described in this page. This applies to both devices and modules. Since the CC256x requires a 1.8V signal, voltage translation might be necessary to meet this specification.

CC256x Functional Diagram CLK.PNG


Clock Frequency Accuracy
Slow Clock 32.768 KHz ±250 ppm
Fast Clock 26 MHz ±20 ppm


Fast Clock

CC256x FastClk.PNG

Figure: Fast Clock using External Crystal

If using a module, the fast clock is inside the module. Otherwise a 26MHz crystal should be placed as close to the chip as possible. The typical values for the trimming capacitors for the crystal, C1 and C2, are listed in the table below. Please refer to the datasheet for the recommended crystal and clock configurations.  

FREQ (MHz) C1 (pF) C2 (pF)
26 15pF typ 15pF typ


Slow Clock

The slow clock can be provided from several sources including: external crystal oscillator and host processor. In either case, it must be 32.768 kHz ±250 ppm within a range of 0 to 1.8V.

Supplied by External Crystal Oscillator

 Pctoolslowclk.png

Note: Circuit shown has oscillator disabled (R35 = 0Ohm). Do not place R35 to enable slow clock.

The part number for the slow clock is ASH7K-32.768KHZ-T from Abracon Corporation.

Figure: Slow Clock in QFN Design

Supplied by Host Processor

 Slowclk.jpg


Some microcontrollers provide clock outputs. For example, the MSP430 has ACLK pin which is output to the BT for supplying the 32KHz slow clock from an oscillator. In the figure above, the 32kHz clock is directly interfaced with the MSP430 which then outputs it to the CC256x Bluetooth device.  


nSHUTD

CC256x Functional Diagram SHUT.PNG


nSHUTD is an active low shutdown input for the CC256x. It behaves similar to a restart switch. The following table summarizes nSHUTD functions:

Value Meaning
LOW Turn off CC256x (Shutdown)
HIGH Turn on CC256x

nSHUTD is used during startup and shutdown procedures. nSHUTD is implemented as a GPIO and may require voltage translation. Refer to the datasheet for the proper sequence.

Host Controller Interface

The CC256x device requires an HCI interface which uses the H4 UART protocol. The CC256x uses HCI_TX and HCI_RX lines to transmit and receive data, respectively. The RTS  and CTS lines are required by the CC256x for flow control. If the MCU does not support flow control, GPIOs should be used to implement flow control. All I/O pins are at 1.8 V. If the host does not output at 1.8V, a voltage translation must be performed before interfacing to the CC256x.  

CC256x Functional Diagram HCI.PNG

Universal Asynchronous Receiver/Transmitter (UART) 

Pctooluart.PNG

Figure: UART pins on CC256x

Most MCUs have peripheral UART modules which includes RX and TX capabilities. In the case they do not, GPIOs can be used to simulate UART behavior. The default baud rate for the BT device is 115.2 kbps, 8N1 configuration as summarized in the following table:

Parameter Value
Bit Rate

Default:115200 bps*

Min: 37500 bps 

Max: 4 Mbps 

Data Length 8 bits
Stop 1 bit
Parity None

Note: Refer to the CC256x VS HCI Commands Document to change the baud rate. 
 

Flow Control

CC256x require the use of HCI_RTS(request-to-send) and HCI_CTS(clear-to-send) lines for UART flow control. When HCI_RTS is low, the host is allowed to send data. When HCI_CTS is low(Host_RTS also low), the CC256x device is allowed to send data. It is also used to carry out a power management protocol (HCILL sleep protocol) to synchronize deep sleep mode between the host and controller. The Host_CTS should be interruptible in case the host decides to go into low power mode and needs to be woken up by HCI_RTS.

PCM/I2S Interface

CC256x Functional Diagram PCM.PNG

The codec interface on the CC256x consists of 4 signals(AUD_FSYNC,AUD_CLK,AUD_IN,AUD_OUT) for audio streaming. It supports both pulse-code modulation (PCM) and Integrated Interchip Sound (I2S) data format protocols. These pins can be directly connected to a dedicated codec which plays the sound through a speaker or it can be connected to general-purpose processors that can decode the data. This is an optional interface which is not required for the basic operation of the CC256x but may be required for a specific use case or application. For example, this interface is required for the Hands Free Profile and Assisted A2DP profiles.

Signal Direction Description
AUD_CLK Input or Output PCM clock
AUD_FSYNC Input or Output PCM frame-sync signal
AUD_IN Input PCM data input
AUD_OUT Output PCM data output


Voltage Levels

The correct range of voltage levels must be applied to each pin as described in the datasheet for proper operation. Level shifters are used to bring down a higher voltage source to the lower voltages needed by the I/O, power, and clock ports. 

Level Shifters for I/Os & Clocks

Feel free to use the reference parts used in the schematic snippets below for 3.3V to 1.8V voltage translation. You can order free samples of these parts from TI. All of following level shifters use Texas Intruments's SN74AVC4T774RSV which are used as unidirectional voltage translators.

HCI UART

PctoolUARTtrans.PNG

Audio

PctoolAudiotrans.PNG

Slow Clock/NSHUTD

PctoolClocktrans.PNG

Bluetooth RF I/O

  CC256x Functional Diagram ANT.PNG

The device requires an antenna to transmit and receive information over the air. There are two options for antennas: chip antennas or copper antennas (copper traces on PCB designed for RF propagation).

BPF

The BPF is required to pass FCC testing. It helps block spurious emissions outside of the 2.4GHz signals. One recommended BPF is the LFB212G45SG8A127.

Antennas

Chip antennas are usually inexpensive, small, and less complex to integrate with a design. Some module vendors support chip antennas (either on or off the module).  

Copper Antenna on PCB are almost as good as chip antenna although it might take up more board space. The CC256x QFN design uses printed PCB antenna.   

Refer to the PCB Design Guide and Antenna Design Guide for more guidelines on designing and placing an antenna.

Coaxial U.FL RF Port

The U.FL port is mainly used for performance evaluation during production line testing. It is used for various purposes including:

  • Verify RF performance with a spectrum analyzer
  • Carry out automated RF SIG tests with a CBT Bluetooth Tester

Note also that the modules do not require these RF tests since they are already certified. It is optional to carry out some acceptance tests after production. 


The U.FL is usually not included in the modules and needs to taken into consideration when designing the board. The U.FL port has to share the BT_RF port with the antenna. Since they both cannot be connected at the same time to the BT_RT port, a multiplexing scheme is used to switch between the antenna and U.FL. One option is a Coaxial Connectors with Switch used in Murata's module which automatically connect/disconnects the U.FL port from BT_RF when a cable is attached/detached to the U.FL connector, respectively. Another option is to implement a simple resistor switch in which a zero ohm resistor is moved in a certain position on the PCB to connect either the antenna or the U.FL to the BT_RF.