Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

CC256x TI Bluetooth Stack PXPDemo App

From Texas Instruments Wiki
Jump to: navigation, search

Return to CC256x MSP430 TI’s Bluetooth stack Basic Demo APPS

Return to CC256x Tiva TI’s Bluetooth stack Basic Demo APPS

Return to CC256x MSP432 TI’s Bluetooth stack Basic Demo APPS

Return to CC256x STM32F4 TI’s Bluetooth stack Basic Demo APPS

Demo Overview

NoteNote: The same instructions can be used to run this demo on the Tiva, MSP432 or STM32F4 Platforms.

The Proximity profile is used to notify the Client about Link Loss and Power Level of the Server device. There are two roles defined in this profile, Server and the Client. Any changes made to the Power Level or Link Loss is also notified by the Server to the Client.

This application allows the user to use a console to use Bluetooth Low Energy (BLE) to establish connection between two BLE devices, Notify Link Loss, Set Alert Levels and Get Transmit Power Levels.

It is recommended that the user visits the kit setup Getting Started Guide for MSP430, Getting Started Guide for TIVA, Getting Started Guide for MSP432 or Getting Started Guide for STM32F4 pages before trying the application described on this page.

Running the Bluetooth Code

Once the code is flashed, connect the board to a PC using a miniUSB or microUSB cable. Once connected, wait for the driver to install. It will show up as MSP-EXP430F5438 USB - Serial Port (COM x), Tiva Virtual COM Port (COM x), XDS110 Class Application/User UART (COM x) for MSP432, under Ports (COM & LPT) in the Device manager. Attach a Terminal program like PuTTY to the serial port x for the board. The serial parameters to use are 115200 Baud, 8, n, 1. Once connected, reset the device using Reset S3 button (located next to the mini USB connector for the MSP430) and you should see the stack getting initialized on the terminal and the help screen will be displayed, which shows all of the commands.


InitializePXP.png


Demo Application

This demo application page provides a description of how to connect two configured boards and communicate over Bluetooth Low Energy (BLE). The included application registers a custom service on a board when the stack is initialized.

Device 1 (Server) setup on the demo application

a) To start, one of the devices has to have the Link Loss Service (LLS), Immediate Alert Szervice (IAS) and Transmit Power Service (TPS) running on it. It can be started by issuing the RegisterLLS, RegisterIAS and RegisterTPS commands.


RegisterServicesPXP.png


b) Next, the device acting as a Server needs to advertise to other devices. This can be done by issuing the AdvertiseLE <Enable/Disable> <Address Type> command.

AdvertiseLEPXP.png

Device 2 (Client) setup on the demo application

NoteNote: Steps c and d are optional if you already know the Bluetooth address of the device that you want to connect to.


c) The Client LE device can try to find which LE devices are in the vicinity issuing the StartScanning command.


d) Once you have found the device, you can stop scanning by issuing the StopScanning.

PASS3.png

Initiating connection from device 2

e) Once the application on the Client side knows the Bluetooth address of the device that is advertising, it can connect to that device by issuing the
ConnectLE <Bluetooth Address of Remote Device> <Remote Address Type> <Own Address Type>

ConnectLEPXP.png

Identify supported services

f) After initialization, the Client needs to find out whether LLS, IAS and TPS services are supported. For this the DiscoverLLS, DiscoverIAS, DiscoverTPS commands are issued on the Client. After the service discovery operations are complete, the LLS, IAS and TPS Service Discovery Summary and list of supported features is shown.

DiscoverServicesPXP.png

Proximity Notification between Client and Server

g) Change the Alert Level from the Client. To change the Alert Level from Client, the commands SetAlertLevel and GetAlertLevel are issued to change and view the updated alert level.

AlertLevelPXP.png

h) Change Transmtheit power level (TxPower) from the Client. To change the TxPower Level, the SetTxPowerLevel command is issued from the Server while to obtain the TxPower Level the GetTxPowerLevel command is issued from the Client.

AlertLevelPXP.png

TxPowerLevelClientPXP.png

Application Commands

TI’s Bluetooth stack is implementation of the upper layers of the Bluetooth protocol stack. TI’s Bluetooth stackprovides a robust and flexible software development tool that implements the Bluetooth Protocols and Profiles above the Host Controller Interface (HCI). TI’s Bluetooth stack's Application Programming Interface (API) provides access to the upper-layer protocols and profiles and can interface directly with the Bluetooth chips.

An overview of the application and other applications can be read at the Getting Started Guidefor MSP430, Getting Started Guide for TIVA M4, Getting Started Guide for MSP432 and Getting Started Guide for STM32F4.

This page describes the various commands that a user of the application can use. Each command is a wrapper over a TI’s Bluetooth stack API which gets invoked with the parameters selected by the user. This is a subset of the APIs available to the user. TI’s Bluetooth stack API documentation (TI_Bluetooth_Stack_Version-Number\Documentation or for STM32F4, TI_Bluetooth_Stack_Version-Number\RTOS_VERSION\Documentation) describes all of the API's in detail.

GAP Commands

The Generic Access Profile defines standard procedures related to the discovery and connection of Bluetooth devices. It defines modes of operation that are generic to all devices and allows for procedures which use those modes to decide how a device can be interacted with by other Bluetooth devices. Discoverability, Connectability, Pairability, Bondable Modes, and Security Modes can all be changed using Generic Access Profile procedures. All of these modes affect the interaction two devices may have with one another. GAP also defines the procedures for how bond two Bluetooth devices.

Help (DisplayHelp)

Description
This command is responsible for displaying the app's command options. The input parameter to this command is completely ignored, and only needs to be passed in because all Commands that can be entered at the Prompt pass in the parsed information. This command displays the current Command Options that are available and always returns zero.

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.

Possible Return Values
This command always returns 0



GetLocalAddress

Description
The GetLocalAddress command is responsible for querying the Bluetooth Device Address of the local Bluetooth Device. This function returns zero on a successful execution and a negative value on all errors. A Bluetooth Stack ID must exist before attempting to call this command.

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the Query.

Possible Return Values
(0) Successfully Query Local Address
(-1) BTPS_ERROR_INVALID_PARAMETER
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-8) INVALID_STACK_ID_ERROR
(-4) FUNCTION_ERROR

API Call
GAP_Query_Local_BD_ADDR(BluetoothStackID, &BD_ADDR);

API Prototype
int BTPSAPI GAP_Query_Local_BD_ADDR(unsigned int BluetoothStackID, BD_ADDR_t *BD_ADDR);

Description of API
This function is responsible for querying (and reporting) the device address of the local Bluetooth device. The second parameter is a pointer to a buffer that is to receive the device address of the local Bluetooth device. If this function is successful, the buffer that the BD_ADDR parameter points to will be filled with the device address read from the local Bluetooth device. If this function returns a negative value, then the device address of the local Bluetooth device was NOT able to be queried (error condition).



SetDiscoverabilityMode

Description
The SetDiscoverabilityMode command is responsible for setting the Discoverability Mode of the local device. This command returns zero on successful execution and a negative value on all errors. The Discoverability Mode in LE is only applicable when advertising, if a device is not advertising it is not discoverable. The value set by this command will be used as a parameter in the command AdvertiseLE.

Parameters
This command requires only one parameter which is an integer value that represents a Discoverability Mode. This value must be specified as 0 (for Non-Discoverable Mode), 1 (for Limited Discoverable Mode), or 2 (for General Discoverable Mode).

Command Call Examples
"SetDiscoverabilityMode 0" Attempts to change the Discoverability Mode of the Local Device to Non-Discoverable. "SetDiscoverabilityMode 1" Attempts to change the Discoverability Mode of the Local Device to Limited Discoverable. "SetDiscoverabilityMode 2" Attempts to change the Discoverability Mode of the Local Device to General Discoverable.

Possible Return Values
(0) Successfully Set Discoverability Mode Parameter
(-6) INVALID_PARAMETERS_ERROR
(-8) INVALID_STACK_ID_ERROR



SetConnectabilityMode

Description
The SetConnectabilityMode command is responsible for setting the Connectability Mode of the local device. This command returns zero on successful execution and a negative value on all errors. The Connectability Mode in LE is only applicable when advertising, if a device is not advertising it is not connectable. The value set by this command will be used as a parameter in the command AdvertiseLE.

Parameters
This command requires only one parameter which is an integer value that represents a Connectability Mode. This value must be specified as 0 (for Non-Connectable) or 1 (for Connectable).

Command Call Examples
"SetConnectabilityMode 0" Attempts to set the Local Device’s Connectability Mode to Non-Connectable. "SetConnectabilityMode 1" Attempts to set the Local Device’s Connectability Mode to Connectable.

Possible Return Values
(0) Successfully Set Connectability Mode Parameter
(-6) INVALID_PARAMETERS_ERROR
(-8) INVALID_STACK_ID_ERROR



SetPairabilityMode

Description
The SetPairabilityMode command is responsible for setting the Pairability Mode of the local device. This command returns zero on successful execution and a negative value on all errors.

Parameters
This command requires only one parameter which is an integer value that represents a Pairability Mode. This value must be specified as 0 (for Non-Pairable) or 1 (for Pairable).

Command Call Examples
“SetPairabilityMode 0” Attempts to set the Local Device’s Pairability Mode to Non-Pairable. “SetPairabilityMode 1” Attempts to set the Local Device’s Pairability Mode to Pairable.

Possible Return Values
(0) Successfully Set Pairability Mode
(-4) FUNCTION_ERROR
(-6) INVALID_PARAMETERS_ERROR
(-8) INVALID_STACK_ID_ERROR

API Call
GAP_LE_Set_Pairability_Mode(BluetoothStackID, PairabilityMode);

API Prototype
int BTPSAPI GAP_LE_Set_Pairability_Mode(unsigned int BluetoothStackID, GAP_LE_Pairability_Mode_t PairableMode);

Description of API
This function is provided to allow the local host the ability to change the pairability mode used by the local host. This function will return zero if successful or a negative return error code if there was an error condition.



ChangePairingParameters

Description
The ChangePairingParameters command is responsible for changing the LE Pairing Parameters that are exchanged during the Pairing procedure. This command returns zero on successful execution and a negative value on all errors.

Parameters
This command requires five parameters which are the I/O Capability, the Bonding Type, the MITM Requirement, the SC Enable and the P256 debug mode.
The first parameter must be specified as 0 (for Display Only), 1 (for Display Yes/No), 2 (for Keyboard Only), 3 (for No Input/Output) or 4 (for Keyboard/Display).
The second parameter must be specified as 0 (for No Bonding) or 1 (for Bonding), when at least one of the devices is set to No Bonding, the LTK won't be stored.
The third parameter must be specified as 0 (for No MITM) or 1 (for MITM required).
The fourth parameter must be specified as 0 (for SC disabled) or 1 (for SC enabled), when using SC disable, legacy pairing procedure will take place.
The fifth parameter must be specified as 0 (for Debug Mode disabled) or 1 (for P256 debug mode enabled), Only when using SC pairing, P256 debug mode is relevant and when it is set, the values of the P256 private and public keys will be pre-defined according to the Bluetooth specification instead of random.

Command Call Examples
"ChangeSimplePairingParameters 3 0 0 0 0" Attempts to set the I/O Capability to No Input/Output, Bonding Type set to No Bonding, turns off MITM Protection, Disable secure connections and disable debug mode.
"ChangeSimplePairingParameters 2 0 1 1 0 " Attempts to set the I/O Capability to Keyboard Only, Bonding Type set to No Bonding, activates MITM Protection, Enabling secure connections and disable debug mode.
"ChangeSimplePairingParameters 1 1 1 1 1" Attempts to set the I/O Capability to Display Yes/No, Bonding Type set to Bonding, activates MITM Protection, Enabling secure connections and enabling debug mode.

Possible Return Values
(0) Successfully Set Pairability Mode
(-6) INVALID_PARAMETERS_ERROR
(-8) INVALID_STACK_ID_ERROR



AdvertiseLE

Description
The AdvertiseLE command is responsible for enabling LE Advertisements. This command returns zero on successful execution and a negative value on all errors.

Note: The MSP430 version of this app requires a second parameter which is the address type of the advertising device. If the advertising device uses a Public address then use 0, if it uses a Random Address then use 1.

Parameters
The only parameter necessary decides whether Advertising Reports are sent or are disabled. To Disable, use 0 as the first parameter, to enable, use 1 instead.

Command Call Examples
“AdvertiseLE 1” Attempts to enable Low Energy Advertising on the local Bluetooth device. “AdvertiseLE 0” Attempts to disable Low Energy Advertising on the local Bluetooth device.

Possible Return Values
(0) Successfully Set Pairability Mode
(-4) FUNCTION_ERROR
(-6) INVALID_PARAMETERS_ERROR
(-8) INVALID_STACK_ID_ERROR
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE
(-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Calls
Depending on the First Parameter Value
GAP_LE_Advertising_Disable(BluetoothStackID);
GAP_LE_Set_Advertising_Data(BluetoothStackID, (Advertisement_Data_Buffer.AdvertisingData.Advertising_Data[0] + 1), &(Advertisement_Data_Buffer.AdvertisingData));
GAP_LE_Set_Scan_Response_Data(BluetoothStackID, (Advertisement_Data_Buffer.ScanResponseData.Scan_Response_Data[0] + 1), &(Advertisement_Data_Buffer.ScanResponseData));
GAP_LE_Advertising_Enable(BluetoothStackID, TRUE, &AdvertisingParameters, &ConnectabilityParameters, GAP_LE_Event_Callback, 0);

API Prototypes
int BTPSAPI GAP_LE_Advertising_Disable(unsigned int BluetoothStackID);
int BTPSAPI GAP_LE_Set_Advertising_Data(unsigned int BluetoothStackID, unsigned int Length, Advertising_Data_t *Advertising_Data);
int BTPSAPI GAP_LE_Set_Scan_Response_Data(unsigned int BluetoothStackID, unsigned int Length, Scan_Response_Data_t *Scan_Response_Data);
int BTPSAPI GAP_LE_Set_Advertising_Data(unsigned int BluetoothStackID, unsigned int Length, Advertising_Data_t *Advertising_Data);
int BTPSAPI GAP_LE_Set_Advertising_Data(unsigned int BluetoothStackID, unsigned int Length, Advertising_Data_t *Advertising_Data);

Description of API
The GAP_LE_Advertising_Disable function is provided to allow the local host the ability to cancel (stop) an on-going advertising procedure. This function will return zero if successful or a negative return error code if there was an error condition. The GAP_LE_Set_Advertising_Data is provided to allow the local host the ability to set the advertising data that is used during the advertising procedure (started via the GAP_LE_Advertising_Enable function). This function will return zero if successful or a negative return error code if there was an error condition. The GAP_LE_Set_Scan_Response_Data function is provided to allow the local host the ability to set the advertising data that is used during the advertising procedure (started via the GAP_LE_Advertising_Enable function). This function will return zero if successful or a negative return error code if there was an error condition. The GAP_LE_Set_Advertising_Data function is provided to allow the local host the ability to set the advertising data that is used during the advertising procedure (started via the GAP_LE_Advertising_Enable function). This function will return zero if successful or a negative return error code if there was an error condition.



StartScanning

Description
The StartScanning command is responsible for starting an LE scan procedure. This command returns zero if successful and a negative value if an error occurred. This command calls the StartScan(unsigned int BluetoothStackID) function which performs the scan.

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the Scan.

Possible Return Values
(0) Successfully started the LE Scan Procedure
(-1) Bluetooth Stack ID is Invalid during the StartScan() call
(-4) FUNCTION_ERROR
(-8) INVALID_STACK_ID_ERROR
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES
(-105) BTPS_ERROR_SCAN_ACTIVE
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE
(-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Call
GAP_LE_Perform_Scan(BluetoothStackID, stActive, 10, 10, latPublic, fpNoFilter, TRUE, GAP_LE_Event_Callback, 0);

API Prototype
int BTPSAPI GAP_LE_Perform_Scan(unsigned int BluetoothStackID, GAP_LE_Scan_Type_t ScanType, unsigned int ScanInterval, unsigned int ScanWindow, GAP_LE_Address_Type_t LocalAddressType, GAP_LE_Filter_Policy_t FilterPolicy, Boolean_t FilterDuplicates, GAP_LE_Event_Callback_t GAP_LE_Event_Callback, unsigned long CallbackParameter);

Description of API
The GAP_LE_Perform_Scan function is provided to allow the local host the ability to begin an LE scanning procedure. This procedure is similar in concept to the inquiry procedure in Bluetooth BR/EDR in that it can be used to discover devices that have been instructed to advertise. This function will return zero if successful, or a negative return error code if there was an error condition.



StopScanning

Description
The StopScanning command is responsible for stopping an LE scan procedure. This command returns zero if successful and a negative value if an error occurred. This command calls the StopScan(unsigned int BluetoothStackID) function which performs the scan.

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of disabling Scanning.

Possible Return Values
(0) Successfully stopped the LE Scan Procedure
(-1) Bluetooth Stack ID is Invalid during the StartScan() call
(-4) FUNCTION_ERROR
(-8) INVALID_STACK_ID_ERROR
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE
(-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Call
GAP_LE_Cancel_Scan(BluetoothStackID);

API Prototype
int BTPSAPI GAP_LE_Cancel_Scan(unsigned int BluetoothStackID);

Description of API
The GAP_LE_Cancel_Scan function is provided to allow the local host the ability to cancel (stop) an on-going scan procedure. This function will return zero if successful or a negative return error code if there was an error condition.



SetRandomAddress

Description
The following function is responsible to Set Random Address. The Input parameter describe random address type , it can be Random static address or Resolvable Private Address or Non-Resolvable Private Address.This function will return zero on success, or a negative return error code if there was an error.

Parameters
The only parameter required is the random address type.

Command Call Examples
“SetRandomAddress 0 Attempts to send set the address as Static Address. “SetRandomAddress 1 Attempts to set the address as Resolvable Private Address.

Possible Return Values
(0) Successfully Set Pairability Mode
(-4) FUNCTION_ERROR
(-6) INVALID_PARAMETERS_ERROR
(-8) INVALID_STACK_ID_ERROR
(-116) BTPS_ERROR_RANDOM_ADDRESS_IN_USE
(-111) BTPS_ERROR_CREATE_CONNECTION_OUTSTANDING
(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE
(-57) BTPS_ERROR_DEVICE_HCI_ERROR
GAP_LE_ERROR_WHITE_LIST_IN_USE

API Calls
GAP_LE_Generate_Static_Address(BluetoothStackID,&RandomAddress);


GAP_LE_Generate_Resolvable_Address(BluetoothStackID,&IRK,&RandomAddress);
GAP_LE_Generate_Non_Resolvable_Address(BluetoothStackID,&RandomAddress);

API Prototypes
int BTPSAPI GAP_LE_Generate_Static_Address(unsigned int BluetoothStackID, BD_ADDR_t *StaticAddress_Result)
"int BTPSAPI GAP_LE_Generate_Resolvable_Address(unsigned int BluetoothStackID, Encryption_Key_t *IRK, BD_ADDR_t *ResolvableAddress_Result)"
int BTPSAPI GAP_LE_Generate_Non_Resolvable_Address(unsigned int BluetoothStackID, BD_ADDR_t *NonResolvableAddress_Result)


Description of API
The GAP_LE_Generate_Static_Address function is provided to allow a means to generate a static random device address. This device address can then be used as a random address by call GAP_LE_Set_Random_Address(). The first parameter is the Bluetooth Stack ID of the Bluetooth device. The second is a pointer to a BD_ADDR_t structure that will contain the generated static private address if this function returns sucess (zero). This function will return zero on success, or a negative return error code if there was an error.

  • NOTE * The Bluetooth Specification has defined that the Static Address should only change once per power cycle, therefore it is the requirement of the application that this function is only used to generate a new Static Address once per power cycle.

The GAP_LE_Generate_Resolvable_Address function is provided to allow a means to generate a resolvable random device address. This device address can then be used as a random address by call to the GAP_LE_Set_Random_Address() function. The first parameter is the Bluetooth Stack ID of the Bluetooth device. The second parameter is the Identity Resolving Key (IRK) that will be used in creating the resolvable address. The next is a pointer to a BD_ADDR_t structure that will contain the generated resolvable private address if this function returns success. This function will return zero on success, or a negative return error code if there was an error.

The GAP_LE_Generate_Non_Resolvable_Address function is provided to allow a means to write a random address to the Bluetooth device. The first parameter is the Bluetooth stack ID of the Bluetooth device. The second is the random address to write into the controller. This function will return zero on success, or a negative return error code if there was an error.

ResolveRemoteAddress

Description
The following function is responsible to determining that Remote Device address is resolvable private address or not. If it is resolvable address then it resolve this address.It takes parameter as address of remote device. This function returns zero on successful execution and a negative value on all errors.

Parameters
The only parameter required is the Bluetooth Address of the remote device. This can easily be found using the StartScanning command if the advertising device is in proximity during the scan.


Command Call Examples
“ResolveRemoteAddress 001bdc05b617” Attempts to resolve the random BD_ADDR of 001bdc05b617. “ResolveRemoteAddress 000275e126FF” Attempts to resolve the random BD_ADDR of 000275e126FF.

Possible Return Values
(0) Successfully Set Pairability Mode
(-1) BTPS_ERROR_INVALID_PARAMETER
(-4) FUNCTION_ERROR
(-6) INVALID_PARAMETERS_ERROR
(-8) INVALID_STACK_ID_ERROR
(-57) BTPS_ERROR_DEVICE_HCI_ERROR
(-103)BTPS_ERROR_FEATURE_NOT_AVAILABLE
API Calls
GAP_LE_Resolve_Address(BluetoothStackID,&IRK,BD_ADDR)

API Prototypes
Boolean_t BTPSAPI GAP_LE_Resolve_Address(unsigned int BluetoothStackID, Encryption_Key_t *IRK, BD_ADDR_t ResolvableAddress)

Description of API
The following function is provided to allow a means to attempt to resolve a resolvable random device address. The first parameter is the Bluetooth stack ID of the Bluetooth device. The second is the Identity Resolving Key (IRK) that will be used in attempting to resolve the resolvable address. The next is the BD_ADDR_t that contains the resolvable private address. This function returns a boolean result, (TRUE) if the resolvable address was resolved using the passed in IRK, FALSE if it was not.

ConnectLE

Description
The ConnectLE command is responsible for connecting to an LE device. This command returns zero if successful and a negative value if an error occurred. This command calls the ConnectLEDevice(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, Boolean_t UseWhiteList) function using ConnectLEDevice(BluetoothStackID, BD_ADDR, FALSE).

Parameters
The only parameter required is the Bluetooth Address of the remote device. This can easily be found using the StartScanning command if the advertising device is in proximity during the scan.

Note: The MSP430 version of this app requires two additional parameters which are the address type of the local and remote device. If the device uses a Public address then use 0, if it uses a Random Address then use 1.

Command Call Examples
“ConnectLE 001bdc05b617” Attempts to send a connection request to the Bluetooth Device with the BD_ADDR of 001bdc05b617. “ConnectLE 000275e126FF” Attempts to send a connection request to the Bluetooth Device with the BD_ADDR of 000275e126FF.

Possible Return Values
(0) Successfully Set Pairability Mode
(-4) FUNCTION_ERROR
(-6) INVALID_PARAMETERS_ERROR
(-8) INVALID_STACK_ID_ERROR
(-116) BTPS_ERROR_RANDOM_ADDRESS_IN_USE
(-111) BTPS_ERROR_CREATE_CONNECTION_OUTSTANDING
(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE
(-57) BTPS_ERROR_DEVICE_HCI_ERROR
GAP_LE_ERROR_WHITE_LIST_IN_USE

API Calls
GAP_LE_Create_Connection(BluetoothStackID, 100, 100, Result?fpNoFilter:fpWhiteList, latPublic, Result?&BD_ADDR:NULL, latPublic, &ConnectionParameters, GAP_LE_Event_Callback, 0);
(these two APIs can generally be ignored unless the WhiteList is enabled in the call to ConnectLEDevice)
GAP_LE_Remove_Device_From_White_List(BluetoothStackID, 1, &WhiteListEntry, &WhiteListChanged);
GAP_LE_Add_Device_To_White_List(BluetoothStackID, 1, &WhiteListEntry, &WhiteListChanged);

API Prototypes
int BTPSAPI GAP_LE_Create_Connection(unsigned int BluetoothStackID, unsigned int ScanInterval, unsigned int ScanWindow, GAP_LE_Filter_Policy_t InitatorFilterPolicy, GAP_LE_Address_Type_t RemoteAddressType, BD_ADDR_t *RemoteDevice, GAP_LE_Address_Type_t LocalAddressType, GAP_LE_Connection_Parameters_t *ConnectionParameters, GAP_LE_Event_Callback_t GAP_LE_Event_Callback, unsigned long CallbackParameter);
int BTPSAPI GAP_LE_Remove_Device_From_White_List( unsigned int BluetoothStackID, unsigned int DeviceCount, GAP_LE_White_List_Entry_t *WhiteListEntries, unsigned int *RemovedDeviceCount);
int BTPSAPI GAP_LE_Add_Device_To_White_List(unsigned int BluetoothStackID, unsigned int DeviceCount, GAP_LE_White_List_Entry_t *WhiteListEntries, unsigned int *AddedDeviceCount);

Description of API
The GAP_LE_Create_Connection function is provided to allow the local host the ability to create a connection to a remote device using the Bluetooth LE radio. The connection process is asynchronous in nature and the caller will be notified via the GAP LE event callback function (specified in this function) when the connection completes. This function will return zero if successful, or a negative return error code if there was an error condition. The GAP_LE_Remove_Device_From_White_List function is provided to allow the local host the ability to remove one (or more) devices from the white list maintained by the local device. This function will attempt to delete as many devices as possible (from the specified list) and will return the number of devices deleted. The GAP_LE_Read_White_List_Size function can be used to determine how many devices the local device supports in the white list (simultaneously). This function will return zero if successful, or a negative return error code if there was an error condition. The GAP_LE_Add_Device_To_White_List function is provided to allow the local host the ability to add one (or more) devices to the white list maintained by the local device. This function will attempt to add as many devices as possible (from the specified list) and will return the number of devices added. The GAP_LE_Read_White_List_Size function can be used to determine how many devices the local device supports in the white list (simultaneously). This function will return zero if successful, or a negative return error code if there was an error condition.



DisconnectLE

Description
The DisconnectLE command is responsible for disconnecting from an LE device. This command returns zero on successful execution and a negative value on all errors. This command requires that a valid Bluetooth Stack ID exists before running.

Parameters
This command required one parameter which is the Bluetooth Address of the (currently connected) remote device that is to be disconnected.

Possible Return Values
(0) Successfully disconnected remote device (-4) FUNCTION_ERROR (-8) INVALID_STACK_ID_ERROR

API Call
GAP_LE_Disconnect(BluetoothStackID, BD_ADDR);

API Prototype
int BTPSAPI GAP_LE_Disconnect(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR);

API Description
The GAP_LE_Disconnect function provides the ability to disconnect from a remote device. This function will return zero if successful, or a negative return error code if there was an error condition.



PairLE

Description
The PairLE command is provided to allow a mechanism of Pairing (or requesting security if a slave) to the connected device. This command calls the SendPairingRequest(BD_ADDR_t BD_ADDR, Boolean_t ConnectionMaster) function using SendPairingRequest(ConnectionBD_ADDR, LocalDeviceIsMaster).

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of Pairing.

Possible Return Values
(0) Successfully Set Pairability Mode
(-4) FUNCTION_ERROR
(-6) INVALID_PARAMETERS_ERROR
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE
(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES
(-107) BTPS_ERROR_INVALID_DEVICE_ROLE_MODE

API Calls
GAP_LE_Pair_Remote_Device(BluetoothStackID, BD_ADDR, &Capabilities, GAP_LE_Event_Callback, 0);
GAP_LE_Request_Security(BluetoothStackID, BD_ADDR, Capabilities.Bonding_Type, Capabilities.MITM, GAP_LE_Event_Callback, 0);

API Prototypes
int BTPSAPI GAP_LE_Pair_Remote_Device(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_LE_Pairing_Capabilities_t *Capabilities, GAP_LE_Event_Callback_t GAP_LE_Event_Callback, unsigned long CallbackParameter);
int BTPSAPI GAP_LE_Request_Security(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_LE_Bonding_Type_t Bonding_Type, Boolean_t MITM, GAP_LE_Event_Callback_t GAP_LE_Event_Callback, unsigned long CallbackParameter);

Description of API
The GAP_LE_Pair_Remote_Device function is provided to allow a means to pair with a remote, connected, device. This function accepts the device address of the currently connected device to pair with, followed by the pairing capabilities of the local device. This function also accepts as input the GAP LE event callback information to use during the pairing process. This function returns zero if successful or a negative error code if there was an error. This function can only be issued by the master of the connection (the initiator of the connection). The reason is that a slave can only request a security procedure, it cannot initiate a security procedure. The GAP_LE_Request_Security function is provided to allow a means for a slave device to request that the master (of the connection) perform a pairing operation or re-establishing prior security. This function can only be called by a slave device. The reason for this is that the slave can only request for security to be initiated, it cannot initiate the security process itself. This function returns zero if successful or a negative error code if there was an error.



LEPassKeyResponse

Description
The LEPassKeyResponse command is responsible for issuing a GAP Authentication Response with a Pass Key value specified via the input parameter. This command returns zero on successful execution and a negative value on all errors.

Parameters
The PassKeyResponse command requires one parameter which is the Pass Key used for authenticating the connection. This is a string value which can be up to 6 digits long (with a value between 0 and 999999).

Command Call Examples
"PassKeyResponse 1234" Attempts to set the Pass Key to "1234.” "PassKeyResponse 999999" Attempts to set the Pass Key to "999999." This value represents the longest Pass Key value of 6 digits.

Possible Return Values
(0) Successful Pass Key Response
(-4) FUNCTION_ERROR
(-6) INVALID_PARAMETERS_ERROR
(-8) INVALID_STACK_ID_ERROR
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-118) BTPS_ERROR_PAIRING_NOT_ACTIVE
(-57) BTPS_ERROR_DEVICE_HCI_ERROR
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE
(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES
(-107) BTPS_ERROR_INVALID_DEVICE_ROLE_MODE

API Call
GAP_LE_Authentication_Response(BluetoothStackID, CurrentRemoteBD_ADDR, &GAP_LE_Authentication_Response_Information);

API Prototype
int BTPSAPI GAP_LE_Authentication_Response(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_LE_Authentication_Response_Information_t *GAP_LE_Authentication_Information);

Description of API
This function is provided to allow a mechanism for the local device to respond to GAP LE authentication events. This function is used to specify the authentication information for the specified Bluetooth device. This function accepts as input, the Bluetooth protocol stack ID of the Bluetooth device that has requested the authentication action, and the authentication response information (specified by the caller).



QueryEncryptionMode

Description
This command is responsible for querying the Encryption Mode of an LE Connection. This command returns zero on successful execution and a negative value on all errors.

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the Query.

Possible Return Values
(0) Successfully Queried Encryption Mode
(-4) FUNCTION_ERROR
(-8) INVALID_STACK_ID_ERROR
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE

API Call
GAP_LE_Query_Encryption_Mode(BluetoothStackID, ConnectionBD_ADDR, &GAP_Encryption_Mode);

API Prototype
int BTPSAPI GAP_LE_Query_Encryption_Mode(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_Encryption_Mode_t *GAP_Encryption_Mode);

Description of API
This function is provided to allow a means to query the current encryption mode for the LE connection that is specified.



SetPasskey

Description
This command is responsible setting a fixed pass key to be used for LE pairing. This command returns zero on successful execution and a negative value on all errors.
Note: SetPasskey Command works only when you are pairing.

Parameters
The SetPasskey command requires one parameter which is the Pass Key used for authenticating the connection. This is a string value which can be up to 6 digits long (with a value between 0 and 999999).

Command Call Examples
“SetPasskey 0” Attempts to remove the Passkey.
“SetPasskey 1 987654” Attempts to set the Passkey to 987654.
“SetPasskey 1” Attempts to set the Passkey to the default Fixed Passkey value.

Possible Return Values
(0) Successful Pass Key Response
(-4) FUNCTION_ERROR
(-6) INVALID_PARAMETERS_ERROR
(-8) INVALID_STACK_ID_ERROR
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE

API Calls
(Depending on the First Parameter one of these will be chosen)
GAP_LE_Set_Fixed_Passkey(BluetoothStackID, &Passkey);
GAP_LE_Set_Fixed_Passkey(BluetoothStackID, NULL);

API Prototype
int BTPSAPI GAP_LE_Set_Fixed_Passkey(unsigned int BluetoothStackID, DWord_t *Fixed_Display_Passkey);

Description of API
This function is provided to allow a means for a fixed passkey to be used whenever the local Bluetooth device is chosen to display a passkey during a pairing operation. This fixed passkey is only used when the local Bluetooth device is chosen to display the passkey, based on the remote I/O Capabilities and the local I/O capabilities.



LEUserConfirmationResponse

Description
The LEUserConfirmationResponse command is responsible for issuing a GAP LE Authentication Response with a User Confirmation value specified via the input parameter. This function returns zero on successful execution and a negative value on all errors.

Parameters
This command requires one parameter which indicates if confirmation is accepted or not. 0 = decline, 1 = accept.

Command Call Examples
“LEUserConfirmationResponse 0” Attempts to Response with a decline value.
“LEUserConfirmationResponse 1” Attempts to Response with a accept value.


Possible Return Values
(0) Success.
(-4) FUNCTION_ERROR.
(-6) INVALID_PARAMETERS_ERROR.
(-1) BTPS_ERROR_INVALID_PARAMETER.
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID.
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED.
(-57) BTPS_ERROR_DEVICE_HCI_ERROR.
(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES.
(-98) BTPS_ERROR_DEVICE_NOT_CONNECTED.
(-103) BTPS_ERROR_FEATURE_NOT_AVAILABLE.
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE.
(-107) BTPS_ERROR_INVALID_DEVICE_ROLE_MODE.
(-118) BTPS_ERROR_PAIRING_NOT_ACTIVE.
(-119) BTPS_ERROR_INVALID_STATE.
(-120) BTPS_ERROR_FEATURE_NOT_CURRENTLY_ACTIVE.
(-122) BTPS_ERROR_NUMERIC_COMPARISON_FAILED.


API Call
GAP_LE_Authentication_Response(BluetoothStackID, CurrentLERemoteBD_ADDR, &GAP_LE_Authentication_Response_Information)

API Prototype
int BTPSAPI GAP_LE_Authentication_Response(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_LE_Authentication_Response_Information_t *GAP_LE_Authentication_Information)

Description of API
The following function is provided to allow a mechanism for the local device to respond to GAP LE authentication events. This function is used to set the authentication information for the specified Bluetooth device. This function accepts as input, the Bluetooth protocol stack ID followed by the remote Bluetooth device address that is currently executing a pairing/authentication process, followed by the authentication response information.This function returns zero if successful, or a negative return error code if there was an error.


EnableSCOnly

Description
The EnableSCOnly command enables LE Secure Connections (SC) only mode. In case this mode is enabled, pairing request from peers that support legacy pairing only will be rejected. Please note that in case this mode is enabled, the SC flag in the LE_Parameters must be set to TRUE. This function returns zero on successful execution and a negative value on all errors.

Parameters
This command requires one parameter which indicates if Secure connections only mode is set or not. 0 = SC Only mode is off, 1 = SC Only mode is on.

Command Call Examples
“EnableSCOnly 0” Disable Secure connections only mode.
“EnableSCOnly 1” Enable Secure connections only mode.


Possible Return Values
(0) Success.
(-4) FUNCTION_ERROR.
(-6) INVALID_PARAMETERS_ERROR.
(-8) INVALID_STACK_ID_ERROR.
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID.
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED.
(-103) BTPS_ERROR_FEATURE_NOT_AVAILABLE.
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE.
(-120) BTPS_ERROR_FEATURE_NOT_CURRENTLY_ACTIVE.

API Call
GAP_LE_SC_Only_Mode(BluetoothStackID, EnableSCOnly)

API Prototype
int BTPSAPI GAP_LE_SC_Only_Mode(unsigned int BluetoothStackID, Boolean_t EnableSCOnly)

Description of API
The following function is provided to allow a configuration of LE Secure Connecions only mode. The upper layer will use this function before the beginning of LE SC pairing, in case it asks to reject a device that supports only legacy pairing. This mode should be used when it is more important for a device to have high security than it is for it to maintain backwards compatibility with devices that do not support SC. This function accepts as parameters the Bluetooth stack ID of the Bluetooth device,and a boolean EnableSCOnly that enable or disable the SC only mode. This function should be used ones, before the first pairing process. This function returns zero if successful or a negative error code.



RegenerateP256LocalKeys

Description
The following function allows the user to generate new P256 private and local keys. This function shall NOT be used in the middle of a pairing process. It is relevant for LE Secure Conenctions pairing only! This function returns zero on successful execution and a negative value on all errors.

Parameters
No parameters are necessary.

Command Call Examples
“RegenerateP256LocalKeys” Attempts to generate new P256 private and local keys.


Possible Return Values
(0) Success.

(-4) FUNCTION_ERROR.
(-8) INVALID_STACK_ID_ERROR.
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID.
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED.
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE.
(-117) BTPS_ERROR_PAIRING_ACTIVE.
(-120) BTPS_ERROR_FEATURE_NOT_CURRENTLY_ACTIVE.

API Call
GAP_LE_SC_Regenerate_P256_Local_Keys(BluetoothStackID)

API Prototype
int BTPSAPI GAP_LE_SC_Regenerate_P256_Local_Keys(unsigned int BluetoothStackID)

Description of API
The following function is provided to allow a regeneration of the P-256 private and local puclic keys. This function is relevant only in case of LE SC pairing. This function accepts as parameters the Bluetooth stack ID of the Bluetooth device. This functions shall NOT be used while performing pairing. This function returns zero if successful or a negative error code.


SCGenerateOOBLocalParams

Description
In order to be able to perform LE SC pairing in OOB method we need to generate local random and confirmation values before the pairing process starts. The following function allows the user to generate OOB local parameters. This function shall NOT be used in the middle of a pairing process. It is relevant for LE SC pairing only! This function returns zero on successful execution and a negative value on all errors.

Parameters
No parameters are necessary.

Command Call Examples
“SCGenerateOOBLocalParams” Attempts to generate local random and confirmation values before the pairing process starts.


Possible Return Values
(0) Success.

(-4) FUNCTION_ERROR.
(-8) INVALID_STACK_ID_ERROR.
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID.
(-56) BTPS_ERROR_GAP_NOT_INITIALIZED.
(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE.
(-117) BTPS_ERROR_PAIRING_ACTIVE.
(-120) BTPS_ERROR_FEATURE_NOT_CURRENTLY_ACTIVE.

API Call
GAP_LE_SC_OOB_Generate_Parameters(BluetoothStackID, &OOBLocalRandom, &OOBLocalConfirmation)

API Prototype
int BTPSAPI GAP_LE_SC_OOB_Generate_Parameters(unsigned int BluetoothStackID, SM_Random_Value_t *OOB_Local_Rand_Result, SM_Confirm_Value_t *OOB_Local_Confirm_Result)

Description of API
The following function is provided to allow the use of LE Secure Connections (SC) pairing in Out Of Band (OOB) association method. The upper layer will use this function to generate the the local OOB random value, and OOB confirmation value (ra/rb and Ca/Cb) as defined in the Bluetooth specification. This function accepts as parameters the Bluetooth stack ID of the Bluetooth device, and pointers to buffers that will recieve the generated local OOB random, and OOB confirmation values. This function returns zero if successful or a negative error code.



DiscoverGAPS

Description
The DiscoverGAPS command is provided to allow an easy mechanism to start a service discovery procedure to discover the Generic Access Profile Service on the connected remote device.

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the service discovery.

Possible Return Values
(0) Successfully discovered the Generic Access Profile Service.
(-4) Function Error (on failure).

API Call
GDIS_Service_Discovery_Start(BluetoothStackID, ConnectionID, (sizeof(UUID)/sizeof(GATT_UUID_t)), UUID, GDIS_Event_Callback, sdGAPS)

API Prototypes
int BTPSAPI GDIS_Service_Discovery_Start(unsigned int BluetoothStackID, unsigned int ConnectionID, unsigned int NumberOfUUID, GATT_UUID_t *UUIDList, GDIS_Event_Callback_t ServiceDiscoveryCallback, unsigned long ServiceDiscoveryCallbackParameter)

Description of API
The GDIS_Service_Discover_Start is in an application module called GDIS that is provided to allow an easy way to perform GATT service discovery. This module can and should be modified for the customers use. This function is called to start a service discovery operation by the GDIS module.



GetLocalName

Description
The GetLocalName command is responsible for querying the name of the local Bluetooth Device. This command returns zero on a successful execution and a negative value on all errors. A Bluetooth Stack ID must exist before attempting to call this command.

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the Query.

Possible Return Values
(0) Successfully Queried Local Device Name
(-8) INVALID_STACK_ID_ERROR
(-4) FUNCTION_ERROR
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-57) BTPS_ERROR_DEVICE_HCI_ERROR
(-65) BTPS_ERROR_INSUFFICIENT_BUFFER_SPACE

API Call
GAP_Query_Local_Device_Name(BluetoothStackID, 257, (char *)LocalName);

API Prototype
int BTPSAPI GAP_Query_Local_Device_Name(unsigned int BluetoothStackID, unsigned int NameBufferLength, char *NameBuffer);

Description of API
This function is responsible for querying (and reporting) the user friendly name of the local Bluetooth device. The final parameters to this function specify the buffer and buffer length of the buffer that is to receive the local device name. The NameBufferLength parameter should be at least (MAX_NAME_LENGTH+1) to hold the maximum allowable device name (plus a single character to hold the NULL terminator). If this function is successful, this function returns zero, and the buffer that NameBuffer points to will be filled with a NULL terminated ASCII representation of the local device name. If this function returns a negative value, then the local device name was NOT able to be queried (error condition).



SetLocalName

Description
The SetLocalName command is responsible for setting the name of the local Bluetooth Device to a specified name. This command returns zero on a successful execution and a negative value on all errors. A Bluetooth Stack ID must exist before attempting to call this command.

Parameters
One parameter is necessary for this command. The specified device name must be the only parameter (which means there should not be spaces in the name or only the first section of the name will be set).

Command Call Examples
"SetLocalName New_Bluetooth_Device_Name" Attempts to set the Local Device Name to "New_Bluetooth_Device_Name." "SetLocalName New Bluetooth Device Name" Attempts to set the Local Device Name to "New Bluetooth Device Name" but only sets the first parameter, which would make the Local Device Name "New." "SetLocalName MSP430" Attempts to set the Local Device Name to "MSP430."

Possible Return Values
(0) Successfully Set Local Device Name
(-1) BTPS_ERROR_INVALID_PARAMETER
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-8) INVALID_STACK_ID_ERROR
(-4) FUNCTION_ERROR
(-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Call
GAP_Set_Local_Device_Name(BluetoothStackID, TempParam->Params[0].strParam);

API Prototype
int BTPSAPI GAP_Set_Local_Device_Name(unsigned int BluetoothStackID, char *Name);

Description of API
This function is provided to allow the changing of the device name of the local Bluetooth device. The Name parameter must be a pointer to a NULL terminated ASCII string of at most MAX_NAME_LENGTH (not counting the trailing NULL terminator). This function will return zero if the local device name was successfully changed, or a negative return error code if there was an error condition.



GetRemoteName

Description
The GetRemoteName command is responsible for querying the Bluetooth Device Name of a Remote Device. This command returns zero on a successful execution and a negative value on all errors. The command requires that a valid Bluetooth Stack ID exists before running and it should be called after using the Inquiry command. The DisplayInquiryList command would be useful in this situation to find which Remote Device goes with which Inquiry Index.

Parameters
The GetRemoteName command requires one parameter which is the Inquiry Index of the Remote Bluetooth Device. This value can be found after an Inquiry or displayed when the command DisplayInquiryList is used. Command Call Examples "GetRemoteName 5" Attempts to query the Device Name for the Remote Device that is at the fifth Inquiry Index. "GetRemoteName 8" Attempts to query the Device Name for the Remote Device that is at the eighth Inquiry Index.

Possible Return Values
(0) Successfully Queried Remote Name
(-6) INVALID_PARAMETERS_ERROR
(-4) FUNCTION_ERROR
(-8) INVALID_STACK_ID_ERROR
(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1) BTPS_ERROR_INVALID_PARAMETER
(-59) BTPS_ERROR_ADDING_CALLBACK_INFORMATION
(-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Call
GAP_Query_Remote_Device_Name(BluetoothStackID, InquiryResultList[(TempParam->Params[0].intParam – 1)], GAP_Event_Callback, (unsigned long)0);

API Prototype
int BTPSAPI GAP_Query_Remote_Device_Name(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_Event_Callback_t GAP_Event_Callback, unsigned long CallbackParameter);

Description of API
This function is provided to allow a mechanism to query the user-friendly Bluetooth device name of the specified remote Bluetooth device. This function accepts as input the Bluetooth device address of the remote Bluetooth device to query the name of and the GAP event callback information that is to be used when the remote device name process has completed. This function returns zero if successful, or a negative return error code if the remote name request was unable to be submitted. If this function returns success, then the caller will be notified via the specified callback when the remote name information has been determined (or there was an error). This function cannot be used to determine the user-friendly name of the local Bluetooth device. The GAP_Query_Local_Name function should be used to query the user-friendly name of the local Bluetooth device. Because this function is asynchronous in nature (specifying a remote device address), this function will notify the caller of the result via the specified callback. The caller is free to cancel the remote name request at any time by issuing the GAP_Cancel_Query_Remote_Name function and specifying the Bluetooth device address of the Bluetooth device that was specified in the original call to this function. It should be noted that when the callback is cancelled, the operation is attempted to be cancelled and the callback is cancelled (i.e. the GAP module still might perform the remote name request, but no callback is ever issued).



SetLocalAppearence

Description
The SetLocalAppearence command is provided to set the local device appearance that is exposed by the GAP Service (GAPS).

Parameters
The SetLocalAppearence command requires one parameter which is the Local Device Appearance you wish to be set.

Possible Return Values
(0) Success.
(-4) Function error (on failure).

API Call
GAPS_Set_Device_Appearance(BluetoothStackID, GAPSInstanceID, Appearance)

API Prototype
int BTPSAPI GAPS_Set_Device_Appearance(unsigned int BluetoothStackID, unsigned int InstanceID, Word_t DeviceAppearance);

Description of API
This function allows a mechanism of setting the local device appearance that is exposed as part of the GAP Service API (GAPS).



GetLocalAppearence

Description
The GetLocalAppearence command is provided to read the local device appearance that is exposed by the GAP Service (GAPS).

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome.

Possible Return Values
(0) Success.
(-4) Function error (on failure).

API Call
GAPS_Query_Device_Appearance(BluetoothStackID, GAPSInstanceID, &Appearance)

API Prototype
int BTPSAPI GAPS_Query_Device_Appearance(unsigned int BluetoothStackID, unsigned int InstanceID, Word_t *DeviceAppearance)

Description of API
This function allows a mechanism of reading the local device appearance that is exposed as part of the GAP Service API (GAPS).



GetRemoteAppearence

Description
The GetRemoteAppearence command is provided to read the device appearance from the connected remote device that is exposed as part of the GAP Service. The GAP Service on the remote device must have already been discovered using the DiscoverGAPS command.

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome

Possible Return Values
(0) Success.
(-4) Function error (on failure).

API Call
GATT_Read_Value_Request(BluetoothStackID, ConnectionID, DeviceInfo->GAPSClientInfo.DeviceAppearanceHandle, GATT_ClientEventCallback_GAPS, (unsigned long)DeviceInfo->GAPSClientInfo.DeviceAppearanceHandle)

API Prototype
int BTPSAPI GATT_Read_Value_Request(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t AttributeHandle, GATT_Client_Event_Callback_t ClientEventCallback, unsigned long CallbackParameter)

Description of API
This function allows a mechanism of reading an attribute from a connected device.

GetMTU

Description
The following function is responsible for reading the current MTU from the specified connection. This function will return zero on successful execution and a negative value on errors.

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the function.

Possible Return Values
(0) Successfully started the LE Scan Procedure
(-1) Bluetooth Stack ID is Invalid during the StartScan() call
(-4) FUNCTION_ERROR
(-8) INVALID_STACK_ID_ERROR
(-1000)BTGATT_ERROR_INVALID_PARAMETER
(-1009)BTGATT_ERROR_INVALID_CONNECTION_ID

API Call
GATT_Query_Connection_MTU(BluetoothStackID, ConnectionID, &RequestedMTU);

API Prototype
int BTPSAPI GATT_Query_Connection_MTU(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t *MTU)

Description of API
The following function is responsible for querying the current MTU of the specified connection. This function accepts the Bluetooth Stack ID of the Bluetooth Stack, the Connection ID of the connection to query the MTU for, and a pointer to store the Connection MTU into. This function will return zero if successful, or a negative return error code if there was an error.

SetMTU

Description
The following function is responsible for setting the current MTU from the specified connection. This function will return zero on successful execution and a negative value on errors.

Parameters
This function requires only one parameter which is the MTU that needs to be set.

Command Call Examples SetMTU 50 sets the MTU to 50 for the current connection. Possible Return Values
(0) Successfully started the LE Scan Procedure
(-1) Bluetooth Stack ID is Invalid during the StartScan() call
(-4) FUNCTION_ERROR
(-103)BTPS_ERROR_FEATURE_NOT_AVAILABLE
(-8) INVALID_STACK_ID_ERROR
(-1000)BTGATT_ERROR_INVALID_PARAMETER
(-1009)BTGATT_ERROR_INVALID_CONNECTION_ID

API Call
GATT_Exchange_MTU_Request(BluetoothStackID, ConnectionID, RequestedMTU, GATT_ClientEventCallback_LLS, 0)

API Prototype
int BTPSAPI GATT_Query_Connection_MTU(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t *MTU)

Description of API
The following function is provided to allow a means of requesting a change of the Connection MTU used with a remote GATT Server. This function accepts as parameters the Bluetooth stack ID of the local Bluetooth stack, followed by the connection ID of the connected device, followed by the requested MTU. The final two parameters specify the GATT Client event callback function and callback parameter (respectively) that will be called when a response is received from the remote device. This function will return the positive, non-zero, Transaction ID of the request or a negative error code.

  • NOTE * The etGATT_Client_Exchange_MTU_Response event will signal when a response is received from the remote GATT Server. The new MTU will be the smaller of the RequestedMTU specified in this function, and the MTU received in the etGATT_Client_Exchange_MTU_Response event.
  • NOTE * If successful the return value will contain the Transaction ID that can be used to cancel the request.
  • NOTE * This function is only valid for LE connections.



Alert Notification Profile Commands



RegisterLLS

Description
This function is responsible for registering a LLS Service. This function will return zero on successful execution and a negative value on errors.

Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.

Possible Return Values
(0) Successfully registered PASP Service
(-4) FUNCTION_ERROR
(-1000)LLS_ERROR_INVALID_PARAMETER
(-1002)LLS_ERROR_INSUFFICIENT_RESOURCES
(-1003)LLS_ERROR_SERVICE_ALREADY_REGISTERED

API Call
LLS_Initialize_Service(BluetoothStackID, PASS_EventCallback, NULL, &PASSInstanceID)

API Prototype
int BTPSAPI LLS_Initialize_Service(unsigned int BluetoothStackID, LLS_Event_Callback_t EventCallback, unsigned long CallbackParameter, unsigned int *ServiceID)

Description of API
The following function is responsible for opening a LLS Server. The first parameter is the Bluetooth Stack ID on which to open the Server. The second parameter is the Callback function to call when an event occurs on this Server Port. The third parameter is a user-defined callback parameter that will be passed to the callback function with each event. The final parameter is a pointer to store the GATT Service ID of the registered LLS service. This can be used to include the service registered by this call. This function returns the positive, non-zero, Instance ID or a negative error code.




UnRegisterLLS

Description
This function is responsible for unregistering the Link Loss Service. This function will return zero on successful execution and a negative value on errors.
Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.
Possible Return Values
(0) Successfully registered PASP Service
(-4) FUNCTION_ERROR
(-1000)LLS_ERROR_INVALID_PARAMETER
(-1004)LLS_ERROR_INVALID_INSTANCE_ID
API Call
LLS_Cleanup_Service(BluetoothStackID, LLSInstanceID)
API Prototype
int BTPSAPI LLS_Cleanup_Service(unsigned int BluetoothStackID, unsigned int InstanceID)
Description of API
The following function is responsible for closing a previously LLS Server. The first parameter is the Bluetooth Stack ID on which to close the Server. The second parameter is the InstanceID that was returned from a successful call to LLS_Initialize_Service(). This function returns a zero if successful or a negative return error code if an error occurs.


DiscoverLLS

Description
This function is responsible for performing a LLS Service Discovery Operation. This function will return zero on successful execution and a negative value on errors.
Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.
Possible Return Values
(0) GDIS_Service_Discovery_Start success
(-4) Function_Error
(-1000)GDIS_ERROR_INVALID_PARAMETER
(-1001)GDIS_ERROR_NOT_INITIALIZED
(-1002)GDIS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1003)GDIS_ERROR_INSUFFICIENT_RESOURCES
(-1009)GDIS_ERROR_SERVICE_DISCOVERY_OUTSTANDING


API Call
GATT_Start_Service_Discovery(BluetoothStackID, ConnectionID, (sizeof(UUID)/sizeof(GATT_UUID_t)), UUID, GATT_Service_Discovery_Event_Callback, sdLLS)
API Prototype
int BTPSAPI GDIS_Service_Discovery_Start(unsigned int BluetoothStackID, unsigned int ConnectionID, unsigned int NumberOfUUID, GATT_UUID_t *UUIDList, GDIS_Event_Callback_t ServiceDiscoveryCallback, unsigned long ServiceDiscoveryCallbackParameter)
Description of API
The following function is used to initiate the Service Discovery process or queue additional requests. The function takes as its first parameter the BluetoothStackID that is associated with the Bluetooth Device. The second parameter is the connection ID of the remote device that is to be searched. The third and fourth parameters specify an optional list of UUIDs to search for. The final two parameters define the Callback function and parameter to use when the service discovery is complete. The function returns zero on success and a negative return value if there was an error.





GetAlertLevel

Description
The following function is responsible for reading the Alert Level. It can be executed by a Server or as a Client with an open connection to a remote Server. If executed as a Client, a GATT read request will be generated, and the results will be returned as a response in the GATT Client event callback. This function will return zero on successful execution and a negative value on errors.
Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.
Possible Return Values
(0) Get Alert Level Request sent
(-4) FUNCTION_ERROR
(-1001) LLS_ERROR_INVALID_BLUETOOTH_STACK_ID (-1004) LLS_ERROR_INVALID_INSTANCE_ID
API Call
GATT_Read_Value_Request(BluetoothStackID, ConnectionID, DeviceInfo->LLS_ClientInfo.Alert_Level, GATT_ClientEventCallback_LLS, DeviceInfo->LLS_ClientInfo.Alert_Level)
API Prototype
int BTPSAPI GATT_Read_Value_Request(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t AttributeHandle, GATT_Client_Event_Callback_t ClientEventCallback, unsigned long CallbackParameter)
Description of API
The following function is provided to allow a means of performing a read request on a remote device for a specific attribute value. The first parameter is the Bluetooth stack ID of the local Bluetooth stack, followed by the connection ID of the connected remote device, followed by the attribute handle to read the value from. The final two parameters specify the GATT Client event callback function and callback parameter (respectively) that will be called when a response is received from the remote device. This function will return the positive, non-zero, Transaction ID of the request or a negative error code.

  • NOTE * If successful the return value will contain the Transaction ID that can be used to cancel the request.




SetAlertLevel

Description
The following function is responsible for writing the Alert Level. It can be executed by a Server or as a Client with an open connection to a remote Server if Client write access is supported. If executed as a Client, a GATT write request will be generated and the results will be returned as a response in the GATT Client event callback. This function will return zero on successful execution and a negative value on errors.
Parameters
SetAlertLevel has only one parameter which is an integer value that represents a Alert Level. This value is 0 = No Alert, 1 = Mild Alert, 2 = High Alert
Possible Return Values
(0) Ringer Setting successfully set
(-4) FUNCTION_ERROR
(-1000)LLS_ERROR_INVALID_PARAMETER
(-1001) LLS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1004)LLS_ERROR_INVALID_INSTANCE_ID
API Call
GATT_Write_Request(BluetoothStackID, ConnectionID, DeviceInfo->LLS_ClientInfo.Alert_Level, sizeof(NonAlignedByte_t), (void *)&Data, GATT_ClientEventCallback_LLS, DeviceInfo->LLS_ClientInfo.Alert_Level)
API Prototype
int BTPSAPI GATT_Write_Request(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t AttributeHandle, Word_t AttributeLength, void *AttributeValue, GATT_Client_Event_Callback_t ClientEventCallback, unsigned long CallbackParameter)
Description of API
The following function is provided to allow a means of performing a write request to a remote device for a specified attribute. The first parameter to this function is the Bluetooth stack ID of the local Bluetooth stack, followed by the connection ID of the connected remote device, followed by the handle of the attribute to write the value of, followed by the length of the value (in bytes), followed by the the actual value data to write. The final two parameters specify the GATT Client event callback function and callback parameter (respectively) that will be called when a response is received from the remote device. This function will return the positive, non-zero, Transaction ID of the request or a negative error code.

  • NOTE * This function will not write an attribute value with a length greater than the current MTU - 3. To write a longer attribute value use the GATT_Prepare_Write_Request() function instead.
  • NOTE * This function may write less than the number of requested bytes. This can happen if the number of bytes to write is less than what can fit in the MTU for the specified connection. The data in the etGATT_Client_Write_Response, that is dispatched if the remote device accepts the request, indicates the number of bytes that were written to the remote device.
  • NOTE * If successful the return value will contain the Transaction ID that can be used to cancel the request.

RegisterIAS

Description
This function is responsible for registering the Immediate Alert Service. This function will return zero on successful execution and a negative value on errors.
Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.
Possible Return Values
0) Successfully registered PASP Service
(-4) FUNCTION_ERROR
(-1000)IAS_ERROR_INVALID_PARAMETER
(-1002)IAS_ERROR_INSUFFICIENT_RESOURCES
(-1003)IAS_ERROR_SERVICE_ALREADY_REGISTERED

API Call
IAS_Initialize_Service(BluetoothStackID,IAS_EventCallback,0,&IASInstanceID)
API Prototype
int BTPSAPI IAS_Initialize_Service(unsigned int BluetoothStackID, IAS_Event_Callback_t EventCallback, unsigned long CallbackParameter, unsigned int *ServiceID)
Description of API
The following function is responsible for opening a IAS Server. The first parameter is the Bluetooth Stack ID on which to open the Server. The second parameter is the Callback function to call when an event occurs on this Server Port. The third parameter is a user-defined callback parameter that will be passed to the callback function with each event. The final parameter is a pointer to store the GATT Service ID of the registered IAS service. This can be used to include the service registered by this call. This function returns the positive, non-zero, Instance ID or a negative error code.

  • NOTE Only 1 IAS may be open at a time, per Bluetooth Stack ID.
  • NOTE All Client Requests will be dispatch to the EventCallback function that is specified by the second parameter to this function.



UnRegisterIAS

Description
This function is responsible for unregistering the Immediate Alert Service. This function will return zero on successful execution and a negative value on errors.
Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.
Possible Return Values
(0) Successfully registered PASP Service
(-4) FUNCTION_ERROR
(-1000)IAS_ERROR_INVALID_PARAMETER
(-1004)IAS_ERROR_INVALID_INSTANCE_ID
API Call
IAS_Cleanup_Service(BluetoothStackID, IASInstanceID)
API Prototype
int BTPSAPI IAS_Cleanup_Service(unsigned int BluetoothStackID, unsigned int InstanceID)
Description of API
The following function is responsible for closing a previously IAS Server. The first parameter is the Bluetooth Stack ID on which to close the Server. The second parameter is the InstanceID that was returned from a successful call to IAS_Initialize_Service(). This function returns a zero if successful or a negative return error code if an error occurs.

DiscoverIAS

Description
This function is responsible for performing an IAS Service Discovery Operation. This function will return zero on successful execution and a negative value on errors.
Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.
Possible Return Values
(0) GDIS_Service_Discovery_Start success
(-4) Function_Error
(-1000)GDIS_ERROR_INVALID_PARAMETER
(-1001)GDIS_ERROR_NOT_INITIALIZED
(-1002)GDIS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1003)GDIS_ERROR_INSUFFICIENT_RESOURCES
(-1009)GDIS_ERROR_SERVICE_DISCOVERY_OUTSTANDING


API Call
GATT_Start_Service_Discovery(BluetoothStackID, ConnectionID, (sizeof(UUID)/sizeof(GATT_UUID_t)), UUID, GATT_Service_Discovery_Event_Callback, sdIAS)
API Prototype
int BTPSAPI GDIS_Service_Discovery_Start(unsigned int BluetoothStackID, unsigned int ConnectionID, unsigned int NumberOfUUID, GATT_UUID_t *UUIDList, GDIS_Event_Callback_t ServiceDiscoveryCallback, unsigned long ServiceDiscoveryCallbackParameter)
Description of API
The following function is used to initiate the Service Discovery process or queue additional requests. The function takes as its first parameter the BluetoothStackID that is associated with the Bluetooth Device. The second parameter is the connection ID of the remote device that is to be searched. The third and fourth parameters specify an optional list of UUIDs to search for. The final two parameters define the Callback function and parameter to use when the service discovery is complete. The function returns zero on success and a negative return value if there was an error.




ConfigureAlertLevel

Description
The following function is responsible for writing the Alert Level Control Point to connected remote device. It can be executed only by a Client. This function will return zero on successful execution and a negative value on errors.
Parameters
SetRingerSetting has only one parameter which is an integer value that represents the Alert Level. This value is 0 = cpNoAlert, 1 = cpMildAlert, 2 = cpHighAlert.
Possible Return Values
(0) Ringer Setting successfully set
(-4) FUNCTION_ERROR
(-1000)IAS_ERROR_INVALID_PARAMETER
(-1003)IAS_ERROR_SERVICE_ALREADY_REGISTERED
(-1004)IAS_ERROR_INVALID_INSTANCE_ID
(-1005)IAS_ERROR_MALFORMATTED_DATA
API Call
GATT_Write_Without_Response_Request(BluetoothStackID, ConnectionID, DeviceInfo->IAS_ClientInfo.Control_Point, IAS_ALERT_LEVEL_CONTROL_POINT_VALUE_LENGTH, ((void *)Buffer))
API Prototype
int BTPSAPI GATT_Write_Without_Response_Request(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t AttributeHandle, Word_t AttributeLength, void *AttributeValue)
Description of API
The following function is provided to allow a means of performing a write without response request to remote device for a specified attribute. The first parameter to this function is the Bluetooth stack ID of the local Bluetooth stack, followed by the connection ID of the connected remote device, followed by the handle of the attribute to write, followed by the length of the value data to write (in bytes), followed by the actual value to write. This function will return the number of bytes written on success or a negative error code.

RegisterTPS

Description
This function is responsible for registering a TPS Service. This function will return zero on successful execution and a negative value on errors.
Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.


Possible Return Values
(0) Successfully registered PASP Service
(-4) FUNCTION_ERROR
(-1000)TPS_ERROR_INVALID_PARAMETER
(-1002)TPS_ERROR_INSUFFICIENT_RESOURCES
(-1003)TPS_ERROR_SERVICE_ALREADY_REGISTERED


API Call
TPS_Initialize_Service(BluetoothStackID, &TPSInstanceID)
API Prototype
int BTPSAPI TPS_Initialize_Service(unsigned int BluetoothStackID, unsigned int *ServiceID)
Description of API
The following function is responsible for opening a TPS Server. The first parameter is the Bluetooth Stack ID on which to open the Server. The second parameter is the Callback function to call when an event occurs on this Server Port. The third parameter is a user-defined callback parameter that will be passed to the callback function with each event. The final parameter is a pointer to store the GATT Service ID of the registered TPS service. This can be used to include the service registered by this call. This function returns the positive, non-zero, Instance ID or a negative error code.

UnRegisterTPS

Description
This function is responsible for unregistering a TPS Service. This function will return zero on successful execution and a negative value on errors.


Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.


Possible Return Values
(0) Successfully registered PASP Service
(-4) FUNCTION_ERROR
(-1000)LLS_ERROR_INVALID_PARAMETER
(-1004)LLS_ERROR_INVALID_INSTANCE_ID


API Call
TPS_Cleanup_Service(BluetoothStackID, TPSInstanceID)
API Prototype
int BTPSAPI TPS_Cleanup_Service(unsigned int BluetoothStackID, unsigned int InstanceID)
Description of API
The following function is responsible for closing a previously TPS Server. The first parameter is the Bluetooth Stack ID on which to close the Server. The second parameter is the InstanceID that was returned from a successful call to TPS_Initialize_Service(). This function returns a zero if successful or a negative return error code if an error occurs.



DiscoverTPS

Description
This function is responsible for performing a TPS Service Discovery Operation. This function will return zero on successful execution and a negative value on errors.
Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.
Possible Return Values
(0) GDIS_Service_Discovery_Start success
(-4) Function_Error
(-1000)GDIS_ERROR_INVALID_PARAMETER
(-1001)GDIS_ERROR_NOT_INITIALIZED
(-1002)GDIS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1003)GDIS_ERROR_INSUFFICIENT_RESOURCES
(-1009)GDIS_ERROR_SERVICE_DISCOVERY_OUTSTANDING


API Call
GATT_Start_Service_Discovery(BluetoothStackID, ConnectionID, (sizeof(UUID)/sizeof(GATT_UUID_t)), UUID, GATT_Service_Discovery_Event_Callback, sdTPS)
API Prototype
int BTPSAPI GDIS_Service_Discovery_Start(unsigned int BluetoothStackID, unsigned int ConnectionID, unsigned int NumberOfUUID, GATT_UUID_t *UUIDList, GDIS_Event_Callback_t ServiceDiscoveryCallback, unsigned long ServiceDiscoveryCallbackParameter)
Description of API
The following function is used to initiate the Service Discovery process or queue additional requests. The function takes as its first parameter the BluetoothStackID that is associated with the Bluetooth Device. The second parameter is the connection ID of the remote device that is to be searched. The third and fourth parameters specify an optional list of UUIDs to search for. The final two parameters define the Callback function and parameter to use when the service discovery is complete. The function returns zero on success and a negative return value if there was an error.





SetTxPowerLevel

Description
The following function is responsible for writing the Tx Power Level. It can be executed only by a Server. This function will return zero on successful execution and a negative value on errors.
Parameters
SetAlertLevel has only one parameter which is an integer value that represents a Tx Power Level.
Possible Return Values
(0) Ringer Setting successfully set
(-4) FUNCTION_ERROR
(-1000)TPS_ERROR_INVALID_PARAMETER
(-1001) TPS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1004)TPS_ERROR_INVALID_INSTANCE_ID

API Call
TPS_Set_Tx_Power_Level(BluetoothStackID, TPSInstanceID, (SByte_t)TempParam->Params[0].intParam)
API Prototype
int BTPSAPI TPS_Set_Tx_Power_Level(unsigned int BluetoothStackID, unsigned int InstanceID, SByte_t Tx_Power_Level)
Description of API
The following function is responsible for setting the Tx Power Level on the specified TPS Instance. The first parameter is the Bluetooth Stack ID of the Bluetooth Device. The second parameter is the InstanceID returned from a successful call to TPS_Initialize_Server(). The final parameter is the Tx Power Level to set for the specified TPS Instance. This function returns a zero if successful or a negative return error code if an error occurs.

GetTxPowerLevel

Description
The following command is responsible for reading the Tx Power Level. It can be executed by a Server or as a Client with an open connection to a remote Server. If executed as a Client, a GATT read request will be generated, and the results will be returned as a response in the GATT Client event callback. This function will return zero on successful execution and a negative value on errors.
Parameters
It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the command.
Possible Return Values
(0) Get Alert Level Request sent
(-4) FUNCTION_ERROR
(-1001) LLS_ERROR_INVALID_BLUETOOTH_STACK_ID
(-1004) LLS_ERROR_INVALID_INSTANCE_ID
API Call
GATT_Read_Value_Request(BluetoothStackID, ConnectionID, DeviceInfo->LLS_ClientInfo.Alert_Level, GATT_ClientEventCallback_LLS, DeviceInfo->LLS_ClientInfo.Alert_Level)


API Prototype
int BTPSAPI GATT_Read_Value_Request(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t AttributeHandle, GATT_Client_Event_Callback_t ClientEventCallback, unsigned long CallbackParameter)
Description of API
The following function is provided to allow a means of performing a read request on a remote device for a specific attribute value. The first parameter is the Bluetooth stack ID of the local Bluetooth stack, followed by the connection ID of the connected remote device, followed by the attribute handle to read the value from. The final two parameters specify the GATT Client event callback function and callback parameter (respectively) that will be called when a response is received from the remote device. This function will return the positive, non-zero, Transaction ID of the request or a negative error code.

  • NOTE If successful the return value will contain the Transaction ID that can be used to cancel the request.