CC2650 SensorTag User's Guide

From Texas Instruments Wiki
Jump to: navigation, search

Back to CC2650 SensorTag main wiki page.

IMPORTANT: When replacing the CR2032 coin cell battery please check the replacement battery temperature ratings and do not use the SensorTag outside of the battery manufacturer specified temperature range. The CC2650 SensorTag is not designed for use in outdoor or extreme environmental conditions, such as but not limited to condensation, moisture, shock, etc.

This wiki page refers to software available through BLE Stack 2.2, available for download here. Please visit the SensorTag portal where, under the "Teardown" tab, you can find smartphone application source code, design files (schematics, layout, BOM, etc.) and links to the sensor data sheets.

The CC2650 SensorTag evaluation kit operates as a Bluetooth low energy (BLE) peripheral slave device based on CC2650 multi-standard wireless MCU platform including five peripheral sensors with a complete software solution for sensor drivers interfaced to a GATT server running on TI BLE-Stack v2. The GATT server contains a primary service for each sensor for configuration and data collection.

New device

(this applies only to devices which have been pre-programmed with BLE 2.2 stack, SensorTag application firmware revision 1.30). On power up first time the application will copy itself onto the external flash as a 'factory reset image'. During the installation both LEDs will blink. When done the application enters normal operation, starts advertising indicated by the green LED blinking.


Power on

After inserting the battery the LEDs are used to indicate the status of the power on self test. If all sensors AND the external flash pass the self test the green LED will blink 5 times in rapid succession. If any of the tested units failed, the red LED will blink. After completing initialisation the green LED will blink every second as long as the device is advertising.


Operation

When disconnected

On start-up, the SensorTag advertises with a 100 millisecond interval indicated by the green LED blinking at a 1 Hz rate. Advertising can be stopped/started by pressing the power button (right). The SensorTag MUST be advertising for the device to be discoverable by a smart phone or any other Bluetooth Smart central device. The central device (e.g., smartphone) can only connect to a SensorTag that is advertising. In the advertising state the central device can:

  • Scan and discover the Sensor Tag. (Scan response contain name “CC2650 SensorTag”)
  • Establish connection based on user defined Connection Parameters

To conserve battery power, the SensorTag uses Limited Advertising and will advertise for approximately 2 minutes (120 sec) after pressing the power (right) button. When the SensorTag is not advertising or established in a BLE connection, the on board sensors are powered down into a low power state and not collecting sensor data.

When connected

The connection is established by a Central Device and the sensors can then be configured to provide measurement data. The Central Device could be any BLE compliant device and the main focus is on BLE compliant mobile phones, running either Android (4.3+) or iOS. When connected the central device can

  • Perform Service Discovery – Discover Characteristic by UUID
  • Operate as a GATT Client - Write to and read from Characteristic Value (configure sensors and read data)
  • Disconnect the device and return it to an advertising state (see 'When disconnected' above)

To obtain the data, the corresponding sensor must first be activated, which is done via a Characteristic Value write to appropriate service. The most power efficient way to obtain measurements for a sensor is to

  1. Enable notification
  2. Enable Sensor
  3. When notification with data is obtained at the Master side, disable the sensor (notification still on though)

Connecting to multiple SensorTags

The SensorTag is configured as a BT4.0 Peripheral device and can thus be connected to at most one Central device (e.g., Smartphone, CC2540USB dongle + BTool, etc.) at a time. A Central device may allow connections to multiple Peripheral devices, so if supported, a Central can connect to multiple SensorTags simultaneously. The multiple connection behavior is determined by the Central and may not be supported by the Central. Consult the documentation for your Central device to see if multiple connections are supported. Note that TI sample Smartphone applications do not support multiple simultaneous connections to SensorTags.

Use of buttons

In a connected state the buttons operated differently from when the device is disconnected. Short key presses has no special interpretation, the state of the buttons is simply fed to the Simple Key Service. There are however two key press sequences that are dealt with is a separate way

  • Power button pressed for three seconds: the SensorTag is disconnected
  • Both buttons pressed for six seconds: factory settings are restored, i.e. the BLE image programmed at the factory is loaded from external flash and executed. This operation is only recommended if you have are using a ZigBee image and want to return to BLE operation.

The LEDs are not used unless they are directly operated via the IO service.

Connecting to the SensorTag without a Smartphone

Since the SensorTag is a Bluetooth low energy accessory, any compliant Central (Master) device can connect to the SensorTag and view its sensor data. All that is required is for the Central device to implement the respective custom sensor service(s) which are documented in the following sections. Note that with Operating Systems that natively support Bluetooth low energy, such as Win8.1 & OSX, an application is required to access data from any custom services (e.g. TI Movement Service). The following is a list of some non-smartphone devices & applications that support reading SensorTag sensor data:


Sensors

The SensorTag has IoT connectivity support for the following sensors:

  • IR Temperature, both object and ambient temperature
  • Movement, 9 axis (accelerometer, gyroscope, magnetometer)
  • Humidity, both relative humidity and temperature
  • Barometer, both pressure and temperature
  • Optical, light intensity
Sensor Overview
Sensor Name Data size Manufacturer
IR Temperature TMP007 2 x 16bit Texas Instruments
Movement MPU9250 9 x 16 bit InvenSense
Humidity HDC1000 2 x 16bit Texas Instruments
Pressure BMP280 2 x 24bit Bosch
Optical OPT3001 1 x 16bit Texas Instruments

The SensorTag can be configured to send notifications for every sensor by writing 0x0001 to the characteristic configuration < GATT_CLIENT_CHAR_CFG_UUID> for the corresponding sensor data, the data is then sent as soon as the data has been updated. The sensors are enabled by writing 0x01 (NB: The movement sensor uses a bitmap to control individual axes) to the corresponding configuration characteristic and then disabled by writing 0x00. For regular data collection the SensorTag does not use any interrupt features provided by the sensors, but the movement sensor (MPU9250) uses interrupt for the wake-on-movement (shake detection).

The SensorTag uses I2C to interface to the sensors. The MPU9250 is assigned a separate I2C-bus (bus #1), and also also separately powered. Also note that the MPU9250 consists of two separate devices in the same package; the magnetometer has its own I2C address. The movement sensor has a WOM (Wake-On-Motion) feature that optionally may be used, so that movement data is only reported when the device is touched. When WOM is enabled the SensorTag reports movement data for 10 seconds after the device has detected a movement.

For infrequent measurements it is advisable not to use notifications at all, then simply

  1. Enable sensor
  2. Read data and verify
  3. Disable sensor

For the latter alternative please keep in mind that sensor take different amount of time to perform measurement. Depending on the connection interval (7.5 – 3200 ms) set by the Central Device, the time for achieving measurement data can vary. The individual sensors require varying delays to complete measurements. Recommended setting is 100 ms for fast movement data updates, if only the environmental data is of interest, the interval can be slower to increase battery life time. Selecting a sensor measurement period that is faster than the connection interval will result in unnecessary battery power consumption since sensor reading can only be sent at scheduled connection events. Notifications can be stopped and the sensors turned on/off. Note that when using iOS or Android the application has no direct control of the connection parameters. The SensorTag does however provide a Connection Control Service to circumvent this limitation.

Calibration

Since the SensorTag reference platform supplies the raw, uncalibrated sensor outputs to the IoT enabled BLE Client (e.g., Smart Device Application), it is up to the system designer to implement & perform the necessary calibration for the intended operating environment. Implementation may require cooperation with the specific sensor supplier(s). Specific calibration may be implemented directly in the CC2640 firmware and/or in the BLE Client. For example, to implement a precision movement sensor solution, e.g., a MPU9250 vibration detection algorithm, TI recommends connecting with the InvenSense Developers Corner.


Gatt Server

The GATT server contains several services and following are used:

  • GAP
  • GATT
  • Device Information
  • IR Temperature
  • Movement
  • Humidity
  • Barometer
  • Simple Keys
  • IO Service
  • Display
  • LED Light
  • Register Service
  • OAD Service
  • Connection Control Service

GAP, GATT, and Device Information Service conform with the official SIG profiles, whilst the other serves as examples of profile service implementation. The complete Attribute Table for the SensorTag can be found here . The sensor profile is a custom profile with 128 bit unique UUIDs. The profile enables a device that has a set of specific sensors to expose status and data measurements to another device. The profile also provides configuration interface to the individual sensors, each supporting a configuration characteristic (enable/disable) and a period characteristic.

The TI Base 128-bit UUID is: F0000000-0451-4000-B000-000000000000. All sensor services use 128-bit UUIDs, but for practical reasons only the 16-bit part is listed in this document. It is embedded in the 128-bit UUID as shown by example. Example: 0xAA01 maps as F000AA01-0451-4000-B000-000000000000. All UUIDs that are mapped to 128-bit values are marked *.

ANDROID Users: If you add, modify or remove a Service, these changes may not be reflected in your phone's application. Please see this E2E post for guidance on how to clear your phone's GATT cache.

Note: The GATT table can change for different firmware revisions, so it is important to do a proper characteristic discovery rather than hard-coding the attribute handles.

IR Temperature Sensor

The temperature sensor used on the SensorTag is Texas Instrument's TMP007. The IR Temperature sensor is implemented with the following source code file:
Application: sensortag_tmp.c
Driver: SensorTmp007.c
Profile: irtempservice.c

IR Temperature Sensor
Type UUID Access Size (bytes) Description
Data AA01* R/N 4 Object[0:7], Object[8:15], Ambience[0:7], Ambience[8:15]
Notification 2902 R/W 2 Write 0x0001 to enable notifications, 0x0000 to disable.
Configuration AA02* R/W 1 Write 0x01 to enable data collection, 0x00 to disable.
Period AA03* R/W 1 Resolution 10 ms. Range 300 ms (0x1E) to 2.55 sec (0xFF). Default 1 second (0x64)

Configuration

When an enable command (0x01) is written to the configuration characteristic, the sensor starts to perform measurements each second (average over four measurements) and the data is stored in the data characteristic. When the disable command (0x00) is issued, the sensor is put in stand-by mode and the no data are cleared and no longer reported.


Data

To obtain data either use notifications or read the data directly. The raw data value read from this sensor are two unsigned 16 bit values, one for die (ambience) temperature and one for object temperature. To convert to temperature in degrees (Celsius), use the algorithm below:

void sensorTmp007Convert(uint16_t rawAmbTemp, uint16_t rawObjTemp, float *tAmb, float *tObj)
{
  const float SCALE_LSB = 0.03125;
  float t;
  int it;
 
  it = (int)((rawObjTemp) >> 2);
  t = ((float)(it)) * SCALE_LSB;
  *tObj = t;
 
  it = (int)((rawAmbTemp) >> 2);
  t = (float)it;
  *tTgt = t * SCALE_LSB;
}


Movement Sensor

The movement sensor used on the SensorTag is MPU9250 from InvenSense. The movement sensor is implemented with the following source code files:
Application: sensortag_mov.c
Driver: SensorMpu9250.c
Profile: movementservice.c


Movement
Type UUID Access Size (bytes) Description
Data AA81* R/N 18 GyroX[0:7], GyroX[8:15], GyroY[0:7], GyroY[8:15], GyroZ[0:7], GyroZ[8:15], AccX[0:7], AccX[8:15], AccY[0:7], AccY[8:15], AccZ[0:7], AccZ[8:15], MagX[0:7], MagX[8:15], MagY[0:7], MagY[8:15], MagZ[0:7], MagZ[8:15]
Notification 2902 R/W 2 Write 0x0001 to enable notifications, 0x0000 to disable.
Configuration AA82* R/W 2 One bit for each gyro and accelerometer axis (6), magnetometer (1), wake-on-motion enable (1), accelerometer range (2). Write any bit combination top enable the desired features. Writing 0x0000 powers the unit off.
Period AA83* R/W 1 Resolution 10 ms. Range 100 ms (0x0A) to 2.55 sec (0xFF). Default 1 second (0x64).

Configuration

The configuration characteristic is used to decide which data (axis) should be activated, if wake-on-motion is to be enabled, and the range of the accelerometer (2, 4, 8 and 16 G).

Bits Usage
0 Gyroscope z axis enable
1 Gyroscope y axis enable
2 Gyroscope x axis enable
3 Accelerometer z axis enable
4 Accelerometer y axis enable
5 Accelerometer x axis enable
6 Magnetometer enable (all axes)
7 Wake-On-Motion Enable
8:9 Accelerometer range (0=2G, 1=4G, 2=8G, 3=16G)
10:15 Not used

The Wake-On-Motion (WOM) feature allows the MPU to operate with only the accelerometer enabled, but will give an interrupt to the CC2650 when motion is detected. After a shake is detected, the SensorTag will provide movement data for 10 seconds before entering the MPU re-enters low power WOM state.


Data

Note that this is raw data, the motion processing capabilities of the MPU9250 have not been invoked. The data consists of nine 16-bit signed values, one for each axis. The order in the data is Gyroscope, Accelerometer, Magnetomer.

Gyroscope raw data make up 0-5 of the data from the movement service, in the order X, Y, Z axis. Data from each axis consists of two bytes, encoded as a signed integer. For conversion from gyroscope raw data to degrees/second, use the algorithm below on each of the first three 16-bit values in the incoming data, one for each axis. Note that the axis data from a disabled axis will be 0, so the size of the incoming data is always 18 bytes. When the WOM feature is enabled, the latest measured data will be continuously transmitted.

float sensorMpu9250GyroConvert(int16_t data)
{
  //-- calculate rotation, unit deg/s, range -250, +250
  return (data * 1.0) / (65536 / 500);
}

Accelerometer raw data make up bytes 6-11 of the data from the movement service, in the order X, Y, Z axis. Data from each axis consists of two bytes, encoded as a signed integer. For conversion from accelerometer raw data to Gravity (G), use the algorithm below on each the three 16-bit values in the incoming data, one for each axis.

// Accelerometer ranges
#define ACC_RANGE_2G      0
#define ACC_RANGE_4G      1
#define ACC_RANGE_8G      2
#define ACC_RANGE_16G     3
 
float sensorMpu9250AccConvert(int16_t rawData)
{
  float v;
 
  switch (accRange)
  {
  case ACC_RANGE_2G:
    //-- calculate acceleration, unit G, range -2, +2
    v = (rawData * 1.0) / (32768/2);
    break;
 
  case ACC_RANGE_4G:
    //-- calculate acceleration, unit G, range -4, +4
    v = (rawData * 1.0) / (32768/4);
    break;
 
  case ACC_RANGE_8G:
    //-- calculate acceleration, unit G, range -8, +8
    v = (rawData * 1.0) / (32768/8);
    break;
 
  case ACC_RANGE_16G:
    //-- calculate acceleration, unit G, range -16, +16
    v = (rawData * 1.0) / (32768/16);
    break;
  }
 
  return v;
}

Magnetometer raw data make up bytes 7-12 of the data from the movement service, in the order X, Y, Z axis. Data from each axis consists of two bytes, encoded as a signed integer. The conversion is done in the SensorTag firmware so there is no calculation involved apart from changing the integer to a float if required. The measurement unit is uT (micro Tesla).

float sensorMpu9250MagConvert(int16_t data)
{
  //-- calculate magnetism, unit uT, range +-4900
  return 1.0 * data;
}


Humidity Sensor

The humidity sensor used on the SensorTag is HDC1000 from Texas Instruments. The humidity sensor is implemented with the following source code files:
Application: sensortag_hum.c
Driver: SensorHdc1000.c
Profile: humidityservice.c

Humidity Sensor
Type UUID Access Size (bytes) Description
Data AA21* R/N 4 Temp[0:7], Temp[8:15], Hum[0:7], Hum[8:15]
Notification 2902 R/W 2 Write 0x0001 to enable notifications, 0x0000 to disable.
Configuration AA22* R/W 1 Write 0x01 to enable data collection, 0x00 to disable.
Period AA23* R/W 1 Resolution 10 ms. Range 100 ms (0x0A) to 2.55 sec (0xFF). Default 1 second (0x64).

Configuration

When an enable command (0x01) is written to the configuration characteristic, the sensor starts to perform measurements each second and the data is stored in the data characteristic. When the disable command (0x00) is issued, the sensor's measurement cycle is stopped, the data are cleared and no longer reported.

Data

The data from the humidity sensor consists of two 16-bit unsigned integers: the temperature in bytes 0 and 1, and the pressure in bytes 2 and 3. Conversion to temperature and relative humidity is done as shown below. The temperature unit is degrees Celsius (°C), the humidity unit is relative humidity (%RH).

void sensorHdc1000Convert(uint16_t rawTemp, uint16_t rawHum,
                        float *temp, float *hum)
{
  //-- calculate temperature [°C]
  *temp = ((double)(int16_t)rawTemp / 65536)*165 - 40;
 
  //-- calculate relative humidity [%RH]
  *hum = ((double)rawHum / 65536)*100;
}


Barometric Pressure Sensor

The pressure sensor used on the SensorTag is BMP280 from Bosch Sensortec. The Barometric Pressure Sensor is implemented with the following source code files:
Application: sensortag_bar.c
Driver: SensorBmp280.c
Profile: barometerservice.c

Humidity Sensor
Type UUID Access Size (bytes) Description
Data AA41* R/N 6 Temp[0:7], Temp[8:15], Temp[16:23], Press[0:7], Press[8:15], Press[16:23]
Notification 2902 R/W 2 Write 0x0001 to enable notifications, 0x0000 to disable.
Configuration AA42* R/W 1 Write 0x01 to enable data collection, 0x00 to disable.
Period AA44* R/W 1 Resolution 10 ms. Range 100 ms (0x0A) to 2.55 sec (0xFF). Default 1 second (0x64).

Configuration

When an enable command (0x01) is written to the configuration characteristic, the sensor starts to perform measurements each second and the data is stored in the data characteristic. When the disable command (0x00) is issued, the sensor's measurement cycle is stopped, the data are cleared and no longer reported.

Data

The data from the pressure sensor consists of two 24-bit unsigned integers: the temperature in bytes 0-2, the pressure in bytes 3-5. The conversion and adjustment calculations is done in firmware, so the application in effect only has to divide the incoming values by 100. Conversion to temperature and pressure is done as shown below. The temperature unit is degrees Celsius, the pressure in hectopascal (hPa).

float calcBmp280(uint32_t rawValue)
{
  return rawValue / 100.0f;
}


Optical Sensor

The optical sensor used on the SensorTag is OPT3001 from Texas Instruments. The Optical Sensor is implemented with the following source code files:
Application: sensortag_opt.c
Driver: SensorOpt3001.c
Profile: opticservice.c


Optical Sensor
Type UUID Access Size (bytes) Description
Data AA71* R/N 2 LightLSB:LightMSB
Notification 2902 R/W 2 Write 0x0001 to enable notifications, 0x0000 to disable
Configuration AA72* R/W 1 Write 0x01 to enable data collection, 0x00 to disable.
Period AA73* R/W 1 Resolution 10 ms. Range 100 ms (0x0A) to 2.55 sec (0xFF). Default is 800 milliseconds (0x50).

Configuration

When an enable command (0x01) is written to the configuration characteristic, the sensor starts to perform measurements each 800 milliseconds and the data is stored in the data characteristic. When the disable command (0x00) is issued, the sensor's measurement cycle is stopped, the data are cleared and no longer reported.

Data

The data from the optical sensor consists of a single 16-bit unsigned integer. Conversion to light intensity (LUX) is shown below.

float sensorOpt3001Convert(uint16_t rawData)
{
  uint16_t e, m;
 
  m = rawData & 0x0FFF;
  e = (rawData & 0xF000) >> 12;
 
  return m * (0.01 * pow(2.0,e));
}


IO Service

The IO service is an interface to digital IO lines on the SensorTag and to the power on self test results. The IO's that can be controlled from this service are the two LEDs and the buzzer. The power on self test result is a bitmap of 7 bits, where each bit represents a sensor's passed/fail status. The IO Service is implemented with the following source code files:
Application: sensortag_io.c
Driver: PIN TI Driver
Profile: ioservice.c


IO Service
Type UUID Access Size (bytes) Description
Data AA65 * R/W 1 Depending on mode set in configuration characteristic.
Configuration AA66 * R/W 1 0: local mode, 1: remote mode, 2: test mode

Configuration

This service operate in three modes, defined by the setting of the configuration characteristic.

IO Service
Mode Name Description
0 Local In local mode the application itself controls the use of the LEDs. By default the green led blinks when advertising, and is also used at start-up to indicate a successful self test.

The red LED is used to indicate any error in the power on self test, under normal operation it is not used. The buzzer is not used by any built in functionality of the firmware.

1 Remote In remote mode the BLE host overrides the IO usage and can activate the LEDs and the buzzer directly.
2 Test In test mode the values of the power on self test can be read.

Reading the characteristic will always yield the value that was previously written to it. After connecting first time it will contain the power on self test result. Writing is permitted irrespective of mode, but will only take effect in remote mode.


Data

Power on self test

The self-test result is available in the data characteristic in test mode and always after start-up. It should always show the value 0x7F which indicates that all sensors are functioning. The Power on self test is implemented with the following source code files:
Application: SensorTagTest.c
Driver: Individual sensor drivers
Profile: Individual sensor profiles

Power on Self Test
Bit Number Description
0 IR temperature sensor
1 Humidity sensor
2 Optical sensor
3 Pressure sensor
4 MPU
5 Magnetometer
6 External Flash
7 Dev Pack


Activating IO

When configured in remote mode the BLE host has direct access to the LEDs and the buzzer through the data characteristic.

Power on Self Test
Bit Number Description
0 Red LED (LED1)
1 Green LED (LED2)
2 Buzzer
3 External flash erase

Note for controlling the Buzzer frequency in BLE-Stack V2.1: See this E2E Buzzer Update for updates to the buzzer driver.

The external flash of the SensorTag can be erased by writing bit '3'. During the process both LEDs will blink. Utmost care should be taken when erasing the external flash. The factory image will be lost so a the factory reset operation (simultaneous button press for 6 seconds) has no effect. If the current image is a factory image (v. 1.30, standard application) it will reinstall itself in the external flash on the next reset.


Simple Keys Service

The Simple Key service reports key and reed relay activity. The Simple Keys Service is implemented with the following source code files:
Application: sensortag_keys.c
Driver: PIN TI Driver
Profile: simplekeys.c

Simple Key Service
Type UUID Access Size (bytes) Description
Data FFE1 N 1 Bit 0: left key (user button), Bit 1: right key (power button), Bit 2: reed relay

It is a notification only service, read and write access is not permitted. Note that this service operates on key presses of a duration of less than 6 seconds.

Longer key presses always has the following effect:

  • Power button > 6 seconds: disconnect device
  • Both buttons > 6 seconds: restore factory settings, i.e. apply the flash image that was programmed at production


OAD Service

THIS OAD SERVICE IS DEPRECATED - For BLE 2.2+ Devices, see OAD Users Guide Included with SDK

This method using the baseloader is for versions < BLE 2.2.0 and has been deprecated.

The SensorTag supports over the air download (OAD) of new firmware images. This allows a peer device or OAD manager (which could be a central BT Smart device such as a smartphone) to push a new firmware image onto the SensorTag (OAD target) and update the firmware. The firmware is first downloaded do the SensorTag's external flash, when this operation has finished and verified (checksum), the new image is copied into the on-chip flash, the device is reset and start executing the new image.

OAD Service
Type UUID Access Size (bytes) Description
OAD Image Identify FFC1* W/N 1-16 (write), 8 (notification) Writing to this characteristic causes either an 8 byte "image identification" notifications to be sent back (about the current image), or an Image Block Request notification at OAD Image Block characteristic (if the new image passes the acceptance criteria).
OAD Image Block FFC2* W/N 18 (write), 2 (notification) Write (2 bytes block number, 16 bytes OAD image data), notification (2 bytes requested block number)

The OAD Image Identify characteristic is used to determine if the new image to be downloaded is accepted. If the image is accepted the OAD Image Block characteristic gets a Bock Request notification for block 0 and the OAD can start. For any OAD to start this operation must be done when initialising the OAD.

The OAD Image Block characteristic is used for the actual transfer of the image and can optionally be used for handshaking. Programming is done in 16 byte blocks written to the OAD Image Block characteristic, and these must be preceded by a two 'block ID' bytes. A block is a unit of 16 bytes.


OAD Execution

In order to start transfer, information about the new image has to be sent to the OAD server running in the SensorTag. The image information consists of 16 bytes of data that must be written to the OAD Image Block characteristic. The content of the image information (header) is as follows:

Byte no Description Value
0-1 CRC CRC16 calculated by client
2-3 CRC shadow Not used, set to 0xFFFF
4-5 Version Always '0 for SensorTag
6-7 Length Length of image in blocks (block size = 16 bytes)
8-11 User ID 'E','E', 'E', 'E' for SensorTag
12-13 Address Starts address of image in block units (block size = 16 bytes)
14 Image type Always '1' (application) for SensorTag
15 Reserved Not used, set to 0xFF

The CRC calculation is CRC16 with a polynomial of 0x1021. The CRC is calculated across the header (bytes 4-15) AND the entire image.


Connection Control Service

Connection Control Service
Type UUID Access Size (bytes) Description
Connection Parameters CCC1* R/N 6 connection interval, slave latency, supervision time-out (2 bytes each)
Request connection parameters CCC2* W 8 bytes write Max connection interval, min connection interval, slave latency, supervision time-out (2 bytes each)
Request disconnect CCC3* W 1 Change the value to disconnect.

This service is a work-around for limitations in the BLE stacks of iOs and Android. Those do not allow the mobile application to modify the connection parameters which in turn places severe limitations on OAD. On iOs the connection interval is not optimal for speedy OAD and on Android it is in some cases too long, and others so short the OAD fails due to flash access timing limitations. The optimal connection interval for OAD is around 15-25 ms which allows enough time for flash write to complete and is also short enough to not slow down the transfer unduly.

The connection parameters are changed by writing four values (8 bytes) to characteristic 0xCCC2. Characteristic 0xCCC1 will give a notification when the values have been updated. After this it is safe to start OAD.


Register Service

The Register Service provides a method for accessing registers of the individual sensors via the RF link. This can be useful for diagnostics purposes, particularly when optimising power consumption. The Register Service is implemented with the following source code files:
Application: sensortag_register.c
Driver: N/A
Profile: registerservice.c

Register Service
Type UUID Access Size (bytes) Description
Register Data AC01* R/W/N 1-4 Data to read or write to the register.
Register Address AC02* R/W 1-5 Byte 0: access size, typically 1 or 2 for an I2C sensor (max 16). Byte 1:4: register address (32 bits).
Register Device ID AC03* R/W 1-2 Byte 0: Interface ID. Byte 1: Device Address

Overview of interface IDs (byte 0 of Register Device ID characteristic)

Interface ID
Value Description
0 I2C bus 0 (humidity sensor, IR temperature sensor, pressure sensor, light sensor)
1 I2C bus 1 (movement sensor)
2 SPI
3 Not used
4 Not used
5 MCU
6 Not used
7 Not used


Device ID
Device ID (interface + address) Device Functionality
00:43 HDC1000 Humidity sensor
00:44 TMP007 IR temperature sensor
00:45 OPT3001 Light sensor
00:77 BMP280 Pressure sensor
01:0B Magnetometer MPU9250
01:68 MPU9250 Gyroscope/Accelerometer
05 MCU CC2650

Accessing I2C devices

  • Select the bus/device (characteristic Register Device ID)
  • Select internal device address (characteristic Register Device Address)
  • Read or write data from/to the selected register (characteristic Register Data)

I2C Examples

Reading OPT3001 "manufacturer ID" register
  • Write 00:45 to Register Device ID (this selects I2C bus 0 and Optical sensor)
  • Write 02:7E to Register Device Address (this selected OPT3001 register "Manufacturer ID", access length 2)
  • Read from Register Data - this should yield the result 54:49 (The manufacturer ID of Texas Instruments)


Reading MPU9250 "Power Management 2" register
  • Start data collection magnetometer enabled and Wake On Motion disabled
  • Write 01:68 to Register Device ID (this selects I2C bus 1 and Movement sensor)
  • Write 01:6C to Register Device Address (this selected MPU9250 register "Power Management 2", access length 1)
  • Read from Register Data - this should yield the 0x3F (all axes disabled)
  • Enable Acceleromter
  • Read from Register Data - this should yield the 0x07 (Accelerometer enabled)

NB! Do not access the MPU9250 unless either magnetometer, gyroscope or accelerometer are producing data. The MPU9250 is powered off when all the axes are disabled.


Accessing MCU address space

The register service can also be used to access the MCU address space, for instance to set/clear an LED. The MCU access feature is intended for accessing GPIO to observe the power consumption effects of the state of the GPIO. NB! It is strongly discouraged to use it for anything else (RAM access etc.) unless you know exactly what you are doing...


GPIO examples

Read GPIO

This small tutorial demonstrates how the register service can be used to observe the status of GPIO inputs, using the two buttons and the reed relay to change the GPIO values.

  • Write 05:00 to Register Device ID (this selects MCU address space)
  • Write 1:C0:20:02:40 (0x400220C0) to Register Device Address. This selects the GPIO data input register bits 0:7, access length 1
  • The read value is expected to be 0x73
  • Enabled notifications on the Register Data' characteristic
  • Press the User Button and observe that the value changes to 0x72 when pressed and reverts to 0x73 when released
  • Press the Power Button and observe that the value changes to 0x63 when pressed and reverts to 0x73 when released
  • Apply a magnet next to the Power Button' and observe that the value changes to 0x7B and reverts to 0x73 when the magnet is removed.

NB! Pressing the power button for more than 3 seconds will cause a disconnect.


Write GPIO

This small tutorial demonstrates how the register service can be used to change the value of GPIO outputs, using the green and the red LED to observe the effect.

  • Write 05:00 to Register Device ID (this selects MCU address space)
  • Write 1:81:20:02:40 (0x40022081) to Register Device Address. This selects the GPIO output register bits 8:15, access length 1
  • Write 0xC0 to the Register Data characteristic and observe that the green LED goes on
  • Write 0xC4 to the Register Data characteristic and observe that the red LED goes on
  • Write 0x40 to the Register Data characteristic and observe that both LEDs go off


Firmware Upgrade

The SensorTag is shipped with a pre-programmed firmware version and should be updated to the latest release to ensure the best IoT experience. SensorTag firmware can be upgraded directly over JTAG using the XDS110 based DevPack Debugger (CC-DEVPACK-DEBUG) or via the Over the Air Download (OAD) feature using supported devices.

The latest SensorTag firmware version is 1.40 which can be programmed with SmartRF Flash Programmer 2 using the JTAG upgrade procedure listed below.

JTAG Upgrade

Using SmartRF Flash Programmer 2

To upgrade, install the latest SmartRF Flash Programmer 2 and obtain the DevPack Debugger (CC-DEVPACK-DEBUG) which uses the XDS110 JTAG debugger. Obtain the latest SensorTag Hex firmware image file. For example, the pre-built SensorTag hex file for BLE-Stack 2.2.1 is located in C:\ti\simplelink\ble_sdk_2_02_01_18\examples\hex

  1. Attach the DevPack Debugger to the SensorTag
  2. For CC2650STK HW revsions prior to 1.3.0: Insert a fresh or sufficiently charged CR2032 coin cell battery into the SensorTag
  3. Attach the micro USB cable to the DevPack Debugger and PC (this step must be performed after inserting the battery)
  4. Open SmartRF Flash Programmer 2
    1. Under Connected Devices, select "Refresh" and then highlight the XDS110 / CC2650
    2. Under Flash Images, browse to the desired hex file. (e.g., C:\ti\simplelink\ble_sdk_2_02_01_18\examples\hex\cc2650stk_sensortag_rel.hex)
    3. Under Actions, select Erase (All unprotected pages), Program (Entire source file), Verify (Readback)
    4. Select Go (Play button) to start the flash programming
    5. If successful, a green bar will display "Success!".


Programming SensorTag Firmware with SmartRF Flash Programmer 2


Over the Air Download (OAD)

SensorTag firmware can be upgraded via the BLE radio link by means of the OAD service. For a description of the OAD service, refer to the "CC2640 BLE OAD User's Guide.pdf" located in Documents folder of the BLE 2.2.1 SDK. The SensorTag uses the "off-chip" OAD method. When the FW image is sent to the SensorTag, it is first stored in external SPI flash memory. Once the entire image is sent, the SensorTag will reboot and install the new image from the external flash memory. Both the iOS and Android SensorTag apps have example firmware files included in the app.


Generating Binary Files for Mobile App OAD

The iOS and Android SensorTag applications take an application image in a binary(*.bin) form. In order to generate these files, the post build steps of the SensorTag IAR and CCS projects need to be updated.
IAR
right click on project > options > Output Converter:

  1. Ensure Generate additional output is clicked
  2. Set output format to binary

CCS
Right click on project > properties > Build > steps > post build steps
Add this line (must be a single line):
"${CCS_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin" "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin" "${CG_TOOL_ROOT}/bin/armofd" "${CG_TOOL_ROOT}/bin/armhex" "${CCS_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin"
Final post-build setting should look like this:
CCS Post Build Steps
Rebuild the project after applying the above settings and the .bin files should be in your output directory.


OAD using the SensorTag iOS App

To update the SensorTag using the iOS, first install the latest SensorTag app from the Apple App Store. The following procedure applies to iOS app version v4.2.

  1. Press the power button to initiate advertising and connect to the SensorTag using the "Sensor View" option in the App.
  2. If prompted with "Old FW detected", select "Upgrade". Otherwise, scroll down to the FW Download menu.
  3. On the FW Download page, the current FW version is shown. Tap "Select FW File" to select a newer image for download.
    • Note that you can import bin files generated by CCS or IAR to the SensorTag app. They will appear at the bottom of the page.
    • One easy way to import a file is to e-mail it to yourself and then select open in SensorTag app.
  4. Select the newest FW file that is marked as compatible. The FW will begin to download as soon as selected.
  5. Once complete, the SensorTag will disconnect and automatically install the new FW image from the external flash memory.
  6. Clear your iOS device's BT cache by switching Bluetooth off then on. This step is required so the iOS device can re-discover any changed GATT characteristics.

Note: SensorTags running FW versions prior to v1.01 must use "Safe Mode" to upgrade. Once v1.01 or later is installed, High Speed Mode can be used. The following screen shots depict the upgrade from v0.91 to v1.12. Click on an image to see an larger version.


OAD using the SensorTag Android App

The workflow for updating the SensorTag firmware using the Android app is similar iOS. Refer to the iOS procedure detailed above. The firmware update menu is labeled "TI OAD Service".

OAD using BLE Device Monitor

A new firmware can be uploaded using the BLE Device Monitor. Follow the connection set up in the BLE Device Monitor User Guide. When the SensorTag is connected to the BLE Device Monitor select 'File' and 'Program (OAD)'. The input are HEX files, and there is by default a restriction on which files can by uploaded by a certain firmware version. If you want to download any file, the filter can be changed to *.* (All files) in the file open dialogue. Before overriding the default file filter, be aware that if you download an image that is not BLE/OAD you can not reset the device to a its original state. The only exception is the provided ZigBee image - factory state may be recovered by pressing both buttons for 6 seconds.


SensorTag firmware images are available in the default location, typically C:\Program Files (x86)\Texas Instruments\SmartRF Tools\BLE Device Monitor\firmware\cc26xx\sensortag.


Firmware Versions

Firmware revisions for Texas InstrumentSimpleLink CC26xx/CC13xx SensorTags and LaunchPads, listed by device and application type. The newest firmware revisions are shown first.

CC2650 SensorTag
Revision BLE SDK Description
1.40 2.2.1 SensorTag application
1.33 2.2.1 beta SensorTag application
1.30 2.2.0 SensorTag application.
1.20 2.1.0 SensorTag application. This FW revision supports download of CC2650 Flash Programmer v 1.22 as an intermediate step to upgrading to version 1.30 and above.
1.12 2.1.0 beta SensorTag application. Supports upgrade to revision 1.20
1.11 2.1.0 beta SensorTag application. This FW revision supports upgrading to any BLE application with revision 1.12 and 1.20. Can download devpack images (LCD and LED Light). Factory reset NOT supported.
1.10 2.1.0 beta SensorTag application. This FW revision supports upgrading to any BLE application with revision 1.11, 1.12 and 1.20. Can download devpack images (LCD and LED Light). Factory reset NOT supported.
1.02 2.0.0 bugfix SensorTag application. This FW revision supports upgrading to any BLE application with revision numbers between 1.10 and 1.20
1.01 2.0.0 feature SensorTag application. Fast OAD added. This FW revision supports upgrading to any BLE application with revisions between 1.01 and 1.20.
1.0 2.0.0 SensorTag application. This FW revision (released with CC26xx RTM) supports upgrading to any BLE application with revision between 1.0 and 1.20.
0.91 2.0.0 beta SensorTag application. This FW revision supports upgrading any BLE SensorTag application with revision 1.0 and above. Factory reset not supported.
0.89 2.0.0 beta SensorTag application. Used Boot Image Manager in page 0/1, application from page 2 (address 0x2000). Supports upgrade to version BLE SensorTag FW 0.91 only. After upgrading to 0.91, an upgrade to the latest BLE FW is recommended. Factory reset not supported.</tbody>
CC2650 LaunchPad
Revision BLE SDK Description
1.20 2.2.1 LaunchPad OOB application
1.11 2.2.0 bugfix LaunchPad OOB application
1.10 2.2.0 LaunchPad OOB application
1.00 2.2.0 beta LaunchPad OOB application, pre-release firmware
CC1350 SensorTag
Revision BLE SDK Description
1.40 2.2.1 feature SensorTag OOB application. Not part of SDK.
1.33 2.2.0 feature SensorTag OOB application. Not part of SDK.
1.31 2.2.0 feature SensorTag OOB application. Not part of SDK.
CC1350 LaunchPad
Revision BLE SDK Description
1.20 2.2.1 LaunchPad OOB application
1.11 2.2.1 beta LaunchPad OOB application
1.10 2.2.0 bugfix LaunchPad OOB application, fixed RTOS configuration bug
1.00 2.2.0 LaunchPad OOB application


Building the SensorTag Firmware

The SensorTag firmware can be built using the source code & project included in the BLE-Stack SDK. Building the firmware is useful for making changes to the default driver behavior, adding additional DevPacks, as well as source level debugging using the DevPack Debugger to better understand the operation of the SensorTag. The build procedure listed below assumes the developer is familiar with the IDE and build environment concepts described in the CC2640 BLE SW Developer's Guide (SWRU393).

In addition to the dual Application & Stack images, the SensorTag uses a Boot Image Manager (BIM) to facilitate firmware upgrades via OAD (Over-the-Air Download). The BIM must be programmed first and must be present before programming the Application and Stack images. In the SensorTag IAR project, the BIM workspace is included, however for CCS, the BIM must be explicitly imported into the workspace. Refer to the "CC2640 BLE OAD User's Guide.pdf" located in Documents folder of the BLE 2.2.x SDK for more details on the BIM and OAD.

SensorTag Project: $SDK_INSTALL_PATH$\examples\cc2650stk\sensortag\ccs
BIM_extflash (for CCS): $SDK_INSTALL_PATH$\examples\util\bim_extflash

Where $SDK_INSTALL_PATH$ is the default SDK install path, e.g., C:\ti\simplelink\ble_sdk_2_02_01_18 for BLE-Stack v2.2.1.

Build & Download Procedure:

  1. Open/Import the SensorTag project in IAR or CCS
    1. CCS Only: Import the BIM_extflash project from the location listed above
  2. Build & download the BIM_extflash project [FlashOnly_ST Configuration]
  3. Build & download the Stack project [FlashROM Configuration]
  4. Build & download the Application project [FlashOnlyOAD Configuration]

When downloading the project, verify that each workspace is configured to use the TI XDS110 if the DevPack Debugger is used. All SensorTag related projects in the BLE 2.2.x SDK are configured to use the XDS110 as the default debugger option.

Note: If the SensorTag is erased (or the BIM is erased), the BIM must be programmed before reprogramming the Application & Stack images. The pre-built cc2650stk_sensortag_rel.hex firmware file included in the BLE-Stack SDK $SDK_INSTALL_PATH$\examples\hex folder contains the BIM, Application & Stack in a super hex file.

Building SensorTag Super Hex File

To create a single, “super hex” SensorTag firmware file consisting of the BIM_extflash, Application & Stack images, the individual hex files for the respective projects need to be merged into one file. As hex files use an open standard, any merge tool can be used provided it supports the appropriate hex standard. TI uses the IntelHex python tools which assumes each hex file in the Intel Extended hex format. To confirm that the resulting hex file in the Intel format, each line should begin with a colon ‘:’.

To merge the files, the procedure as documented in the BLE SW Developer Guide (SWRU393) can be used. When the BIM is used, the Application image should start at flash address 0x1000. Refer to the “Working with Hex Files” section. Example procedure to generate a sensortag_super.hex super file:

$ C:\Python27\Scripts>python hexmerge.py -o sensortag_super.hex -r 0000:1FFFF sensortag_cc2650stk_app.hex:0000:1EFFF sensortag_cc2650stk_stack.hex bim_extflash.hex:0000:1FFFF --overlap=error

Where “sensortag_cc2650stk_app.hex” is the application; “sensortag_cc2650stk_stack.hex“ is the protocol stack; and “bim_extflash.hex” is the BIM input hex files. Note that the names of the input hex files may differ. Use the actual App, Stack & BIM_extflash hex files generated by the respective build environment.

Building SimpleBLEPeripheral OAD_IMAGE_FULL SuperHex File

Use similar procedure as above to generate a OAD_IMAGE_FULL.hex file:

python "C:/Python27/Scripts/hexmerge.py" -o "${PROJECT_LOC}/FlashOnly_ST_OAD_ExtFlash/OAD_IMAGE_FULL.hex" -r "1000:1EFFF" --overlap=error "${PROJECT_LOC}/FlashOnly_ST_OAD_ExtFlash/${ProjName}.hex" "${PROJECT_LOC}/../SimpleBLEPeripheralStack/FlashROM/SimpleBLEPeripheralStack

Modify this in your CCS project post build settings to build the correct image to be used for Off-chip OAD.

Excluding Features from the Firmware

The SensorTag firmware can be built with specific sensor/functionality support excluded from the build. This can be useful to prototype the SensorTag application on a board that does not populate all of the sensors used by the CC2650STK SensorTag. To exclude a feature or features from the build, define one or more of the following Predefined Symbols in the SensorTag application project:

  • EXCLUDE_AUDIO - Excludes the Audio service and related driver
  • EXCLUDE_BAR - Excludes the barometric service and related driver
  • EXCLUDE_BATT - Excludes the battery service
  • EXCLUDE_FACTORY_RESET - Excludes factory reset support
  • EXCLUDE_HUM - Excludes the humidity service and related driver
  • EXCLUDE_IO - Excludes the IO service (LED and buzzer control)
  • EXCLUDE_KEYS - Excludes simple keys service
  • EXCLUDE_MOV - Excludes the movement service and related MPU9250 driver
  • EXCLUDE_OAD - Excludes the OAD (firmware upgrade) service
  • EXCLUDE_OPT - Excludes the optical service and related driver
  • EXCLUDE_REG - Excludes the register service
  • EXCLUDE_TMP - Excludes the temperature service and related driver

Note: Some SensorTag sample applications included in the SDK require specific sensors to be excluded in order to provide adequate memory resources.


Running other Sample Applications on the SensorTag

Since the SensorTag incorporates a CC2650 wireless MCU, you can run any CC2640 BLE sample application on the SensorTag HW. This list includes all simpleBLExxx projects, HostTest, Heart Rate, Eddystone, etc. The following items must be considered when porting a sample application to the SensorTag (or any custom board):

  1. It is recommended to use the SensorTag board file. For example, simpleBLEPeripheral uses the SmartRF06EBK board file by default, so switching the IDE project to use the SensorTag board file is required for proper IO pin mapping.
  2. Use of external peripherals (e.g., LCD, buttons) needs to be disabled or modified in the code or project Preprocessor options to use the available HW on the SensorTag board. For example, when using simpleBLECentral, the default LCD and button usage from the SmartRF06EBK must be disabled when this sample application is built for the SensorTag.
  3. Accessing external IOs needs to match what is available on the SensorTag board or DevPack accessories.
  4. Optional: Since the SensorTag has many sensors populated on the PCB, maximum board power saving will only occur when these sensors are placed in their lowest power state. This requires having some drivers in your project to configure/control these sensors. Refer to this E2E thread for a functional example. Note that the power usage of the CC2640/50 is optimized, sensors on the SensorTag PCB may consume additional power thus leading to higher overall board current consumption.

Refer to the CC2640 BLE SW Developer's Guide (SWRU393) for guidance on how to configure the board file and modify certain Preprocessor options.

Example projects that use the SensorTag:


Back to Bluetooth SensorTag main page