Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

CC26xx Range Extender Control

From Texas Instruments Wiki
Jump to: navigation, search

Using a range extender with the CC26xx

The RF Core has 4 internal logical outputs, 2 of these can be used for range extender control. The default configuration of RF Core Data Out 0 is to be high when the LNA is enabled and similarly RF Core Data Out 1 is configured to be high when the PA is active. These RF Core Data outputs can be directly assigned to DIOs through the IO Control registers IOCFGx (x = DIO number) bits 5-0. See the technical reference manual chapter 11.3.2.1 details.

Example:

Let's say the PA_enable signal is on DIO7, the LNA_enable signal is on DIO13 and HGM is on DIO14. We thus need to connect RF Core Data Out 0 to DIO13 and RF Core Data Out 1 to DIO7.

Thus the following registers must be set using the CC26xxware driverLib:

  • IOCFG7 = 0x30
  • IOCFG13 = 0x2F

which can be done through the IOCPortConfigureSet function:

    #include <driverlib/ioc.h>
    // Map RFC_GPO0 to DIO13
    IOCPortConfigureSet(IOID_13, IOC_PORT_RFC_GPO0,
                    IOC_IOMODE_NORMAL);
    // Map RFC_GPO1 to DIO7
    IOCPortConfigureSet(IOID_7, IOC_PORT_RFC_GPO1,
                    IOC_IOMODE_NORMAL);


  • Note: Remove the associated PA_enable & LNA_enable DIO pins from the BoardGpioInitTable (typically located in the respective board.c file) when configuring the PIN driver. Attempting to initialize the PIN driver with pins defined in the BoardGpioInitTable that are directly opened by driverLib, e.g., IOCPortConfigureSet function, may cause undefined software behavior.
  • Note: On the CC2640R2F the PA enable signal has a flaw in which it does not de-assert when the internal PA is turned off. It will only go low when the RF Core is shut down. A work-around for external PA control is to use the TX Start signal instead. This signal will also follow the internal PA control signal, but will go high approximately 10 us earlier than PA enable. TX Start is mapped to RFC_GPO3.



Range extender control implemented in SimpleBLEPeripheral (yellow is PA enable, blue is LNA enable):

Advertise range extender.jpg


Advertise range extender2.jpg