CC3000 Wi-Fi MSP-EXP430F5529
From Texas Instruments Embedded Processors Wiki
Contents |
Overview
The CC3000 EM module has been designed with connectors that mate to the Texas Instruments EM interface provided on the MSP-EXP430F5529.
Supported Applications
The CC3000 + MSP-EXP430F5529 is supported by the following application:
- Download CC3000 Basic WiFi Application for F5529
For more information, please see CC3000 Basic WiFi Application Information
User Interface
There is a red LED (LED1) used to indicate successful connection to an access point (AP connect). There is a green LED used to indicate power (eZPWR)
Power Supply
The CC3000 is powered via the USB interface on the MSP-EXP430F5529
Configuring the HyperTerminal
General Notes
The HyperTerminal is the interface through which commands are sent to the CC3000 basic Wi-Fi example application. The HyperTerminal connects to the MSP-EXP430F5529 board, as shown in the figure above.
Baud Rate Configuration
Configure the baud rate as follows:
- Bits per second: 9600
- Data bits: 8
- Parity: None
- Stop bits: 1
- Flow control: None
Support
E2E Community
For further information or to ask questions directly to other Engineers, visit the WLAN Applications Forum in the E2E Community.
External Links
Note
The basic WiFi application was ported to this platform by Pacific Design Engineering (PDE), a full-service company engaged in custom product design and development. PDE, a Texas Instruments Elite Design House Network partner, provides contract engineering support in specialized areas or will assume turnkey design responsibility for a product, from idea to production.
Site Map