CC3000 Wi-Fi TivaC M4 Launchpad

From Texas Instruments Wiki
Jump to: navigation, search

Overview

The CC3000 EM module has been designed with connectors that mate to the Texas Instruments EM interface that is common to many Texas Instruments development platforms. This guide discusses how to connect the CC3000 EM module to a TivaC M4 Launchpad

CC3xxx TivaC.png


Supported Applications

The CC3000 + Stellaris Cortex M4 is supported by the following application:

User Interface

There is a green LED (Power LED) that is used to indicate power status.

Hardware Interface

The CC3000 Booster pack plugs into the bottom side of the TivaC M4 Launchpad using connectors J1 and J2.
The CC3000 is powered via the USB interface on the TivaC M4 Launchpad

Support

E2E Community

For further information or to ask questions directly to other Engineers, visit the WLAN Applications Forum in the E2E Community.

External Links

Note

The Web Server and Client application was developed and the basic WiFi application was ported to this platform by Pacific Design Engineering (PDE), a full-service company engaged in custom product design and development. PDE, a Texas Instruments Elite Design House Network partner, provides contract engineering support in specialized areas or will assume turnkey design responsibility for a product, from idea to production.