Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

CC3100 & CC3200

From Texas Instruments Wiki
Jump to: navigation, search


Welcome to the SimpleLink™ Wi-Fi® CC3100/CC3200 Main Page.

Cc31-3200withLogo NoBackground.png The objective of this wiki is to provide extensive self-help resources including technical collateral and information for CC3100/CC3200 Wi-Fi® SimpleLink customers. Created for the Internet of Things, the SimpleLink™ Wi-Fi® family dramatically simplifies the implementation of Internet connectivity by integrating & embedding all the protocols for Wi-Fi, Internet and security on the chip. It is a complete platform solution including various tools and software, sample applications, user guides, programming guides, reference designs and the TI E2E™ Community for support. The SimpleLink Wi-Fi family consists of:
  • CC3100 - A Wireless Network Processor with on-chip Wi-Fi, internet, and robust security protocols. It can be used to connect any low-cost, low-power microcontroller (MCU) to the Internet of Things (IoT)!
  • CC3200 - A Wireless MCU integrating high-performance ARM® Cortex™-M4 MCU with on-chip Wi-Fi, internet, and robust security protocols. It can be used to develop an entire IoT application with a single IC.
SimpleLink Wi-Fi Platform Overview
News Latest Software Release
[Jun 21, 2016] New Provisioning Package released! Check out CC3100 & CC3200 Provisioning Features pages. This is TI's recommended provisioning method for new designs.
[Mar 10, 2016] New SDK 1.2.0 released! Check out CC3100 Release Notes and CC3200 Release Notes pages! All related documents and software updated as well.
[Oct 9, 2015] New Serial Flash Guide wiki page is created.
[Aug 14, 2015] New Radio Tool version 1.1_fix is released. Check out Radio Tool page for more information.
[Jul 9, 2015] New Power Management Optimizations and Measurements tools and guidelines are released. Check out CC3100 and CC3200 pages for more information.
[May 20, 2015] New Uniflash 3.2.1.00000 & 3.3.0.00058 released. Check out the Uniflash Download page.
[May 17, 2015] CC3100 Host Programming released! Check out CC3100 SDK Example Host Programming section!
[Mar 13, 2015] New SDK 1.1.0 released! Check out CC3100 Release Notes and CC3200 Release Notes pages!
[Feb 5, 2015] New Uniflash 3.2.0.0012 released! Check out the Uniflash Download page!
[Jan 19, 2015] New page CC3100 & CC3200 Production Line Guide added.
[Nov 7, 2014] New Service Pack 1.0.0.1.2 released! Check out CC3100 Release Notes and CC3200 Release Notes pages!
[Oct 20, 2014] CC3100 and CC3200 devices are the first to be Wi-Fi CERTIFIED™ at the chip level! News
[Oct 17, 2014] New Service Pack 1.0.0.1.1 released! Check out CC3100 Release Notes and CC3200 Release Notes pages!
[Sept 12, 2014] New SDK 1.0.0 released! Check out CC3100 Release Notes and CC3200 Release Notes pages!
Service Pack: 1.0.1.11-2.9.0.0

CC3100 SDK: 1.2.0
CC3200 SDK: 1.3.0

Getting Started Hardware System Software System Tools, Test, Certification
CC3100 SimpleLink Wi-Fi for MCU Applications

Where to Start

Things to Consider

Hardware Basics

Hardware Advanced

Releases

Guides

Tools

System Tests

Certification

CC3200 SimpleLink Wi-Fi, a Single Chip Wireless MCU

Where to Start

Things to Consider

Hardware Basics

Hardware Advanced

Releases

Guides

Tools & Tests

Tests

Certification

Development Tools SimpleLink Videos/Demos Support and Community

Integrated Development Environment (IDE)

Internet of Things Ecosystem

Support

CC31xx & CC32xx Obsolete Pages