Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

CC3100 BoosterPack Hardware

From Texas Instruments Wiki
Jump to: navigation, search
Cc31xx cc32xx return home.png

Introduction

The CC3100 SimpleLink™™ Wi-Fi®™ solution provides the flexibility to add Wi-Fi to any microcontroller (MCU).

This user guide explains the various configurations of the CC3100 hardware BoosterPack™. This internet on a chip solution contains all you need to easily create IoT solutions – security, quick connection, cloud support and more. The CC3100 Boosterpack can be used in several ways. First, it can be connected to a TI MCU Launchpad (software examples provided for MSP-EXP430F5529LP). Second, it can be plugged into a CC31XXEMUBOOST board and connected to a PC for MCU Emulation. Finally,it can be connected onto an adapter board (MCU-ADAPT), which allows customers to use CC3100BOOST with additional platforms beyond TI Launchpads. The user can refer to the CC31xx programming guide for instructions on porting driver and sample code.

CC31xx Hardware Guide

Date Description Link
August 2014 CC3100 SimpleLink Wi-Fi and IoT Solution Boosterpack Hardware SWRU371

Errata

1. There is no pull-down resistor connected to pin-19 of the device. This can cause the device to show high currents in the LPDS modes. In case the issue is noticed, add a 100K resistor to ground using blue wiring.

Links