Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

CC3100 SLS XMPP Reference Application

From Texas Instruments Wiki
Jump to: navigation, search
Cc31xx cc32xx return home.png
Cc31xx return sample apps.png

Overview and application details

This sample application demonstrates how to connect and work with XMPP server using CC31xx. It receives/sends an XMPP messages from/to the server.

For information on how to use Visual-Studio or Eclipse to compile and run this application, refer to cc3100_getting_started_guide_swru375 in '<cc3100/>docs' folder.

By default, this application communicates w/ CC3100 over SPI. The SDK has UART-Drivers as well for 'SimpleLink Studio' platform. For using the UART interface to communicate w/ CC3100, macro SL_IF_TYPE_UART has to be defined in the application-project's properties. Also, COMM_PORT_NUM in main.c needs to be changed to the first com-port that gets enumerated for 'J6' of 'CC31xxEMUBOOST Brd'. In case four ports are getting enumerated, user should use the third com-port.

NoteNote: This wiki page is only applicable for CC3100-SDK v1.0.0 and upward releases. For documentation on older SDKs' examples, refer corresponding file in <cc3100-sdk-installation-location>\cc3100-sdk\docs\examples\

Source Files briefly explained

  1. main - Initializes the device, connects to an access-point and configures the email
  2. xmpp - Wrapper functions to configure/connect to XMPP-Server and send/receive chat-messages. These functions are called from main
  3. base64 - Functions to convert the raw bytes in quasi-big-endian order to Base64 string

Usage

  • Open config.h and change values for XMPP_USER and XMPP_PWD for setting up the xmpp account credentials.
  • Log-in your 'gtalk' account and add configured xmpp account to your friends list
  • Build the application using Visual-Studio or Eclipse. Download and execute it on the target device
  • User will be prompted to configure the AP parameters for establishing a Wi-Fi connection - Follow the instructions on the console to test the application
  • Once the connection is established successfully, wait for 'slcc3100@gmail.com' to appear ONLINE in your friends' list
Sls_XMPP_1.png

  • When ONLINE, send messages to CC3100. The device shall receive and relay the messages back to the sender
Sls_XMPP_2.png

  • On success, below message will be displayed on the console
Scrshot_sls_xmpp_client.png

Limitations/Known Issues

  • The size of the message is currently limited to 48
  • Since example doesn't implement a complete XMPP stack:
  1. Retreiving the full friend roster isn't supported
  2. Checking the remote friend status (online, offline) before sending him a message is not supported

Links