Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

CC3100 & CC3200 Debug Support

From Texas Instruments Wiki
Jump to: navigation, search
Cc31xx cc32xx return home.png

Overview

The SimpleLink Wi-Fi devices can be connected to several emulator for debug capabilities. This page provides suggestions on project's modification, in order to various off the shelf emulators.

Connecting JLINK to CC3200 LP

This script enables debugging CC3200 using Segger J-Link Emulator.

J-Link emulator supports ARM 20 JTAG and to attach J-Link to CC3200 LP, disconnect the on board FTDI from the JTAG lines by removing jumpers J8, J9 J10 and J11.Following table give the mapping of the ARM 20 pin header to CC3200 LP.

cc3200_jlink_script_pinout.png



Attaching J-Link Script to a IAR Project

  • Open Project->Options->Debugger and select J-Link/J-Trace from the Driver drop down.


cc3200_jlink_script_options.png

  • Press OK.
  • Start the debug session by pressing “Download and Debug” session button.
  • This debug session will fail to connect to target.
  • Click the J-Link icon from notification area on task bar to open up the J-Link Control Panel


cc3200_jlink_script_control Panel.png


  • Go to ‘Setting’ tab and select the script file to execute.
  • Close the control panel.
  • On IAR, terminate the debug session and restart the session.


Download

CC3200_JLinkScript.zip

Links

Important Notice

Texas Instruments and its subsidiaries (TI) reserve the right to make changes to their products or to discontinue any product or service without notice, and advise customers to obtain the latest version of relevant information to verify, before placing orders, that information being relied on is current and complete. All products are sold subject to the terms and conditions of sale supplied at the time of order acknowledgement, including those pertaining to warranty, patent infringement, and limitation of liability.

TI warrants performance of its semiconductor products to the specifications applicable at the time of sale in accordance with TI’s standard warranty. Testing and other quality control techniques are utilized to the extent TI deems necessary to support this warranty. Specific testing of all parameters of each device is not necessarily performed, except those mandated by government requirements.

CERTAIN APPLICATIONS USING SEMICONDUCTOR PRODUCTS MAY INVOLVE POTENTIAL RISKS OF DEATH, PERSONAL INJURY, OR SEVERE PROPERTY OR ENVIRONMENTAL DAMAGE (“CRITICAL APPLICATIONS”). TI SEMICONDUCTOR PRODUCTS ARE NOT DESIGNED, AUTHORIZED, OR WARRANTED TO BE SUITABLE FOR USE IN LIFE–SUPPORT DEVICES OR SYSTEMS OR OTHER CRITICAL APPLICATIONS. INCLUSION OF TI PRODUCTS IN SUCH APPLICATIONS IS UNDERSTOOD TO BE FULLY AT THE CUSTOMER’S RISK.

In order to minimize risks associated with the customer’s applications, the customer to minimize inherent or procedural hazards must provide adequate design and operating safeguards.

TI assumes no liability for applications assistance or customer product design. TI does not warrant or represent that any license, either express or implied, is granted under any patent right, copyright, mask work right, or other intellectual property right of TI covering or relating to any combination, machine, or process in which such semiconductor products or services might be or are used. TI’s publication of information regarding any third party’s products or services does not constitute TI’s approval, warranty or endorsement thereof.