CCS Project OMAP-L137 HelloDSP DSPLINK example

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Introduction

This page describes how to make the DSP side of the Example application using DSP Link on OMAPL1x into a CCS project.

Adapted Project

Find attached the same helloDSP example with a pjt.


It assumes that you installed the package:

OMAPL137_dsp_setupwin32_1_00_00_11.exe

Not the package:

C674x_dsp_setupwin32_1_00_00_10.exe

From the download site. So if you installed the C674x_dsp_setupwin32_1_00_00_10.exe package, please go back to the download site and get OMAPL137_dsp_setupwin32_1_00_00_11.exe and install in the default path.


After installing it, please edit the file:

C:\OMAPL137_dsp_1_00_00_11\dsplink-1_61_03-prebuilt\packages\dsplink\dsp\inc\DspBios\5.XX\OMAPL1XXGEM\dsplink-omapl1xxgem-base.tci

Comment the line below:

/*prog.module("GBL").PROCID          = parseInt (arguments [0]) ;*/


And add the line below to replace it:

prog.module("GBL").PROCID          = 0;


If you do not change the procedure above, you will get the error: js: "dsplink-omapl1xxgem-base.tci", line 44: Illegal type change: GBL.PROCID changed from type integer to type float


Also, please make sure you have the DSPLINK env variable set in Windows. To do that go to Start-> Control Pannel-> System, choose tab Advanced. At the bottom, click on Environment Variables. At “System variables” click “New”. Put the values:

Variable name: DSPLINK

Variable Value: C:\OMAPL137_dsp_1_00_00_11\dsplink-1_61_03-prebuilt\packages\dsplink

Attention:If you point to the DSPLink your windows machine for the DSP application, and you use the DSPLink in your Linux machine for your Linux application, you might have conflicts – especially if you rebuild DSPLink in your Linux machine. One creative solution would be to access your Linux machine from your Windows machine using samba (search the net for more info on how to do this). This way you can set your DSPLINK environmental variable to point to your Linux machine like:

\\(IP of your Linux machine)\user\OMAPL137_arm_1_00_00_10\dsplink-1_61_03-prebuilt\packages\dsplink

For your project to compile you in CCS, you have access your Linux machine (Start->Run, type the IP of the Linux machine)


It also assume that it can find the BSL (.lib) at:

C:\CCStudio_v3.3\boards\evmomapl137_v1\dsp\lib

And the include files for bsl at:

C:\CCStudio_v3.3\boards\evmomapl137_v1\dsp\include

Step by step of what was done

Here is a sumarized step by step of what was done to adapt it:


1) Add the DSPLINK = C:\OMAPL137_dsp_1_00_00_11\dsplink-1_61_03-prebuilt\packages\dsplink to env varialbes at windows (Control Panel, System, Advanced, Environment Variables) - need to restart CCS to take effect.


2) Adapting dsplink-omapl1xxgem-base.tci

The file should be at: C:\OMAPL137_dsp_1_00_00_11\dsplink-1_61_03-prebuilt\packages\dsplink\dsp\inc\DspBios\5.XX\OMAPL1XXGEM\dsplink-omapl1xxgem-base.tci

Comment the line below:

/*prog.module("GBL").PROCID          = parseInt (arguments [0]) ;*/


And add the line below to replace it:

prog.module("GBL").PROCID          = 0;


3) Create a new project in CCS

Go to the CCS menu, Project-> New... and create a new project. Give it a name and leave the defaulf settings.


4) Adding source files to project

Right click on your project and "Add Files to Project..." and add the followinf files:

helloDSP.tcf, main.c, tskMessage.c, helloDSP_config.c, and led_test.c.

The led_test.c should be taken from spectrum's digital website here. The build options described assume that you downloaded the code from Spectrum Digital and put it at:

C:\CCStudio_v3.3\boards\


5) Added path to find .tcis:

Right click on the project, select build options, DdspBiosBuilder tab, categoty basic, put the path (do that for DEBUG and RELEASE): %DSPLINK%\dsp\inc\DspBios\5.XX\OMAPL1XXGEM

Make sure you can open tcf in the graphical edit


6) Include in your CCS project the LIBS that you need for DSPLINK (see LIBS variable at the DSP makefile from HelloDSP)

Right click on the project, choose Build Options..., Linker tab, Category Libraries. Add the folowing libraries to the field Incl. Libraries (-l) (do that for DEBUG and RELEASE):

dsplink.lib;dsplinkpool.lib;dsplinkmpcs.lib;dsplinkmplist.lib;dsplinkmsg.lib;dsplinknotify.lib;dsplinkringio.lib;evmomapl137bsl.lib


Add the following paths to the Search Patch (-i) field for RELEASE:

%DSPLINK%\dsp\export\BIN\DspBios\OMAPL1XX\OMAPL1XXGEM_0\RELEASE;C:\CCStudio_v3.3\boards\evmomapl137_v1\dsp\lib


Add the following paths to the Search Patch (-i) field for DEBUG:

%DSPLINK%\dsp\export\BIN\DspBios\OMAPL1XX\OMAPL1XXGEM_0\DEBUG\;C:\CCStudio_v3.3\boards\evmomapl137_v1\dsp\lib


7) Define the necessary symbols at preprocessor (see DEFS variable in the DSP Makefile from HelloDSP)

Right click on project, choose Build Options..., Compiler tab, Category Preprocessor and add the folowing symbols to the field Pre-Define Symbol(-d) (do that for DEBUG and RELEASE):

MAX_DSPS=1;MAX_PROCESSORS=2;ID_GPP=1;OMAPL1XX;PROC_COMPONENT;POOL_COMPONENT;NOTIFY_COMPONENT;MPCS_COMPONENT;RINGIO_COMPONENT;MPLIST_COMPONENT;MSGQ_COMPONENT;MSGQ_ZCPY_LINK;CHNL_COMPONENT;CHNL_ZCPY_LINK;ZCPY_LINK;PROCID=0;DA8XXGEM;DOS_LINUX;DA8XXGEM_INTERFACE=SHMEM_INTERFACE;PHYINTERFACE=SHMEM_INTERFACE


8) Innclude the paths to header files needed (see CINCLUDES variable in the DSP Makefile from HelloDSP)

Right click on project, choose Build Options..., Compiler tab, Category Preprocessor, and add the folowing paths to the field Include Search Path (-i) (do that for DEBUG and RELEASE):

%DSPLINK%\dsp\inc;%DSPLINK%/dsp/inc/DspBios;%DSPLINK%\dsp\inc\DspBios\5.XX;%DSPLINK%\dsp\inc\DspBios\5.XX\OMAPL1XXGEM\;%DSPLINK%\dsp\inc\C64XX;%DSPLINK%\dsp\export\INCLUDE\DspBios\OMAPL1XX


9) Change MV option option according to article:

-mv option to use with the C6747


10) Add .cmd files:

Compile the project to make the tcf file generate a .cmd (you will get some linking errors at this point).

Add the .cmd file generated by the tcf file to your project: helloDSPcfg.cmd. Add also the file helloDSP.cmd.

References

Example application using DSP Link on OMAPL1x

E2e.jpg For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article CCS Project OMAP-L137 HelloDSP DSPLINK example here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment

Comments

Comments on CCS Project OMAP-L137 HelloDSP DSPLINK example


Wushibin said ...

I just want to translate the last paragraph to chinese.

当首次编译的时候会产生链接错误(error: symbol referencing errors - './Debug/helloDSP.out' not built),在工程中添加工程中自动生成的 *.cmd 文件,即可以解决产生的错误。

--Wushibin 20:12, 13 October 2010 (CDT)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox